7.9.8.68. GEL_SetSemihostingMainArgs

Set the arguments that must be forwarded to the target program’s main function in response to a SYS_GET_CMDLINE semihosting call.

GEL_SetSemihostingMainArgs(args);

Parameters

args - String of arguments to be passed

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_SetSemihostingMainArgs(“arg1 arg2 arg3 arg4 arg5”) will pass an array of size 5 containing [arg1,arg2,arg3,arg4,arg5]

GEL_SetSemihostingMainArgs(“arg1 "arg2 with space” arg3 arg4”) will pass an array of size 4 containing [arg1, arg2 with space, arg3, arg4]

Related Topics

This function should be called to set the desired behaviour prior to calling GEL_Load to start a program load