Skip navigation links
A B C D E F G H I J K L M N O P R S T U V W X 

C

C24 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C27 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C28 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C54 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C55 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C56 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C62 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C64 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C66 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C67 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
C71 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
calculateChecksum() - Method in class com.ti.debug.engine.scripting.Flash
Calculates the checksum on flash.
CallStack - Class in com.ti.debug.engine.scripting
This class encapsulates the methods related to the callstack.
callStack - Variable in class com.ti.debug.engine.scripting.DebugSession
 
CallStack.RegisterContext - Class in com.ti.debug.engine.scripting
 
CALLSTACK_ERROR - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Error obtaining the call stack
canDelete(Object) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
canMoveDown(Object) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
canMoveUp(Object) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
changedEvent(Object, boolean) - Method in interface com.ti.debug.engine.scripting.setup.SystemSetupEditor.IChangedListener
 
CHECKBOX_PROPERTY - Static variable in class com.ti.debug.engine.scripting.setup.SystemSetupEditor.AbstractProperty
 
CHOICE_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CHOICE_TYPE - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CHOICE_VALUE_ATTRIBUTE - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CHOICELIST_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
choices - Variable in class com.ti.debug.engine.scripting.setup.SystemSetupEditor.DropListProperty
 
cleanDataCache() - Method in class com.ti.debug.engine.scripting.ArmAdvancedFeatures
Cleans the data cache
clear() - Method in class com.ti.debug.engine.scripting.CallStack.RegisterContext
 
clock - Variable in class com.ti.debug.engine.scripting.DebugSession
 
COFF - Static variable in class com.ti.debug.engine.scripting.Memory.IOFormat
 
com.ti.ccstudio.scripting - package com.ti.ccstudio.scripting
 
com.ti.ccstudio.scripting.environment - package com.ti.ccstudio.scripting.environment
 
com.ti.debug.engine.scripting - package com.ti.debug.engine.scripting
 
com.ti.debug.engine.scripting.setup - package com.ti.debug.engine.scripting.setup
 
compareTo(SystemSetupReader.ErrorReport) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupReader.ErrorReport
 
compareTo(SystemSetupWriter.SetupItem) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupWriter.SetupItem
 
CONFIG - Static variable in class com.ti.ccstudio.scripting.environment.TraceLevel
Configurarion messages.
CONFIGURATION_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CONFIGURATIONS_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
connect(String, String) - Method in class com.ti.debug.engine.scripting.Pin
Connects a data file to an external interrupt pin (Simulators only).
connect(long, int, int, int, String) - Method in class com.ti.debug.engine.scripting.Port
Connect a data file to a memory (port) address (Simulator only) allowing you to read or write data to that file through the memory address.
connect() - Method in class com.ti.debug.engine.scripting.Target
Connect/reconnect the debugger to the target.
connect(boolean) - Method in class com.ti.debug.engine.scripting.Target
This is the same as connect() except that if false is passed in, and the target is not in an accessible state after connecting, it will return and won't wait for the state to become valid.
CONNECTION_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CONNECTION_TYPE_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
ConnectionDropListProperty() - Constructor for class com.ti.debug.engine.scripting.setup.SystemSetupEditor.ConnectionDropListProperty
 
connectionType - Variable in class com.ti.debug.engine.scripting.setup.SystemSetupWriter.SetupItem
 
ContextStep - Class in com.ti.debug.engine.scripting
This class encapsulates the context sensitive step methods.
contextStep - Variable in class com.ti.debug.engine.scripting.Target
 
convertToAbsPath(File, String, String[]) - Static method in class com.ti.debug.engine.scripting.setup.HardwareDatabaseReader
 
convertToFlatFile(Tag, String, String[]) - Method in class com.ti.debug.engine.scripting.setup.HardwareDatabaseReader
 
copyAttribute(Tag, String) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
copyAttribute(Tag, String, String, String[]) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
CORE_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CORTEX_A15 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_A53 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_A8 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_A9 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_M0 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_M3 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_M33 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
CORTEX_R4 - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
countChildren(Object) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
countChildrenByName(String) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
CountChildrenByName(Node, String) - Static method in class com.ti.debug.engine.scripting.setup.XMLParser
 
Cpu(SystemSetupReader.Cpu) - Constructor for class com.ti.debug.engine.scripting.setup.SystemSetupReader.Cpu
 
CPU_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CreateBooleanNode(String, boolean) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
createChild(String, String, String) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
createChild(String, String, String, Node) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
createChild(String, int, String) - Method in class com.ti.debug.engine.scripting.setup.Tag
 
createConfiguration(String) - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Creates a CCXML configuration file with the given name in the user folder based on the Connection (via setConnection()) + Board/Device (via setBoard() or setDevice()) pair

PreCondition:
- setUserDirectory() needs to be called first if not using default directory
- setConnection() needs to be called with valid connection
- setDevice() or setBoard() needs to be called with valid device/board
CreateEntityNode(String) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
CreateEvents(DebugSession) - Static method in class com.ti.debug.engine.scripting.SessionEventsFactory
 
createFlatNodeFromFile(Tag, String, String, String, String[], Node) - Method in class com.ti.debug.engine.scripting.setup.HardwareDatabaseReader
 
CreateIntegerNode(String, long) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
createNewConfiguration(String, SystemSetupWriter.SetupItem, SystemSetupWriter.SetupItem) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupWriter
Create system configuration ccxml file.
createNewConfiguration(OutputStream, String, SystemSetupWriter.SetupItem, SystemSetupWriter.SetupItem) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupWriter
Create system configuration ccxml file.
CreateNewDocument(String) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
createProperties(int) - Method in class com.ti.debug.engine.scripting.Breakpoint
Create a BreakpointProperties object with a particular breakpoint type.
createProperties() - Method in class com.ti.debug.engine.scripting.Breakpoint
Create a BreakpointProperties object
createRegisterContext() - Method in class com.ti.debug.engine.scripting.CallStack
 
CreateStringNode(String, String) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
createTargetConfigurationEditor() - Method in class com.ti.debug.engine.scripting.DebugServer
 
createTargetConfigurationGenerator() - Method in class com.ti.debug.engine.scripting.DebugServer
Return the TargetConfigurationGenerator interface for generating target configuration files
CURRENT_CHOICE_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
CURRENT_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
currentMode() - Method in class com.ti.debug.engine.scripting.PageTable
 
A B C D E F G H I J K L M N O P R S T U V W X 
Skip navigation links