Skip navigation links
A B C D E F G H I J K L M N O P R S T U V W X 

R

READ - Static variable in class com.ti.debug.engine.scripting.Port
Read Access
read() - Method in class com.ti.debug.engine.scripting.ProfileClock
Read the current value of the Profile Clock counter.
readData(int, long, int) - Method in class com.ti.debug.engine.scripting.Memory
Read a single integer value from the target and return the result as an unsigned integer.
readData(int, long, int, boolean) - Method in class com.ti.debug.engine.scripting.Memory
Read a single integer value from the target.
readData(int, long, int, int) - Method in class com.ti.debug.engine.scripting.Memory
Read mulitple values from the target and return the result as an array of integers.
readData(int, long, int, int, boolean) - Method in class com.ti.debug.engine.scripting.Memory
Read mulitple values from the target and return the result as an array of integers.
readRegister(String) - Method in class com.ti.debug.engine.scripting.Memory
Read the value of a register from the target.
readRegister(String, boolean) - Method in class com.ti.debug.engine.scripting.Memory
Read the value of a register from the target.
readWord(int, long) - Method in class com.ti.debug.engine.scripting.Memory
Read a single word (of the default word-size for the current target) from the target and return the result as an unsigned integer.
readWord(int, long, boolean) - Method in class com.ti.debug.engine.scripting.Memory
Read a single word (of the default word-size for the current target) from the target and return the result.
readWord(int, long, int) - Method in class com.ti.debug.engine.scripting.Memory
Read mulitple words (of the default word-size for the current target) from the target and return the result as an array of unsigned integers.
readWord(int, long, int, boolean) - Method in class com.ti.debug.engine.scripting.Memory
Read mulitple words (of the default word-size for the current target) from the target and return the result as an array of integers.
REGISTER_NOT_FOUND - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Specified register could not be found
registerSession(ScriptSession) - Method in interface com.ti.ccstudio.scripting.IScriptServer
Register a ScriptSession object to the current Server object
reload(String) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
reloadProgram() - Method in class com.ti.debug.engine.scripting.Memory
Reload the last-loaded program onto current target/CPU.
remove(int) - Method in class com.ti.debug.engine.scripting.Breakpoint
Remove a breakpoint that was set previously using add().
remove(long, int) - Method in class com.ti.debug.engine.scripting.MemoryMap
This function deletes a range of memory from the memory map.
remove(String) - Method in class com.ti.debug.engine.scripting.Symbol
Remove all of the symbols in the given file from the debugger's symbol manager.
removeAll() - Method in class com.ti.debug.engine.scripting.Breakpoint
Remove all user-created breakpoints.
removeChangeListener(SystemSetupEditor.IChangedListener) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
removeListener(IDebugServerEventListener) - Method in class com.ti.debug.engine.scripting.DebugServer
 
rename(Object, String) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
renameBoard(Object, String) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
replaceComponent(Object, SystemSetupWriter.SetupItem, File) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
reset() - Method in class com.ti.debug.engine.scripting.MemoryMap
This function resets the memory map by making all memory non-readable and non-writeable.
reset() - Method in class com.ti.debug.engine.scripting.ProfileClock
Reset the Profile Clock counter.
reset() - Method in class com.ti.debug.engine.scripting.Target
Reset the target.
RESET_ERROR - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Unable to reset the target
resetProperty(Object) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
resetScriptTimeout() - Method in class com.ti.debug.engine.scripting.DebugSession
Resets the timeout value (which specifies the amount of time to wait for underlying calls to the DebugServer to return) for the session.
ResetType - Class in com.ti.debug.engine.scripting
This class encapsulates a reset type that is supported by the target.
restart() - Method in class com.ti.debug.engine.scripting.Target
Restart the target
RESTART_ERROR - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Unable to restart the target
reverseLookup(long) - Method in class com.ti.debug.engine.scripting.PageTable
 
reverseLookupAll(long) - Method in class com.ti.debug.engine.scripting.PageTable
 
ROUTER_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
RTDX - Static variable in class com.ti.ccstudio.scripting.environment.Error
Base for RTDX Scripting Error Codes
run() - Method in class com.ti.debug.engine.scripting.Simultaneous
Simultaneously run all targets belonging to open unterminated sessions.
run(DebugSession[]) - Method in class com.ti.debug.engine.scripting.Simultaneous
Simultaneously run the targets belonging to the specified sessions.
run() - Method in class com.ti.debug.engine.scripting.Target
Issue a run command to the target but don't return control to the host application/script until the target has been halted due to to hitting a breakpoint, hitting the end of a program or timing out.
RUN_ERROR - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Unable to run the target
runAsynch() - Method in class com.ti.debug.engine.scripting.Simultaneous
Simultaneously run all targets belonging to open unterminated sessions.
runAsynch(DebugSession[]) - Method in class com.ti.debug.engine.scripting.Simultaneous
Simultaneously run the targets belonging to the specified sessions.
runAsynch() - Method in class com.ti.debug.engine.scripting.Target
Issue a run command to the target and return control immediately (even if target is still running) to the host application/script.
runBenchmark() - Method in class com.ti.debug.engine.scripting.ProfileClock
 
runBenchmark(String) - Method in class com.ti.debug.engine.scripting.ProfileClock
 
runBenchmark(int) - Method in class com.ti.debug.engine.scripting.ProfileClock
 
A B C D E F G H I J K L M N O P R S T U V W X 
Skip navigation links