Skip navigation links
A B C D E F G H I J K L M N O P R S T U V W X 

P

pageTable - Variable in class com.ti.debug.engine.scripting.DebugSession
 
PageTable - Class in com.ti.debug.engine.scripting
 
parse(String) - Method in class com.ti.debug.engine.scripting.setup.ProcessorID
 
ParseAndValidate(String, String) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
ParseAndValidate(InputSource, String) - Method in class com.ti.debug.engine.scripting.setup.XMLParser
 
PARTNUM_ATTRIBUTE - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
paste(Object, Object, boolean) - Method in class com.ti.debug.engine.scripting.setup.SystemSetupEditor
 
performOperation(String) - Method in class com.ti.debug.engine.scripting.Flash
Performs the Flash operation associated with the opCode.
pin - Variable in class com.ti.debug.engine.scripting.DebugSession
 
Pin - Class in com.ti.debug.engine.scripting
This class serves as a encapsulates the Pin Connect methods (used with supported simulators to simulate external interrupts).
PLATFORM_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
port - Variable in class com.ti.debug.engine.scripting.DebugSession
 
Port - Class in com.ti.debug.engine.scripting
This class serves as a encapsulates the Port Connect methods (used with supported simulators to allow reading and writing of a file through a memory address).
print() - Method in class com.ti.debug.engine.scripting.CallStack
Prints all frames of the current call stack to stdout on this target
printAvailableOptions() - Method in class com.ti.debug.engine.scripting.TargetConfigurationEditor
Prints out the available (CPU) options for the current configuration file.
printCachedFileDetails(String, String) - Static method in class com.ti.debug.engine.scripting.setup.SystemSetupReader
 
printCombinedDeviceBoardsList() - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Prints the list of devices, boards and simulator configurations in the install targetDB directory.
printListOfBoards() - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Prints the list of boards in the install targetDB directory.
printListOfConfigurations() - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Prints the list of configurations in the install targetDB directory.
printListOfConnections() - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Prints the list of connections in the install targetDB directory.
printListOfDevices() - Method in class com.ti.debug.engine.scripting.TargetConfigurationGenerator
Prints the list of devices in the install targetDB directory.
printOptionById(String) - Method in class com.ti.debug.engine.scripting.Options
Prints information on an option based on the ID, or if it is a node/group, print information on all options that are children properties of the property matching the ID.
printOptions(String) - Method in class com.ti.debug.engine.scripting.Options
Prints information on all options which match the given regular expression.
printProperties() - Method in class com.ti.debug.engine.scripting.BreakpointProperties
Prints the tree of properties represented by this BreakpointProperties object
ProcessorID - Class in com.ti.debug.engine.scripting.setup
 
ProcessorID() - Constructor for class com.ti.debug.engine.scripting.setup.ProcessorID
 
ProcessorID(long) - Constructor for class com.ti.debug.engine.scripting.setup.ProcessorID
 
ProcessorID.DriverType - Class in com.ti.debug.engine.scripting.setup
 
PROCESSORS_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
PROCID_ATTRIBUTE - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
PROFILE_CONFIG - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Unable to configure profiling
PROFILE_DATA - Static variable in class com.ti.debug.engine.scripting.DebugserverError
Unable to access profile data
ProfileClock - Class in com.ti.debug.engine.scripting
This class provides access to the Profile Clock methods.
PROGRAM - Static variable in class com.ti.debug.engine.scripting.Memory.Page
Program memory page
programPassword() - Method in class com.ti.debug.engine.scripting.Flash
Programs the given password to flash.
Property - Class in com.ti.debug.engine.scripting
// Create Environment and open a debug session
ScriptingEnvironment env = new ScriptingEnvironment();
DebugServer myServer = (DebugServer) env.getServer("DebugServer.1");
DebugSession mySession = myServer.openSession("*", "*");

...

// get a boolean Property object
ProfileActivity myActivity = mySession.profileSetup.getActivity(activityName);
Property myProperty = myActivity.getProperty(propertyPath);
// set value of property myProperty.setBoolean(true);
Property(ScriptingEnvironment, DebugSession, IActivity, IProperties, IProperty) - Constructor for class com.ti.debug.engine.scripting.Property
 
PROPERTY_NAME_ATTRIBUTE - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
PROPERTY_TAG - Static variable in class com.ti.debug.engine.scripting.setup.HWDB
 
PRU - Static variable in class com.ti.debug.engine.scripting.Target.ISA
 
publish(LogRecord) - Method in class com.ti.ccstudio.scripting.environment.SessionAwareFileHandler
 
A B C D E F G H I J K L M N O P R S T U V W X 
Skip navigation links