Version

The version driver provides a function which can be used to check the version number of the driverlib.lib that is in use.

group version_api

Defines

VERSION_NUMBER 5040000U

Version number to be returned by Version_getLibVersion()

Functions

uint32_t Version_getLibVersion(void)

Returns the driverlib version number

This function can be used to check the version number of the driverlib.lib that is in use. The version number will take the format x.xx.xx.xx, so for example, if the function returns 2100200, the driverlib version being used is 2.10.02.00.

Return

Returns an integer value indicating the driverlib version.

The code for this module is contained in driverlib/version.c, with driverlib/version.h containing the API declarations for use by applications.