FLASH Module¶
The Flash driver provides functions to configure the fallback power modes and the active grace periods of flash banks and pump, and the pump wake-up time. This driver also provides functions to configure the flash wait-states, prefetch, cache and ECC features. It also provides functions to access the Flash ECC test mode registers and the Flash ECC error status registers.
-
group
flash_api Defines
-
FLASH_FAIL_0_CLR0x1¶ Fail-0 clear.
-
FLASH_FAIL_1_CLR0x2¶ Fail-1 clear.
-
FLASH_UNC_ERR_CLR0x4¶ Uncorrectable error Clear.
-
FLASH_NO_ERROR0x0¶ No error.
-
FLASH_SINGLE_ERROR0x1¶ Single bit error.
-
FLASH_UNC_ERROR0x2¶ Uncorrectable error.
-
FLASH_DELAY_CONFIG__asm(" RPT #7 || NOP")¶
-
FLASH_PUMP_KEY0x5A5A0000UL¶ Pump semaphore key.
Enums
-
enum
Flash_BankNumber¶ Values that can be passed to Flash_setBankPowerMode() as the bank parameter.
Values:
-
enumerator
FLASH_BANK= 0x0¶ Bank.
-
enumerator
-
enum
Flash_PumpOwnership¶ Values that can be passed to Flash_claimPumpSemaphore() in order to claim the pump semaphore.
Values:
-
enumerator
FLASH_CPU1_WRAPPER= 0x2¶ CPU1 Wrapper.
-
enumerator
FLASH_CPU2_WRAPPER= 0x1¶ CPU2 Wrapper.
-
enumerator
-
enum
Flash_BankPowerMode¶ Values that can be passed to Flash_setBankPowerMode() as the powerMode parameter.
Values:
-
enumerator
FLASH_BANK_PWR_SLEEP= 0x0¶ Sleep fallback mode.
-
enumerator
FLASH_BANK_PWR_STANDBY= 0x1¶ Standby fallback mode.
-
enumerator
FLASH_BANK_PWR_ACTIVE= 0x3¶ Active fallback mode.
-
enumerator
-
enum
Flash_PumpPowerMode¶ Values that can be passed to Flash_setPumpPowerMode() as the powerMode parameter.
Values:
-
enumerator
FLASH_PUMP_PWR_SLEEP= 0x0¶ Sleep fallback mode.
-
enumerator
FLASH_PUMP_PWR_ACTIVE= 0x1¶ Active fallback mode.
-
enumerator
-
enum
Flash_ErrorStatus¶ Type that correspond to values returned from Flash_getLowErrorStatus() and Flash_getHighErrorStatus() determining the error status code.
Values:
-
enumerator
FLASH_NO_ERR= 0x0¶ No error.
-
enumerator
FLASH_FAIL_0= 0x1¶ Fail on 0.
-
enumerator
FLASH_FAIL_1= 0x2¶ Fail on 1.
-
enumerator
FLASH_UNC_ERR= 0x4¶ Uncorrectable error.
-
enumerator
-
enum
Flash_ErrorType¶ Values that can be returned from Flash_getLowErrorType() and Flash_getHighErrorType() determining the error type.
Values:
-
enumerator
FLASH_DATA_ERR= 0x0¶ Data error.
-
enumerator
FLASH_ECC_ERR= 0x1¶ ECC error.
-
enumerator
-
enum
Flash_SingleBitErrorIndicator¶ Values that can be returned from Flash_getECCTestSingleBitErrorType().
Values:
-
enumerator
FLASH_DATA_BITS= 0x0¶ Data bits.
-
enumerator
FLASH_CHECK_BITS= 0x1¶ ECC bits.
-
enumerator
Functions
-
void
Flash_setWaitstates(uint32_t ctrlBase, uint16_t waitstates)¶ Sets the random read wait state amount.
This function sets the number of wait states for a flash read access. The
waitstates parameter is a number between 0 and 15. It is important to look at your device’s datasheet for information about what the required minimum flash wait-state is for your selected SYSCLK frequency.- Parameters
ctrlBase: is the base address of the flash wrapper control registers.waitstates: is the wait-state value.
By default the wait state amount is configured to the maximum 15.
- Return
None.
-
void
Flash_setBankPowerMode(uint32_t ctrlBase, Flash_BankNumber bank, Flash_BankPowerMode powerMode)¶ Sets the fallback power mode of a flash bank.
This function sets the fallback power mode of the flash bank specified by them
bank parameter. The power mode is specified by the powerMode parameter with one of the following values:- Parameters
ctrlBase: is the base address of the flash wrapper registers.bank: is the flash bank that is being configured.powerMode: is the power mode to be entered.
FLASH_BANK_PWR_SLEEP - Sense amplifiers and sense reference disabled.
FLASH_BANK_PWR_STANDBY - Sense amplifiers disabled but sense reference enabled.
FLASH_BANK_PWR_ACTIVE - Sense amplifiers and sense reference enabled.
Note: There is only one Flash_BankNumber value on this device (FLASH_BANK).
- Return
None.
-
void
Flash_setPumpPowerMode(uint32_t ctrlBase, Flash_PumpPowerMode powerMode)¶ Sets the fallback power mode of the charge pump.
This function sets the fallback power mode flash charge pump.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.powerMode: is the power mode to be entered.
FLASH_PUMP_PWR_SLEEP - All circuits disabled.
FLASH_PUMP_PWR_ACTIVE - All pump circuits active.
- Return
None.
-
void
Flash_enablePrefetch(uint32_t ctrlBase)¶ Enables prefetch mechanism.
- Return
None.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
-
void
Flash_disablePrefetch(uint32_t ctrlBase)¶ Disables prefetch mechanism.
- Return
None.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
-
void
Flash_enableCache(uint32_t ctrlBase)¶ Enables data cache.
- Return
None.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
-
void
Flash_disableCache(uint32_t ctrlBase)¶ Disables data cache.
- Return
None.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
-
void
Flash_enableECC(uint32_t eccBase)¶ Enables flash error correction code (ECC) protection.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_disableECC(uint32_t eccBase)¶ Disables flash error correction code (ECC) protection.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_setBankActiveGracePeriod(uint32_t ctrlBase, uint32_t period)¶ Sets the bank active grace period.
This function sets the bank active grace period specified by the
period parameter. The period is a value between 0 and 255. This value must be greater than 1 when the fallback mode is not Active.- Parameters
ctrlBase: is the base address of the flash wrapper control registers.period: is the starting count value for the BAGP down counter.
- Return
None.
-
void
Flash_setPumpWakeupTime(uint32_t ctrlBase, uint16_t sysclkCycles)¶ Sets the pump wake up time.
This function sets the wakeup time with
sysclkCycles parameter. The sysclkCycles is a value between 0 and 8190. When the charge pump exits sleep power mode, it will take sysclkCycles to wakeup.- Parameters
ctrlBase: is the base address of the flash wrapper control registers.sysclkCycles: is the number of SYSCLK cycles it takes for the pump to wakeup.
- Return
None.
-
bool
Flash_isBankReady(uint32_t ctrlBase, Flash_BankNumber bank)¶ Reads the bank active power state.
- Return
Returns true if the Bank is in Active power state and false otherwise.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.bank: is the flash bank that is being used.
-
bool
Flash_isPumpReady(uint32_t ctrlBase)¶ Reads the pump active power state.
- Return
Returns true if the Pump is in Active power state and false otherwise.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
-
uint32_t
Flash_getSingleBitErrorAddressLow(uint32_t eccBase)¶ Gets the single error address low.
This function returns the 32-bit address of the single bit error that occurred in the lower 64-bits of a 128-bit memory-aligned data. The returned address is to that 64-bit aligned data.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the 32 bits of a 64-bit aligned address where a single bit error occurred.
-
uint32_t
Flash_getSingleBitErrorAddressHigh(uint32_t eccBase)¶ Gets the single error address high.
This function returns the 32-bit address of the single bit error that occurred in the upper 64-bits of a 128-bit memory-aligned data. The returned address is to that 64-bit aligned data.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the 32 bits of a 64-bit aligned address where a single bit error occurred.
-
uint32_t
Flash_getUncorrectableErrorAddressLow(uint32_t eccBase)¶ Gets the uncorrectable error address low.
This function returns the 32-bit address of the uncorrectable error that occurred in the lower 64-bits of a 128-bit memory-aligned data. The returned address is to that 64-bit aligned data.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the 32 bits of a 64-bit aligned address where an uncorrectable error occurred.
-
uint32_t
Flash_getUncorrectableErrorAddressHigh(uint32_t eccBase)¶ Gets the uncorrectable error address high.
This function returns the 32-bit address of the uncorrectable error that occurred in the upper 64-bits of a 128-bit memory-aligned data. The returned address is to that 64-bit aligned data.
- Parameters
eccBase: is the base address of the flash wrapper ECC base.
- Return
Returns the 32 bits of a 64-bit aligned address where an uncorrectable error occurred.
-
Flash_ErrorStatus
Flash_getLowErrorStatus(uint32_t eccBase)¶ Gets the error status of the Lower 64-bits.
This function returns the error status of the lower 64-bits of a 128-bit aligned address.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns value of the low error status bits which can be used with Flash_ErrorStatus type.
-
Flash_ErrorStatus
Flash_getHighErrorStatus(uint32_t eccBase)¶ Gets the error status of the Upper 64-bits.
This function returns the error status of the upper 64-bits of a 128-bit aligned address.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns value of the high error status bits which can be used with Flash_ErrorStatus type.
-
uint32_t
Flash_getLowErrorPosition(uint32_t eccBase)¶ Gets the error position of the lower 64-bits for a single bit error.
This function returns the error position of the lower 64-bits. If the error type is FLASH_ECC_ERR, the position ranges from 0-7 else it ranges from 0-63 for FLASH_DATA_ERR.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the position of the lower error bit.
-
uint32_t
Flash_getHighErrorPosition(uint32_t eccBase)¶ Gets the error position of the upper 64-bits for a single bit error.
This function returns the error position of the upper 64-bits. If the error type is FLASH_ECC_ERR, the position ranges from 0-7 else it ranges from 0-63 for FLASH_DATA_ERR.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the position of the upper error bit.
-
void
Flash_clearLowErrorPosition(uint32_t eccBase)¶ Clears the error position bit of the lower 64-bits for a single bit error.
This function clears the error position bit of the lower 64-bits.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
None
-
void
Flash_clearHighErrorPosition(uint32_t eccBase)¶ Clears the error position of the upper 64-bits for a single bit error.
This function clears the error position bit of the upper 64-bits.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
None.
-
Flash_ErrorType
Flash_getLowErrorType(uint32_t eccBase)¶ Gets the error type of the lower 64-bits.
This function returns the error type of the lower 64-bits. The error type can be FLASH_ECC_ERR or FLASH_DATA_ERR.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the type of the lower 64-bit error.
-
Flash_ErrorType
Flash_getHighErrorType(uint32_t eccBase)¶ Gets the error type of the upper 64-bits.
This function returns the error type of the upper 64-bits. The error type can be FLASH_ECC_ERR or FLASH_DATA_ERR.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the type of the upper 64-bit error.
-
void
Flash_clearLowErrorStatus(uint32_t eccBase, uint16_t errorStatus)¶ Clears the errors status of the lower 64-bits.
FLASH_FAIL_0_CLR
FLASH_FAIL_1_CLR
FLASH_UNC_ERR_CLR
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.errorStatus: is the error status to clear. errorStatus is a uint16_t. errorStatus is a bitwise OR of the following value:
- Return
None.
-
void
Flash_clearHighErrorStatus(uint32_t eccBase, uint16_t errorStatus)¶ Clears the errors status of the upper 64-bits.
FLASH_FAIL_0_CLR
FLASH_FAIL_1_CLR
FLASH_UNC_ERR_CLR
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.errorStatus: is the error status to clear. errorStatus is a uint16_t. errorStatus is a bitwise OR of the following value:
- Return
None.
-
uint32_t
Flash_getErrorCount(uint32_t eccBase)¶ Gets the single bit error count.
- Return
Returns the single bit error count.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_setErrorThreshold(uint32_t eccBase, uint16_t threshold)¶ Sets the single bit error threshold.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.threshold: is the single bit error threshold. Valid ranges are from 0-65535.
-
uint32_t
Flash_getInterruptFlag(uint32_t eccBase)¶ Gets the error interrupt.
This function returns the type of error interrupt that occurred. The values can be used with
FLASH_NO_ERROR
FLASH_SINGLE_ERROR
FLASH_UNC_ERROR
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the interrupt flag.
-
void
Flash_clearSingleErrorInterruptFlag(uint32_t eccBase)¶ Clears the single error interrupt flag.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_clearUncorrectableInterruptFlag(uint32_t eccBase)¶ Clears the uncorrectable error interrupt flag.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_setDataLowECCTest(uint32_t eccBase, uint32_t data)¶ Sets the Data Low Test register for ECC testing.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.data: is a 32-bit value that is the low double word of selected 64-bit data
-
void
Flash_setDataHighECCTest(uint32_t eccBase, uint32_t data)¶ Sets the Data High Test register for ECC testing.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.data: is a 32-bit value that is the high double word of selected 64-bit data
-
void
Flash_setECCTestAddress(uint32_t eccBase, uint32_t address)¶ Sets the test address register for ECC testing.
This function left shifts the address 1 bit to convert it to a byte address
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.address: is a 32-bit value containing an address. Bits 21-3 will be used as the flash word (128-bit) address.
- Return
None.
-
void
Flash_setECCTestECCBits(uint32_t eccBase, uint16_t ecc)¶ Sets the ECC test bits for ECC testing.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.ecc: is a 32-bit value. The least significant 8 bits are used as the ECC Control Bits in the ECC Test.
-
void
Flash_enableECCTestMode(uint32_t eccBase)¶ Enables ECC Test mode.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_disableECCTestMode(uint32_t eccBase)¶ Disables ECC Test mode.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_selectLowECCBlock(uint32_t eccBase)¶ Selects the ECC block on bits [63:0] of bank data.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_selectHighECCBlock(uint32_t eccBase)¶ Selects the ECC block on bits [127:64] of bank data.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_performECCCalculation(uint32_t eccBase)¶ Performs the ECC calculation on the test block.
- Return
None.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
uint32_t
Flash_getTestDataOutHigh(uint32_t eccBase)¶ Gets the ECC Test data out high 63:32 bits.
- Return
Returns the ECC TEst data out High.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
uint32_t
Flash_getTestDataOutLow(uint32_t eccBase)¶ Gets the ECC Test data out low 31:0 bits.
- Return
Returns the ECC Test data out Low.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
uint32_t
Flash_getECCTestStatus(uint32_t eccBase)¶ Gets the ECC Test status.
This function returns the ECC test status. The values can be used with
FLASH_NO_ERROR
FLASH_SINGLE_ERROR
FLASH_UNC_ERROR
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
- Return
Returns the ECC test status.
-
uint32_t
Flash_getECCTestErrorPosition(uint32_t eccBase)¶ Gets the ECC Test single bit error position.
- Return
Returns the ECC Test single bit error position. If the error type is check bits than the position can range from 0 to 7. If the error type is data bits than the position can range from 0 to 63.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
Flash_SingleBitErrorIndicator
Flash_getECCTestSingleBitErrorType(uint32_t eccBase)¶ Gets the single bit error type.
- Return
Returns the single bit error type as a Flash_SingleBitErrorIndicator. FLASH_DATA_BITS and FLASH_CHECK_BITS indicate where the single bit error occurred.
- Parameters
eccBase: is the base address of the flash wrapper ECC registers.
-
void
Flash_claimPumpSemaphore(Flash_PumpOwnership wrapper)¶ Claim the flash pump semaphore.
- Return
None.
- Parameters
wrapper: is the Flash_PumpOwnership wrapper claiming the pump semaphore.
-
void
Flash_releasePumpSemaphore(void)¶ Release the flash pump semaphore.
- Return
None.
-
void
Flash_initModule(uint32_t ctrlBase, uint32_t eccBase, uint16_t waitstates)¶ Initializes the flash control registers.
This function initializes the flash control registers. At reset bank and pump are in sleep. A flash access will power up the bank and pump automatically. This function will power up Flash bank and pump and set the fallback mode of flash and pump as active.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.eccBase: is the base address of the flash wrapper ECC registers.waitstates: is the wait-state value.
This function also sets the number of wait-states for a flash access (see Flash_setWaitstates() for more details), and enables cache, the prefetch mechanism, and ECC.
- Return
None.
-
void
Flash_powerDown(uint32_t ctrlBase)¶ Powers down the flash.
This function powers down the flash bank(s) and the flash pump.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
Note: For this device, you must claim the flash pump semaphore before calling this function and powering down the pump. Afterwards, you may want to relinquish the flash pump.
- Return
None.
-
void
Flash_wakeFromLPM(uint32_t ctrlBase)¶ Wakes the flash from low power mode.
This function will power up Flash bank and pump and set the fallback mode of flash and pump as active.
- Parameters
ctrlBase: is the base address of the flash wrapper control registers.
- Return
None.
-
The code for this module is contained in driverlib/flash.c, with driverlib/flash.h containing the API declarations for use by applications.