EMIF Module

The external memory interface (EMIF) API provides a set of functions to configure device’s EMIF module. The driver provides functions to initialize the module, configure external memory parameters, obtain status information and to manage interrupts. APIs for both asynchronous and synchronous modes are supported.

group emif_api

Defines

EMIF_ACCPROT0_FETCHPROT MEMCFG_EMIF1ACCPROT0_FETCHPROT_EMIF1

This flag is used to specify whether CPU fetches are allowed/blocked for EMIF.

EMIF_ACCPROT0_CPUWRPROT MEMCFG_EMIF1ACCPROT0_CPUWRPROT_EMIF1

This flag is used to specify whether CPU writes are allowed/blocked for EMIF.

EMIF_ACCPROT0_DMAWRPROT MEMCFG_EMIF1ACCPROT0_DMAWRPROT_EMIF1

This flag is used to specify whether DMA writes are allowed/blocked for EMIF. It is valid only for EMIF1 instance.

EMIF_ACCPROT0_MASK_EMIF1 ((uint16_t)MEMCFG_EMIF1ACCPROT0_FETCHPROT_EMIF1

|\

(uint16_t)

MEMCFG_EMIF1ACCPROT0_CPUWRPROT_EMIF1

|\

(uint16_t)

MEMCFG_EMIF1ACCPROT0_DMAWRPROT_EMIF1)
EMIF_ACCPROT0_MASK_EMIF2 ((uint16_t)MEMCFG_EMIF2ACCPROT0_FETCHPROT_EMIF2

|\

(uint16_t)

MEMCFG_EMIF2ACCPROT0_CPUWRPROT_EMIF2)
EMIF_ASYNC_CS_CR_MASK ((uint32_t)EMIF_ASYNC_CS2_CR_R_HOLD_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_R_STROBE_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_R_SETUP_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_W_HOLD_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_W_STROBE_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_W_SETUP_M

| \

(uint32_t)

EMIF_ASYNC_CS2_CR_TA_M)
EMIF_ASYNC_INT_MASK ((uint16_t)EMIF_INT_MSK_SET_AT_MASK_SET

| \

(uint16_t)

EMIF_INT_MSK_SET_LT_MASK_SET

| \

(uint16_t)

EMIF_INT_MSK_SET_WR_MASK_SET_M)
EMIF_ASYNC_INT_AT EMIF_INT_MSK_SET_AT_MASK_SET

This flag is used to allow/block EMIF to generate Masked Asynchronous Timeout interrupt.

EMIF_ASYNC_INT_LT EMIF_INT_MSK_SET_LT_MASK_SET

This flag is used to allow/block EMIF to generate Masked Line Trap interrupt.

EMIF_ASYNC_INT_WR EMIF_INT_MSK_SET_WR_MASK_SET_M

This flag is used to allow/block EMIF to generate Masked Wait Rise interrupt.

EMIF_MSEL_KEY 0x93A5CE70U
EMIF_SYNC_SDRAM_CR_MASK ((uint32_t)EMIF_SDRAM_CR_PAGESIGE_M

| \

(uint32_t)

EMIF_SDRAM_CR_IBANK_M

| \

(uint32_t)

EMIF_SDRAM_CR_BIT_11_9_LOCK

| \

(uint32_t)

EMIF_SDRAM_CR_CL_M

| \

(uint32_t)

EMIF_SDRAM_CR_NM

| \

(uint32_t)

EMIF_SDRAM_CR_SR)
EMIF_SYNC_SDRAM_TR_MASK ((uint32_t)EMIF_SDRAM_TR_T_RRD_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_RC_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_RAS_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_WR_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_RCD_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_RP_M

| \

(uint32_t)

EMIF_SDRAM_TR_T_RFC_M)

Enums

enum EMIF_AsyncCSOffset

Values that can be passed to EMIF_setAsyncMode(), EMIF_setAsyncTimingParams(), EMIF_setAsyncDataBusWidth(), EMIF_enableAsyncExtendedWait() and EMIF_disableAsyncExtendedWait() as the offset parameter. Three chip selects are available in asynchronous memory interface so there are three configuration registers available for each EMIF instance. All the three chip select offsets are valid for EMIF1 while only EMIF_ASYNC_CS2_OFFSET is valid for EMIF2.

Values:

enumerator EMIF_ASYNC_CS2_OFFSET = 0x8U

Async chip select 2 offset.

enumerator EMIF_ASYNC_CS3_OFFSET = 0xAU

Async chip select 3 offset.

enumerator EMIF_ASYNC_CS4_OFFSET = 0xCU

Async chip select 4 offset.

enum EMIF_AsyncDataWidth

Values that can be passed to EMIF_setAsyncDataBusWidth() as the width parameter.

Values:

enumerator EMIF_ASYNC_DATA_WIDTH_8 = 0x0000U

ASRAM/FLASH with 8 bit data bus.

enumerator EMIF_ASYNC_DATA_WIDTH_16 = 0x0001U

ASRAM/FLASH with 16 bit data bus.

enumerator EMIF_ASYNC_DATA_WIDTH_32 = 0x0002U

ASRAM/FLASH with 32 bit data bus.

enum EMIF_AsyncMode

Values that can be passed to EMIF_setAsyncMode() as the mode parameter.

Values:

enumerator EMIF_ASYNC_STROBE_MODE = 0x80000000U

Enables ASRAM/FLASH strobe mode.

enumerator EMIF_ASYNC_NORMAL_MODE = 0x00000000U

Disables ASRAM/FLASH strobe mode.

enum EMIF_AsyncWaitPolarity

Values that can be passed to EMIF_setAsyncWaitPolarity() as the polarity parameter.

Values:

enumerator EMIF_ASYNC_WAIT_POLARITY_LOW = 0x00000000U

EMxWAIT pin polarity is low.

enumerator EMIF_ASYNC_WAIT_POLARITY_HIGH = 0x10000000U

EMxWAIT pin polarity is high.

enum EMIF_ControllerSelect

Values that can be passed to EMIF_selectController() as the select parameter.

Values:

enumerator EMIF_CONTROLLER_CPU1_NG = 0x00000000U

CPU1 is controller but not grabbed.

enumerator EMIF_CONTROLLER_CPU1_G = 0x00000001U

CPU1 is controller & grabbed.

enumerator EMIF_CONTROLLER_CPU2_G = 0x00000002U

CPU2 is controller & grabbed.

enumerator EMIF_CONTROLLER_CPU1_NG2 = 0x00000003U

CPU1 is controller but not grabbed.

enum EMIF_SyncNarrowMode

Values that can be passed to EMIF_setSyncMemoryConfig() as the config parameter member.

Values:

enumerator EMIF_SYNC_NARROW_MODE_TRUE = 0x00004000U

MemBusWidth=SystemBusWidth/2.

enumerator EMIF_SYNC_NARROW_MODE_FALSE = 0x00000000U

MemBusWidth=SystemBusWidth.

enum EMIF_SyncBank

Values that can be passed to EMIF_setSyncMemoryConfig() as the config parameter member.

Values:

enumerator EMIF_SYNC_BANK_1 = 0x00000000U

1 Bank SDRAM device

enumerator EMIF_SYNC_BANK_2 = 0x00000010U

2 Bank SDRAM device

enumerator EMIF_SYNC_BANK_4 = 0x00000020U

4 Bank SDRAM device

enum EMIF_SyncCASLatency

Values that can be passed to EMIF_setSyncMemoryConfig() as the config parameter member.

Values:

enumerator EMIF_SYNC_CAS_LAT_2 = 0x00000500U

SDRAM with CAS Latency 2.

enumerator EMIF_SYNC_CAS_LAT_3 = 0x00000700U

SDRAM with CAS Latency 3.

enum EMIF_SyncPageSize

Values that can be passed to EMIF_setSyncMemoryConfig() as the config parameter member.

Values:

enumerator EMIF_SYNC_COLUMN_WIDTH_8 = 0x00000000U

256-word pages in SDRAM

enumerator EMIF_SYNC_COLUMN_WIDTH_9 = 0x00000001U

512-word pages in SDRAM

enumerator EMIF_SYNC_COLUMN_WIDTH_10 = 0x00000002U

1024-word pages in SDRAM

enumerator EMIF_SYNC_COLUMN_WIDTH_11 = 0x00000003U

2048-word pages in SDRAM

Functions

void EMIF_selectController(uint32_t configBase, EMIF_ControllerSelect select)

Selects the EMIF Controller.

This function selects the controller for an EMIF1 instance among CPU1 or CPU2.

It is valid only for EMIF1 instance and not for EMIF2 instance. Valid value for configBase parameter is EMIF1CONFIG_BASE. Valid values for select parameter can be EMIF_CONTROLLER_CPU1_NG, EMIF_CONTROLLER_CPU1_G, EMIF_CONTROLLER_CPU2_G or EMIF_CONTROLLER_CPU1_NG2.
Parameters
  • configBase: is the configuration address of the EMIF instance used.

  • select: is the required controller configuration for EMIF1.

Return

None.

void EMIF_setAccessProtection(uint32_t configBase, uint16_t access)

Sets the access protection.

This function sets the access protection for an EMIF instance from CPU and DMA. The

access parameter can be any of EMIF_ACCPROT0_FETCHPROT, EMIF_ACCPROT0_CPUWRPROT EMIF_ACCPROT0_DMAWRPROT values or their combination. EMIF_ACCPROT0_DMAWRPROT value is valid as access parameter for EMIF1 instance only .
Parameters
  • configBase: is the configuration address of the EMIF instance used.

  • access: is the required access protection configuration.

Return

None.

void EMIF_commitAccessConfig(uint32_t configBase)

Commits the lock configuration.

This function commits the access protection for an EMIF instance from CPU & DMA.

Parameters
  • configBase: is the configuration address of the EMIF instance used.

Return

None.

void EMIF_lockAccessConfig(uint32_t configBase)

Locks the write to access configuration fields.

This function locks the write to access configuration fields i.e ACCPROT0 & Mselect fields, for an EMIF instance.

Parameters
  • configBase: is the configuration address of the EMIF instance used.

Return

None.

void EMIF_unlockAccessConfig(uint32_t configBase)

Unlocks the write to access configuration fields.

This function unlocks the write to access configuration fields such as ACCPROT0 & Mselect fields, for an EMIF instance.

Parameters
  • configBase: is the configuration address of the EMIF instance used.

Return

None.

void EMIF_setAsyncMode(uint32_t base, EMIF_AsyncCSOffset offset, EMIF_AsyncMode mode)

Selects the asynchronous mode of operation.

This function sets the mode of operation for asynchronous memory between Normal or Strobe mode. Valid values for param

offset can be EMIF_ASYNC_CS2_OFFSET, EMIF_ASYNC_CS3_OFFSET & EMIF_ASYNC_C43_OFFSET for EMIF1 and EMIF_ASYNC_CS2_OFFSET for EMIF2. Valid values for param mode can be EMIF_ASYNC_STROBE_MODE or EMIF_ASYNC_NORMAL_MODE.
Parameters
  • base: is the base address of the EMIF instance used.

  • offset: is the offset of asynchronous chip select of EMIF instance.

  • mode: is the desired mode of operation for external memory.

Return

None.

void EMIF_enableAsyncExtendedWait(uint32_t base, EMIF_AsyncCSOffset offset)

Enables the Extended Wait Mode.

This function enables the extended wait mode for an asynchronous external memory.Valid values for param

offset can be EMIF_ASYNC_CS2_OFFSET, EMIF_ASYNC_CS3_OFFSET & EMIF_ASYNC_C43_OFFSET for EMIF1 and EMIF_ASYNC_CS2_OFFSET for EMIF2.
Parameters
  • base: is the base address of the EMIF instance used.

  • offset: is the offset of asynchronous chip select of the EMIF instance

Return

None.

void EMIF_disableAsyncExtendedWait(uint32_t base, EMIF_AsyncCSOffset offset)

Disables the Extended Wait Mode.

This function disables the extended wait mode for an asynchronous external memory.Valid values for param

offset can be EMIF_ASYNC_CS2_OFFSET, EMIF_ASYNC_CS3_OFFSET & EMIF_ASYNC_C43_OFFSET for EMIF1 and EMIF_ASYNC_CS2_OFFSET for EMIF2.
Parameters
  • base: is the base address of the EMIF instance used.

  • offset: is the offset of asynchronous chip select of EMIF instance.

Return

None.

void EMIF_setAsyncWaitPolarity(uint32_t base, EMIF_AsyncWaitPolarity polarity)

Sets the wait polarity.

This function sets the wait polarity for an asynchronous external memory. Valid values for param

polarity can be EMIF_ASYNC_WAIT_POLARITY_LOW or EMIF_ASYNC_WAIT_POLARITY_HIGH.
Parameters
  • base: is the base address of the EMIF instance used.

  • polarity: is desired wait polarity.

Return

None.

void EMIF_setAsyncMaximumWaitCycles(uint32_t base, uint16_t value)

Sets the Maximum Wait Cycles.

This function sets the maximum wait cycles for extended asynchronous cycle. Valid values for parameter

value lies b/w 0x0U-0xFFU or 0-255.
Parameters
  • base: is the base address of the EMIF instance used.

  • value: is the desired maximum wait cycles.

Return

None.

void EMIF_setAsyncTimingParams(uint32_t base, EMIF_AsyncCSOffset offset, const EMIF_AsyncTimingParams *tParam)

Sets the Asynchronous Memory Timing Characteristics.

This function sets timing characteristics for an external asynchronous memory to be interfaced. Valid values for param

offset can be EMIF_ASYNC_CS2_OFFSET, EMIF_ASYNC_CS3_OFFSET and EMIF_ASYNC_C43_OFFSET for EMIF1 & EMIF_ASYNC_CS2_OFFSET for EMIF2.
Parameters
  • base: is the base address of the EMIF instance used.

  • offset: is the offset of asynchronous chip select of EMIF instance.

  • tParam: is the desired timing parameters.

Return

None.

void EMIF_setAsyncDataBusWidth(uint32_t base, EMIF_AsyncCSOffset offset, EMIF_AsyncDataWidth width)

Sets the Asynchronous Data Bus Width.

This function sets the data bus size for an external asynchronous memory to be interfaced. Valid values for param

offset can be EMIF_ASYNC_CS2_OFFSET, EMIF_ASYNC_CS3_OFFSET & EMIF_ASYNC_C43_OFFSET for EMIF1 and EMIF_ASYNC_CS2_OFFSET for EMIF2. Valid values of param width can be EMIF_ASYNC_DATA_WIDTH_8, EMIF_ASYNC_DATA_WIDTH_16 or EMIF_ASYNC_DATA_WIDTH_32.
Parameters
  • base: is the base address of the EMIF instance used.

  • offset: is the offset of asynchronous chip select of EMIF instance.

  • width: is the data bus width of the memory.

Return

None.

void EMIF_enableAsyncInterrupt(uint32_t base, uint16_t intFlags)

Enables the Asynchronous Memory Interrupts.

This function enables the desired interrupts for an external asynchronous memory interface. Valid values for param

intFlags can be EMIF_ASYNC_INT_AT, EMIF_ASYNC_INT_LT, EMIF_ASYNC_INT_WR or their combination.
Parameters
  • base: is the base address of the EMIF instance used.

  • intFlags: is the mask for desired interrupts.

Return

None.

void EMIF_disableAsyncInterrupt(uint32_t base, uint16_t intFlags)

Disables the Asynchronous Memory Interrupts.

This function disables the desired interrupts for an external asynchronous memory interface. Valid values for param

intFlags can be EMIF_ASYNC_INT_AT, EMIF_ASYNC_INT_LT, EMIF_ASYNC_INT_WR or their combination.
Parameters
  • base: is the base address of the EMIF instance used.

  • intFlags: is the mask for interrupts to be disabled.

Return

None.

uint16_t EMIF_getAsyncInterruptStatus(uint32_t base)

Gets the interrupt status.

This function gets the interrupt status for an EMIF instance.

Parameters
  • base: is the base address of the EMIF instance used.

Return

Returns the current interrupt status.

void EMIF_clearAsyncInterruptStatus(uint32_t base, uint16_t intFlags)

Clears the interrupt status for an EMIF instance.

This function clears the interrupt status for an EMIF instance. The

intFlags parameter can be any of EMIF_INT_MSK_SET_AT_MASK_SET, EMIF_INT_MSK_SET_LT_MASK_SET, or EMIF_INT_MSK_SET_WR_MASK_SET_M values or their combination.
Parameters
  • base: is the base address of the EMIF instance used.

  • intFlags: is the mask for the interrupt status to be cleared.

Return

None.

void EMIF_setSyncTimingParams(uint32_t base, const EMIF_SyncTimingParams *tParam)

Sets the Synchronous Memory Timing Parameters.

This function sets the timing characteristics for an external synchronous memory to be interfaced.

Parameters
  • base: is the base address of an EMIF instance.

  • tParam: is parameters from memory datasheet in ns.

Return

None.

void EMIF_setSyncSelfRefreshExitTmng(uint32_t base, uint16_t tXs)

Sets the SDRAM Self Refresh Exit Timing.

This function sets the self refresh exit timing for an external synchronous memory to be interfaced. tXs values must lie between 0x0U-0x1FU or 0-31.

Parameters
  • base: is the base address of an EMIF instance.

  • tXs: is the desired timing value.

Return

None.

void EMIF_setSyncRefreshRate(uint32_t base, uint16_t refRate)

Sets the SDR Refresh Rate.

This function sets the refresh rate for an external synchronous memory to be interfaced. Valid values for refRate lies b/w 0x0U-0x1FFFU or 0-8191.

Parameters
  • base: is the base address of an EMIF instance.

  • refRate: is the refresh rate.

Return

None.

void EMIF_setSyncMemoryConfig(uint32_t base, const EMIF_SyncConfig *config)

Sets the Synchronous Memory configuration parameters.

This function sets configuration parameters like CL, NM, IBANK and PAGESIZE for an external synchronous memory to be interfaced.

Parameters
  • base: is the base address of the EMIF instance used.

  • config: is the desired configuration parameters.

Return

None.

void EMIF_enableSyncSelfRefresh(uint32_t base)

Enables Self Refresh.

This function enables Self Refresh Mode for EMIF.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

void EMIF_disableSyncSelfRefresh(uint32_t base)

Disables Self Refresh.

This function disables Self Refresh Mode for EMIF.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

void EMIF_enableSyncPowerDown(uint32_t base)

Enables Power Down.

This function Enables Power Down Mode for synchronous memory to be interfaced.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

void EMIF_disableSyncPowerDown(uint32_t base)

Disables Power Down.

This function disables Power Down Mode for synchronous memory to be interfaced.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

void EMIF_enableSyncRefreshInPowerDown(uint32_t base)

Enables Refresh in Power Down.

This function enables Refresh in Power Down Mode for synchronous memory to be interfaced.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

void EMIF_disableSyncRefreshInPowerDown(uint32_t base)

Disables Refresh in Power Down.

This function disables Refresh in Power Down Mode for synchronous memory to be interfaced.

Parameters
  • base: is the base address of the EMIF instance used.

Return

None.

uint32_t EMIF_getSyncTotalAccesses(uint32_t base)

Gets total number of SDRAM accesses.

This function returns total number of SDRAM accesses from a controller(CPUx/CPUx.DMA).

Parameters
  • base: is the base address of the EMIF instance used.

Return

Returns total number of accesses to SDRAM.

uint32_t EMIF_getSyncTotalActivateAccesses(uint32_t base)

Gets total number of SDRAM accesses which require activate command.

This function returns total number of accesses to SDRAM which require activate command.

Parameters
  • base: is the base address of the EMIF instance used.

Return

Returns total number of accesses to SDRAM which require activate.

struct EMIF_AsyncTimingParams
#include <emif.h>

Values that can be passed to EMIF_setAsyncTimingParams() as the tParam parameter.

struct EMIF_SyncConfig
#include <emif.h>

Values that can be passed to EMIF_setSyncMemoryConfig() as the config parameter.

struct EMIF_SyncTimingParams
#include <emif.h>

Values that can be passed to EMIF_setSyncTimingParameters() as the tParam parameter.

The EMIF API include functions to select master for EMIF module, set, lock/unlock, commit access configuration, set external asynchronous and synchronous memory configuration parameters and to manage asynchronous interrupts.

For interfacing asynchronous memories, functions are provided to configure EMIF registers to set mode of operation to strobe or normal mode, set enable/disable extended wait mode, set wait polarity, set maximum wait cycles, set async memory timing parameters, set memory data bus width as per the external memory to be interfaced and enable/disable, clear and get status for interrupts.

For interfacing synchronous memories, functions are provided to configure EMIF registers to set timing parameters, set self refresh exit timing, set refresh rate, set other memory specific parameters based on the external memory to be interfaced, enable/disable self refresh mode, enable/disable power down mode, enable/disable refresh in power down mode and to get total number of SDRAM accesses.

The code for this module is contained in driverlib/emif.c, with driverlib/emif.h containing the API declarations for use by applications.