SDFM Module¶
The Sigma-Delta Filter Module (SDFM) API provides a set of functions for configuring and using the SDFM module. The functions provided allow the user to setup and configure the Input data type to SDFM filters, the Primary (data) and Secondary (comparator) filters, Data FIFO, the PWM - SDFM sync signals, comparator threshold values and interrupt sources. Functions are also provided to read the filter data and the status of the SDFM module components.
Note that the Secondary (comparator) Filter configuration APIs have the “Comp” key word embedded to represent access to the Comparator sub-module. For example the function SDFM_setComparatorFilterType() sets the comparator filter type while SDFM_setFilterType() sets the primary filter type.
APIs providing higher level abstraction are also available in the sdfm.c source file. These APIs can be used to configure the Comparator, Data Filter and the Data filter FIFO.
{color{red} textsc{Note: The Manchester modulator clock mode is no longer supported in SDFM for this device. The required software changes are scoped for next C2000Ware release and are not supported in this release. Users are advised to not use this feature on this device.}}
-
group
sdfm_api Defines
-
SDFM_GET_LOW_THRESHOLD(C) ((uint16_t)(C))¶ Macro to get the low threshold
-
SDFM_GET_HIGH_THRESHOLD(C) ((uint16_t)((uint32_t)(C) >> 16U))¶ Macro to get the high threshold
-
SDFM_GET_LOW_THRESHOLD_BOTH(C1, C2) ((((uint32_t)(SDFM_GET_LOW_THRESHOLD(C2))) << 16U) | \
((uint32_t)(
SDFM_GET_LOW_THRESHOLD(C1))))¶ Macro to get the high threshold 1 & 2 to be passed as lowThreshold parameter to SDFM_setCompFilterLowThreshold().
-
SDFM_GET_HIGH_THRESHOLD_BOTH(C1, C2) ((((uint32_t)(SDFM_GET_HIGH_THRESHOLD(C2))) << 16U) | \
((uint32_t)(
SDFM_GET_HIGH_THRESHOLD(C1))))¶ Macro to get the high threshold 1 & 2 to be passed as highThreshold parameter to SDFM_setCompFilterHighThreshold().
-
SDFM_SET_OSR(X) (((X) - 1U) << 8U)¶ Macro to convert comparator over sampling ratio to acceptable bit location
-
SDFM_SHIFT_VALUE(X) ((X) << 2U)¶ Macro to convert the data shift bit values to acceptable bit location
-
SDFM_THRESHOLD(H, L) ((((uint32_t)(H)) << 16U) | (L))¶ Macro to combine high threshold and low threshold values
-
SDFM_SET_FIFO_LEVEL(X) ((X) << 7U)¶ Macro to set the FIFO level to acceptable bit location
-
SDFM_SET_ZERO_CROSS_THRESH_VALUE(X) (0x8000 | (X))¶ Macro to set and enable the zero cross threshold value.
-
SDFM_FILTER_DISABLE0x0U¶ Macros to enable or disable filter.
-
SDFM_FILTER_ENABLE0x2U¶
-
SDFM_SDFIL_OFFSET(SDFM_O_SDCTLPARM2 - SDFM_O_SDCTLPARM1)¶ < SD filter offset
Event Digital filter offset
-
SDFM_DIGFIL_OFFSET(SDFM_O_SDCOMP2CTL - SDFM_O_SDCOMP1CTL)¶ Offset between high threshold 1 & 2 registers.
-
SDFM_SDFLT1CMPHx_OFFSET(SDFM_O_SDFLT1CMPH2 - SDFM_O_SDFLT1CMPH1)¶ Offset between low threshold 1 & 2 registers.
-
SDFM_SDFLT1CMPLx_OFFSET(SDFM_O_SDFLT1CMPL2 - SDFM_O_SDFLT1CMPL1)¶
-
SDFM_COMPEVT_FILTER_CONFIG_M(SDFM_SDCOMP1EVT1FLTCTL_SAMPWIN_M| \
SDFM_SDCOMP1EVT1FLTCTL_THRESH_M)¶
-
SDFM_COMPEVT_FILTER_LOCK_M(SDFM_SDCOMPLOCK_SDCOMPCTL | \
SDFM_SDCOMPLOCK_COMP)
¶
-
SDFM_CLOCK_SYNCHRONIZERSDFM_SDCTLPARM1_SDCLKSYNC¶ Define for Clock synchronizer Configuration.
-
SDFM_DATA_SYNCHRONIZERSDFM_SDCTLPARM1_SDDATASYNC¶ Define for Data Synchronizer Configuration.
-
SDFM_MODULATOR_FAILURE_INTERRUPT0x200U¶ Interrupt is generated if Modulator fails.
-
SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT0x40U¶ Interrupt on Comparator low-level threshold.
-
SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT0x20U¶ Interrupt on Comparator high-level threshold.
-
SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT0x1U¶ Interrupt on Acknowledge flag
-
SDFM_FIFO_INTERRUPT0x1000U¶ Interrupt on FIFO level
-
SDFM_FIFO_OVERFLOW_INTERRUPT0x8000U¶ Interrupt on FIFO overflow
-
SDFM_MAIN_INTERRUPT_FLAG0x80000000U¶ Main interrupt flag
-
SDFM_FILTER_1_HIGH_THRESHOLD_FLAG0x1U¶ Filter 1 high -level threshold flag
-
SDFM_FILTER_1_LOW_THRESHOLD_FLAG0x2U¶ Filter 1 low -level threshold flag
-
SDFM_FILTER_2_HIGH_THRESHOLD_FLAG0x4U¶ Filter 2 high -level threshold flag
-
SDFM_FILTER_2_LOW_THRESHOLD_FLAG0x8U¶ Filter 2 low -level threshold flag
-
SDFM_FILTER_3_HIGH_THRESHOLD_FLAG0x10U¶ Filter 3 high -level threshold flag
-
SDFM_FILTER_3_LOW_THRESHOLD_FLAG0x20U¶ Filter 3 low -level threshold flag
-
SDFM_FILTER_4_HIGH_THRESHOLD_FLAG0x40U¶ Filter 4 high -level threshold flag
-
SDFM_FILTER_4_LOW_THRESHOLD_FLAG0x80U¶ Filter 4 low -level threshold flag
-
SDFM_FILTER_1_MOD_FAILED_FLAG0x100U¶ Filter 1 modulator failed flag
-
SDFM_FILTER_2_MOD_FAILED_FLAG0x200U¶ Filter 2 modulator failed flag
-
SDFM_FILTER_3_MOD_FAILED_FLAG0x400U¶ Filter 3 modulator failed flag
-
SDFM_FILTER_4_MOD_FAILED_FLAG0x800U¶ Filter 4 modulator failed flag
-
SDFM_FILTER_1_NEW_DATA_FLAG0x1000U¶ Filter 1 new data flag
-
SDFM_FILTER_2_NEW_DATA_FLAG0x2000U¶ Filter 2 new data flag
-
SDFM_FILTER_3_NEW_DATA_FLAG0x4000U¶ Filter 3 new data flag
-
SDFM_FILTER_4_NEW_DATA_FLAG0x8000U¶ Filter 4 new data flag
-
SDFM_FILTER_1_FIFO_OVERFLOW_FLAG0x10000U¶ Filter 1 FIFO overflow flag
-
SDFM_FILTER_2_FIFO_OVERFLOW_FLAG0x20000U¶ Filter 2 FIFO overflow flag
-
SDFM_FILTER_3_FIFO_OVERFLOW_FLAG0x40000U¶ Filter 3 FIFO overflow flag
-
SDFM_FILTER_4_FIFO_OVERFLOW_FLAG0x80000U¶ Filter 4 FIFO overflow flag
-
SDFM_FILTER_1_FIFO_INTERRUPT_FLAG0x100000U¶ Filter 1 FIFO overflow flag
-
SDFM_FILTER_2_FIFO_INTERRUPT_FLAG0x200000U¶ Filter 2 FIFO overflow flag
-
SDFM_FILTER_3_FIFO_INTERRUPT_FLAG0x400000U¶ Filter 3 FIFO overflow flag
-
SDFM_FILTER_4_FIFO_INTERRUPT_FLAG0x800000U¶ Filter 4 FIFO overflow flag
Enums
-
enum
SDFM_OutputThresholdStatus¶ Values that can be returned from SDFM_getThresholdStatus()
Values:
-
enumerator
SDFM_OUTPUT_WITHIN_THRESHOLD= 0¶ SDFM output is within threshold.
-
enumerator
SDFM_OUTPUT_ABOVE_THRESHOLD= 1¶ SDFM output is above threshold.
-
enumerator
SDFM_OUTPUT_BELOW_THRESHOLD= 2¶ SDFM output is below threshold.
-
enumerator
-
enum
SDFM_FilterNumber¶ Values that can be passed to all functions as the filterNumber parameter.
Values:
-
enumerator
SDFM_FILTER_1= 0¶ Digital filter 1.
-
enumerator
SDFM_FILTER_2= 1¶ Digital filter 2.
-
enumerator
SDFM_FILTER_3= 2¶ Digital filter 3.
-
enumerator
SDFM_FILTER_4= 3¶ Digital filter 4.
-
enumerator
-
enum
SDFM_FilterType¶ Values that can be passed to SDFM_setFilterType(), SDFM_setComparatorFilterType() as the filterType parameter.
Values:
-
enumerator
SDFM_FILTER_SINC_FAST= 0x00¶ Digital filter with SincFast structure.
-
enumerator
SDFM_FILTER_SINC_1= 0x10¶ Digital filter with Sinc1 structure.
-
enumerator
SDFM_FILTER_SINC_2= 0x20¶ Digital filter with Sinc3 structure.
-
enumerator
SDFM_FILTER_SINC_3= 0x30¶ Digital filter with Sinc4 structure.
-
enumerator
-
enum
SDFM_ModulatorClockMode¶ Values that can be passed to SDFM_setupModulatorClock(),as the clockMode parameter.
Values:
-
enumerator
SDFM_MODULATOR_CLK_EQUAL_DATA_RATE= 0¶ Modulator clock is identical to the data rate.
-
enumerator
-
enum
SDFM_OutputDataFormat¶ Values that can be passed to SDFM_setOutputDataFormat(),as the dataFormat parameter.
Values:
-
enumerator
SDFM_DATA_FORMAT_16_BIT= 0¶ Filter output is in 16 bits 2’s complement format.
-
enumerator
SDFM_DATA_FORMAT_32_BIT= 1¶ Filter output is in 32 bits 2’s complement format.
-
enumerator
-
enum
SDFM_DataReadyInterruptSource¶ Values that can be passed to SDFM_setDataReadyInterruptSource(),as the dataReadySource parameter.
Values:
-
enumerator
SDFM_DATA_READY_SOURCE_DIRECT= 0¶ Data ready interrupt source is direct (non -FIFO).
-
enumerator
SDFM_DATA_READY_SOURCE_FIFO= 1¶ Data ready interrupt source is FIFO.
-
enumerator
-
enum
SDFM_PWMSyncSource¶ Values that can be passed to SDFM_setPWMSyncSource(),as the syncSource parameter.
Values:
-
enumerator
SDFM_SYNC_PWM1_SOCA= 0¶ SDFM sync source is PWM1 SOCA.
-
enumerator
SDFM_SYNC_PWM1_SOCB= 1¶ SDFM sync source is PWM1 SOCB.
-
enumerator
SDFM_SYNC_PWM2_SOCA= 4¶ SDFM sync source is PWM2 SOCA.
-
enumerator
SDFM_SYNC_PWM2_SOCB= 5¶ SDFM sync source is PWM2 SOCB.
-
enumerator
SDFM_SYNC_PWM3_SOCA= 8¶ SDFM sync source is PWM3 SOCA.
-
enumerator
SDFM_SYNC_PWM3_SOCB= 9¶ SDFM sync source is PWM3 SOCB.
-
enumerator
SDFM_SYNC_PWM4_SOCA= 12¶ SDFM sync source is PWM4 SOCA.
-
enumerator
SDFM_SYNC_PWM4_SOCB= 13¶ SDFM sync source is PWM4 SOCB.
-
enumerator
SDFM_SYNC_PWM5_SOCA= 16¶ SDFM sync source is PWM5 SOCA.
-
enumerator
SDFM_SYNC_PWM5_SOCB= 17¶ SDFM sync source is PWM5 SOCB.
-
enumerator
SDFM_SYNC_PWM6_SOCA= 20¶ SDFM sync source is PWM6 SOCA.
-
enumerator
SDFM_SYNC_PWM6_SOCB= 21¶ SDFM sync source is PWM6 SOCB.
-
enumerator
SDFM_SYNC_PWM7_SOCA= 24¶ SDFM sync source is PWM7 SOCA.
-
enumerator
SDFM_SYNC_PWM7_SOCB= 25¶ SDFM sync source is PWM7 SOCB.
-
enumerator
SDFM_SYNC_PWM8_SOCA= 28¶ SDFM sync source is PWM8 SOCA.
-
enumerator
SDFM_SYNC_PWM8_SOCB= 29¶ SDFM sync source is PWM8 SOCB.
-
enumerator
SDFM_SYNC_PWM9_SOCA= 32¶ SDFM sync source is PWM9 SOCA.
-
enumerator
SDFM_SYNC_PWM9_SOCB= 33¶ SDFM sync source is PWM9 SOCB.
-
enumerator
SDFM_SYNC_PWM10_SOCA= 36¶ SDFM sync source is PWM10 SOCA.
-
enumerator
SDFM_SYNC_PWM10_SOCB= 37¶ SDFM sync source is PWM10 SOCB.
-
enumerator
SDFM_SYNC_PWM11_SOCA= 40¶ SDFM sync source is PWM11 SOCA.
-
enumerator
SDFM_SYNC_PWM11_SOCB= 41¶ SDFM sync source is PWM11 SOCB.
-
enumerator
SDFM_SYNC_PWM12_SOCA= 44¶ SDFM sync source is PWM12 SOCA.
-
enumerator
SDFM_SYNC_PWM12_SOCB= 45¶ SDFM sync source is PWM12 SOCB.
-
enumerator
SDFM_SYNC_PWM13_SOCA= 48¶ SDFM sync source is PWM13 SOCA.
-
enumerator
SDFM_SYNC_PWM13_SOCB= 49¶ SDFM sync source is PWM13 SOCB.
-
enumerator
SDFM_SYNC_PWM14_SOCA= 52¶ SDFM sync source is PWM14 SOCA.
-
enumerator
SDFM_SYNC_PWM14_SOCB= 53¶ SDFM sync source is PWM14 SOCB.
-
enumerator
SDFM_SYNC_PWM15_SOCA= 56¶ SDFM sync source is PWM15 SOCA.
-
enumerator
SDFM_SYNC_PWM15_SOCB= 57¶ SDFM sync source is PWM15 SOCB.
-
enumerator
SDFM_SYNC_PWM16_SOCA= 60¶ SDFM sync source is PWM16 SOCA.
-
enumerator
SDFM_SYNC_PWM16_SOCB= 61¶ SDFM sync source is PWM16 SOCB.
-
enumerator
-
enum
SDFM_FIFOClearSyncMode¶ Values that can be passed to SDFM_setFIFOClearOnSyncMode(),as the fifoClearSyncMode parameter.
Values:
-
enumerator
SDFM_FIFO_NOT_CLEARED_ON_SYNC= 0¶ SDFM FIFO buffer is not cleared on Sync signal.
-
enumerator
SDFM_FIFO_CLEARED_ON_SYNC= 1¶ SDFM FIFO buffer is cleared on Sync signal.
-
enumerator
-
enum
SDFM_WaitForSyncClearMode¶ Values that can be passed to SDFM_setWaitForSyncClearMode(),as the syncClearMode parameter.
Values:
-
enumerator
SDFM_MANUAL_CLEAR_WAIT_FOR_SYNC= 0¶ Wait for sync cleared using software.
-
enumerator
SDFM_AUTO_CLEAR_WAIT_FOR_SYNC= 1¶ Wait for sync cleared automatically.
-
enumerator
-
enum
SDFM_CompEventNumber¶ Values that can be passed to SDFM_selectCompEventSource() as the compEventNum parameter.
Values:
-
enumerator
SDFM_COMP_EVENT_1= 11U¶ Selects CEVT1.
-
enumerator
SDFM_COMP_EVENT_2= 14U¶ Selects CEVT2.
-
enumerator
-
enum
SDFM_CompEventSource¶ Values that can be passed to SDFM_selectCompEventSource() as the compEventSource parameter.
Values:
-
enumerator
SDFM_COMP_EVENT_SRC_COMPH1= 0¶ COMPH1 event is the source.
-
enumerator
SDFM_COMP_EVENT_SRC_COMPH1_L1= 1¶ Either of COMPH1 or COMPL1 event can be the source
-
enumerator
SDFM_COMP_EVENT_SRC_COMPH2= 2¶ COMPH2 event is the source.
-
enumerator
SDFM_COMP_EVENT_SRC_COMPH2_L2= 3¶ Either of COMPH2 or COMPL2 event can be the source
-
enumerator
SDFM_COMP_EVENT_SRC_COMPL1= 0¶ COMPL1 event is the source.
-
enumerator
SDFM_COMP_EVENT_SRC_COMPL2= 2¶ COMPL2 event is the source.
-
enumerator
-
enum
SDFM_ClockSource¶ Values that can be passed to SDFM_selectClockSource() as the clkSource parameter.
Values:
-
enumerator
SDFM_CLK_SOURCE_CHANNEL_CLK= 0x0¶ Source is respective channel clock.
-
enumerator
SDFM_CLK_SOURCE_SD1_CLK= 0x8U¶ Source is SD1 channel clock is the source.
-
enumerator
-
enum
SDFM_CompEventHighSource¶ Values that can be passed to SDFM_selectCompEventHighSource() as the source parameter.
Values:
-
enumerator
SDFM_COMPHOUT_SOURCE_COMPHIN= 0x0¶ Comparator event high source is unfiltered event.
-
enumerator
SDFM_COMPHOUT_SOURCE_FILTER= 0x8¶ Comparator event high source is filtered event.
-
enumerator
-
enum
SDFM_CompEventLowSource¶ Values that can be passed to SDFM_selectCompEventLowSource() as the source parameter.
Values:
-
enumerator
SDFM_COMPLOUT_SOURCE_COMPLIN= 0x000¶ Comparator event low source is unfiltered event.
-
enumerator
SDFM_COMPLOUT_SOURCE_FILTER= 0x800¶ Comparator event low source is filtered event.
-
enumerator
Functions
-
void
SDFM_enableExternalReset(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable external reset
This function enables data filter to be reset by an external source (PWM compare output).
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableExternalReset(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable external reset
This function disables data filter from being reset by an external source (PWM compare output).
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_enableFilter(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable filter
This function enables the filter specified by the
filterNumber variable.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableFilter(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable filter
This function disables the filter specified by the
filterNumber variable.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_enableFIFOBuffer(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable FIFO buffer
This function enables the filter FIFO buffer specified by the
filterNumber variable.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableFIFOBuffer(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable FIFO buffer
This function disables the filter FIFO buffer specified by the
filterNumber variable.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
bool
SDFM_getZeroCrossTripStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Return the Zero Cross Trip status
This function returns the Zero Cross Trip status for the filter specified by filterNumber variable.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
true if Comparator filter output >= High-level threshold (Z) false if Comparator filter output < High-level threshold (Z)
-
void
SDFM_clearZeroCrossTripStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Clear the Zero Cross Trip status
This function clears the Zero Cross Trip status for the filter specified by filterNumber variable.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_enableComparator(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable Comparator.
This function enables the Comparator for the selected filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableComparator(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable Comparator.
This function disables the Comparator for the selected filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_selectCompEventSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_CompEventNumber compEventNum, SDFM_CompEventSource compEventSource)¶ Selects Comparator Event Source.
This function selects the comparator event source. Valid values for
compEventNum are:SDFM_COMP_EVENT_1 - Selects comparator event 1
SDFM_COMP_EVENT_2 - Selects comparator event 2 Valid values for SDFM_COMP_EVENT_1 are:
SDFM_COMP_EVENT_SRC_COMPH1 - COMPH1 event is the source for selected event
SDFM_COMP_EVENT_SRC_COMPH1_L1 - Either of COMPH1 or COMPL1 event can be the source for selected event
SDFM_COMP_EVENT_SRC_COMPH2 - COMPH2 event is the source for selected event
SDFM_COMP_EVENT_SRC_COMPH2_L2 - Either of COMPH2 or COMPL2 event can be the source for selected event
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter numbercompEventNum: is the event numbercompEventSource: is the event source
Valid values for SDFM_COMP_EVENT_2 are:
SDFM_COMP_EVENT_SRC_COMPL1 - COMPL1 event is the source for selected event
SDFM_COMP_EVENT_SRC_COMPH1_L1 - Either of COMPH1 or COMPL1 event can be the source for selected event
SDFM_COMP_EVENT_SRC_COMPL2 - COMPL2 event is the source for selected event
SDFM_COMP_EVENT_SRC_COMPH2_L2 - Either of COMPH2 or COMPL2 event can be the source for selected event
- Return
None.
-
void
SDFM_setFilterType(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_FilterType filterType)¶ Set filter type.
This function sets the filter type or structure to be used as specified by filterType for the selected filter number as specified by filterNumber.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.filterType: is the filter type or structure.
- Return
None.
-
void
SDFM_setFilterOverSamplingRatio(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t overSamplingRatio)¶ Set data filter over sampling ratio.
This function sets the filter oversampling ratio for the filter specified by the filterNumber variable.Valid values for the variable overSamplingRatio are 0 to 255 inclusive. The actual oversampling ratio will be this value plus one.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.overSamplingRatio: is the data filter over sampling ratio.
- Return
None.
-
void
SDFM_setupModulatorClock(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_ModulatorClockMode clockMode)¶ Set modulator clock mode.
This function sets the modulator clock mode specified by clockMode for the filter specified by filterNumber.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.clockMode: is the modulator clock mode.
- Note
This function also enables the data and clock synchronizers for the specified filter.
- Return
None.
-
void
SDFM_setOutputDataFormat(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_OutputDataFormat dataFormat)¶ Set the output data format
This function sets the output data format for the filter specified by filterNumber.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.dataFormat: is the output data format.
- Return
None.
-
void
SDFM_setDataShiftValue(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t shiftValue)¶ Set data shift value.
This function sets the shift value for the 16 bit 2’s complement data format. The valid maximum value for shiftValue is 31.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.shiftValue: is the data shift value.
Note: Use this function with 16 bit 2’s complement data format only.
- Return
None.
-
void
SDFM_setCompFilterHighThreshold(uint32_t base, SDFM_FilterNumber filterNumber, uint32_t highThreshold)¶ Set Filter output high-level threshold.
This function sets the unsigned high-level threshold value for the Comparator filter output. If the output value of the filter exceeds highThreshold and interrupt generation is enabled, an interrupt will be issued. The param
highThreshold takes both high threshold 1 & 2 values. The upper 16-bits represent the high threshold 2 value while lower 16-bits represent the threshold 1 values.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.highThreshold: is the high-level threshold 1 & 2.
- Return
None.
-
void
SDFM_setCompFilterLowThreshold(uint32_t base, SDFM_FilterNumber filterNumber, uint32_t lowThreshold)¶ Set Filter output low-level threshold.
This function sets the unsigned low-level threshold value 1 or 2 for the Comparator filter output. If the output value of the filter gets below lowThreshold and interrupt generation is enabled, an interrupt will be issued. The param
lowThreshold takes both low threshold 1 & 2 values. The upper 16-bits represent the low threshold 2 value while lower 16-bits represent the threshold 1 values.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter numberlowThreshold: is the low-level threshold
- Return
None.
-
void
SDFM_setCompFilterZeroCrossThreshold(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t zeroCrossThreshold)¶ Set Filter output zero-cross threshold.
This function sets the unsigned zero-cross threshold value for the Comparator filter output.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.zeroCrossThreshold: is the zero-cross threshold.
- Return
None.
-
void
SDFM_enableZeroCrossEdgeDetect(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable zero-cross Edge detect mode.
This function enables Zero Cross Edge detection.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableZeroCrossEdgeDetect(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable zero-cross Edge detect mode.
This function disables Zero Cross Edge detection.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_enableInterrupt(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t intFlags)¶ Enable SDFM interrupts.
This function enables the low threshold , high threshold or modulator failure interrupt as determined by intFlags for the filter specified by filterNumber. Valid values for intFlags are: SDFM_MODULATOR_FAILURE_INTERRUPT , SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT, SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT, SDFM_FIFO_INTERRUPT, SDFM_FIFO_OVERFLOW_INTERRUPT,SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.intFlags: is the interrupt source.
- Return
None.
-
void
SDFM_disableInterrupt(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t intFlags)¶ Disable SDFM interrupts.
This function disables the low threshold , high threshold or modulator failure interrupt as determined by intFlags for the filter specified by filterNumber. Valid values for intFlags are: SDFM_MODULATOR_FAILURE_INTERRUPT , SDFM_LOW_LEVEL_THRESHOLD_INTERRUPT, SDFM_HIGH_LEVEL_THRESHOLD_INTERRUPT, SDFM_FIFO_INTERRUPT, SDFM_FIFO_OVERFLOW_INTERRUPT,SDFM_DATA_FILTER_ACKNOWLEDGE_INTERRUPT
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.intFlags: is the interrupt source.
- Return
None.
-
void
SDFM_setComparatorFilterType(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_FilterType filterType)¶ Set the comparator filter type.
This function sets the Comparator filter type or structure to be used as specified by filterType for the selected filter number as specified by filterNumber.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.filterType: is the comparator filter type or structure.
- Return
None.
-
void
SDFM_setCompFilterOverSamplingRatio(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t overSamplingRatio)¶ Set Comparator filter over sampling ratio.
This function sets the comparator filter oversampling ratio for the filter specified by the filterNumber.Valid values for the variable overSamplingRatio are 0 to 31 inclusive. The actual oversampling ratio will be this value plus one.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.overSamplingRatio: is the comparator filter over sampling ration.
- Return
None.
-
uint32_t
SDFM_getFilterData(uint32_t base, SDFM_FilterNumber filterNumber)¶ Get the filter data output.
This function returns the latest data filter output. Depending on the filter data output format selected, the valid value will be the lower 16 bits or the whole 32 bits of the returned value.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns the latest data filter output.
-
SDFM_OutputThresholdStatus
SDFM_getThresholdStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Get the Comparator threshold status.
This function returns the Comparator output threshold status for the given filterNumber.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns the following status flags.
SDFM_OUTPUT_WITHIN_THRESHOLD if the output is within the specified threshold.
SDFM_OUTPUT_ABOVE_THRESHOLD if the output is above the high threshold
SDFM_OUTPUT_BELOW_THRESHOLD if the output is below the low threshold.
-
bool
SDFM_getModulatorStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Get the Modulator status.
This function returns the Modulator status.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns true if the Modulator is operating normally Returns false if the Modulator has failed
-
bool
SDFM_getNewFilterDataStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Check if new Filter data is available.
This function returns new filter data status.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns true if new filter data is available Returns false if no new filter data is available
-
bool
SDFM_getFIFOOverflowStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Check if FIFO buffer is overflowed.
This function returns the status of the FIFO buffer overflow for the given filter value.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns true if FIFO buffer is overflowed Returns false if FIFO buffer is not overflowed
-
bool
SDFM_getFIFOISRStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Check FIFO buffer interrupt status.
This function returns the status of the FIFO buffer interrupt for the given filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns true if FIFO buffer interrupt has occurred. Returns false if FIFO buffer interrupt has not occurred.
-
bool
SDFM_getIsrStatus(uint32_t base)¶ Get pending interrupt.
This function returns any pending interrupt status.
- Parameters
base: is the base address of the SDFM module
- Return
Returns true if there is a pending interrupt. Returns false if no interrupt is pending.
-
void
SDFM_clearInterruptFlag(uint32_t base, uint32_t flag)¶ Clear pending flags.
This function clears the specified pending interrupt flag. Valid values are SDFM_MAIN_INTERRUPT_FLAG,SDFM_FILTER_1_NEW_DATA_FLAG, SDFM_FILTER_2_NEW_DATA_FLAG,SDFM_FILTER_3_NEW_DATA_FLAG, SDFM_FILTER_4_NEW_DATA_FLAG,SDFM_FILTER_1_MOD_FAILED_FLAG, SDFM_FILTER_2_MOD_FAILED_FLAG,SDFM_FILTER_3_MOD_FAILED_FLAG, SDFM_FILTER_4_MOD_FAILED_FLAG,SDFM_FILTER_1_HIGH_THRESHOLD_FLAG, SDFM_FILTER_1_LOW_THRESHOLD_FLAG,SDFM_FILTER_2_HIGH_THRESHOLD_FLAG, SDFM_FILTER_2_LOW_THRESHOLD_FLAG,SDFM_FILTER_3_HIGH_THRESHOLD_FLAG, SDFM_FILTER_3_LOW_THRESHOLD_FLAG,SDFM_FILTER_4_HIGH_THRESHOLD_FLAG, SDFM_FILTER_4_LOW_THRESHOLD_FLAG,SDFM_FILTER_1_FIFO_OVERFLOW_FLAG, SDFM_FILTER_2_FIFO_OVERFLOW_FLAG,SDFM_FILTER_3_FIFO_OVERFLOW_FLAG SDFM_FILTER_4_FIFO_OVERFLOW_FLAG,SDFM_FILTER_1_FIFO_INTERRUPT_FLAG, SDFM_FILTER_2_FIFO_INTERRUPT_FLAG,SDFM_FILTER_3_FIFO_INTERRUPT_FLAG SDFM_FILTER_4_FIFO_INTERRUPT_FLAG or any combination of the above flags.
- Parameters
base: is the base address of the SDFM moduleflag: is the SDFM status
- Return
None
-
void
SDFM_enableMainInterrupt(uint32_t base)¶ Enable main interrupt.
This function enables the main SDFM interrupt.
- Parameters
base: is the base address of the SDFM module
- Return
None
-
void
SDFM_disableMainInterrupt(uint32_t base)¶ Disable main interrupt.
This function disables the main SDFM interrupt.
- Parameters
base: is the base address of the SDFM module
- Return
None
-
void
SDFM_enableMainFilter(uint32_t base)¶ Enable main filter.
This function enables main filter.
- Parameters
base: is the base address of the SDFM module
- Return
None
-
void
SDFM_disableMainFilter(uint32_t base)¶ Disable main filter.
This function disables main filter.
- Parameters
base: is the base address of the SDFM module
- Return
None
-
uint16_t
SDFM_getFIFODataCount(uint32_t base, SDFM_FilterNumber filterNumber)¶ Return the FIFO data count
This function returns the FIFO data count.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns the number of data words available in FIFO buffer.
-
uint16_t
SDFM_getComparatorSincData(uint32_t base, SDFM_FilterNumber filterNumber)¶ Return the Comparator sinc filter data
This function returns the Comparator sinc filter data output.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns the Comparator sinc filter data output.
-
uint32_t
SDFM_getFIFOData(uint32_t base, SDFM_FilterNumber filterNumber)¶ Return the FIFO data
This function returns the latest FIFO data.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns the latest FIFO data.
- Note
Discard the upper 16 bits if the output data format is 16bits.
-
void
SDFM_setFIFOInterruptLevel(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t fifoLevel)¶ Set the FIFO interrupt level.
This function sets the FIFO interrupt level. Interrupt is generated when the FIFO buffer word count gets to or exceeds the value of
fifoLevel. Maximum value for fifoLevel is 16.- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.fifoLevel: is the FIFO interrupt level.
- Return
None.
-
void
SDFM_setDataReadyInterruptSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_DataReadyInterruptSource dataReadySource)¶ Set data ready interrupt source.
This function sets the data ready interrupt source. Valid values for
dataReadySource:SDFM_DATA_READY_SOURCE_DIRECT - Direct data ready
SDFM_DATA_READY_SOURCE_FIFO - FIFO data ready.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.dataReadySource: is the data ready interrupt source.
- Return
None.
-
bool
SDFM_getWaitForSyncStatus(uint32_t base, SDFM_FilterNumber filterNumber)¶ Get the wait-for-sync event status.
This function returns the Wait-for-Sync event status.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
Returns true if sync event has occurred. Returns false if sync event has not occurred.
-
void
SDFM_clearWaitForSyncFlag(uint32_t base, SDFM_FilterNumber filterNumber)¶ Clear the Wait-for-sync event status.
This function clears the Wait-for-sync event status.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_enableWaitForSync(uint32_t base, SDFM_FilterNumber filterNumber)¶ Enable wait for sync mode.
This function enables the wait for sync mode. Data to FIFO will be written only after PWM sync event.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_disableWaitForSync(uint32_t base, SDFM_FilterNumber filterNumber)¶ Disable wait for sync mode.
This function disables the wait for sync mode. Data to FIFO will be written every Data ready event.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_setPWMSyncSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_PWMSyncSource syncSource)¶ Set the PWM sync mode.
This function sets the PWM sync source for the specific SDFM filter. Valid values for syncSource are SDFM_SYNC_PWMx_CMPy. Where x ranges from 1 to 8 Representing PWM1 to PWM8 respectively and y ranges from A to D representing PWM comparators A to D.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.syncSource: is the PWM sync source.
- Return
None.
-
void
SDFM_setFIFOClearOnSyncMode(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_FIFOClearSyncMode fifoClearSyncMode)¶ Set FIFO clear on sync mode.
This function sets the FIFO clear mode for the specified filter when a sync happens depending on the value of fifoClearSyncMode. Valid values for fifoClearSyncMode are:
SDFM_FIFO_NOT_CLEARED_ON_SYNC - FIFO is not cleared on sync.
SDFM_FIFO_CLEARED_ON_SYNC - FIFO is cleared on sync.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.fifoClearSyncMode: is the FIFO clear on sync mode.
- Return
None.
-
void
SDFM_setWaitForSyncClearMode(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_WaitForSyncClearMode syncClearMode)¶ Set Wait-for-sync clear mode.
This function sets the Wait-For-sync clear mode depending on the value of syncClearMode. Valid values for syncClearMode are:
SDFM_MANUAL_CLEAR_WAIT_FOR_SYNC - Wait-for-sync flag is cleared by invoking SDFM_clearWaitForSyncFlag().
SDFM_AUTO_CLEAR_WAIT_FOR_SYNC - Wait-for-sync flag is cleared automatically on FIFO interrupt.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.syncClearMode: is the wait-for-sync clear mode.
- Return
None.
-
void
SDFM_selectClockSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_ClockSource clkSource)¶ Selects clock source for SDFM channels.
This function selects the clock for SDFM module filter channels. Valid values for clkSource are:
SDFM_CLK_SOURCE_CHANNEL_CLK - Respective channel’s clk is the source
SDFM_CLK_SOURCE_SD1_CLK - Filter 1 clock is the source
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.clkSource: is the clock source
- Return
None.
-
void
SDFM_enableSynchronizer(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t syncConfig)¶ Enables Input Synchronizer.
This function enables either data or clock or both synchronizer. Valid values for syncConfig can be the logical OR of any of the values:
SDFM_CLOCK_SYNCHRONIZER - Enable SDFM input clock synchronizer
SDFM_DATA_SYNCHRONIZER - Enable SDFM input data synchronizer
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.syncConfig: defines which synchronizer to be enabled
- Return
None.
-
void
SDFM_disableSynchronizer(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t syncConfig)¶ Disables Input Synchronizer.
This function disables either data or clock or both synchronizer. Valid values for syncConfig can be the logical OR of any of the values:
SDFM_CLOCK_SYNCHRONIZER - Disable SDFM input clock synchronizer
SDFM_DATA_SYNCHRONIZER - Disable SDFM input data synchronizer
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.syncConfig: defines which synchronizer to be disabled
- Return
None.
-
void
SDFM_selectCompEventHighSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_CompEventHighSource source)¶ Selects comparator event high source.
This function selects the source for comparator event high. Valid values for source are:
SDFM_COMPHOUT_SOURCE_COMPHIN - Original COMPHIN/CEVT1 signal is source
SDFM_COMPHOUT_SOURCE_FILTER - Filtered COMPHIN/CEVT1 signal is source
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.source: is the comparator event high source
- Return
None.
-
void
SDFM_selectCompEventLowSource(uint32_t base, SDFM_FilterNumber filterNumber, SDFM_CompEventLowSource source)¶ Selects comparator event low source.
This function selects the source for comparator event low. Valid values for source are:
SDFM_COMPLOUT_SOURCE_COMPLIN - Original COMPLIN/CEVT2 signal is source
SDFM_COMPHOUT_SOURCE_FILTER - Filtered COMPLIN/CEVT2 signal is source
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.source: is the comparator event low source
- Return
None.
-
void
SDFM_initCompEventLowFilter(uint32_t base, SDFM_FilterNumber filterNumber)¶ Initializes Comparator Event Low Filter.
This function initializes Comparator Event Low Filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_initCompEventHighFilter(uint32_t base, SDFM_FilterNumber filterNumber)¶ Initializes Comparator Event High Filter.
This function initializes Comparator Event High Filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.
- Return
None.
-
void
SDFM_lockCompEventFilterConfig(uint32_t base, SDFM_FilterNumber filterNumber, uint16_t lockConfig)¶ Lock Comparator Event Filter Configurations
This function locks the comparator event filter configurations. Valid values of the lockConfig can be logical OR of any of the following values:
SDFM_SDCOMPLOCK_SDCOMPCTL - Locks write access to SDCOMPCTL register
SDFM_SDCOMPLOCK_COMP - Locks write access to SDCOMPxFILCTL & SDCOMPxFILCLKCTL register
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.lockConfig: defines the configurations to be locked
- Return
None.
-
void
SDFM_configComparator(uint32_t base, uint16_t config1, uint32_t config2, uint16_t config3)¶ Configures SDFM comparator for filter config & threshold values
This function configures the comparator filter for filter config and threshold values based on provided inputs.
- Parameters
base: is the base address of the SDFM moduleconfig1: is the filter number, filter type and over sampling ratio.config2: is high-level and low-level threshold 1 values.config3: is the zero-cross threshold value.
The config1 parameter is the logical OR of the filter number, filter type and oversampling ratio. The bit definitions for config1 are as follow:
config1.[3:0] filter number
config1.[7:4] filter type
config1.[15:8] Over sampling Ratio Valid values for filter number and filter type are defined in SDFM_FilterNumber and SDFM_FilterType enumerations respectively. SDFM_SET_OSR(X) macro can be used to set the value of the oversampling ratio ,which ranges [1,32] inclusive, in the appropriate bit location. For example the value (SDFM_FILTER_1 | SDFM_FILTER_SINC_2 | SDFM_SET_OSR(16)) will select Filter 1, SINC 2 type with an oversampling ratio of 16.
The config2 parameter is the logical OR of the filter high and low threshold 1 values. The bit definitions for config2 are as follow:
config2.[15:0] low threshold 1
config2.[31:16] high threshold 1 The upper 16 bits define the high threshold 1 and the lower 16 bits define the low threshold 1. SDFM_THRESHOLD(H,L) can be used to combine the high and low thresholds. The config3 parameter is the logical OR of the zero cross threshold enable flag and the zero-cross threshold value. The bit definitions for config3 are as follow:
config3.[15] - Enable or disable zero cross threshold. Valid values are 1 or 0 to enable or disable the zero cross threshold respectively. -config3.[14:0] - Zero Cross Threshold value. The SDFM_SET_ZERO_CROSS_THRESH_VALUE(X) macro can be used to specify the zero-cross threshold value and OR the 1 to enable it.
- Return
None.
-
void
SDFM_configEnhancedComparator(uint32_t base, uint16_t filterConfig, uint32_t highLowThreshold1, uint32_t highLowThreshold2, uint16_t zeroCrossThreshold)¶ Configure SDFM enhanced comparator for filter config & threshold values
This function configures the comparator filter for filter config and threshold values based on input parameters.
- Parameters
base: is the base address of the SDFM modulefilterConfig: is the filter number, filter type & over sampling ratio.highLowThreshold1: is high-level and low-level threshold 1 values.highLowThreshold2: is high-level and low-level threshold 2 values.zeroCrossThreshold: is the zero-cross threshold value.
The filterConfig parameter is the logical OR of the filter number, filter type and oversampling ratio. The bit definitions for filterConfig are as follow:
filterConfig.[3:0] filter number
filterConfig.[7:4] filter type
filterConfig.[15:8] Over sampling Ratio Valid values for filter number and filter type are defined in SDFM_FilterNumber and SDFM_FilterType enumerations respectively. SDFM_SET_OSR(X) macro can be used to set the value of the oversampling ratio ,which ranges [1,32] inclusive, in the appropriate bit location. For example the value (SDFM_FILTER_1 | SDFM_FILTER_SINC_2 | SDFM_SET_OSR(16)) will select Filter 1, SINC 2 type with an oversampling ratio of 16.
The highLowThreshold1 parameter is the logical OR of the filter high & low threshold 1 values. The bit definitions for highLowThreshold1 are as follow:
highLowThreshold1.[15:0] low threshold 1
highLowThreshold1.[31:16] high threshold 1 The upper 16 bits define the high threshold and the lower 16 bits define the low threshold. SDFM_THRESHOLD(H,L) can be used to combine the high and low thresholds.
The highLowThreshold2 parameter is the logical OR of the filter high & low threshold 2 values. The bit definitions for highLowThreshold2 are as follow:
highLowThreshold2.[15:0] low threshold 2
highLowThreshold2.[31:16] high threshold 2 The upper 16 bits define the high threshold and the lower 16 bits define the low threshold. SDFM_THRESHOLD(H,L) can be used to combine the high & low thresholds.
The zeroCrossThreshold parameter is the logical OR of the zero cross threshold enable flag and the zero-cross threshold value. The bit definitions for zeroCrossThreshold are as follows:
zeroCrossThreshold.[15] - Enable or disable zero cross threshold. Valid values are 1 or 0 to enable or disable the zero cross threshold respectively.
zeroCrossThreshold.[14:0] - Zero Cross Threshold value. The SDFM_SET_ZERO_CROSS_THRESH_VALUE(X) macro can be used as parameter zeroCrossThreshold to enable & specify the zero-cross threshold value.
- Return
None.
-
void
SDFM_configDataFilter(uint32_t base, uint16_t config1, uint16_t config2)¶ Configure SDFM data filter
This function configures the data filter based on configurations config1 and config2.
- Parameters
base: is the base address of the SDFM moduleconfig1: is the filter number, filter type and over sampling ratio configuration.config2: is filter switch, data representation and data shift values configuration.
The config1 parameter is the logical OR of the filter number, filter type and oversampling ratio. The bit definitions for config1 are as follow:
config1.[3:0] Filter number
config1.[7:4] Filter type
config1.[15:8] Over sampling Ratio Valid values for filter number and filter type are defined in SDFM_FilterNumber and SDFM_FilterType enumerations respectively. SDFM_SET_OSR(X) macro can be used to set the value of the oversampling ratio , which ranges [1,256] inclusive , in the appropriate bit location for config1. For example the value (SDFM_FILTER_2 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(64)) will select Filter 2 , SINC 3 type with an oversampling ratio of 64.
The config2 parameter is the logical OR of data representation, filter switch, and data shift values The bit definitions for config2 are as follow:
config2.[0] Data representation
config2.[1] Filter switch
config2.[15:2] Shift values Valid values for data representation are given in SDFM_OutputDataFormat enumeration. SDFM_FILTER_DISABLE or SDFM_FILTER_ENABLE will define the filter switch values.SDFM_SHIFT_VALUE(X) macro can be used to set the value of the data shift value,which ranges [0,31] inclusive, in the appropriate bit location for config2. The shift value is valid only in SDFM_DATA_FORMAT_16_BIT data representation format.
- Return
None.
-
void
SDFM_configZeroCrossComparator(uint32_t base, uint16_t config1, uint16_t config2)¶ Configure SDFM comparator Zero Cross threshold
This function configures the comparator filter zero cross threshold values based on configurations config1 and config2.
- Parameters
base: is the base address of the SDFM moduleconfig1: is the filter number, filter type and over sampling ratio.config2: is the zero cross threshold value.
The config1 parameter is the logical OR of the filter number, filter type and oversampling ratio. The bit definitions for config1 are as follow:
config1.[3:0] filter number
config1.[7:4] filter type
config1.[15:8] Over sampling Ratio Valid values for filter number and filter type are defined in SDFM_FilterNumber and SDFM_FilterType enumerations respectively. SDFM_SET_OSR(X) macro can be used to set the value of the oversampling ratio ,which ranges [1,32] inclusive, in the appropriate bit location. For example the value (SDFM_FILTER_1 | SDFM_FILTER_SINC_2 | SDFM_SET_OSR(16)) will select Filter 1 , SINC 2 type with an oversampling ratio of 16.
The config2 parameter is the value of the zero cross threshold. The maximum acceptable value is 32767.
- Return
None.
-
void
SDFM_configDataFilterFIFO(uint32_t base, uint16_t config1, uint16_t config2)¶ Configure SDFM data filter FIFO
This function enables and configures the data filter FIFO based on configurations config1 and config2.
- Parameters
base: is the base address of the SDFM moduleconfig1: is the filter number, filter type and over sampling ratio configuration.config2: is filter switch, data representation and data shift values and FIFO level configuration.
The config1 parameter is the logical OR of the filter number, filter type and oversampling ratio. The bit definitions for config1 are as follow:
config1.[3:0] filter number
config1.[7:4] filter type
config1.[15:8] Over sampling Ratio Valid values for filter number and filter type are defined in SDFM_FilterNumber and SDFM_FilterType enumerations respectively. SDFM_SET_OSR(X) macro can be used to set the value of the oversampling ratio , which ranges [1,256] inclusive , in the appropriate bit location for config1. For example the value (SDFM_FILTER_2 | SDFM_FILTER_SINC_3 | SDFM_SET_OSR(64)) will select Filter 2 , SINC 3 type with an oversampling ratio of 64.
The config2 parameter is the logical OR of data representation, filter switch, data shift value, and FIFO level The bit definitions for config2 are as follow:
config2.[0] Data representation
config2.[1] filter switch.
config2.[6:2] shift values.
config2.[15:7] FIFO level Valid values for data representation are given in SDFM_OutputDataFormat enumeration. SDFM_FILTER_DISABLE or SDFM_FILTER_ENABLE will define the filter switch values.SDFM_SHIFT_VALUE(X) macro can be used to set the value of the data shift value,which ranges [0,31] inclusive, in the appropriate bit location for config2. The value of FIFO level ranges [1,16] inclusive. The macro SDFM_SET_FIFO_LEVEL(X) can be used to set the value of the FIFO level.
- Return
None.
-
void
SDFM_configCompEventLowFilter(uint32_t base, SDFM_FilterNumber filterNumber, const SDFM_CompEventFilterConfig *config)¶ Configure Comparator Event Low Filter
This function configures the sample window, threshold and clock prescale configurations for the comparator event low filter.
- Parameters
base: is the base address of the SDFM modulefilterNumber: is the filter number.config: is the comparator event low source
- Return
None.
-
void
SDFM_configCompEventHighFilter(uint32_t base, SDFM_FilterNumber filterNumber, const SDFM_CompEventFilterConfig *config)¶ Configure Comparator Event High Filter
This function configures the sample window, threshold and clock prescale configurations for the comparator event high filter.
- Parameters
base: is the base address of the SDFM module.filterNumber: is the filter number.config: is the comparator event high source
- Return
None.
-
struct
SDFM_CompEventFilterConfig¶ - #include <sdfm.h>
Values that can be passed to SDFM_configCompEventLowFilter() & SDFM_configCompEventHighFilter() as the filterNumber.
-
The code for this module is contained in driverlib/sdfm.c, with driverlib/sdfm.h containing the API declarations for use by applications.