HTTP/1.1 Client API.
More...
|
file | httpstd.c |
|
file | httpstd.h |
| Standard Definitions for HTTP Status Codes, Content Type and Fields.
|
|
|
void | HTTPCli_Params_init (HTTPCli_Params *params) |
| Initialize the HTTPCli Params structure to default values. More...
|
|
int | HTTPCli_initSockAddr (struct sockaddr *addr, const char *uri, int flags) |
| Initialize the socket address structure for the given URI. More...
|
|
void | HTTPCli_construct (HTTPCli_Struct *cli) |
| Create a new instance object in the provided structure. More...
|
|
HTTPCli_Handle | HTTPCli_create () |
| Allocate and initialize a new instance object and return its handle. More...
|
|
int | HTTPCli_connect (HTTPCli_Handle cli, const struct sockaddr *addr, int flags, const HTTPCli_Params *params) |
| Open a connection to an HTTP server. More...
|
|
void | HTTPCli_delete (HTTPCli_Handle *cli) |
| Destroy the HTTP client instance and free the previously allocated instance object. More...
|
|
void | HTTPCli_destruct (HTTPCli_Struct *cli) |
| Destroy the HTTP client instance. More...
|
|
void | HTTPCli_disconnect (HTTPCli_Handle cli) |
| Disconnect from the HTTP server and destroy the HTTP client instance. More...
|
|
HTTPCli_Field * | HTTPCli_setRequestFields (HTTPCli_Handle cli, const HTTPCli_Field *fields) |
| Set an array of header fields to be sent for every HTTP request. More...
|
|
char ** | HTTPCli_setResponseFields (HTTPCli_Handle cli, const char *fields[]) |
| Set the header fields to filter the response headers. More...
|
|
int | HTTPCli_sendRequest (HTTPCli_Handle cli, const char *method, const char *requestURI, bool moreFlag) |
| Make an HTTP 1.1 request to the HTTP server. More...
|
|
int | HTTPCli_sendField (HTTPCli_Handle cli, const char *name, const char *value, bool lastFlag) |
| Send an header field to the HTTP server. More...
|
|
int | HTTPCli_sendRequestBody (HTTPCli_Handle cli, const char *body, int len) |
| Send the request message body to the HTTP server. More...
|
|
int | HTTPCli_getResponseStatus (HTTPCli_Handle cli) |
| Process the response header from the HTTP server and return status. More...
|
|
int | HTTPCli_getResponseField (HTTPCli_Handle cli, char *value, int len, bool *moreFlag) |
| Process a response header from the HTTP server and return field. More...
|
|
int | HTTPCli_readResponseHeader (HTTPCli_Handle cli, char *header, int len, bool *moreFlag) |
| Read a response header from the HTTP server. More...
|
|
int | HTTPCli_readResponseBody (HTTPCli_Handle cli, char *body, int len, bool *moreFlag) |
| Read the parsed response body data from the HTTP server. More...
|
|
int | HTTPCli_readRawResponseBody (HTTPCli_Handle cli, char *body, int len) |
| Read the raw response message body from the HTTP server. More...
|
|
void | HTTPCli_setProxy (const struct sockaddr *addr) |
| Set the proxy address. More...
|
|
int | HTTPCli_getSocketError (HTTPCli_Handle cli) |
| Get the error code from the socket/TLS layer. More...
|
|
HTTP/1.1 Client API.
This module provides an HTTP client implementation of IETF standard for HTTP/1.1 - RFC 2616 and TLS support to interact with HTTP/1.1 servers.
Features
- Supports GET, POST, PUT, HEAD, OPTIONS, DELETE methods, request and response headers/bodies, and redirection response handling.
- Using this module, connections can be opened/closed to HTTP servers. Each connection is an instance which can be configured with a set of repeated requests/responses parameters so that they can be used across multiple transactions.
- For supporting small memory devices, the module has been specially designed with split request/response APIs which enables sending requests and responses in smaller chunks, and static memory based APIs to eliminate the need for dynamic memory allocations.
- Supports security features which include TLS and communication through proxy.
- Supports two types of programming models: synchronous and asynchronous modes. In the default synchronous mode, an application uses APIs to make a request to the server and blocks until the server responds. With asynchronous mode, a thread to handle the response is created which invokes callbacks registered with the module.
- Supports TI-RTOS NDK, SimpleLink WiFi and Linux networking stacks. At IP level supports both IPv4 and IPv6.
- Supports conditional compilation of the module to include/exclude some of the features mentioned above.
Limitations
- HTTP client on SimpleLink WiFi supports IPv4 only.
- HTTP servers sending response header field name > 24 bytes are skipped. This length is controlled by the 'MAX_FIELD_NAME_LEN' macro in 'httpcli.c'. Modify the macro and rebuild the library if needed.
Deprecated Macros
The macros HTTPCli_METHOD* and HTTPCli_FIELD_NAME* have been deprecated. Use HTTPStd_* macros.
For backward compatibility, the old macros can still be used if -Dti_net_http_HTTPCli__deprecated is added to the compile options.
Minimal HTTP Client library
A minimal flavor of the library without asynchronous callback support which includes status handling, content handling and redirection handling can be built. The default library has support for these features.
To rebuild the library, add "-DHTTPCli_LIBTYPE_MIN" to the compile line and rebuild. The same option has to be added on application compile line also.
See also
Examples
The basic flow of managing an HTTP client is shown in the pseudo codes below. For clarity, return values are ignored - in a real application, these should be checked for errors.
- HTTP GET Example
{ NULL, NULL }
};
char respFields[2] = {
NULL
};
do {
if (ret == 0) {
len = (int)strtoul(buf, NULL, 0);
}
while (len > 0) {
}
}
- HTTPS POST Example
{ NULL, NULL }
};
char respFields[2] = {
NULL
};
do {
if (ret == 0) {
len = (int)strtoul(buf, NULL, 0);
}
while (len > 0) {
}
}
§ HTTPCli_BUF_LEN
#define HTTPCli_BUF_LEN 128 |
Modify the HTTP client object's internal buffer length and rebuild the library if needed.
§ HTTPCli_RECV_BUFLEN
#define HTTPCli_RECV_BUFLEN 32 |
Minimum size required to hold content length string
§ HTTPCli_ESOCKETFAIL
#define HTTPCli_ESOCKETFAIL (-101) |
§ HTTPCli_ECONNECTFAIL
#define HTTPCli_ECONNECTFAIL (-102) |
§ HTTPCli_ESENDFAIL
#define HTTPCli_ESENDFAIL (-103) |
§ HTTPCli_ERECVFAIL
#define HTTPCli_ERECVFAIL (-104) |
§ HTTPCli_ETLSFAIL
#define HTTPCli_ETLSFAIL (-105) |
§ HTTPCli_EHOSTNAME
#define HTTPCli_EHOSTNAME (-106) |
Failed to resolve host name.
§ HTTPCli_ESENDBUFSMALL
#define HTTPCli_ESENDBUFSMALL (-107) |
Internal send buffer is not big enough.
Modify the SEND_BUFLEN macro in the httpcli.c and rebuild the library if needed.
§ HTTPCli_ERECVBUFSMALL
#define HTTPCli_ERECVBUFSMALL (-108) |
§ HTTPCli_EASYNCMODE
#define HTTPCli_EASYNCMODE (-109) |
§ HTTPCli_ETHREADFAIL
#define HTTPCli_ETHREADFAIL (-110) |
§ HTTPCli_EPROXYTUNNELFAIL
#define HTTPCli_EPROXYTUNNELFAIL (-111) |
Failed to create an HTTP tunnel through proxy.
§ HTTPCli_ERESPONSEINVALID
#define HTTPCli_ERESPONSEINVALID (-112) |
Response recieved from the server is not a valid HTTP/1.1 response.
§ HTTPCli_ECONTENTLENLARGE
#define HTTPCli_ECONTENTLENLARGE (-114) |
§ HTTPCli_EREDIRECTURILONG
#define HTTPCli_EREDIRECTURILONG (-115) |
Redirection URI returned is too long to be read into the buffer.
Modify the URI_BUFLEN macro in the httpcli.c and rebuild the library if needed.
§ HTTPCli_ECONTENTTYPELONG
#define HTTPCli_ECONTENTTYPELONG (-116) |
Content type returned is too long to be read into buffer.
§ HTTPCli_ENOCONTENTCALLBACK
#define HTTPCli_ENOCONTENTCALLBACK (-117) |
Received content type does not match any registered callback.
Modify the CONTENT_BUFLEN macro in the httpcli.c and rebuild the library if needed.
§ HTTPCli_ENOTCHUNKDATA
#define HTTPCli_ENOTCHUNKDATA (-118) |
Data is not of chunked type.
§ HTTPCli_EINPROGRESS
#define HTTPCli_EINPROGRESS (-119) |
Operation could not be completed. Try again.
§ HTTPCli_EINTERNALBUFSMALL
#define HTTPCli_EINTERNALBUFSMALL (-120) |
Internal instance buffer to send/recieve data is too small.
§ HTTPCli_ESETNOTIFYFAIL
#define HTTPCli_ESETNOTIFYFAIL (-121) |
Could not setup the notify callbacks.
§ HTTPCli_EURILENLONG
#define HTTPCli_EURILENLONG (-122) |
Input domain name length is too long to be read into buffer.
Modify the DOMAIN_BUFLEN macro in the httpcli.c and rebuild the library if needed.
§ HTTPCli_EHOSTFIELDNOTFOUND
#define HTTPCli_EHOSTFIELDNOTFOUND (-123) |
Request Field 'Host' is not found in the set array.
'Host' should be set in the 'fields' parameter of HTTPCli_setRequestFields(). This is used to set up an HTTP tunnel through proxy servers.
§ HTTPCli_TYPE_TLS
#define HTTPCli_TYPE_TLS (0x02) |
§ HTTPCli_TYPE_IPV6
#define HTTPCli_TYPE_IPV6 (0x04) |
§ HTTPCli_FIELD_ID_DUMMY
#define HTTPCli_FIELD_ID_DUMMY (-11) |
§ HTTPCli_FIELD_ID_END
#define HTTPCli_FIELD_ID_END (-12) |
§ HTTPCli_Field
HTTPCli request header field.
§ HTTPCli_StatusCallback
typedef void(* HTTPCli_StatusCallback) (void *cli, int status) |
HTTPCli callback function for status handling.
- Parameters
-
[in] | cli | Instance of the HTTP connection |
[in] | status | Response status code |
§ HTTPCli_StatusHandler
HTTPCli response status code handler type.
§ HTTPCli_ContentCallback
typedef int(* HTTPCli_ContentCallback) (void *cli, int status, char *body, int len, bool moreFlag) |
HTTPCli callback function for content handling.
- Parameters
-
[in] | cli | Instance of the HTTP connection |
[in] | status | Response status code |
[in] | body | Data from the response body |
[in] | len | Length of response body buffer |
[in] | moreFlag | Set if more response data is available |
- Returns
- 1 to continue or 0 to stop further processing.
§ HTTPCli_ContentHandler
HTTPCli content handler type.
§ HTTPCli_RedirectCallback
typedef void(* HTTPCli_RedirectCallback) (void *cli, int status, char *uri) |
HTTPCli callback function prototype for redirection handling.
- Parameters
-
[in] | cli | Instance of the HTTP connection |
[in] | status | Response status code |
[in] | uri | The new URI string |
§ HTTPCli_Struct
§ HTTPCli_Params
HTTPCli instance paramaters.
§ HTTPCli_Handle
§ HTTPCli_Params_init()
Initialize the HTTPCli Params structure to default values.
- Parameters
-
§ HTTPCli_initSockAddr()
int HTTPCli_initSockAddr |
( |
struct sockaddr * |
addr, |
|
|
const char * |
uri, |
|
|
int |
flags |
|
) |
| |
Initialize the socket address structure for the given URI.
The supported URI format is:
- [http[s]://]host_name[:port_number][/request_uri]
For cases where port is not provided, the default port number is set.
- Parameters
-
[out] | addr | Handle to the sockaddr structure |
[in] | uri | A null terminated URI string |
[in] | flags | Set HTTPCli_TYPE_IPV6 for IPv6 addresses. |
- Returns
- 0 on success or error code on failure.
§ HTTPCli_construct()
Create a new instance object in the provided structure.
- Parameters
-
[out] | cli | Instance of an HTTP client |
§ HTTPCli_create()
Allocate and initialize a new instance object and return its handle.
- Returns
- handle of the HTTP client instance on success or NULL on failure.
§ HTTPCli_connect()
Open a connection to an HTTP server.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | addr | IP address of the server. Can be NULL when proxy is set. |
[in] | flags | Reserved for future use |
[in] | params | Per-instance config params, or NULL for default values |
- Returns
- 0 on success or error code on failure.
§ HTTPCli_delete()
Destroy the HTTP client instance and free the previously allocated instance object.
- Parameters
-
[in] | cli | Pointer to the HTTP client instance |
§ HTTPCli_destruct()
Destroy the HTTP client instance.
- Parameters
-
[in] | cli | Instance of the HTTP client |
§ HTTPCli_disconnect()
Disconnect from the HTTP server and destroy the HTTP client instance.
- Parameters
-
[in] | cli | Instance of the HTTP client |
§ HTTPCli_setRequestFields()
Set an array of header fields to be sent for every HTTP request.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | fields | An array of HTTP request header fields terminated by an object with NULL fields, or NULL to get previously set array. |
- Returns
- previously set array
§ HTTPCli_setResponseFields()
char** HTTPCli_setResponseFields |
( |
HTTPCli_Handle |
cli, |
|
|
const char * |
fields[] |
|
) |
| |
Set the header fields to filter the response headers.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | fields | An array of HTTP response header field strings terminated by a NULL, or NULL to get previously set array. |
- Returns
- previously set array
§ HTTPCli_sendRequest()
int HTTPCli_sendRequest |
( |
HTTPCli_Handle |
cli, |
|
|
const char * |
method, |
|
|
const char * |
requestURI, |
|
|
bool |
moreFlag |
|
) |
| |
Make an HTTP 1.1 request to the HTTP server.
Sends an HTTP 1.1 request-line and the header fields from the user set array (see HTTPCli_setRequestFields()) to the server.
Additionally, more fields apart from the user set array of header fields can be sent to the server. To send more fields, set the moreFlag
when calling this function and then call HTTPCli_sendField() with more fields.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | method | HTTP 1.1 method (ex: HTTPStd_GET) |
[in] | requestURI | the path on the server to open and any CGI parameters |
[in] | moreFlag | Set this flag when more fields will sent to the server |
- Returns
- 0 on success or error code on failure
§ HTTPCli_sendField()
int HTTPCli_sendField |
( |
HTTPCli_Handle |
cli, |
|
|
const char * |
name, |
|
|
const char * |
value, |
|
|
bool |
lastFlag |
|
) |
| |
Send an header field to the HTTP server.
This is a complementary function to HTTPCli_sendRequest() when more header fields are to be sent to the server.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | name | HTTP 1.1 request header field (ex: HTTPStd_FIELD_NAME_HOST) |
[in] | value | HTTP 1.1 request header field value |
[in] | lastFlag | Set this flag when sending the last header field |
- Returns
- 0 on success or error code on failure
§ HTTPCli_sendRequestBody()
int HTTPCli_sendRequestBody |
( |
HTTPCli_Handle |
cli, |
|
|
const char * |
body, |
|
|
int |
len |
|
) |
| |
Send the request message body to the HTTP server.
Make a call to this function after HTTPCli_sendRequest() (always) and HTTPCli_sendField() (if applicable).
- Parameters
-
[in] | cli | Instance of an HTTP client |
[in] | body | Request body buffer |
[in] | len | Length of the request body buffer |
- Returns
- 0 on success or error code on failure
§ HTTPCli_getResponseStatus()
Process the response header from the HTTP server and return status.
- Parameters
-
[in] | cli | Instance of an HTTP client |
- Returns
- On success, status code from the server or error code on failure.
§ HTTPCli_getResponseField()
int HTTPCli_getResponseField |
( |
HTTPCli_Handle |
cli, |
|
|
char * |
value, |
|
|
int |
len, |
|
|
bool * |
moreFlag |
|
) |
| |
Process a response header from the HTTP server and return field.
Filters the response headers based on the array of fields (see HTTPCli_setResponseFields()).
Repeatedly call this function until HTTPCli_FIELD_ID_END is returned.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[out] | value | Field value string. |
[in] | len | Length of field value string |
[out] | moreFlag | Flag set if the field value could not be completely read into value . A subsequent call to this function will read the remaining field value into value and will return HTTPCli_FIELD_ID_DUMMY. |
- Returns
- On Success, the index of the field set in the HTTPCli_setResponseFields() or HTTPCli_FIELD_ID_END or HTTPCli_FIELD_ID_DUMMY, or error code on failure.
§ HTTPCli_readResponseHeader()
int HTTPCli_readResponseHeader |
( |
HTTPCli_Handle |
cli, |
|
|
char * |
header, |
|
|
int |
len, |
|
|
bool * |
moreFlag |
|
) |
| |
Read a response header from the HTTP server.
Repeatedly call this function until zero is returned.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[out] | header | Buffer to hold Response Header string |
[in] | len | Length of the buffer |
[out] | moreFlag | Flag set if the field value could not be completely read into header . A subsequent call to this function will read the remaining field value into header |
- Returns
- The number of characters read (including NULL character) on success or error code on failure
§ HTTPCli_readResponseBody()
int HTTPCli_readResponseBody |
( |
HTTPCli_Handle |
cli, |
|
|
char * |
body, |
|
|
int |
len, |
|
|
bool * |
moreFlag |
|
) |
| |
Read the parsed response body data from the HTTP server.
This function parses the response body if the content type is chunked transfer encoding or if the content length field is returned by the HTTP server.
Make a call to this function only after the call to HTTPCli_getResponseStatus() and HTTPCli_getResponseField().
- Parameters
-
[in] | cli | Instance of an HTTP client |
[out] | body | Response body buffer |
[in] | len | Length of response body buffer |
[out] | moreFlag | Set if more data is available |
- Returns
- The number of characters read on success or error code on failure
§ HTTPCli_readRawResponseBody()
int HTTPCli_readRawResponseBody |
( |
HTTPCli_Handle |
cli, |
|
|
char * |
body, |
|
|
int |
len |
|
) |
| |
Read the raw response message body from the HTTP server.
Make a call to this function only after the call to HTTPCli_getResponseStatus() and HTTPCli_getResponseField().
Repeatedly call this function until entire response message is read.
- Parameters
-
[in] | cli | Instance of an HTTP client |
[out] | body | Response body buffer |
[in] | len | Length of response body buffer |
- Returns
- The number of characters read on success or error code on failure
§ HTTPCli_setProxy()
void HTTPCli_setProxy |
( |
const struct sockaddr * |
addr | ) |
|
Set the proxy address.
- Parameters
-
[in] | addr | IP address of the proxy server |
§ HTTPCli_getSocketError()