Network Services API
1.40.00.04
|
#include <stdbool.h>
#include <ti/net/ssock.h>
#include <ti/net/tls.h>
#include <ti/net/http/httpstd.h>
Go to the source code of this file.
Data Structures | |
struct | HTTPCli_Field |
HTTPCli request header field. More... | |
struct | HTTPCli_StatusHandler |
HTTPCli response status code handler type. More... | |
struct | HTTPCli_ContentHandler |
HTTPCli content handler type. More... | |
struct | HTTPCli_Struct |
HTTPCli instance type. More... | |
struct | HTTPCli_Params |
HTTPCli instance paramaters. More... | |
Macros | |
#define | HTTPCli_BUF_LEN 128 |
#define | HTTPCli_RECV_BUFLEN 32 |
HTTP Client Error Codes | |
#define | HTTPCli_ESOCKETFAIL (-101) |
Socket create failed. More... | |
#define | HTTPCli_ECONNECTFAIL (-102) |
Cannot connect to the remote host. More... | |
#define | HTTPCli_ESENDFAIL (-103) |
Cannot send to the remote host. More... | |
#define | HTTPCli_ERECVFAIL (-104) |
Cannot recieve data from the remote host. More... | |
#define | HTTPCli_ETLSFAIL (-105) |
Failed to configure the socket with TLS parameters. More... | |
#define | HTTPCli_EHOSTNAME (-106) |
Failed to resolve host name. More... | |
#define | HTTPCli_ESENDBUFSMALL (-107) |
Internal send buffer is not big enough. More... | |
#define | HTTPCli_ERECVBUFSMALL (-108) |
Receive buffer is not big enough. More... | |
#define | HTTPCli_EASYNCMODE (-109) |
HTTPCli_getResponseStatus() should not be called in async mode More... | |
#define | HTTPCli_ETHREADFAIL (-110) |
Thread create failed. More... | |
#define | HTTPCli_EPROXYTUNNELFAIL (-111) |
Failed to create an HTTP tunnel through proxy. More... | |
#define | HTTPCli_ERESPONSEINVALID (-112) |
Response recieved from the server is not a valid HTTP/1.1 response. More... | |
#define | HTTPCli_ECONTENTLENLARGE (-114) |
Content length returned is too large. More... | |
#define | HTTPCli_EREDIRECTURILONG (-115) |
Redirection URI returned is too long to be read into the buffer. More... | |
#define | HTTPCli_ECONTENTTYPELONG (-116) |
Content type returned is too long to be read into buffer. More... | |
#define | HTTPCli_ENOCONTENTCALLBACK (-117) |
Received content type does not match any registered callback. More... | |
#define | HTTPCli_ENOTCHUNKDATA (-118) |
Data is not of chunked type. More... | |
#define | HTTPCli_EINPROGRESS (-119) |
Operation could not be completed. Try again. More... | |
#define | HTTPCli_EINTERNALBUFSMALL (-120) |
Internal instance buffer to send/recieve data is too small. More... | |
#define | HTTPCli_ESETNOTIFYFAIL (-121) |
Could not setup the notify callbacks. More... | |
#define | HTTPCli_EURILENLONG (-122) |
Input domain name length is too long to be read into buffer. More... | |
#define | HTTPCli_EHOSTFIELDNOTFOUND (-123) |
Request Field 'Host' is not found in the set array. More... | |
HTTP Client Configuration Types | |
#define | HTTPCli_TYPE_TLS (0x02) |
#define | HTTPCli_TYPE_IPV6 (0x04) |
HTTP Client Field ID | |
Special return codes for HTTPCli_getResponseField(). | |
#define | HTTPCli_FIELD_ID_DUMMY (-11) |
#define | HTTPCli_FIELD_ID_END (-12) |
Typedefs | |
typedef struct HTTPCli_Field | HTTPCli_Field |
HTTPCli request header field. More... | |
typedef void(* | HTTPCli_StatusCallback) (void *cli, int status) |
HTTPCli callback function for status handling. More... | |
typedef struct HTTPCli_StatusHandler | HTTPCli_StatusHandler |
HTTPCli response status code handler type. More... | |
typedef int(* | HTTPCli_ContentCallback) (void *cli, int status, char *body, int len, bool moreFlag) |
HTTPCli callback function for content handling. More... | |
typedef struct HTTPCli_ContentHandler | HTTPCli_ContentHandler |
HTTPCli content handler type. More... | |
typedef void(* | HTTPCli_RedirectCallback) (void *cli, int status, char *uri) |
HTTPCli callback function prototype for redirection handling. More... | |
typedef struct HTTPCli_Struct | HTTPCli_Struct |
HTTPCli instance type. More... | |
typedef struct HTTPCli_Params | HTTPCli_Params |
HTTPCli instance paramaters. More... | |
typedef HTTPCli_Struct * | HTTPCli_Handle |
Functions | |
void | HTTPCli_Params_init (HTTPCli_Params *params) |
Initialize the HTTPCli Params structure to default values. More... | |
int | HTTPCli_initSockAddr (struct sockaddr *addr, const char *uri, int flags) |
Initialize the socket address structure for the given URI. More... | |
void | HTTPCli_construct (HTTPCli_Struct *cli) |
Create a new instance object in the provided structure. More... | |
HTTPCli_Handle | HTTPCli_create () |
Allocate and initialize a new instance object and return its handle. More... | |
int | HTTPCli_connect (HTTPCli_Handle cli, const struct sockaddr *addr, int flags, const HTTPCli_Params *params) |
Open a connection to an HTTP server. More... | |
void | HTTPCli_delete (HTTPCli_Handle *cli) |
Destroy the HTTP client instance and free the previously allocated instance object. More... | |
void | HTTPCli_destruct (HTTPCli_Struct *cli) |
Destroy the HTTP client instance. More... | |
void | HTTPCli_disconnect (HTTPCli_Handle cli) |
Disconnect from the HTTP server and destroy the HTTP client instance. More... | |
HTTPCli_Field * | HTTPCli_setRequestFields (HTTPCli_Handle cli, const HTTPCli_Field *fields) |
Set an array of header fields to be sent for every HTTP request. More... | |
char ** | HTTPCli_setResponseFields (HTTPCli_Handle cli, const char *fields[]) |
Set the header fields to filter the response headers. More... | |
int | HTTPCli_sendRequest (HTTPCli_Handle cli, const char *method, const char *requestURI, bool moreFlag) |
Make an HTTP 1.1 request to the HTTP server. More... | |
int | HTTPCli_sendField (HTTPCli_Handle cli, const char *name, const char *value, bool lastFlag) |
Send an header field to the HTTP server. More... | |
int | HTTPCli_sendRequestBody (HTTPCli_Handle cli, const char *body, int len) |
Send the request message body to the HTTP server. More... | |
int | HTTPCli_getResponseStatus (HTTPCli_Handle cli) |
Process the response header from the HTTP server and return status. More... | |
int | HTTPCli_getResponseField (HTTPCli_Handle cli, char *value, int len, bool *moreFlag) |
Process a response header from the HTTP server and return field. More... | |
int | HTTPCli_readResponseHeader (HTTPCli_Handle cli, char *header, int len, bool *moreFlag) |
Read a response header from the HTTP server. More... | |
int | HTTPCli_readResponseBody (HTTPCli_Handle cli, char *body, int len, bool *moreFlag) |
Read the parsed response body data from the HTTP server. More... | |
int | HTTPCli_readRawResponseBody (HTTPCli_Handle cli, char *body, int len) |
Read the raw response message body from the HTTP server. More... | |
void | HTTPCli_setProxy (const struct sockaddr *addr) |
Set the proxy address. More... | |
int | HTTPCli_getSocketError (HTTPCli_Handle cli) |
Get the error code from the socket/TLS layer. More... | |