SimpleLink MCU SDK Driver APIs
tidrivers_msp43x_3_01_01_03
|
MSP432 specfic extension to ADCBuf_Params. More...
#include <ADCBufMSP432.h>
Data Fields | |
ADCBufMSP432_Sampling_Duration | samplingDuration |
MSP432 specfic extension to ADCBuf_Params.
To use non-default MSP432 specific parameters when calling ADCBuf_open(), a pointer to an instance of this struct must be specified in ADCBuf_Params::custom. Alternatively, these values can be set using the control function after calling ADCBuf_open().
ADCBufMSP432_Sampling_Duration ADCBufMSP432_ParamsExtension::samplingDuration |