66 #ifndef ti_drivers_watchdog_WatchdogMSP432__include
67 #define ti_drivers_watchdog_WatchdogMSP432__include
78 #include <ti/drivers/dpl/HwiP.h>
uint8_t clockSource
Definition: WatchdogMSP432.h:144
struct WatchdogMSP432_Object WatchdogMSP432_Object
Watchdog Object for MSP432.
enum Watchdog_ResetMode_ Watchdog_ResetMode
Watchdog reset mode settings.
uint8_t intPriority
Definition: WatchdogMSP432.h:143
bool isOpen
Definition: WatchdogMSP432.h:156
HwiP_Handle hwiHandle
Definition: WatchdogMSP432.h:155
Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be...
Definition: WatchdogMSP432.h:140
Watchdog driver interface.
uint8_t clockDivider
Definition: WatchdogMSP432.h:145
const Watchdog_FxnTable WatchdogMSP432_fxnTable
Watchdog function table for MSP432.
uint32_t baseAddr
Definition: WatchdogMSP432.h:141
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:346
uint8_t intNum
Definition: WatchdogMSP432.h:142
Watchdog_ResetMode resetMode
Definition: WatchdogMSP432.h:154
struct WatchdogMSP432_HWAttrs WatchdogMSP432_HWAttrs
Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be...
Watchdog Object for MSP432.
Definition: WatchdogMSP432.h:153