Debugging

External Resources

Debug Interfaces

The CC2640R2F platform supports the cJTAG (2-wire) and JTAG (4-wire) interfaces. Any debuggers that support cJTAG, like the TI XDS100v3 and XDS200, work natively. Others interfaces, like the IAR I-Jet and Segger J-Link, can only be used in JTAG mode but their drivers inject a cJTAG sequence which enables JTAG mode when connecting. The hardware resources included on the devices for debugging are listed as follows. Not all debugging functionality is available in all combinations of debugger and IDE.

  • Breakpoint unit (FBP) – 6 instruction comparators, 2 literal comparators
  • Data watchpoint unit (DWT) – 4 watchpoints on memory access
  • Instrumentation Trace Module (ITM) – 32 × 32 bit stimulus registers
  • Trace Port Interface Unit (TPIU) – serialization and time-stamping of DWT and ITM events

The SmartRF06 Board contains a XDS100v3 debug probe, and the CC2650 LaunchPad contains the XDS110 debug probe. These debuggers are used by default in the respective sample projects.

Connecting to the XDS Debugger

If only one debugger is attached, the IDE uses it automatically when you click the img_icon_debug_ccs button in CCS or img_icon_debug_iar in IAR.

If multiple debuggers are connected, you must choose the individual debugger to use. The following steps detail how to select a debugger in CCS and IAR.

Configuring Debugger in CCS

To select a specific debugger in CCS, do as follows:

Find Serial Number

To find the serial number for XDS100v3 debuggers, do as follows.

  1. Open a command prompt.
  2. Run C:\ti\ccsv6\ccs_base\common\uscif\xds100serial.exe to get a list of serial numbers of the connected debuggers.

For XDS110 debuggers (Launchpads), run the following command: c:\ti\ccsv6\ccs_base\common\uscif\xds110\xdsdfu.exe -e

Configure serial number

  1. Open the target configuration file.
../_images/ccs_targetconfig_file.png
  1. Open the Advanced pane.
 
  1. Choose the top-level debugger entry.
../_images/ccs_targetconfig_probe.png
  1. Enter the serial number.
../_images/ccs_targetconfig_serial.png

Configuring Debugger in IAR

To debug using IAR, do as follows.

  1. Open the project options (Project -> Options)
  2. Go to the Debugger entry.
  3. Go to Extra options.
  4. Add the following command line option: --drv\_communication=USB:#select

Adding this command line option makes the IAR prompt which debugger to use for every connection.

Breakpoints

Both IAR and CCS reserve one of the instruction comparators for stepping etc. Five hardware breakpoints are available for debugging. This section describes setting breakpoints in IAR and CCS.

Breakpoints in CCS

To toggle a breakpoint, do any of the following.

  • Double-click the area to the left of the line number.
  • Press Ctrl+Shift+B.
  • Right-click on the line.

A breakpoint set on line 207 looks like the following.

../_images/ccs_breakpoint_ex.png

Figure 95. Breakpoint on line 207. Debugger halted at start of main().

For an overview of the active and inactive breakpoints, click on View –> Breakpoints.

../_images/ccs_breakpoint_list.png

Figure 96. List of breakpoints. Right-click to edit options, or de-select to deactivate.

To set a conditional break, do as follows.

  1. Right-click the breakpoint in the overview.
  2. Choose Properties.

When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.

Note

Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.

Breakpoints in IAR

To toggle a breakpoint, do any of the following.

  • Single-click the area to the left of the line number.
  • Go to the line and press F9 to toggle breakpoint
  • Right-click on the line and select Toggle Breakpoint (Code).

A breakpoint looks like this:

../_images/iar_breakpoint_ex.png

Figure 97. Breakpoint on PIN_init(). Debugger halted at start of main().

For an overview of the active and inactive breakpoints, click View –> Breakpoints.

../_images/iar_breakpoint_list.png

Figure 98. List of breakpoints. Right-click to edit options, or de-select to deactivate.

To set a conditional break, do as follows.

  1. Right-click the breakpoint in the overview.
  2. Choose Edit....

When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.

Note

Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.

Considerations on Breakpoints

Breakpoints and Timing

Synchronous RF protocols like the Bluetooth low energy protocol are timing sensitive, and breakpoints can easily halt the execution long enough to lose network timing and break the link.

To still be able to debug, place breakpoints as close as possible to where the relevant debug information can be read or step through the relevant code segment to debug.

After you hit a breakpoint and read out the necessary debug information, it is recommended that you reset the device and re-establish the connection.

Breakpoints and Optimization

When compiler optimizations are enabled, toggling a breakpoint on a line of C code may not result in the expected behavior. Some examples include the following.

Code is removed or not compiled in
Toggling a breakpoint in the IDE results in a breakpoint some other unintended place and not on the selected line. Some IDEs disable breakpoints on nonexisting code.
Code block is part of a common subexpression
For example, a breakpoint might toggle inside a function called from one other function, but can also break due to a call from another unintended function.
An if clause is represented by a conditional branch in assembly
A breakpoint inside an if clause always breaks on the conditional statement, even if not executed.

TI recommends selecting an optimization level as low as possible when debugging. See Optimizations for information on modifying optimization levels.

Watching Variables and Registers

IAR and CCS provide several ways of viewing the state of a halted program. Global variables are statically placed during link-time and can end up anywhere in the RAM available to the project or potentially in flash if they are declared as a constant value. These variables can be accessed at any time through the Watch and Expression windows.

Unless removed due to optimizations, global variables are always available in these views. Local variables or variables that are only valid inside a limited scope are placed on the stack of the active task. Such variables can also be viewed with the Watch or Expression views, but can also be automatically displayed when breaking or stepping through code. To view the variables through IAR and CCS, do as follows.

Variables in CCS

You can view Global Variables by doing either of the following.

  • Select View –> Expressions
  • Select a variable name in code.
    • Right-click and select Add Watch Expression.
../_images/ccs_watch.png

Figure 99. Variable watch window. Note that you can cast values, get address and sizeof, etc.

  • Select View –> Variables to auto-variables that are present at the current location when stepping through code.
../_images/ccs_locals.png

Figure 100. Local variables. This screenshot is taken during execution of the Simple Peripheral init function.

Variables in IAR

To view Global Variables, do either of the following.

  • Right-click on the variable.
    • Select Add to Watch: varName.
  • Select View –> Watch n
    • Enter the name of the variable.
../_images/iar_watch.png

Figure 101. Variable watch window. Note that you can cast values, get address and sizeof, etc.

View –> Locals show the local variables in IAR.

../_images/iar_locals.png

Figure 102. Local variables. This screenshot is taken during execution of the Simple Peripheral init function.

Considerations When Viewing Variables

Local variables are often placed in CPU registers and not on the stack. These variables also have a limited lifetime even within the scope in which they are valid, depending on the optimization performed. Both CCS and IAR may struggle to show a particular variable due to its limited lifetime. The solution when debugging is as follows.

  • Move the variable to global scope, so it remains accessible in RAM.
  • Make the variable volatile, so the compiler doesn’t place the value in a register.
  • Make a shadow copy of the variable that is global and volatile.

IAR may remove the variable during optimization and inline the usage of the value. If so, add the __root directive in front.

Memory Watchpoints

As mentioned in Chapter 9. the DWT module contains four memory watchpoints that allow breakpoints on memory access. The hardware match functionality looks only at the address. If intended for use on a variable, the variable must be global. Using watchpoints is described for IAR and CCS as follows.

Note

If a data watchpoint with value match is used, two of the four watchpoints are used.

Watchpoints in CCS

  1. Right-click on a global variable.
  2. Select Breakpoint –> Hardware Watchpoint
  3. Go to the list of breakpoints (View –> Breakpoints)
  4. Right-click and edit the Breakpoint Properties to configure the watchpoint.
../_images/ccs_watchpoint_add.png

Figure 103. Adding a watchpoint on a variable.

This example configuration ensures that if 0x42 is written to the memory location for Characteristic 1 in the Bluetooth low energy simple_peripheral example project the device halts execution.

../_images/ccs_watchpoint_configure.png

Figure 104. Configuring a hardware watchpoint to break on 8-bit write with value 0x42.

Watchpoints in IAR

  1. Right-click a variable (global).
  2. Select Set Data Breakpoint for 'myVar' to add it to the active breakpoints.
  3. Go to the list of breakpoints (View –> Breakpoints)
  4. Choose Edit... to set up whether the watchpoint should match on read, write, or any access.
../_images/iar_watchpoint_configure.png

Figure 105. Configuring a hardware watchpoint to break on 8-bit write with value 0x42.

TI-RTOS Object Viewer

Both IAR and CCS include the RTOS Object Viewer (ROV) plug-in that provides insight into the current state of TI-RTOS, including task states, stacks, and so forth. Because both CCS and IAR have a similar interface, these examples discuss only CCS.

To access the ROV in IAR:

  • Use the TI-RTOS menu on the menu bar.
  • Select a subview.

To access the ROV in CCS:

  • Click the Tools menu.
  • Click RTOS Object View (ROV).

This section discusses some ROV views useful for debugging and profiling. More details can be found in the TI-RTOS User’s Guide, including documentation on how to add log events to application code.

Scanning the BIOS for Errors

The BIOS Scan for errors view goes through the available ROV modules and reports on errors. This functionality can be a good point to start if anything has gone wrong. This scan only shows errors related to TI-RTOS modules and only the errors it can catch.

../_images/rov_bios_scan.png

Figure 106. Scan for errors. Here a Task Stack has been overrun.

Viewing the State of Each Task

The Task Detailed view is useful for seeing the state of each task and its related runtime stack usage. This example shows the state the first time the user-thread is called. Figure 107. shows the Bluetooth low energy stack task, represented by its ICall proxy, the Idle task, the simple_peripheral task and the GAPRole task.

../_images/rov_task_detailed.png

Figure 107. Detailed view of the Tasks. Notice the address of the overrun task matches the instance id from Scan for errors.

The following list explains the column in Figure 107.

address
This column shows the memory location of the Task_Struct instance for each task.
priority
This column shows the TI-RTOS priority for the task.
mode
This column shows the current state of the task.
fxn
This column shows the name of the entry function of the task.
arg0, arg1
These columns show abitrary values that can be given to entry function of the task. In the image, the ICall_taskEntry is given 0xb001, which is the flash location of the entry function of the RF stack image and 0x20003a30 (the location of bleUserCfg_t user0Cfg, defined in main()).
stackPeak
This column shows the maximum run-time stack memory used based on watermark in RAM, where the stacks are prefilled with 0xBE and there is a sentinel word at the end of the run-time stack.

Note

Function calls may push the stack pointer out of the run-time stack, but not actually write to the entire area. A stack peak near stackSize but not exceeding it may indicate stack overflow.

stackSize
This column shows the size of the runtime stack, configured when instantiating a task.
stackBase
This column shows the logical top of the runtime stack of the task (usage starts at stackBase + stackSize and grows down to this address).

Viewing the System Stack

The Hwi –> Module view allows profiling of the system stack used during boot or for main(), Hwi execution, and SWI execution. See System Stack for more information on the system stack.

../_images/rov_hwi_module.png

Figure 108. Viewing the System Stack in Hwi

The hwiStackPeak, hwiStackSize, and hwiStackBase can be used to check for system stack overflow.

Using the Memory Browser

Both IAR and CCS are able to show a representation of the memory on the device. In CCS you can index by address or by symbol name. As an example, consider the stack that was overrun in Figure 107.:

Simple Peripheral Task’s stack. Note BE watermark GAPRole Task’s stack. Note it’s completely filled.
../_images/mem_browser_sbp_stack.png
../_images/mem_browser_gaprole_stack.png

The solution in this case would be to increase the stack size for the failing task, and see what the stack peak really is. The stackPeak reported is relying on how many watermark bytes are overwritten, so it can’t know how much the overrun amounts to.

Because stacks are utilized from higher addresses towards lower addressed (upwards in the picture), stacks that overrun will tend to overwrite data at locations immediately before the stack.

Profiling the ICall Heap Manager (heapmgr.h)

As described in Dynamic Memory Allocation, the ICall Heap Manager and its heap are used to allocate messages between the Bluetooth low energy stack task and the application task and as dynamic memory allocations in the tasks.

Profiling functionality is provided for the ICall heap but is not enabled by default. Therefore, it must be compiled in by adding HEAPMGR_METRICS to the defined preprocessor symbols. This functionality is useful for finding potential sources for unexplained behavior and to optimize the size of the heap. When HEAPMGR_METRICS is defined, the variables and functions listed as follows become available. Global variables:

heapmgrBlkMax
The maximum amount of simultaneous allocated blocks
heapmgrBlkCnt
The current amount of allocated blocks
heapmgrBlkFree
The current amount of free blocks
heapmgrMemAlo
The current total memory allocated in bytes
heapmgrMemMax
The maximum amount of simultaneous allocated memory in blocks (this value must not exceed the size of the heap)
heapmgrMemUb
The furthest memory location of an allocated block, measured as an offset from the start of the heap
heapmgrMemFail
The amount of memory allocation failure (instances where ICall_malloc() has returned NULL)

Functions

void ICall_heapGetMetrics(u16 *pBlkMax, u16 *pBlkCnt, u16 *pBlkFree, u16 *pMemAlo, u16 *pMemMax, u16 *pMemUb)
Returns the previously described variables in the pointers passed in as parameters
int heapmgrSanityCheck(void)
Returns 0 if the heap is ok; otherwise, returns a nonzero (that is, an array access has overwritten a header in the heap)

Determining the Auto Heap Size

The following procedure can be used to view the size of the ICall heap when the auto heap size feature is enabled (HEAPMGR_SIZE=0).

At runtime, view the value of the global memory symbol HEAPMGR_SIZE after ICall_init() has been executed in main(). The value of HEAPMGR_SIZE is the total size of the ICall heap. See HEAPMGR_INIT() in heapmgr.h for the source code implementation.

  • In IAR: View -> Watch -> Watch 1, add HEAPMGR_SIZE
  • In CCS Debug Session: View -> Expressions, add HEAPMGR_SIZE

Note

The auto heap size feature does not determine the amount of heap needed for the application. The system designer must ensure that the heap has the required space to meet the application’s runtime memory requirements.

Due to memory placement, the actual heap size may be up to 4 bytes less.

To calculate the size of the ICall heap by inspecting the application map file in IAR:

The size of the ICall heap is the difference between the address of the last item in the .bss section and the start address of the system stack (CSTACK). For example, the simple_peripheral\cc2650lp\app.map file, at the end of the PLACEMENT SUMMARY:

Listing 67. The gap between .bss end and CSTACK start is used for ICall heap.
      .bss                  zero     0x20001cf8     0x2  app_ble_prm3.orm3 [2]
      .bss                  zero     0x20001cfa     0x1  TRNGCC26XX.o [1]
      .bss                  zero     0x20001cfb     0x1  driverlib_release.o [8]
                                   - 0x20001cfc  0x1af4

  "A3":                                           0x400
    CSTACK                           0x20003f50   0x400  <Block>
      CSTACK                uninit   0x20003f50   0x400  <Block tail>
                                   - 0x20004350   0x400

The size of the ICall heap in this example is the address of the start of CSTACK minus the address of the last item in .bss: 0x20003f50 - 0x20001cfc = 0x2254 or 8788 bytes for the heap.

To calculate the size of the ICall heap by inspecting the application map file in CCS:

The size of the heap is determined by the heapStart and heapEnd global symbol addresses which are emitted by the linker. For example, the simple_peripheral_cc2650lp_app.map file:

Listing 68. The gap between heapStart end and heapEnd start is used for ICall heap in CCS.
20003f48  heapEnd
20001cc1  heapStart

The size of the ICall heap in this example is defined as: 0x20003f48 - 0x20001cc1 = 0x2287 or 8839 bytes for the heap.

Optimizations

While debugging, turn off or lower optimizations to ease single-stepping through code. Optimization level can be configured at the project, file and function levels.

Project-Wide Optimizations

For debugging, ideally, the project-wide settings for optimization should be as low as possible. There may not be enough available space on the target to do this, but lowering just a couple of levels can be helpful.

In IAR

Project Options –> C/C++ Compiler –> Optimizations

../_images/iar_optim_level_project.png

Figure 109. Project-level optimization setting in IAR

In CCS

Project Properties –> CCS Build –> ARM Compiler –> Optimization

../_images/ccs_optim_level_project.png

Figure 110. Project-level optimization setting in CCS

Single-File Optimizations

Note

Do single-file optimizations with care because this also overrides the project-wide preprocessor symbols.

In IAR

  1. Right-click on the file in the Workspace pane.
  2. Choose Options.
  3. Check Override inherited Settings.
  4. Choose the optimization level.

In CCS

  1. Right-click on the file in the Workspace pane.
  2. Choose Properties.
  3. Change the optimization level of the file using the same menu in the CCS project-wide optimization menu.

Single-Function Optimizations

Using compiler directives, you can control the optimization level of a single function.

In IAR

Use #pragma optimize=none before the function definition to deoptimize the entire function, that is, as follows.

Listing 69. Function-level optimization setting in IAR
#pragma optimize=none
static void myFunction(int number)
{
  // ...
  return yourFunction(other_number);
}

In CCS

Listing 70. Function-level optimization setting in CCS
#pragma FUNCTION_OPTIONS(myFunction, "--opt_level=0")
static void myFunction(int number)
{
  // ...
  return yourFunction(other_number);
}

Loading TI-RTOS in ROM Symbols

Some of the TI-RTOS kernel modules are included in ROM, and executed from ROM in order to save Flash space for the application. This can lead to some confusion, when only addresses are shown in the disassembly view and the call-stack view.

All TI-RTOS kernel code in ROM starts with address 0x1001xxxx. In order to make sense of the ROM’ed code, you need to include the symbol files in your debug session.

In IAR

../_images/rtos_symbols_add_iar.png

Figure 111. Adding symbol information for the BIOS kernel in ROM

  • In the project options, go to Debugger and Images, then add the image
  • <SDK\_INSTALL\_DIR>\kernel\tirtos\packages\ti\sysbios\rom\cortexm\cc26xx\r2\golden\CC26xx\rtos_rom.xem3
  • Check the box for ‘Debug info only’, and use Offset = 0.

In CCS

../_images/rtos_symbols_add_ccs.png

Figure 112. Adding symbol information for the BIOS kernel in ROM, via Add Symbols.

  • While in debug mode, click the drop-down button next to the Load Program icon
  • Select Add Symbols..
  • Select Browse.. and find
  • <SDK\_INSTALL\_DIR>\kernel\tirtos\packages\ti\sysbios\rom\cortexm\cc26xx\r2\golden\CC26xx\rtos_rom.xem3

Deciphering CPU Exceptions

Several possible exception causes exist. If an exception is caught, an exception handler function can be called. Depending on the project settings, this handler may be a default handler in ROM, which is just an infinite loop or a custom function called from this default handler instead of a loop.

When an exception occurs, the exception may be caught and halted in debug mode immediately, depending on the debugger. If the execution halted manually later through the Break debugger, it is then stopped within the exception handler loop.

Exception Cause

With the default setup using TI-RTOS, the exception cause can be found in the System Control Space register group (CPU_SCS) in the register CFSR (Configurable Fault Status Register). The ARM Cortex-M3 User Guide describes this register. Most exception causes fall into the following three categories.

  • Stack overflow or corruption leads to arbitrary code execution.
    • Almost any exception is possible.
  • A NULL pointer has been dereferenced and written to.
    • Typically (IM)PRECISERR exceptions
  • A peripheral module (like UART, Timer, and so forth) is accessed without being powered.
    • Typically (IM)PRECISERR exceptions

The CFSR register is available in View –> Registers in IAR and CCS.

When an access violation occurs, the exception type is IMPRECISERR because writes to flash and peripheral memory regions are mostly buffered writes.

If the CFSR:BFARVALID flag is set when the exception occurs (typical for PRECISERR), the BFAR register in CPU_SCS can be read out to find which memory address caused the exception.

If the exception is IMPRECISERR, PRECISERR can be forced by manually disabling buffered writes. Set [CPU_SCS:ACTRL:DISDEFWBUF] to 1, by either manually setting the bit in the register view in IAR/CCS or by including <hw_cpu_scs.h> from Driverlib and calling the following.

#include <ti/devices/cc26x0r2/inc/hw_cpu_scs.h>
//..
int main()
{
  // Disable write-buffering. Note that this negatively affect performance.
  HWREG(CPU_SCS_BASE + CPU_SCS_O_ACTLR) = CPU_SCS_ACTLR_DISDEFWBUF;

  // ..
}

Using TI-RTOS and ROV to Parse Exceptions

To enable exception decoding in the RTOS Object View (ROV) without using too much memory, use the Minimal exception handler in TI-RTOS. The default choice in the BLE-Stack 3.00.00 projects is to use no exception handler.

To set this up, change the section of the TI-RTOS configuration file that relates to M3Hwi so that it looks like the code below:

//m3Hwi.enableException = true;
m3Hwi.enableException = false;
//m3Hwi.excHandlerFunc = null;
m3Hwi.excHookFunc = "&execHandlerHook";

Then, make a function somewhere with the signature void (*Hwi_ExceptionHookFuncPtr)(Hwi_ExcContext*); such as the one below:

#include <ti/sysbios/family/arm/m3/Hwi.h>
// ...
volatile uintptr_t *excPC = 0;
volatile uintptr_t *excCaller = 0;
// ...
void execHandlerHook(Hwi_ExcContext *ctx)
{
    excPC = ctx->pc;     // Program counter where exception occurred
    excCaller = ctx->lr; // Link Register when exception occurred

    while(2);
}

Setting m3Hwi.enableException to false enables the minimal handler, which fills out the global Hwi_ExcContext structure that the ROV looks at to show the decoded exception. By setting up an excHookFunc, the minimal exception handler will call this function and pass along a pointer to the exception context for the user to work with. This structure is defined in <ti/sysbios/family/arm/m3/Hwi.h>.

When an exception occurs, the device should end up in that infinite loop. Inspect the ROV -> Hwi -> Exception information.

../_images/rov_hwi_exception.png

Figure 113. Decoded exception, intentional write to address 0x0013 which is illegal. Note that writebuffering has been disabled to get a precise error location, and that m3Hwi.enableException has been set to false to get the decoding.

In this case, a bus fault was forced in the function writeToAddress by dereferencing address 0x0013 and trying to write to it:

Listing 71. Write to an address in the FLASH memory region.
void writeToAddress(uintptr_t *addr, int val)
{
   *(int *)addr = val;
}

// ..

void taskFxn(...)
{
   // ..
   writeToAddress( (void*)19, 4 ); // Randomly chosen values
}

The write instruction was placed on line 79 of application.c, as indicated. To get a precise location, the write buffer was disabled as described earlier.

It can be instructive to look at the disassembly view for the locations specified by PC (program counter) and LR (link register). PC is the presumed exception location, and LR is normally the location the failing function should have returned to. As an example, the PC at this exception:

../_images/exception_pc_of_write.png

Figure 114. Here the pc from the decoded exception was looked up in the disassembly view.

Some forensics is required here. We have from the Hwi decoding in ROV (and from the exception context in the exception hook) that the program counter was 0x708e when the exception occurred.

At that location there is a store instruction str r0, [r1] meaning, store the value in R0 to the memory address in R1. The business with SP in the figure above is related to optimization being turned off, so all local variables are stored on the stack, even though in this case R0 and R1 could have been used directly from the caller.

Now we know that the exception occured because soneone called writeToAddress with an invalid address.

Thanks to the exception decoder we can easily find the call site by looking at the call stack, but if the call stack isn’t helpful, we can look at lr, which is seen in the exception decoder to be 0x198f

../_images/exception_lr_of_write.png

Figure 115. Call site as specified in lr. Note that lr is the instruction after the call to writeToAddress because execution would have resumed here.

We can see here that R0 and R1 are initialized with constants. This means that some programmer has intentionally called the write function with an address that causes a busfault.

Most often the reason for a bus-fault is that a pointer is not initialized and a function like writeToAddress gets the pointer, assumes it’s valid and dereferences the pointer and writes to the invalid address.

Debugging Memory Problems

This section describes how to debug a situation where the program runs out of memory, either on the heap or on the runtime stack for the individual thread contexts. Exceeding array bounds or dynamically allocating too little memory for a structure corrupts the memory and can cause an exception like INVPC, INVSTATE, IBUSERR to appear in the CFSR register.

Task and System Stack Overflow

If an overflow on the runtime stack of the task or the system stack occurs (as found using the ROV plug-in), perform the following steps.

  1. Note the current size of the runtime stack of each task.
  2. Increase by a few 100 bytes as described in Initializing a Task and System Stack
  3. Reduce the runtime stack sizes so that they are larger than their respective stackPeaks to save some memory.

Dynamic Allocation Errors

Profiling the ICall Heap Manager (heapmgr.h) describes how to use the ICall Heap profiling functionality. To check if dynamic allocation errors occurred, do as follows:

  1. Check whether heapmgrMemAlo or heapmgrMemAlo are close to HEAPMGR_SIZE
  2. Check memFail to see if allocation failures have occurred.
  3. Call the sanity check function.

If the heap is sane but there are allocation errors, increase HEAPMGR_SIZE and see if the problem persists.

You can set a breakpoint in heapmgr.h in HEAPMGR_MALLOC() on the line hdr = NULL; to find an allocation that is failing.

To disable a symbol, put an x in front of the name. To disable power management, change POWER_SAVING to xPOWER_SAVING.

Options

Table 21. lists the preprocessor symbols used by the application in the simple_peripheral project. Symbols that must remain unmodified are marked with an N in the Modify column while modifiable; configurable symbols are marked with a Y.

Table 21. Application Preprocessor Symbols
Preprocessor Symbol Description Modify
USE_ICALL Required to use ICall Bluetooth low energy and primitive services. N
POWER_SAVING Power management is enabled when defined, and disabled when not defined. Requires same option in stack project. Y
HEAPMGR_SIZE=0 Defines the size in bytes of the ICall heap. Memory is allocated in .bss section. When zero, the heap is auto sized. See Dynamic Memory Allocation Y
ICALL_MAX_NUM_TASKS=3 Defines the number of ICall aware tasks. Modify only if adding a new TI-RTOS task that uses ICall services. Y
ICALL_MAX_NUM_ENTITIES=6 Defines maximum number of entities that use ICall, including service entities and application entities. Modify only if adding a new TI-RTOS task that uses ICall services. Y
Display_DISABLE_ALL All Display statements are removed and no display operations will take place. See Display.h for more details found in the Drivers virtual folder in the project. Y
BOARD_DISPLAY_EXCLUDE_UART Define this symbol to exclude the UART used in the display driver. Y
BOARD_DISPLAY_EXCLUDE_LCD Define this symbol to exclude the LCD used in the display driver. Y
MAX_NUM_BLE_CONNS=1 This is the maximum number of simultaneous Bluetooth low energy collections allowed. Adding more connections uses more RAM and may require increasing HEAPMGR_SIZE. Profile heap usage accordingly. Y
CC26XX This selects the chipset. N
<Board_Type> In Simplelink CC2640R2 SDK, only CC2640R2_LAUNCHXL is supported. N
xdc_runtime_Assert_DISABLE_ALL Disables XDC run-time assert N
xdc_runtime_Log_DISABLE_ALL Disables XDC run-time logging N
HEAPMGR_METRICS Enables collection of ICall heap metrics. See Dynamic Memory Allocation for details on how to profile heap usage. Y

Table 22. lists the only stack preprocessor options that may be modified:

Table 22. Stack Preprocessor Symbols
Preprocessor Symbol Description Modify
POWER_SAVING Power management is enabled when Y
  defined, and disabled when not defined. Requires the same option in application project.  
GATT_NO_CLIENT When defined, the GATT client is not included to save flash. GATT client is excluded from most peripheral projects, included in central and certain peripheral projects (for example, TimeApp). Y
BLE_NO_SECURITY Unlink security functions from the dispatcher, used in conjunction with disabling GAP bond manager and SNV to further reduce flash space. Y
OSAL_SNV=1 Select the number of NV pages to use for SNV. Each page is 4kB of flash. A minimum of one page is required when GAP_BOND_MANAGER is defined. See Using Simple NV for Flash Storage Y
OSAL_MAX_NUM_PROXY_TASKS=2 Number of ICall-aware tasks the protocol task can communicate with. Default is 2. Increase this value if more RTOS tasks are added that make ICall protocol stack API calls. Y
EXT_HAL_ASSERT Extended assert enables support for application callback for asserts. Y

Check System Flash and RAM Usage With Map File

Both application and stack projects produce a map file which can be used to compute the combined flash and RAM system memory usage. Both projects have their own memory space and both map files must be analyzed to determine the total system memory usage. The map file is in the output folder of the respective project in IAR. To compute the total memory usage, do as follows.

  1. Open the application map file (that is, simple_peripheral_cc2650r2lp_app.map).

Note

At the end of the file, three lines contain a breakdown of memory usage for read-only code, read-only data, and read/write data.

  1. Add the two values for read-only code and read-only data memory.

Note

This sum is the total flash memory usage for the application project. The read/write data memory is the total RAM usage by the application project.

  1. Note these values.
  2. Open the stack map file.
  3. Compute the same flash and RAM values for the stack project.
  4. Add the total flash memory value from the application with the total flash usage of the stack to determine the total system flash usage.
  5. Add the total RAM usage from the application with the stack to get the total system RAM usage.

For CCS, the map file of the respective project gives a summary of flash and RAM usage. To determine the remaining available memory for each project, see Flash and RAM. Due to section placement and alignment requirements, some remaining memory may be unavailable. The map file memory usage is valid only if the project builds and links successfully.

Debugging a Program Exit

The program must never exit the main() function. The usual cause for this is that some software module has called abort().

Both IAR and CCS will halt execution when this happens, and the disassembly and call stack will show some type of __exit symbol.

The BLE Stack will call ICall_abort() when one of the below happens:

  • Calling an ICall function from a stack callback
  • Misconfiguring of additional ICall tasks or entities
  • Incorrect ICall task registering

Should the call stack not give enough information to deduce the cause of the abort, a breakpoint can be set in the ICall_abort function to trace from where this error is coming.

HAL Assert Handling

Asserts can be useful when debugging, to trap undesirable states in the code. The BLE Stack projects are by default set up to have the global preprocessor symbol EXT_HAL_ASSERT enabled, which will try to call an assert handler that the user application can define.

Catching Stack Asserts in the Application

The application has an assert callback to catch asserts in the stack project. The assert callback is registered in main() function of each project:

/* Register Application callback to trap asserts raised in the Stack */
RegisterAssertCback(AssertHandler);

The main.c file also contains an example AssertHandler function.

Some generic assert causes that can be returned in the callback include HAL_ASSERT_CAUSE_TRUE, HAL_ASSERT_CAUSE_OUT_OF_MEMORY, and HAL_ASSERT_CAUSE_ICALL_ABORT.

The user can decide how to handle these asserts in the callback. By default, it goes into spinlock for most of the asserts.

The assert can also define a subcause that gives a more specific reason for the assert. An example of a subcause is HAL_ASSERT_OUT_OF_HEAP, which describes the type of memory causing the assert for HAL_ASSERT_CAUSE_OUT_OF_MEMORY.

If no application callback is registered, the default assert callback is called and returns without further action unless HAL_ASSERT_SPIN is defined in the application project, which traps the application in an infinite while loop. In addition, one of the following can also be defined in the stack project if it is not caught in the application callback:

  • HAL_ASSERT_RESET: Resets the device
  • HAL_ASSERT_LIGHTS: Turn on the hazard lights (to be configured by user)
  • HAL_ASSERT_SPIN: Spinlock in a while loop indefinitely

Enable these by ensuring that one of the above corresponding symbols are defined in the preprocessor symbols.

See hal_assert.h and hal_assert.c in the stack project for implementation details.

Preprocessor Options

Preprocessor symbols configure system behavior, features, and resource usage at compile time. Some symbols are required as part of the Bluetooth low energy system, while others are configurable. See Accessing Preprocessor Symbols or Accessing Preprocessor Symbols for details on accessing preprocessor symbols. Symbols defined in a particular project are defined in all files within the project.

Modifying

To disable a symbol, put an x in front of the name. To disable power management, change POWER_SAVING to xPOWER_SAVING.

Options

Table 23. lists the preprocessor symbols used by the application in the simple_peripheral project. Symbols that must remain unmodified are marked with an N in the Modify column while modifiable; configurable symbols are marked with a Y.

Table 23. BLE Application Preprocessor Symbols
Preprocessor Symbol Description Modify
USE_ICALL Required to use ICall Bluetooth low energy and primitive services. N
POWER_SAVING Power management is enabled when defined, and disabled when not defined. Requires same option in stack project. Y
HEAPMGR_SIZE=0 Defines the size in bytes of the ICall heap. Memory is allocated in .bss section. When zero, the heap is auto sized. See Dynamic Memory Allocation. Y
ICALL_MAX_NUM_TASKS=3 Defines the number of ICall aware tasks. Modify only if adding a new TI-RTOS task that uses ICall services. Y
ICALL_MAX_NUM_ENTITIES=6 Defines maximum number of entities that use ICall, including service entities and application entities. Modify only if adding a new TI-RTOS task that uses ICall services. Y
Display_DISABLE_ALL All Display statements are removed and no display operations will take place. See Display.h for more details found in the Drivers virtual folder in the project. Y
BOARD_DISPLAY_EXCLUDE_UART Define this symbol to exclude the UART used in the display driver. Y
BOARD_DISPLAY_EXCLUDE_LCD Define this symbol to exclude the LCD used in the display driver. Y
MAX_NUM_BLE_CONNS=1 This is the maximum number of simultaneous Bluetooth low energy collections allowed. Adding more connections uses more RAM and may require increasing HEAPMGR_SIZE. Profile heap usage accordingly. Y
CC26XX This selects the chipset. N
<Board_Type> In Simplelink CC2640R2 SDK, only CC2640R2_LAUNCHXL is supported. N
xdc_runtime_Assert_DISABLE_ALL Disables XDC run-time assert N
xdc_runtime_Log_DISABLE_ALL Disables XDC run-time logging N
HEAPMGR_METRICS Enables collection of ICall heap metrics. See Dynamic Memory Allocation for details on how to profile heap usage. Y

Table 24. lists the only stack preprocessor options that may be modified:

Table 24. BLE Stack Preprocessor Symbols
Preprocessor Symbol Description Modify
POWER_SAVING Power management is enabled when defined, and disabled when not defined. Requires the same option in application project. Y
GATT_NO_CLIENT When defined, the GATT client is not included to save flash. GATT client is excluded from most peripheral projects, included in central and certain peripheral projects (for example, TimeApp). Y
BLE_NO_SECURITY Unlink security functions from the dispatcher, used in conjunction with disabling GAP bond manager and SNV to further reduce flash space. Y
OSAL_SNV=1 Select the number of NV pages to use for SNV. Each page is 4kB of flash. A minimum of one page is required when GAP_BOND_MANAGER is defined. See Using Simple NV for Flash Storage Y
OSAL_MAX_NUM_PROXY_TASKS=2 Number of ICall-aware tasks the protocol task can communicate with. Default is 2. Increase this value if more TI-RTOS tasks are added that make ICall protocol stack API calls. Y
EXT_HAL_ASSERT Extended assert enables support for application callback for asserts. Y