XDM ISPHDEC1 Speech/Voice Decoder Interface

Data Structures

struct  ISPHDEC1_Obj
 This must be the first field of all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Params
 Defines the creation time parameters for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control(). More...
struct  ISPHDEC1_InArgs
 Defines the input arguments for all ISPHDEC1 instance process function. More...
struct  ISPHDEC1_Status
 Defines instance status parameters. More...
struct  ISPHDEC1_OutArgs
 Defines the run time output arguments for all ISPHDEC1 instance objects. More...
struct  ISPHDEC1_Fxns
 Defines all of the operations on ISPHDEC1 objects. More...

Defines

#define ISPHDEC1_EOK   XDM_EOK
#define ISPHDEC1_EFAIL   XDM_EFAIL
#define ISPHDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Typedefs

typedef struct ISPHDEC1_ObjISPHDEC1_Handle
 Opaque handle to an ISPHDEC1 objects.
typedef IALG_Cmd ISPHDEC1_Cmd
 Defines the control commands for the ISPHDEC1 module.

Enumerations

enum  ISPHDEC1_FrameType {
  ISPHDEC1_FTYPE_SPEECHGOOD = 0,
  ISPHDEC1_FTYPE_SIDUPDATE = 1,
  ISPHDEC1_FTYPE_NODATA = 2,
  ISPHDEC1_FTYPE_SPEECHLOST = 3,
  ISPHDEC1_FTYPE_DEGRADED = 4,
  ISPHDEC1_FTYPE_BAD = 5,
  ISPHDEC1_FTYPE_SIDFIRST = 6,
  ISPHDEC1_FTYPE_SIDBAD = 7,
  ISPHDEC1_FTYPE_ONSET = 8
}
 

Decoder frame types.

More...

Detailed Description

This is the XDM ISPHDEC1 Speech/Voice Decoder Interface.


Define Documentation

#define ISPHDEC1_EOK   XDM_EOK

Success.

#define ISPHDEC1_EFAIL   XDM_EFAIL

General failure.

#define ISPHDEC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.


Typedef Documentation

typedef struct ISPHDEC1_Obj* ISPHDEC1_Handle

Opaque handle to an ISPHDEC1 objects.

Defines the control commands for the ISPHDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional control commands.
See also:
XDM_CmdId
ISPHDEC1_Fxns::control()

Enumeration Type Documentation

Decoder frame types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
ISPHDEC1_InArgs.frameType
Enumerator:
ISPHDEC1_FTYPE_SPEECHGOOD 

Regular speech frame received without errors/loss.

ISPHDEC1_FTYPE_SIDUPDATE 

SID update frames.

ISPHDEC1_FTYPE_NODATA 

Untransmitted frame for codecs which support internal DTX.

ISPHDEC1_FTYPE_SPEECHLOST 

Complete loss of speech frame.

ISPHDEC1_FTYPE_DEGRADED 

Speech frame with a correct CRC, some invalid data.

ISPHDEC1_FTYPE_BAD 

Speech frame (likely), but invalid.

ISPHDEC1_FTYPE_SIDFIRST 

The first frame of comfort noise.

ISPHDEC1_FTYPE_SIDBAD 

Corrupt SID update frame.

ISPHDEC1_FTYPE_ONSET 

Frames which precede the first speech frame of a speech burst.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated