IALG - XDAIS Algorithm Interface

Data Structures

struct  IALG_MemRec
 Memory records. More...
struct  IALG_Obj
 Algorithm instance object definition. More...
struct  IALG_Params
 Algorithm instance creation parameters. More...
struct  IALG_Status
 Pointer to algorithm specific status structure. More...
struct  IALG_Fxns
 Defines the fields and methods that must be supplied by all XDAIS algorithms. More...

Defines

#define IALG_DEFMEMRECS   4
#define IALG_OBJMEMREC   0
#define IALG_SYSCMD   256
#define IALG_EOK   0
#define IALG_EFAIL   -1
#define IALG_CUSTOMFAILBASE   -2048
#define IALG_CUSTOMFAILEND   -256
#define IALG_MPROG   0x0008
#define IALG_MXTRN   0x0010
#define IALG_isProg(s)
#define IALG_isOffChip(s)

Typedefs

typedef struct IALG_ObjIALG_Handle
 Handle to an algorithm instance object.
typedef unsigned int IALG_Cmd
 Algorithm specific command.

Enumerations

enum  IALG_MemAttrs {
  IALG_SCRATCH,
  IALG_PERSIST,
  IALG_WRITEONCE
}
 

Memory attributes.

More...
enum  IALG_MemSpace {
  IALG_EPROG,
  IALG_IPROG,
  IALG_ESDATA,
  IALG_EXTERNAL,
  IALG_DARAM0 = 0,
  IALG_DARAM1 = 1,
  IALG_SARAM = 2,
  IALG_SARAM0 = 2,
  IALG_SARAM1 = 3,
  IALG_DARAM2 = 4,
  IALG_SARAM2 = 5
}
 

Defined memory spaces.

More...

Detailed Description

This is the XDAIS IALG interface.


Define Documentation

#define IALG_DEFMEMRECS   4

Default number of memory records.

#define IALG_OBJMEMREC   0

Memory record index of instance object.

#define IALG_SYSCMD   256

Minimum "system" IALG_Cmd value.

#define IALG_EOK   0

Successful return status code.

#define IALG_EFAIL   -1

Unspecified error return status code.

#define IALG_CUSTOMFAILBASE   -2048

Algorithm-specific failure code end.

Remarks:
This is 0xfffff800.
#define IALG_CUSTOMFAILEND   -256

Algorithm-specific failure code base.

Remarks:
This is 0xffffff00.
#define IALG_MPROG   0x0008

Program memory space bit.

#define IALG_MXTRN   0x0010

External memory space bit.

#define IALG_isProg (  ) 
Value:
(        \
    (((int)(s)) & IALG_MPROG)   \
)
#define IALG_isOffChip (  ) 
Value:
(     \
    (((int)(s)) & IALG_MXTRN)   \
)

Typedef Documentation

typedef struct IALG_Obj* IALG_Handle

Handle to an algorithm instance object.

typedef unsigned int IALG_Cmd

Algorithm specific command.

Remarks:
This command is used in conjunction with IALG_Status to get and set algorithm specific attributes via the algControl() method.

Enumeration Type Documentation

Memory attributes.

Enumerator:
IALG_SCRATCH 

Scratch memory.

IALG_PERSIST 

Persistent memory.

IALG_WRITEONCE 

Write-once persistent memory.

Defined memory spaces.

Enumerator:
IALG_EPROG 

External program memory

IALG_IPROG 

Internal program memory

IALG_ESDATA 

Off-chip data memory (accessed sequentially)

IALG_EXTERNAL 

Off-chip data memory (accessed randomly)

IALG_DARAM0 

Dual access on-chip data memory

IALG_DARAM1 

Block 1, if independant blocks required

IALG_SARAM 

Single access on-chip data memory

IALG_SARAM0 

Block 0, equivalent to IALG_SARAM

IALG_SARAM1 

Block 1, if independant blocks required

IALG_DARAM2 

Block 2, if a 3rd independent block required

IALG_SARAM2 

Block 2, if a 3rd independent block required

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated