SOCK6PCB Struct Reference

The structure describes the IPv6 Socket Protocol specific properties. More...

#include <sockif.h>


Data Fields

IP6N IPAddrLocal
 Local IPv6 Address.
UINT16 PortLocal
 Local IP Port.
IP6N IPAddrForeign
 Foreign host's IPv6 Address.
UINT16 PortForeign
 Foreign IP Port.
UINT32 State
 Socket state (protocol dependent).


Detailed Description

The structure describes the IPv6 Socket Protocol specific properties.


The documentation for this struct was generated from the following file:
Copyright 2009, Texas Instruments Incorporated