src/stack/icmpv6/icmpv6.c File Reference

The file has functions which handle the ICMPv6 Protocol. More...


Functions

void ICMPv6Init (void)


Detailed Description

The file has functions which handle the ICMPv6 Protocol.

NOTE: (C) Copyright 2008, Texas Instruments, Inc.

Function Documentation

void ICMPv6Init ( void   ) 

Description
The function is used to initialize the ICMPv6 Protocol stack.

This is for *internal* NDK Stack Usage.

Return values:
Not Applicable.


Copyright 2009, Texas Instruments Incorporated