50 #ifndef ti_sdo_fc_rman__RMAN_
51 #define ti_sdo_fc_rman__RMAN_
53 #define ti_sdo_fc_ires_NOPROTOCOLREV
73 #define RMAN_MODNAME "ti.sdo.fc.rman"
78 #define RMAN_GTNAME "ti.sdo.fc.rman"
83 #define RMAN_PROTOCOLNAMESIZE 200
96 (Int scratchId, Bool yieldFlag);
381 IRES_Fxns * resFxns, Int scratchGroupId);
409 IRES_Fxns * resFxns, Int scratchGroupId);
IRES_Status
IRES_Status defines the standard error and success codes returned by IRES APIs.
Definition: ires_common.h:57
Configuration Parameters required by the Resource Manager implementation. These can be extended by in...
Definition: iresman.h:82
void RMAN_yield(IRES_YieldResourceType resource, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs)
Yield function specifically for use when DSKT2 based algorithms need cooperative preemption and multi...
UInt32 ti_sdo_fc_rman_RMAN_ipcKey
Base key value ofr RMAN Linux IPC Objects.
Algorithm instance object definition.
Definition: ialg.h:159
__FAR__ RMAN_Params RMAN_PARAMS
Initialization parameters for the generic Resource Manager.
__FAR__ IRESMAN_Params ** RMAN_registryResmanArgs
Initialization arguments for the entries to be registered Set this variable to NULL if no static conf...
The module configuration structure for RMAN. It is set at design time by the system integrator to reg...
Definition: rman.h:108
IRES_Status RMAN_freeAllocatedResources(Int requestId, IRES_ResourceDescriptor *resDesc, Int numResources, Int scratchGroupId)
Free resources held by the algorithm resource handle.
IRES_Status RMAN_freeResources(IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Free resources held by the algorithm resource handle.
Void(* IRES_YieldFxn)(IRES_YieldResourceType resourceType, IRES_YieldContextHandle algYieldContext, IRES_YieldArgs yieldArgs)
The 'yield function' pointer and 'yield arguments' are supplied to an algorithm during its IRES inter...
Definition: ires.h:159
IRES_Obj holds the private state associated with each logical resource.
Definition: ires_common.h:176
Void( IRESMAN_PersistentFreeFxn)(IALG_MemRec *memTab, Int numRecs)
Memory free functions for all of ResMan and other IRES protocol's memory requirements.
Definition: iresman.h:74
IRES Interface Definitions - Allows algorithms to request and receive handles representing private lo...
IRESMAN_PersistentAllocFxn * allocFxn
Memory allocation function for all RMAN memory requirements.
Definition: rman.h:118
__FAR__ IRESMAN_Fxns ** RMAN_registryEntries
To allow for static configuration of the Resource Registry table this can be set to a valid configura...
ti_sdo_fc_rman_RMAN_YieldArgsFxn ti_sdo_fc_rman_RMAN_setYieldArgs
Function to set yield arguments to pass to yield function set in RMAN_PARAMS.
IRES_Status RMAN_register(IRESMAN_Fxns *resmanFxns, IRESMAN_Params *initArgs)
Register the protocol/protocol revision and the device specific resource manager implementation with ...
Bool( IRESMAN_PersistentAllocFxn)(IALG_MemRec *memTab, Int numRecs)
Memory allocation function for all of ResMan and other IRES protocol's memory requirements.
Definition: iresman.h:68
__FAR__ IRESMAN_Fxns * RMAN_TABLE[]
RMAN Table to hold IRESMAN registrations.
Bool yieldSamePriority
Flag indicating if yield to same priority is okay.
Definition: rman.h:134
IRES_YieldArgs(* ti_sdo_fc_rman_RMAN_YieldArgsFxn)(Int scratchId, Bool yieldFlag)
Type declaration for the "yield fxn" which is required if if RMAN has been configured to yield execut...
Definition: rman.h:96
__FAR__ unsigned int ** RMAN_iresVTable
Table that holds the mapping from algorithms IALG_Fxns to IRES_Fxns.
Descriptor to Logical Resource.
Definition: ires_common.h:122
IRESMAN_PersistentFreeFxn * freeFxn
Memory free function for all RMAN memory requirements.
Definition: rman.h:123
__FAR__ unsigned int ti_sdo_fc_rman_RMAN_MAXALGS
Maximum number of algorithm instances that will use RMAN.
IRES_Status RMAN_unregister(IRESMAN_Fxns *resmanFxns)
Unregister the protocol and the corresponding resource manager implementation from the Resource Regis...
These fxns are used to query/grant the resources requested by the algorithm at initialization time...
Definition: ires.h:168
IRES_Status RMAN_assignResources(IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Assign resources to the algorithm indicated by algHandle. The resource requirements can be determined...
IRES_Status RMAN_init(Void)
Initialize the RMAN object with static information from the headers/configuration etc...
Specifies the algorithm specific handles and context save & restore function pointers and arguments t...
Definition: ires.h:84
Device specific Resource Manager Interface Definitions IRESMAN - Interface that needs to be implement...
Void * IRES_YieldArgs
Definition: ires.h:140
IRES_Status RMAN_activateResource(IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Activate resource identified by the resourceHandle held by the algorithm.
__FAR__ short RMAN_FREE_ENTRIES[]
Free Table to hold entries freed from RMAN Table.
IRES_YieldFxn yieldFxn
Yield function used to yield to same/higher priority algorithms. If yielding is supported set to vali...
Definition: rman.h:129
IRES_Status RMAN_deactivateAllResources(IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Deactivate all resources held by the algorithm.
short numRegistries
Number of registry entries in the RMAN table.
Definition: rman.h:113
__FAR__ short RMAN_numRegistryEntries
Number of entries statically configured for the Resource Registry table. Set this variable to zero if...
IRES_Status RMAN_deactivateResource(IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Deactivate resource identified by the resourceHandle held by the algorithm.
struct Sem_Obj * RMAN_SemHandle
Declare abstract handle for Semaphore object.
Definition: rman.h:88
IRES_Status RMAN_activateAllResources(IALG_Handle algHandle, IRES_Fxns *resFxns, Int scratchGroupId)
Activate all resources held by the algorithm.
IRES_Status RMAN_allocateResources(Int requestId, IRES_ResourceDescriptor *resDesc, Int numResources, Int scratchGroupId)
Directly allocate IRES resources by client without implementing IRES_Fxns.
IRES_Status RMAN_exit(Void)
Delete the generic IRES RMAN and release memory back.
struct RMAN_Params RMAN_Params
The module configuration structure for RMAN. It is set at design time by the system integrator to reg...
IRES_YieldResourceType
Definition: ires.h:60