Framework Components Application Programming Interface (API)
fc-w02
|
Descriptor to Logical Resource. More...
#include <ires_common.h>
Data Fields | |
String | resourceName |
struct IRES_ProtocolArgs * | protocolArgs |
Pointer to the Resource Protocol Arguments. More... | |
IRES_ProtocolRevision * | revision |
The revision of the IRES_ResourceProtocol Interface expected by the client algorithm. More... | |
struct IRES_Obj * | handle |
Descriptor to Logical Resource.
String IRES_ResourceDescriptor::resourceName |
String containing the package name to identify the resource.
struct IRES_ProtocolArgs* IRES_ResourceDescriptor::protocolArgs |
Pointer to the Resource Protocol Arguments.
resourceName
, and uses the protocol to construct the IRES Resource Handle. IRES_ProtocolRevision* IRES_ResourceDescriptor::revision |
The revision of the IRES_ResourceProtocol Interface expected by the client algorithm.
struct IRES_Obj* IRES_ResourceDescriptor::handle |
The handle to the object representing the requested resource. The handle is initially set to 'null' by the requesting algorithm. The 'resource manager' allocates the resource and constructs the handle.