Framework Components Application Programming Interface (API)
fc-w02
|
Device specific Resource Manager Interface Definitions IRESMAN - Interface that needs to be implemented and registered with the generic RMAN Resource Registry that are called to manage corresponding IRES resources.
Go to the source code of this file.
Data Structures | |
struct | IRESMAN_Params |
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required. More... | |
struct | IRESMAN_Fxns |
Typedefs | |
typedef Bool( | IRESMAN_PersistentAllocFxn )(IALG_MemRec *memTab, Int numRecs) |
Memory allocation function for all of ResMan and other IRES protocol's memory requirements. More... | |
typedef Void( | IRESMAN_PersistentFreeFxn )(IALG_MemRec *memTab, Int numRecs) |
Memory free functions for all of ResMan and other IRES protocol's memory requirements. More... | |
typedef struct IRESMAN_Params | IRESMAN_Params |
Configuration Parameters required by the Resource Manager implementation. These can be extended by individual resource managers if required. More... | |
typedef struct IRESMAN_Fxns | IRESMAN_Fxns |