Data Structures | Defines | Typedefs

ISPHDEC - XDM Speech Decoder Interface

Data Structures

struct  ISPHDEC_Obj
 This must be the first field of all ISPHDEC instance objects. More...
struct  ISPHDEC_Params
 Defines the creation time parameters for all ISPHDEC instance objects. More...
struct  ISPHDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls. More...
struct  ISPHDEC_InArgs
 Defines the input arguments for all ISPHDEC instance process function. More...
struct  ISPHDEC_Status
 Defines instance status parameters (read-only). More...
struct  ISPHDEC_OutArgs
 Defines the run time output arguments for all ISPHDEC instance objects. More...
struct  ISPHDEC_Fxns
 Defines all of the operations on ISPHDEC objects. More...

Defines

#define ISPHDEC_CID   "ti.xdais.dm.ISPHDEC"
#define ISPHDEC_ERUNTIME   XDM_ERUNTIME
#define ISPHDEC_EOK   XDM_EOK
#define ISPHDEC_EFAIL   XDM_EFAIL

Typedefs

typedef struct ISPHDEC_Obj ISPHDEC_Obj
 This must be the first field of all ISPHDEC instance objects.
typedef struct ISPHDEC_ObjISPHDEC_Handle
 Opaque handle to an ISPHDEC objects.
typedef struct ISPHDEC_Params ISPHDEC_Params
 Defines the creation time parameters for all ISPHDEC instance objects.
typedef struct
ISPHDEC_DynamicParams 
ISPHDEC_DynamicParams
 This structure defines the codec parameters that can be modified after creation via control() calls.
typedef struct ISPHDEC_InArgs ISPHDEC_InArgs
 Defines the input arguments for all ISPHDEC instance process function.
typedef struct ISPHDEC_Status ISPHDEC_Status
 Defines instance status parameters (read-only).
typedef struct ISPHDEC_OutArgs ISPHDEC_OutArgs
 Defines the run time output arguments for all ISPHDEC instance objects.
typedef IALG_Cmd ISPHDEC_Cmd
 Defines the control commands for the ISPHDEC module.
typedef struct ISPHDEC_Fxns ISPHDEC_Fxns
 Defines all of the operations on ISPHDEC objects.

Detailed Description

This is the XDM ISPHDEC Speech Decoder Interface.

Deprecated:
This XDM speech decoder interface has been deprecated, and superceeded by newer ISPHDECx speech decoder interfaces.

Define Documentation

#define ISPHDEC_CID   "ti.xdais.dm.ISPHDEC"

ISPHDEC Class ID

#define ISPHDEC_ERUNTIME   XDM_ERUNTIME

General runtime failure.

#define ISPHDEC_EOK   XDM_EOK

Success.

#define ISPHDEC_EFAIL   XDM_EFAIL

General failure.


Typedef Documentation

typedef struct ISPHDEC_Obj ISPHDEC_Obj

This must be the first field of all ISPHDEC instance objects.

typedef struct ISPHDEC_Obj* ISPHDEC_Handle

Opaque handle to an ISPHDEC objects.

Defines the creation time parameters for all ISPHDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::control()

Defines the input arguments for all ISPHDEC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::process()

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::control()

Defines the run time output arguments for all ISPHDEC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::process()

Defines the control commands for the ISPHDEC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
ISPHDEC_Fxns::control()
typedef struct ISPHDEC_Fxns ISPHDEC_Fxns

Defines all of the operations on ISPHDEC objects.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated