|
|
- Global CE_DECLARE_TYPE (name, types)
- No need to use this macro when using CE_LOCAL_ALG2
- Global CE_LOCAL_ALG (name, algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType)
- Use CE_LOCAL_ALG2 instaead.
- Global Engine_ATTRS
- Engine_ATTRS is no longer recommended. Please use Engine_initAttrs() instead.
- Global Engine_getUsedMem (Engine_Handle engine)
- This service has been replaced by Server_getMemStat() to better indicate that this API is not intended for obtaining the current processor's memory statistics, rather it obtains the memory statistics of a remote Server. Also, Server_getMemStat() provides more granularity than Engine_getUsedMem().
- Global IAUDIO_ChannelId
- This enumeration is only supported on 0.9 XDM. To use it, you must define "XDM_INCLUDE_DOT9_SUPPORT" prior to including this file. In XDM 1.00, this has been superceded by IAUDIO_ChannelMode.
- Global ti_sdo_ce_osal_Memory_contigAlloc (UInt size, UInt align)
- This function has been superceded by ti_sdo_ce_osal_Memory_alloc() and will be removed in a future release. Users are recommended to modify their applications to use the new, more flexible ti_sdo_ce_osal_Memory_alloc() instead.
- Group ti_xdais_dm_IAUDDEC
- This XDM audio decoder interface has been deprecated, and superceeded by newer IAUDDECx audio decoder interfaces.
- Group ti_xdais_dm_IAUDENC
- This XDM audio encoder interface has been deprecated, and superceeded by newer IAUDENCx audio encoder interfaces.
- Group ti_xdais_dm_IIMGDEC
- This XDM image decoder interface has been deprecated, and superceeded by newer IIMGDECx image decoder interfaces.
- Group ti_xdais_dm_IIMGENC
- This XDM image encoder interface has been deprecated, and superceeded by newer IIMGENCx image encoder interfaces.
- Group ti_xdais_dm_ISPHDEC
- This XDM speech decoder interface has been deprecated, and superceeded by newer ISPHDECx speech decoder interfaces.
- Group ti_xdais_dm_ISPHENC
- This XDM speech encoder interface has been deprecated, and superceeded by newer ISPHENCx speech encoder interfaces.
- Group ti_xdais_dm_IVIDDEC
- This XDM video decoder interface has been deprecated, and superceeded by newer IVIDDECx video decoder interfaces.
- Group ti_xdais_dm_IVIDDEC1
- This XDM video decoder interface has been deprecated, and superceeded by newer IVIDDECx video decoder interfaces.
- Group ti_xdais_dm_IVIDENC
- This XDM video encoder interface has been deprecated, and superceeded by newer IVIDENCx video encoder interfaces.
- Global XDM_ERUNTIME
- This is only supported on 0.9 XDM. To use it, you must define "XDM_INCLUDE_DOT9_SUPPORT". In XDM 1.00+, it is required that codecs return "EFAIL", as "ERUNTIME" is not supported.
- Global XDM_MEMTYPE_ROW
- The XDM_MEMTYPE_ROW value is deprecated. Please use XDM_MEMTYPE_RAW (which, by design, has the same underyling value) instead.
Copyright 2012, Texas Instruments Incorporated