Data Fields

LINKCFG_Dsp_tag Struct Reference

#include <linkcfgdefs.h>

Data Fields

Char8 name [DSP_MAX_STRLEN]
Uint32 dspArch
Char8 loaderName [DSP_MAX_STRLEN]
Bool autoStart
Char8 execName [DSP_MAX_STRLEN]
DSP_BootMode doDspCtrl
Uint32 resumeAddr
Uint32 resetVector
Uint32 resetCodeSize
Uint32 maduSize
Uint32 cpuFreq
Uint32 endian
Uint32 wordSwap
Uint32 memTableId
Uint32 memEntries
Uint32 linkDrvId
Uint32 arg1
Uint32 arg2
Uint32 arg3
Uint32 arg4
Uint32 arg5

Field Documentation

Char8 LINKCFG_Dsp_tag::name[DSP_MAX_STRLEN]

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated