Defines | Typedefs

gpptypes.h File Reference


Detailed Description

Defines the type system for DSP/BIOS Link.

============================================================================

Path:
/gpp/inc/usr/
Version:
1.65.02.09 ============================================================================
Copyright:
Copyright (C) 2002-2012, Texas Instruments Incorporated - https://www.ti.com/

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ============================================================================

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Defines

#define IN
 Argument specification syntax ============================================================================.
#define OUT
#define CONST   const
#define USES(filename)
 Empty macro to indicate header file dependency ============================================================================.
#define Void   void
#define FALSE   0u
 Boolean constants ============================================================================.
#define TRUE   1u
#define NULL   ((void *)0)
 Definition is language specific ============================================================================.
#define NULL_CHAR   '\0'
 String terminator. ============================================================================.
#define REG8(A)   (*(volatile Char8 *) (A))
 Macros to access register fields. ============================================================================.
#define REG16(A)   (*(volatile Uint16 *) (A))
#define REG32(A)   (*(volatile Uint32 *) (A))

Typedefs

typedef signed char Int8
 Basic data types ============================================================================.
typedef signed short int Int16
typedef signed long int Int32
typedef unsigned char Uint8
typedef unsigned short int Uint16
typedef unsigned long int Uint32
typedef float Real32
typedef double Real64
typedef short int Bool
typedef char Char8
typedef short Char16
typedef unsigned char Uchar8
typedef unsigned short Uchar16
typedef int Int
typedef void * Pvoid
typedef Char8Pstr
typedef Uchar8Pustr
typedef Uint32 ProcessorId
 These types are used across DSP/BIOS Link. ============================================================================.
typedef Uint32 ChannelId

PoolId

This type is used for identifying the different pools used by DSPLINK. ============================================================================

============================================================================


#define STATIC   static
 Free for OEMs to add their own generic stuff, if they so desire ============================================================================.
#define EXTERN   extern
#define NORMAL_API   CDECL
#define IMPORT_API   DLLIMPORT
#define EXPORT_API   DLLEXPORT
typedef Uint16 PoolId

Define Documentation

#define IN

Argument specification syntax ============================================================================.

============================================================================

Macro:
IN/OUT/OPTIONAL/CONST
#define OUT
#define CONST   const
#define USES (   filename )

Empty macro to indicate header file dependency ============================================================================.

============================================================================

Macro:
USES
#define Void   void
#define FALSE   0u

Boolean constants ============================================================================.

============================================================================

Constant:
TRUE/FALSE
#define TRUE   1u
#define NULL   ((void *)0)

Definition is language specific ============================================================================.

============================================================================

Constant:
NULL
#define NULL_CHAR   '\0'

String terminator. ============================================================================.

============================================================================

Constant:
NULL_CHAR
#define REG8 (   A )    (*(volatile Char8 *) (A))

Macros to access register fields. ============================================================================.

============================================================================

Macro:
REG8/REG16/REG32
#define REG16 (   A )    (*(volatile Uint16 *) (A))
#define REG32 (   A )    (*(volatile Uint32 *) (A))
#define STATIC   static

Free for OEMs to add their own generic stuff, if they so desire ============================================================================.

============================================================================

Macro:
OS Specific standard definitions ============================================================================
Macro:
Calling convention

Definition of CDECL, DLLIMPORT, DLLEXPORT can be defined by OEM for his compiler ============================================================================

#define EXTERN   extern
#define NORMAL_API   CDECL
#define IMPORT_API   DLLIMPORT
#define EXPORT_API   DLLEXPORT

Typedef Documentation

typedef signed char Int8

Basic data types ============================================================================.

============================================================================

Macro:
Data types
typedef signed short int Int16
typedef signed long int Int32
typedef unsigned char Uint8
typedef unsigned short int Uint16
typedef unsigned long int Uint32
typedef float Real32
typedef double Real64
typedef short int Bool
typedef char Char8
typedef short Char16
typedef unsigned char Uchar8
typedef unsigned short Uchar16
typedef int Int
typedef void* Pvoid
typedef Char8* Pstr
typedef Uchar8* Pustr

These types are used across DSP/BIOS Link. ============================================================================.

============================================================================

Macro:
DSP/BIOS Link specific types
typedef Uint32 ChannelId
typedef Uint16 PoolId
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated