Defines | Functions

proc.h File Reference


Detailed Description

Defines the interfaces and data structures for the API sub-component PROC.

============================================================================

Path:
/gpp/inc/usr/
Version:
1.65.02.09 ============================================================================
Copyright:
Copyright (C) 2002-2012, Texas Instruments Incorporated - https://www.ti.com/

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ============================================================================

#include <dsplink.h>
#include <procdefs.h>
#include <linkcfgdefs.h>
Include dependency graph for proc.h:

Go to the source code of this file.

Defines

#define PROC_Destroy   PROC_destroy
#define PROC_Attach   PROC_attach
#define PROC_Detach   PROC_detach
#define PROC_GetState   PROC_getState
#define PROC_Load   PROC_load
#define PROC_LoadSection   PROC_loadSection
#define PROC_Read   PROC_read
#define PROC_Write   PROC_write
#define PROC_Start   PROC_start
#define PROC_Stop   PROC_stop
#define PROC_Control   PROC_control

Functions

DLLEXPORT DSP_STATUS PROC_setup (IN LINKCFG_Object *linkCfg)
 Sets up the necessary data structures for the PROC sub-component.
DLLEXPORT DSP_STATUS PROC_destroy (void)
 Destroys the data structures for the PROC component, allocated earlier by a call to PROC_setup ().
DLLEXPORT DSP_STATUS PROC_attach (IN ProcessorId procId, PROC_Attrs *attr)
 Attaches the client to the specified DSP and also initializes the DSP (if required).
DLLEXPORT DSP_STATUS PROC_detach (IN ProcessorId procId)
 Detaches the client from specified processor. If the caller is the owner of the processor, this function releases all the resources that this component uses and puts the DSP in an unusable state (from application perspective).
DLLEXPORT DSP_STATUS PROC_getState (IN ProcessorId procId, OUT PROC_State *procState)
 Gets the current status of DSP by querying the Link Driver.
DLLEXPORT DSP_STATUS PROC_load (IN ProcessorId procId, IN Char8 *imagePath, IN Uint32 argc, IN Char8 **argv)
 Loads the specified DSP executable on the target DSP. It ensures that the caller owns the DSP.
DLLEXPORT DSP_STATUS PROC_loadSection (IN ProcessorId procId, IN Char8 *imagePath, IN Uint32 sectID)
 Loads the specified section of DSP executable onto the target DSP. It ensures that the client owns the DSP.
DLLEXPORT DSP_STATUS PROC_read (IN ProcessorId procId, IN Uint32 dspAddr, IN Uint32 numBytes, IN OUT Pvoid buffer)
 This function allows GPP side applications to read from the DSP memory space.
DLLEXPORT DSP_STATUS PROC_write (IN ProcessorId procId, IN Uint32 dspAddr, IN Uint32 numBytes, IN Pvoid buffer)
 This function allows GPP side applications to write to the DSP memory space.
DLLEXPORT DSP_STATUS PROC_start (IN ProcessorId procId)
 Starts execution of the loaded code on DSP from the starting point specified in the DSP executable loaded earlier by call to PROC_load ().
DLLEXPORT DSP_STATUS PROC_stop (IN ProcessorId procId)
 Stops the DSP.
DLLEXPORT DSP_STATUS PROC_control (IN ProcessorId procId, IN Int32 cmd, Pvoid arg)
 Provides a hook to perform device dependent control operations on the DSP.
DLLEXPORT DSP_STATUS PROC_GetSymbolAddress (IN ProcessorId procId, IN Char8 *symbolName, OUT Uint32 *dspAddr)
 Gets the DSP address corresponding to a symbol within a DSP executable currently loaded on the DSP.
DLLEXPORT DSP_STATUS PROC_sendTerminateEvent (IN ProcessorId procId)
 Send an IPS terminate event to the DSP.
DLLEXPORT DSP_STATUS PROC_Setup (void)

Define Documentation

#define PROC_Destroy   PROC_destroy

============================================================================

Deprecated:
The deprecated API PROC_Destroy has been replaced with PROC_destroy. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Attach   PROC_attach

============================================================================

Deprecated:
The deprecated API PROC_Attach has been replaced with PROC_attach. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Detach   PROC_detach

============================================================================

Deprecated:
The deprecated API PROC_Detach has been replaced with PROC_detach. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_GetState   PROC_getState

============================================================================

Deprecated:
The deprecated API PROC_GetState has been replaced with PROC_getState. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Load   PROC_load

============================================================================

Deprecated:
The deprecated API PROC_Load has been replaced with PROC_load. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_LoadSection   PROC_loadSection

============================================================================

Deprecated:
The deprecated API PROC_LoadSection has been replaced with PROC_loadSection. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Read   PROC_read

============================================================================

Deprecated:
The deprecated API PROC_Read has been replaced with PROC_read. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Write   PROC_write

============================================================================

Deprecated:
The deprecated API PROC_Write has been replaced with PROC_write. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Start   PROC_start

============================================================================

Deprecated:
The deprecated API PROC_Start has been replaced with PROC_start. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Stop   PROC_stop

============================================================================

Deprecated:
The deprecated API PROC_Stop has been replaced with PROC_stop. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

#define PROC_Control   PROC_control

============================================================================

Deprecated:
The deprecated API PROC_Control has been replaced with PROC_control. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================


Function Documentation

DLLEXPORT DSP_STATUS PROC_setup ( IN LINKCFG_Object linkCfg )

Sets up the necessary data structures for the PROC sub-component.

============================================================================

Function:
PROC_setup
Parameters:
linkCfgPointer to the configuration information structure for DSP/BIOS LINK. If NULL, indicates that default configuration should be used.
Returns:
DSP_SOK Operation successfully completed. DSP_SALREADYSETUP The DSPLink driver is already setup in this process. DSP_ECONFIG Error in specified dynamic configuration. Please check CFG_<PLATFORM>.c DSP_EMEMORY Operation failed due to memory error. DSP_EFAIL General failure.
Precondition:
The configuration information structure has been updated with application specific information. If no configuration is specified the default configuration will be used.
Postcondition:
None
See also:
PROC_destroy ============================================================================
DLLEXPORT DSP_STATUS PROC_destroy ( void   )

Destroys the data structures for the PROC component, allocated earlier by a call to PROC_setup ().

============================================================================

Function:
PROC_destroy
Parameters:
None
Returns:
DSP_SOK Operation successfully completed. DSP_SDESTROYED The final client has finalized the driver. DSP_EACCESSDENIED The DSPLink driver was not setup in this process. DSP_ESETUP The DSPLink driver was not setup. DSP_EMEMORY Operation failed due to memory error. DSP_EFAIL General failure.
Precondition:
All DSP/BIOS Link operations are complete.
Postcondition:
None
See also:
PROC_setup ============================================================================
DLLEXPORT DSP_STATUS PROC_attach ( IN ProcessorId  procId,
PROC_Attrs attr 
)

Attaches the client to the specified DSP and also initializes the DSP (if required).

============================================================================

Function:
PROC_attach
Parameters:
procIdDSP identifier.
attrAttributes for the processor on which attach is to be done.
Returns:
DSP_SOK Operation successfully completed. DSP_SALREADYATTACHED Successful attach. Also, indicates that another client has already attached to DSP. DSP_EINVALIDARG Parameter ProcId is invalid. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_EALREADYCONNECTED Another thread of the same process has already attached to the processor. DSP_EWRONGSTATE Incorrect state for completing the requested operation. DSP_EFAIL General failure, unable to attach to processor.
Precondition:
procId must be valid. PROC_setup has been successful.
Postcondition:
None
See also:
PROC_detach ============================================================================
DLLEXPORT DSP_STATUS PROC_detach ( IN ProcessorId  procId )

Detaches the client from specified processor. If the caller is the owner of the processor, this function releases all the resources that this component uses and puts the DSP in an unusable state (from application perspective).

============================================================================

Function:
PROC_detach
Parameters:
procIdDSP identifier.
Returns:
DSP_SOK Operation successfully completed. DSP_SDETACHED The final process has detached from the specific processor. DSP_EINVALIDARG Invalid ProcId parameter. DSP_ESETUP The DSPLink driver was not setup. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_EATTACHED Not attached to the target processor. DSP_EWRONGSTATE Incorrect state for completing the requested operation. DSP_EFAIL General failure, unable to detach.
Precondition:
procId must be valid. All DSP/BIOS Link operations are complete.
Postcondition:
None
See also:
PROC_attach ============================================================================
DLLEXPORT DSP_STATUS PROC_getState ( IN ProcessorId  procId,
OUT PROC_State procState 
)

Gets the current status of DSP by querying the Link Driver.

============================================================================

Function:
PROC_getState
Parameters:
procIdDSP identifier.
procStatePlaceholder for processor state.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid ProcId and/or procState argument.
Precondition:
procId must be valid. procState must be a valid pointer.
Postcondition:
None
See also:
PROC_load, PROC_start, PROC_stop, PROC_Idle ============================================================================
DLLEXPORT DSP_STATUS PROC_load ( IN ProcessorId  procId,
IN Char8 imagePath,
IN Uint32  argc,
IN Char8 **  argv 
)

Loads the specified DSP executable on the target DSP. It ensures that the caller owns the DSP.

============================================================================

Function:
PROC_load
Parameters:
procIdDSP identifier.
imagePathFull path to the image file to load on DSP.
argcNumber of argument to be passed to the base image upon start.
argvArguments to be passed to DSP main application.
Returns:
DSP_SOK Operation successfully completed. DSP_SALREADYLOADED The specified processor has already been loaded. DSP_EINVALIDARG Invalid ProcId argument. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_ESETUP The DSPLink driver has not been setup. DSP_EATTACHED This process has not attached to the specified processor. DSP_EPENDING H/W specific error. The request can’t be serviced at this point of time. DSP_EFILE Invalid base image. DSP_ESIZE Size of the .args section is not sufficient to hold the passed arguments. DSP_EFAIL General failure, unable to load image on DSP. DSP_EWRONGSTATE Incorrect state for completing the requested operation.
Precondition:
procId must be valid. imagePath must be a valid pointer. If argc is 0 then argv must be NULL pointer. If argc is non-zero then argv must be a valid pointer. PROC_setup and PROC_attach have been successful.
Postcondition:
None
See also:
PROC_attach, PROC_loadSection ============================================================================
DLLEXPORT DSP_STATUS PROC_loadSection ( IN ProcessorId  procId,
IN Char8 imagePath,
IN Uint32  sectID 
)

Loads the specified section of DSP executable onto the target DSP. It ensures that the client owns the DSP.

============================================================================

Function:
PROC_loadSection
Parameters:
procIdDSP identifier.
imagePathFull path to the image file.
sectIDSection ID of section to load.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid ProcId argument. DSP_EPENDING H/W specific error. The request can’t be serviced at this point of time. DSP_EFILE Invalid ImagePath parameter. DSP_EINVALIDSECTION Invalid section name. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_EFAIL General failure, unable to load section on DSP. DSP_EWRONGSTATE Incorrect state for completing the requested operation.
Precondition:
procId must be valid. imagePath must be a valid pointer. PROC_attach has been successful.
Postcondition:
None
See also:
PROC_attach, PROC_load ============================================================================
DLLEXPORT DSP_STATUS PROC_read ( IN ProcessorId  procId,
IN Uint32  dspAddr,
IN Uint32  numBytes,
IN OUT Pvoid  buffer 
)

This function allows GPP side applications to read from the DSP memory space.

============================================================================

Function:
PROC_read
Parameters:
procIdProcessor ID of the target DSP.
dspAddrAddress of the DSP memory region from where to read.
numBytesNumber of bytes to be read
bufferUser specified buffer to contain the data from DSP memory space
Returns:
DSP_SOK Operation successfully completed. DSP_EPENDING H/W specific error. The request can’t be serviced at this point of time. DSP_EINVALIDARG Invalid argument. DSP_EFAIL General failure, unable to load section on DSP.
Precondition:
procId must be valid. buffer must be valid. PROC_attach has been successful. For DM642, the memory region must be mapped to GPP address space.
Postcondition:
None
See also:
PROC_write ============================================================================
DLLEXPORT DSP_STATUS PROC_write ( IN ProcessorId  procId,
IN Uint32  dspAddr,
IN Uint32  numBytes,
IN Pvoid  buffer 
)

This function allows GPP side applications to write to the DSP memory space.

============================================================================

Function:
PROC_write
Parameters:
procIdProcessor ID of the target DSP.
dspAddrAddress of the DSP memory region from where the data is to be written to.
numBytesNumber of bytes to be written
bufferUser specified buffer with data to be written into DSP memory space
Returns:
DSP_SOK Operation successfully completed. DSP_EPENDING H/W specific error. The request can’t be serviced at this point of time. DSP_EINVALIDARG Invalid argument. DSP_EFAIL General failure, unable to load section on DSP.
Precondition:
procId must be valid. buffer must be valid. PROC_attach has been successful. For DM642, the memory region must be mapped to GPP address space.
Postcondition:
None
See also:
PROC_read ============================================================================
DLLEXPORT DSP_STATUS PROC_start ( IN ProcessorId  procId )

Starts execution of the loaded code on DSP from the starting point specified in the DSP executable loaded earlier by call to PROC_load ().

============================================================================

Function:
PROC_start
Parameters:
procIdDSP Identifier.
Returns:
DSP_SOK Operation successfully completed. DSP_SALREADYSTARTED The specified processor has already been started. DSP_EINVALIDARG Invalid ProcId argument. DSP_EPENDING H/W specific error. The request can’t be serviced at this point of time. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_ESETUP The DSPLink driver has not been setup. DSP_EATTACHED This process has not attached to the specified processor. DSP_EALREADYSTARTED The specified processor has already been started in this process DSP_EWRONGSTATE Incorrect state for completing the requested operation. DSP_ECONFIG The specified processor could not be started. Driver handshake failed due to DSP driver initialization/configuration failure. DSP_EFAIL General failure, unable to start DSP.
Precondition:
procId must be valid. PROC_attach has been successful. If the application uses POOL, POOL_open i.e POOL configuration has been successful. All setup and initialization needed for DSP to start execution has been done.
Postcondition:
None
See also:
PROC_attach, PROC_load, PROC_stop ============================================================================
DLLEXPORT DSP_STATUS PROC_stop ( IN ProcessorId  procId )

Stops the DSP.

============================================================================

Function:
PROC_stop
Parameters:
procIdDSP Identifier.
Returns:
DSP_SOK Operation successfully completed. DSP_SSTOPPED The final process has stopped the DSP execution. DSP_EINVALIDARG Invalid ProcId argument. DSP_EACCESSDENIED Not allowed to access the DSP. DSP_ESETUP The DSPLink driver has not been setup. DSP_EATTACHED This process has not attached to the specified processor. DSP_ESTARTED The specified processor has not been started. DSP_EWRONGSTATE Incorrect state for completing the requested operation. DSP_EFAIL General failure, unable to stop DSP.
Precondition:
procId must be valid. All DSP/BIOS Link operations are complete.
Postcondition:
None
See also:
PROC_attach, PROC_load, PROC_start ============================================================================
DLLEXPORT DSP_STATUS PROC_control ( IN ProcessorId  procId,
IN Int32  cmd,
Pvoid  arg 
)

Provides a hook to perform device dependent control operations on the DSP.

============================================================================

Function:
PROC_control
Parameters:
procIdDSP Identifier.
cmdCommand id.
argOptional argument for the specified command.
Returns:
DSP_SOK Operation successfully completed. DSP_EFAIL General failure.
Precondition:
procId must be valid. PROC_attach has been successful.
Postcondition:
None
See also:
PROC_attach ============================================================================
DLLEXPORT DSP_STATUS PROC_GetSymbolAddress ( IN ProcessorId  procId,
IN Char8 symbolName,
OUT Uint32 dspAddr 
)

Gets the DSP address corresponding to a symbol within a DSP executable currently loaded on the DSP.

============================================================================

Function:
PROC_GetSymbolAddress
Parameters:
procIdDSP Identifier.
symbolNamename of the symbol.
dspAddrpointer to get the dsp address corresponding to symbolName.
Modifies:
None ============================================================================
DLLEXPORT DSP_STATUS PROC_sendTerminateEvent ( IN ProcessorId  procId )

Send an IPS terminate event to the DSP.

============================================================================

Function:
PROC_sendTerminateEvent
Parameters:
procIdDSP Identifier.
Returns:
DSP_SOK Operation successfully completed. DSP_EFAIL General failure. DSP_EINVALIDARG Given procId is invalid.
Precondition:
procId must be valid. PROC_start has been successful.
Postcondition:
None
See also:
PROC_start ============================================================================
DLLEXPORT DSP_STATUS PROC_Setup ( void   )

============================================================================

Deprecated:
The deprecated API POOL_TranslateAddr has been replaced with POOL_translateAddr. This has been done to follow DSP/BIOS codinf guidelines and have a uniform naming convention for the API's on both GPP as well as DSP.

============================================================================

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated