Defines | Functions

ringio.h File Reference

#include <dsplink.h>
#include <ringiodefs.h>
Include dependency graph for gpp/inc/ringio.h:

Go to the source code of this file.

Defines

#define RingIO_getAcquiredOffset(client)   (((RingIO_Client *) client)->acqStart)
 Returns the current acquire offset for the client.
#define RingIO_getAcquiredSize(client)   (((RingIO_Client *) client)->acqSize)
 Returns the size of buffer currently acquired.
#define RingIO_getWatermark(client)   (((RingIO_Client *) client)->notifyWaterMark)
 Returns the current watermark level specified by the client.
#define RingIO_init(procId)   RINGIO_SUCCESS
 This function initializes the RingIO component. This function has been deprecated and is provided for backward compatibility.
#define RingIO_exit(procId)   RINGIO_SUCCESS
 This function finalizes the RingIO component. This function has been deprecated and is provided for backward compatibility.

Functions

DLLEXPORT Uint32 RingIO_getValidSize (IN RingIO_Handle handle)
 Returns the current valid data size.
DLLEXPORT Uint32 RingIO_getEmptySize (IN RingIO_Handle handle)
 Returns the current empty buffer size.
DLLEXPORT Uint32 RingIO_getValidAttrSize (IN RingIO_Handle handle)
 Returns the current valid attribute size.
DLLEXPORT Uint32 RingIO_getEmptyAttrSize (IN RingIO_Handle handle)
 Returns the current empty attribute buffer size.
DLLEXPORT DSP_STATUS RingIO_create (IN ProcessorId procId, IN Char8 *name, IN RingIO_Attrs *attrs)
 This function creates a RingIO instance in Shared memory using the creation params specified.
DLLEXPORT DSP_STATUS RingIO_delete (IN ProcessorId procId, IN Char8 *name)
 This function deletes a RingIO channel.
DLLEXPORT RingIO_Handle RingIO_open (IN Char8 *name, IN RingIO_OpenMode openMode, IN Uint32 flags)
 This function opens a RingIO channel. This function is used to open an RingIO Channel either for reading or writing. Only one reader and one writer can be opened on a RingIO.
DLLEXPORT DSP_STATUS RingIO_close (IN RingIO_Handle handle)
 This function closes a RingIO instance.
DLLEXPORT DSP_STATUS RingIO_acquire (IN RingIO_Handle handle, OUT RingIO_BufPtr *dataBuf, IN OUT Uint32 *size)
 This function acquires a data buffer from RingIO for reading or writing, depending on the mode in which the client (represented by the handle) has been opened.
DLLEXPORT DSP_STATUS RingIO_release (IN RingIO_Handle handle, IN Uint32 size)
 This function releases a data buffer to RingIO. This function releases an acquired buffer or part of it.
DLLEXPORT DSP_STATUS RingIO_cancel (IN RingIO_Handle handle)
 This function cancels any data buffers acquired by reader or writer. In the case of writer, all attributes that are set since the first acquire are removed. In the case of reader, all attributes that were obtained since the first acquired are re-instated in the RingIO instance.
DLLEXPORT DSP_STATUS RingIO_getvAttribute (IN RingIO_Handle handle, OUT Uint16 *type, OUT Uint32 *param, IN RingIO_BufPtr vptr, IN OUT Uint32 *size)
 This function gets an attribute with a variable-sized payload from the attribute buffer. If an attribute is present, the attribute type, the optional parameter, a pointer to the optional payload and the payload size are returned.
DLLEXPORT DSP_STATUS RingIO_setvAttribute (IN RingIO_Handle handle, IN Uint32 offset, IN Uint16 type, IN Uint32 param, IN RingIO_BufPtr pdata, IN Uint32 size)
 This function sets an attribute with a variable sized payload at the offset provided in the acquired data buffer. If the offset is not in the range of the acquired data buffer, the attribute is not set, and an error is returned. One exception to this rule is when no data buffer has been acquired. In this case an attribute is set at the next data buffer offset that can be acquired.
DLLEXPORT DSP_STATUS RingIO_getAttribute (IN RingIO_Handle handle, OUT Uint16 *type, OUT Uint32 *param)
 This function gets a fixed-size attribute from the attribute buffer. If an attribute is present, the attribute type and a related parameter are returned.
DLLEXPORT DSP_STATUS RingIO_setAttribute (IN RingIO_Handle handle, IN Uint32 offset, IN Uint16 type, IN Uint32 param)
 This function sets a fixed-size attribute at the offset provided in the acquired data buffer. If the offset is not in the range of the acquired data buffer, the attribute is not set, and an error is returned. One exception to this rule is when no data buffer has been acquired. In this case an attribute is set at the next data buffer offset that can be acquired.
DLLEXPORT DSP_STATUS RingIO_flush (IN RingIO_Handle handle, IN Bool hardFlush, OUT Uint16 *type, OUT Uint32 *param, OUT Uint32 *bytesFlushed)
 This function flushes the data buffer. This function is used to flush the data from the RingIO. Behavior of this function depends on the value of hardFlush argument When hardFlush is false: If function is called for the writer, all the valid data in buffer after the first attribute location will be discarded. In case there are no attributes, no data will be cleared from the buffer. Note that this does not include the data that has been already acquired by the reader. Note that the attribute will also be cleared from the attribute buffer. For the reader, all the data till the next attribute location will be discarded. And if there is no attribute in the buffer, all valid data will get discarded. Note that the attribute will remain the attribute buffer. This is different from the behavior mentioned for the writer. When hardFlush is true: If function is called from the writer, all committed data and attributes that is not acquired by reader are removed from the RingIO instance. The writer pointer is moved to point to reader's head pointer If function is called from the reader, all data and attributes that can be subsequently acquired from the reader are removed.
DLLEXPORT DSP_STATUS RingIO_setNotifier (IN RingIO_Handle handle, IN RingIO_NotifyType notifyType, IN Uint32 notifyWatermark, IN RingIO_NotifyFunc notifyFunc, IN RingIO_NotifyParam notifyParam)
 This function sets Notification parameters for the RingIO Client. Both the reader and writer can set their notification mechanism using this function.
DLLEXPORT DSP_STATUS RingIO_sendNotify (IN RingIO_Handle handle, IN RingIO_NotifyMsg msg)
 Send a notification to the other client manually.

Define Documentation

#define RingIO_getAcquiredOffset (   client )    (((RingIO_Client *) client)->acqStart)

Returns the current acquire offset for the client.

============================================================================

Function:
RingIO_getAcquiredOffset
Parameters:
handleHandle to the RingIO Client.
Returns:
<client's current acquired offset>
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
#define RingIO_getAcquiredSize (   client )    (((RingIO_Client *) client)->acqSize)

Returns the size of buffer currently acquired.

============================================================================

Function:
RingIO_getAcquiredSize
Parameters:
handleHandle to the RingIO Client.
Returns:
<current acquired="" buffer="" size>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
#define RingIO_getWatermark (   client )    (((RingIO_Client *) client)->notifyWaterMark)

Returns the current watermark level specified by the client.

============================================================================

Function:
RingIO_getWatermark
Parameters:
handleHandle to the RingIO Client.
Returns:
<current watermark="" level="" set="" by="" the="" client>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle)
Postcondition:
None.
See also:
None. ============================================================================
#define RingIO_init (   procId )    RINGIO_SUCCESS

This function initializes the RingIO component. This function has been deprecated and is provided for backward compatibility.

============================================================================

Deprecated:
RingIO_init
Parameters:
procIdProcessor Id
Returns:
RINGIO_SUCCESS Operation successfully completed.
Precondition:
None.
Postcondition:
None.
See also:
None. ============================================================================
#define RingIO_exit (   procId )    RINGIO_SUCCESS

This function finalizes the RingIO component. This function has been deprecated and is provided for backward compatibility.

============================================================================

Deprecated:
RingIO_exit
Parameters:
procIdProcessor Id
Returns:
RINGIO_SUCCESS Operation successfully completed.
Precondition:
None.
Postcondition:
None.
See also:
None. ============================================================================

Function Documentation

DLLEXPORT Uint32 RingIO_getValidSize ( IN RingIO_Handle  handle )

Returns the current valid data size.

============================================================================

Function:
RingIO_getValidSize
Parameters:
handleHandle to the RingIO Client.
Returns:
<current valid="" data="" size>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT Uint32 RingIO_getEmptySize ( IN RingIO_Handle  handle )

Returns the current empty buffer size.

============================================================================

Function:
RingIO_getEmptySize
Parameters:
handleHandle to the RingIO Client.
Returns:
<current empty="" buffer="" size>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT Uint32 RingIO_getValidAttrSize ( IN RingIO_Handle  handle )

Returns the current valid attribute size.

============================================================================

Function:
RingIO_getValidAttrSize
Parameters:
handleHandle to the RingIO Client.
Returns:
<current valid="" attribute="" size>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT Uint32 RingIO_getEmptyAttrSize ( IN RingIO_Handle  handle )

Returns the current empty attribute buffer size.

============================================================================

Function:
RingIO_getEmptyAttrSize
Parameters:
handleHandle to the RingIO Client.
Returns:
<current empty="" attribute="" buffer="" size>="">
Precondition:
client must be a valid pointer(i.e valid RingIO Handle).
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_create ( IN ProcessorId  procId,
IN Char8 name,
IN RingIO_Attrs attrs 
)

This function creates a RingIO instance in Shared memory using the creation params specified.

============================================================================

Function:
RingIO_create
Parameters:
procIdProcessor Identifier (Not available in legacy suuport)
nameUnique name identifying the RingIO instance.
attrsPointer to the RingIO creation attributes.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments. DSP_EACCESSDENIED The RINGIO component has not been initialized. DSP_EMEMORY Operation failed due to a memory error. RINGIO_EALREADYEXISTS The specified RINGIO name is already in use. DSP_EFAIL General failure.
Precondition:
RINGIO name must be valid. RINGIO creation attributes must be a valid. PROC_attach has been successful. Application specific POOL configuration is complete.
Postcondition:
None.
See also:
RINGIO_delete. ============================================================================
DLLEXPORT DSP_STATUS RingIO_delete ( IN ProcessorId  procId,
IN Char8 name 
)

This function deletes a RingIO channel.

============================================================================

Function:
RingIO_delete
Parameters:
procIdProcessor Identifier (Not available in legacy suuport)
nameName of the RingIO channel to be deleted.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EALREADYEXISTS The specified RINGIO name is already in use. DSP_EACCESSDENIED The RINGIO component has not been initialized. DSP_EFAIL General failure.
Precondition:
RINGIO name must be valid. All RINGIO operations are complete.
Postcondition:
None.
See also:
RINGIO_create. ============================================================================
DLLEXPORT RingIO_Handle RingIO_open ( IN Char8 name,
IN RingIO_OpenMode  openMode,
IN Uint32  flags 
)

This function opens a RingIO channel. This function is used to open an RingIO Channel either for reading or writing. Only one reader and one writer can be opened on a RingIO.

============================================================================

Function:
RingIO_open
Parameters:
nameName of the RingIO channel to be opened.
openModeMode with which the RingIO channel is to be opened (Reader/Writer).
flagsCache usage and other notifification flags.
Returns:
Handle to the RingIO client structure. Operation successfully completed. NULL General failure, name not found.
Precondition:
RINGIO name must be valid. openMode must be either RINGIO_MODE_READ or RINGIO_MODE_WRITE RINGIO_create has been successful.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_close ( IN RingIO_Handle  handle )

This function closes a RingIO instance.

============================================================================

Function:
RingIO_close
Parameters:
handleHandle to the RingIO Client.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments. DSP_EACCESSDENIED The RINGIO component has not been initialized. DSP_EFAIL General failure.
Precondition:
handle must be valid. All RINGIO operations are complete.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_acquire ( IN RingIO_Handle  handle,
OUT RingIO_BufPtr dataBuf,
IN OUT Uint32 size 
)

This function acquires a data buffer from RingIO for reading or writing, depending on the mode in which the client (represented by the handle) has been opened.

============================================================================

Function:
RingIO_acquire
Parameters:
handleHandle to the RingIO Client.
dataBufLocation to store the pointer to the acquired data buffer.
sizePointer to the size of data buffer acquired. Holds the size of buffer to be acquired. Returns the size of buffer actually acquired.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_SPENDINGATTRIBUTE No data buffer could be acquired because an attribute was present at the current read offset. RINGIO_EBUFFULL Requested size of data buffer could not be returned because the total available size is less than requested size. A smaller sized buffer may have been returned, if available. RINGIO_EBUFWRAP Requested size of data buffer could not be returned because the available contiguous size till end of buffer is less than requested size. A smaller sized buffer may have been returned, if available. RINGIO_EFAILURE General failure. RINGIO_ENOTCONTIGUOUSDATA Valid data is present but is not contiguous because the data has been acquired using the foot buffer.
Precondition:
handle must be valid. dataBuf must be a valid pointer. size must be a valid pointer. RINGIO_open (for reading/writing) has been successful.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_release ( IN RingIO_Handle  handle,
IN Uint32  size 
)

This function releases a data buffer to RingIO. This function releases an acquired buffer or part of it.

============================================================================

Function:
RingIO_release
Parameters:
handleHandle to the RingIO Client.
sizeSize of data buffer to be released.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments.
Precondition:
RINGIO_acquire has been successful.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_cancel ( IN RingIO_Handle  handle )

This function cancels any data buffers acquired by reader or writer. In the case of writer, all attributes that are set since the first acquire are removed. In the case of reader, all attributes that were obtained since the first acquired are re-instated in the RingIO instance.

============================================================================

Function:
RingIO_cancel
Parameters:
handleHandle to the RingIO Client.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure.
Precondition:
handle must be valid. RINGIO_acquire has been successful.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_getvAttribute ( IN RingIO_Handle  handle,
OUT Uint16 type,
OUT Uint32 param,
IN RingIO_BufPtr  vptr,
IN OUT Uint32 size 
)

This function gets an attribute with a variable-sized payload from the attribute buffer. If an attribute is present, the attribute type, the optional parameter, a pointer to the optional payload and the payload size are returned.

============================================================================

Function:
RingIO_getvAttribute
Parameters:
handleHandle to the RingIO Client.
typeLocation to receive the user-defined type of attribute.
paramLocation to receive an optional parameter which depends on the attribute type.
vptrPointer to buffer to receive the optional payload.
sizeLocation with the size of the variable attribute. On return, this stores the actual size of the payload.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_SPENDINGATTRIBUTE Additional attributes are present at the current read offset. RINGIO_EVARIABLEATTRIBUTE No buffer has been provided to receive the variable attribute payload. RINGIO_EPENDINGDATA More data must be read before reading the attribute. RINGIO_EFAILURE No valid attributes are present, or general failure. DSP_EINVALIDARG Invalid arguments.
Precondition:
handle must be a valid pointer. type must be valid. param must be valid. RingIO_setvAttribute has been successful.
Postcondition:
None.
See also:
RingIO_getAttribute () ============================================================================
DLLEXPORT DSP_STATUS RingIO_setvAttribute ( IN RingIO_Handle  handle,
IN Uint32  offset,
IN Uint16  type,
IN Uint32  param,
IN RingIO_BufPtr  pdata,
IN Uint32  size 
)

This function sets an attribute with a variable sized payload at the offset provided in the acquired data buffer. If the offset is not in the range of the acquired data buffer, the attribute is not set, and an error is returned. One exception to this rule is when no data buffer has been acquired. In this case an attribute is set at the next data buffer offset that can be acquired.

============================================================================

Function:
RingIO_setvAttribute
Parameters:
handleHandle to the RingIO Client.
offsetOffset in the acquired data buffer to which the attribute corresponds
typeUser-defined type of attribute.
paramOptional parameter which depends on the attribute type.
pdataPointer to attribute payload buffer.
sizeSize of the attribute payload.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments. RINGIO_EWRONGSTATE Failure to set attribute when data buffer is full with valid data and buffer is wrapped around.
Precondition:
handle must be a valid pointer.
Postcondition:
None.
See also:
RingIO_setAttribute (), RingIO_getvAttribute () ============================================================================
DLLEXPORT DSP_STATUS RingIO_getAttribute ( IN RingIO_Handle  handle,
OUT Uint16 type,
OUT Uint32 param 
)

This function gets a fixed-size attribute from the attribute buffer. If an attribute is present, the attribute type and a related parameter are returned.

============================================================================

Function:
RingIO_getAttribute
Parameters:
handleHandle to the RingIO Client.
typeLocation to receive the user-defined type of attribute.
paramLocation to receive an optional parameter which depends on the attribute type.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_SPENDINGATTRIBUTE Additional attributes are present at the current read offset. RINGIO_EVARIABLEATTRIBUTE A variable atrtibute exists. The application must call RingIO_getvAttribute () to get the variable attribute. RINGIO_EPENDINGDATA More data must be read before reading the attribute. RINGIO_EFAILURE No valid attributes are present, or general failure.
Precondition:
handle must be a valid pointer. type must be valid. param must be valid. RingIO_setAttribute has been successful.
Postcondition:
None.
See also:
RingIO_getvAttribute () ============================================================================
DLLEXPORT DSP_STATUS RingIO_setAttribute ( IN RingIO_Handle  handle,
IN Uint32  offset,
IN Uint16  type,
IN Uint32  param 
)

This function sets a fixed-size attribute at the offset provided in the acquired data buffer. If the offset is not in the range of the acquired data buffer, the attribute is not set, and an error is returned. One exception to this rule is when no data buffer has been acquired. In this case an attribute is set at the next data buffer offset that can be acquired.

============================================================================

Function:
RingIO_setAttribute
Parameters:
handleHandle to the RingIO Client.
offsetOffset in the acquired data buffer to which the attribute corresponds
typeUser-defined type of attribute.
paramOptional parameter which depends on the attribute type.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments.
Precondition:
handle must be valid.
Postcondition:
None.
See also:
RingIO_setvAttribute (), RingIO_getAttribute () ============================================================================
DLLEXPORT DSP_STATUS RingIO_flush ( IN RingIO_Handle  handle,
IN Bool  hardFlush,
OUT Uint16 type,
OUT Uint32 param,
OUT Uint32 bytesFlushed 
)

This function flushes the data buffer. This function is used to flush the data from the RingIO. Behavior of this function depends on the value of hardFlush argument When hardFlush is false: If function is called for the writer, all the valid data in buffer after the first attribute location will be discarded. In case there are no attributes, no data will be cleared from the buffer. Note that this does not include the data that has been already acquired by the reader. Note that the attribute will also be cleared from the attribute buffer. For the reader, all the data till the next attribute location will be discarded. And if there is no attribute in the buffer, all valid data will get discarded. Note that the attribute will remain the attribute buffer. This is different from the behavior mentioned for the writer. When hardFlush is true: If function is called from the writer, all committed data and attributes that is not acquired by reader are removed from the RingIO instance. The writer pointer is moved to point to reader's head pointer If function is called from the reader, all data and attributes that can be subsequently acquired from the reader are removed.

============================================================================

Function:
RingIO_flush
Parameters:
handleHandle to the RingIO Client.
hardFlushMode in which the flush operation discards committed data and attributes
typeLocation to receive the User-defined type of attribute.
paramLocation to receive an optional parameter which depends on the attribute type.
bytesFlushedLocation to recieve the size of the buffer flushed.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments.
Precondition:
handle must be a valid pointer. type must be valid. param must be valid.
Postcondition:
None.
See also:
None. ============================================================================
DLLEXPORT DSP_STATUS RingIO_setNotifier ( IN RingIO_Handle  handle,
IN RingIO_NotifyType  notifyType,
IN Uint32  notifyWatermark,
IN RingIO_NotifyFunc  notifyFunc,
IN RingIO_NotifyParam  notifyParam 
)

This function sets Notification parameters for the RingIO Client. Both the reader and writer can set their notification mechanism using this function.

============================================================================

Function:
RingIO_setNotifier
Parameters:
handleHandle to the RingIO client.
notifyTypeType of notification.
notifyWatermarkWatermark for notification
notifyFuncFunction to call when notification is required
notifyParamPointer to the notification parameter. The type of the pointer and its size depends on the notification function
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure. DSP_EINVALIDARG Invalid arguments.
Precondition:
RingIO_open for both reader and writer has been successful. No DSP/BIOS Link API should be called from a callback function registered through the RingIO or NOTIFY module. On DSP-side or on operating systems such as PrOS, the callback functions are run from ISR context and must not perform any operations that may take a lock or block, which is done by most DSPLink APIs. Minimum functionality must be used in the callback functions, most often limited to posting a semaphore on which application is waiting, posting SWI etc.
Postcondition:
None.
See also:
RingIO_NotifyType, RingIO_NotifyFunc, RingIO_NotifyParam ============================================================================
DLLEXPORT DSP_STATUS RingIO_sendNotify ( IN RingIO_Handle  handle,
IN RingIO_NotifyMsg  msg 
)

Send a notification to the other client manually.

============================================================================

Function:
RingIO_sendNotify
Parameters:
handleHandle to the RingIO Client. arg msg Message to be sent along with notification.
Returns:
RINGIO_SUCCESS Operation successfully completed. RINGIO_EFAILURE General failure.
Precondition:
None.
Postcondition:
None.
See also:
None. ============================================================================
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated