AM65X_SR1 DMA Device Descriptions

Introduction

This chapter provides information on the DMA devices in the AM6 SoC. Some System Firmware TISCI messages take device specific inputs. This chapter provides information on the valid values for DMA TISCI message parameters.

DMA Device IDs

Some System Firmware TISCI message APIs require the DMA device ID be provided as part of the request. Based on AM6 Device IDs these are the valid DMA device IDs.

DMA Device Name DMA Device ID
AM6_DEV_NAVSS0_UDMAP0 188
AM6_DEV_MCU_NAVSS0_UDMAP0 194

DMA Channel and Flow Indices

This section describes valid DMA channel indexes for each DMA channel type. Receive flow index range type information is also described if applicable to the DMA being described.

Warning

Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.

navss0_udmap0

Tx Channel Type Tx Channel Index Range
TX_HCHAN (RESERVED BY SYSTEM FIRMWARE) 0 to 0
TX_HCHAN 1 to 7
TX_CHAN 8 to 119
TX_ECHAN 120 to 151
Rx Channel Type Rx Channel Index Range
RX_HCHAN (RESERVED BY SYSTEM FIRMWARE) 0 to 1
RX_HCHAN 2 to 7
RX_CHAN 8 to 149

NOTE: The host that owns configurable, also known as common or shared, flows is able to delegate them to another host for configuration in order to aid some use case configurations. The configurable flows can be delegated using TISCI_MSG_RM_UDMAP_FLOW_DELEGATE

Rx Flow Type Rx Flow Index Range
DEFAULT (RESERVED BY SYSTEM FIRMWARE) 0 to 1
DEFAULT 2 to 149
CONFIGURABLE 150 to 299

mcu_navss0_udmap0

Tx Channel Type Tx Channel Index Range
TX_HCHAN 0 to 1
TX_CHAN 2 to 47
Rx Channel Type Rx Channel Index Range
RX_HCHAN 0 to 1
RX_CHAN 2 to 47
Rx Flow Type Rx Flow Index Range
DEFAULT 0 to 47
CONFIGURABLE 48 to 95