Derived KEK TISCI Description¶
This chapter provides information on System Firmware API for Derived Key Encryption Key(DKEK) management. The available API are listed below.
| TISCI Message ID | Message Name | Available in GP | Avialable in HS-FS | Previous Message Name | 
|---|---|---|---|---|
| 0x9003 | TISCI_MSG_CRYPTO_SET_DKEK | Yes* | Yes | TISCI_MSG_SA2UL_SET_DKEK | 
| 0x9004 | TISCI_MSG_CRYPTO_RELEASE_DKEK | Yes* | Yes | TISCI_MSG_SA2UL_RELEASE_DKEK | 
| 0x9029 | TISCI_MSG_CRYPTO_GET_DKEK | Yes* | Yes | TISCI_MSG_SA2UL_GET_DKEK | 
Note
The TISCI Message ID macros have been renamed. Please update your code to use the new names.
On GP devices, DKEK APIs return unconditional success but do not actually involve any step to derive or program the DKEK values
This document must be read along side
- Using Derived KEK on HS devices and
 - Security Board Configuration, specifically Derived KEK Management
 
API Description¶
TISCI Message ID¶
TISCI_MSG_CRYPTO_SET_DKEK          (0x9003U)
Message to derive a KEK and set DKEK register
struct tisci_msg_crypto_set_dkek_req
TISCI Request for setting DKEK in crypto engine registers
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
| instance | u8 | crypto engine instance number - set to 0 | 
| kdf_label_len | u8 | Length of “Label” input to KDF | 
| kdf_context_len | u8 | Length of “Context” input to KDF | 
| kdf_label_and_context | u8 | ”Label” and “Context” bytes are stored in this array one after another. Maximum length of this field is KDF_LABEL_AND_CONTEXT_LEN_MAX | 
struct tisci_msg_crypto_set_dkek_resp
TISCI Response for setting DKEK in crypto engine registers
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
KDF_LABEL_AND_CONTEXT_LEN_MAX          41U
Note
The structures tisci_msg_sa2ul_set_dkek_req and tisci_msg_sa2ul_set_dkek_resp have been renamed to tisci_msg_crypto_set_dkek_req and tisci_msg_crypto_set_dkek_resp respectively.
Please update your code to use the new names.
See API Notes below.
TISCI Message ID¶
TISCI_MSG_CRYPTO_RELEASE_DKEK          (0x9004U)
Message to erase the DKEK register
struct tisci_msg_crypto_release_dkek_req
TISCI Request for releasing DKEK
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
| instance | u8 | Crypto instance number - set to 0 | 
struct tisci_msg_crypto_release_dkek_resp
TISCI Response for Releasing DKEK
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
Note
The structures tisci_msg_sa2ul_release_dkek_req and tisci_msg_sa2ul_release_dkek_resp have been renamed to tisci_msg_crypto_release_dkek_req and tisci_msg_crypto_release_dkek_resp respectively.
Please update your code to use the new names.
See API Notes below.
TISCI Message ID¶
TISCI_MSG_CRYPTO_GET_DKEK          (0x9029U)
Message to derive a KEK and return it via TISCI
CRYPTO_DKEK_KEY_LEN          (32U)
struct tisci_msg_crypto_get_dkek_req
TISCI Request for getting DKEK via TISCI
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
| instance | u8 | Crypto engine instance number - set to 0 | 
| kdf_label_len | u8 | Length of “Label” input to KDF | 
| kdf_context_len | u8 | Length of “Context” input to KDF | 
| kdf_label_and_context | u8 | ”Label” and “Context” bytes are stored in this array one after another. Maximum length of this field is KDF_LABEL_AND_CONTEXT_LEN_MAX | 
struct tisci_msg_crypto_get_dkek_resp
TISCI Response for requesting DKEK
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Generic TISCI message header. | 
| dkek | u8 | Array containing Derived KEK. Length is 32 bytes | 
Note
The structures tisci_msg_sa2ul_get_dkek_req and tisci_msg_sa2ul_get_dkek_resp have been renamed to tisci_msg_crypto_get_dkek_req and tisci_msg_crypto_get_dkek_resp respectively.
Also, the MACRO SA2UL_DKEK_KEY_LEN has been renamed to CRYPTO_DKEK_KEY_LEN.
Please update your code to use the new names.
See API Notes below.
API Notes¶
- The total length of the Label and Context fields below is limited by the size of the TISCI messages(see Secure Messaging Header) to 41 bytes.
 - System Firmware only support 
instancevalue of 0 in the API below.