EDGEAI API
Data Fields
DAP_PipelineConfiguration Struct Reference

DAP pipeline configuration. More...

#include <ti/ai/edge_ai/dap/DAP.h>

Collaboration diagram for DAP_PipelineConfiguration:
Collaboration graph

Data Fields

DAP_PipelineMode mode
 
uint8_t inferenceModelIndex
 
uint8_t inferenceSensorsIndex [10]
 

Detailed Description

DAP pipeline configuration.

This structure holds the configuration for the application pipeline. The host is in charge of sending a DAP command with the pipline configuration.

Field Documentation

§ mode

DAP_PipelineMode DAP_PipelineConfiguration::mode

§ inferenceModelIndex

uint8_t DAP_PipelineConfiguration::inferenceModelIndex

§ inferenceSensorsIndex

uint8_t DAP_PipelineConfiguration::inferenceSensorsIndex[10]

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale