EDGEAI API
Data Structures | Enumerations | Functions
DAP.h File Reference

Detailed Description

PRELIMINARY DAP for EdgeAI

PRELIMINARY DAP interface


WARNING These APIs are PRELIMINARY, and subject to change in the next few months.

To use the DAP, include this header file in the application as follows:

#include <ti/ai/edge_ai/DAP.h>

Overview

The Device Agent Protocol (DAP) is a serial communication protocol using packets that facilitates interaction between Edge AI Studio (the host) and TI Microcontrollers (the target devices). This protocol is specifically designed to support edge AI applications.

Communication follows a controller-responder model where the host initiates all transfers or commands, and the target device must acknowledge each command with a response. Depending on the command type, the target may send additional responses.

Application execution is controlled by the host through a variety of commands. The application can be configured to operate in one of four distinct pipeline modes, as specified in the DAP_PipelineMode enumeration.

Configuration details specific to each pipeline mode are maintained in the DAP_PipelineConfiguration structure. To retrieve this configuration information, the DAP_getPipelineConfiguration() function can be utilized.

Depending on the active operation mode, the host may request various types of data from the target device. The readiness for data streaming can be determined using the DAP_isReadyToStartStreaming function. When streaming is available, data transmission is performed via the DAP_sendData() function. The DAP_SendDataType enumeration defines the supported data types for transmission.

Design Architecture

This protocol operates in duplex mode, enabling simultaneous transmission and reception of data packets. The implementation achieves this capability by separating functionality into dedicated RX (receiving) and TX (transmitting) tasks.

The RX task is in charge of receiving the packets, decoding them and constructing the response packet. The response packet is then posted in a message queue shared with the TX task.

The TX task is in charge of reading packets from the message queue and sending them over to the host through the transport layer.

The transport layer utilizes a serial communication protocol, with its backend implementation located in the ti/ai/edge_ai/dap/core/DAP_core.h file.


Usage

To use the DAP the application calls the following APIs:


This file contains data from the application, to be modified by the user.

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/UART2.h>
#include <ti/drivers/dpl/MessageQueueP.h>
Include dependency graph for DAP.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  DAP_PipelineConfiguration
 DAP pipeline configuration. More...
 
struct  DAP_Handle
 DAP configuration. More...
 

Enumerations

enum  DAP_PipelineMode {
  DAP_PIPELINE_MODE_UNINITIALIZED = 0x00,
  DAP_PIPELINE_MODE_DATA_ACQUISITION = 0x01,
  DAP_PIPELINE_MODE_SENSOR_INFERENCING = 0x02,
  DAP_PIPELINE_MODE_HOST_INFERENCING = 0x03,
  DAP_PIPELINE_MODE_LOOPBACK = 0x04
}
 DAP pipeline modes. More...
 
enum  DAP_SendDataType {
  DAP_SEND_DATA_TYPE_SENSOR_SIGNAL = 0x01,
  DAP_SEND_DATA_TYPE_INFERENCING_SIGNAL = 0x03,
  DAP_SEND_DATA_TYPE_INFERENCING_RESULT = 0x04,
  DAP_SEND_DATA_TYPE_INFERENCING_VALUE = 0x05,
  DAP_SEND_DATA_TYPE_INFERENCING_LOG = 0x06
}
 

Functions

float DAP_swapEndianness (float value)
 Swap Endianess value to support the endianess format expected by EdgeAI Studio. More...
 
void DAP_init (void)
 Initialize the DAP. More...
 
void DAP_open (void)
 Open the DAP. More...
 
DAP_PipelineConfiguration DAP_getPipelineConfiguration (void)
 Get Pipeline Configuration. More...
 
uint32_t DAP_getSamplesToSend (void)
 Get samples to send. More...
 
uint32_t DAP_getSamplingFrequency (void)
 Get samplign frequency. More...
 
bool DAP_isReadyToStartStreaming (void)
 Check if the DAP is ready for data streaming. More...
 
void DAP_sendData (DAP_SendDataType sendDataType, void *data, size_t dataSize)
 Send Data to host. More...
 

Enumeration Type Documentation

§ DAP_PipelineMode

DAP pipeline modes.

This enum defines the modes of operation for the application inferencing pipeline.

Enumerator
DAP_PIPELINE_MODE_UNINITIALIZED 

Mode not yet initialized

DAP_PIPELINE_MODE_DATA_ACQUISITION 

Real time data acquisition streaming from a sensor.

DAP_PIPELINE_MODE_SENSOR_INFERENCING 

Real time inferencing streaming from a sensor.

DAP_PIPELINE_MODE_HOST_INFERENCING 

Non-real time inferencing streaming from the host.

DAP_PIPELINE_MODE_LOOPBACK 

Non-real time streaming data from the host back to the host.

§ DAP_SendDataType

Enumerator
DAP_SEND_DATA_TYPE_SENSOR_SIGNAL 

Raw sensor output sent from target device to the host.

DAP_SEND_DATA_TYPE_INFERENCING_SIGNAL 

Output signal from inferencing, same format as sensor signal data.

DAP_SEND_DATA_TYPE_INFERENCING_RESULT 

The result from inferencing, like object detection regions or classification class.

DAP_SEND_DATA_TYPE_INFERENCING_VALUE 

Inferencing values like average cpu usage, or inferencing time.

DAP_SEND_DATA_TYPE_INFERENCING_LOG 

Textual log for displaying to the user during live demo.

Function Documentation

§ DAP_swapEndianness()

float DAP_swapEndianness ( float  value)

Swap Endianess value to support the endianess format expected by EdgeAI Studio.

Parameters
[in]valueScalar float value to be modified.

§ DAP_init()

void DAP_init ( void  )

Initialize the DAP.

§ DAP_open()

void DAP_open ( void  )

Open the DAP.

Initialize the serial protocol, the message queue, and the RX and TX tasks.

§ DAP_getPipelineConfiguration()

DAP_PipelineConfiguration DAP_getPipelineConfiguration ( void  )

Get Pipeline Configuration.

Returns
Returns a structure with the pipeline configuration

§ DAP_getSamplesToSend()

uint32_t DAP_getSamplesToSend ( void  )

Get samples to send.

Returns
Returns the number of samples to send to the host

§ DAP_getSamplingFrequency()

uint32_t DAP_getSamplingFrequency ( void  )

Get samplign frequency.

Returns
Returns the sampling frequency in hertz

§ DAP_isReadyToStartStreaming()

bool DAP_isReadyToStartStreaming ( void  )

Check if the DAP is ready for data streaming.

Returns
Returns if the DAP is ready for data streaming

§ DAP_sendData()

void DAP_sendData ( DAP_SendDataType  sendDataType,
void *  data,
size_t  dataSize 
)

Send Data to host.

Parameters
[in]sendDataTypeType of the data sent
[in]datapointer to a buffer with the data
[in]dataSizesize of the data buffer in bytes
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale