#include <ADCBufMSP432E4.h>
§ mutex
SemaphoreP_Handle ADCBufMSP432E4_Object::mutex |
§ convertComplete
SemaphoreP_Handle ADCBufMSP432E4_Object::convertComplete |
§ sequencerHwiHandles
HwiP_Handle ADCBufMSP432E4_Object::sequencerHwiHandles[4] |
§ pingpongFlag
uint_fast8_t ADCBufMSP432E4_Object::pingpongFlag[4] |
§ channelCount
uint_fast8_t ADCBufMSP432E4_Object::channelCount[4] |
§ conversions
§ callBackFxn
§ sampleBuffer
uint16_t* ADCBufMSP432E4_Object::sampleBuffer[4] |
§ sampleIndex
uint_fast16_t ADCBufMSP432E4_Object::sampleIndex[4] |
§ sampleCount
uint_fast16_t ADCBufMSP432E4_Object::sampleCount[4] |
§ samplingDuration
§ semaphoreTimeout
uint32_t ADCBufMSP432E4_Object::semaphoreTimeout |
§ samplingFrequency
uint32_t ADCBufMSP432E4_Object::samplingFrequency |
§ recurrenceMode
§ returnMode
§ dmaHandle
§ isOpen
bool ADCBufMSP432E4_Object::isOpen |
The documentation for this struct was generated from the following file: