NVS driver implementation for MSP432E4 devices.
============================================================================
This NVS driver implementation is designed to work with FLASH memory on MSP432E4 devices. FLASH memory sectors on these devices are 16 kilobytes in size.
The NVS header file should be included in an application as follows:
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
struct | NVSMSP432E4_HWAttrs |
NVSMSP432E4 attributes. More... | |
struct | NVSMSP432E4_Object |
Variables | |
const NVS_FxnTable | NVSMSP432E4_fxnTable |
const NVS_FxnTable NVSMSP432E4_fxnTable |