![]() |
![]() |
CRC driver implementation for MSP432E4.
============================================================================
The CRC header file should be included in an application as follows:
This driver supports the following CRCs:
This driver supports only the following size options. Data processing is only supported for CRC_DATA_SIZE_32BIT.
Go to the source code of this file.
Data Structures | |
struct | CRCMSP432E4_Object |
CRCMSP432E4 Hardware Attributes. More... | |