CRCMSP432E4.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
59 #ifndef ti_drivers_crc_CRCMSP432E4__include
60 #define ti_drivers_crc_CRCMSP432E4__include
61 
62 #include <stdint.h>
63 #include <stdbool.h>
64 
65 #include <ti/drivers/CRC.h>
66 
67 #ifdef __cplusplus
68 extern "C" {
69 #endif
70 
83 typedef struct {
85  uint32_t timeout;
86  uint32_t seed;
87  uint32_t finalXorValue;
88  uint32_t configRegister;
90  uint32_t resultRawPartial;
95  uint8_t isOpen;
96  uint8_t ongoingPartial;
98 
99 #ifdef __cplusplus
100 }
101 #endif
102 
103 #endif /* ti_drivers_crc_CRCMSP432E4__include */
CRC_ByteSwap byteSwapInput
Definition: CRCMSP432E4.h:93
uint32_t finalXorValue
Definition: CRCMSP432E4.h:87
CRC_ReturnBehavior
The way in which CRC function calls return after completing.
Definition: CRC.h:329
uint32_t timeout
Definition: CRCMSP432E4.h:85
void * resultLocation
Definition: CRCMSP432E4.h:89
uint32_t seed
Definition: CRCMSP432E4.h:86
CRC_ByteSwap
These byte swapping configurations are primarily for dealing with endianness mismatch. Not all implementations support all configurations.
Definition: CRC.h:384
CRC_DataSize
The CRC driver will consume data in blocks of this size. Not all implementations support all sizes...
Definition: CRC.h:395
uint32_t resultProcessedPartial
Definition: CRCMSP432E4.h:91
uint32_t resultRawPartial
Definition: CRCMSP432E4.h:90
void(* CRC_CallbackFxn)(CRC_Handle handle, int_fast16_t status, void *result)
The definition of a callback function used by the CRC driver when used in CALLBACK mode...
Definition: CRC.h:412
CRC_DataSize dataSize
Definition: CRCMSP432E4.h:92
CRC driver interface.
uint8_t isOpen
Definition: CRCMSP432E4.h:95
CRC_ReturnBehavior returnBehavior
Definition: CRCMSP432E4.h:94
CRC_CallbackFxn callbackFxn
Definition: CRCMSP432E4.h:84
uint32_t configRegister
Definition: CRCMSP432E4.h:88
CRCMSP432E4 Hardware Attributes.
Definition: CRCMSP432E4.h:83
uint8_t ongoingPartial
Definition: CRCMSP432E4.h:96
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale