![]() |
![]() |
MSP432E4 DriverLib API Guide
1.11.00.03
|
Functions | |
void | I2CMasterInitExpClk (uint32_t ui32Base, uint32_t ui32I2CClk, bool bFast) |
void | I2CSlaveInit (uint32_t ui32Base, uint8_t ui8SlaveAddr) |
void | I2CSlaveAddressSet (uint32_t ui32Base, uint8_t ui8AddrNum, uint8_t ui8SlaveAddr) |
void | I2CMasterEnable (uint32_t ui32Base) |
void | I2CSlaveEnable (uint32_t ui32Base) |
void | I2CMasterDisable (uint32_t ui32Base) |
void | I2CSlaveDisable (uint32_t ui32Base) |
void | I2CIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
void | I2CIntUnregister (uint32_t ui32Base) |
void | I2CMasterIntEnable (uint32_t ui32Base) |
void | I2CMasterIntEnableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
void | I2CSlaveIntEnable (uint32_t ui32Base) |
void | I2CSlaveIntEnableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
void | I2CMasterIntDisable (uint32_t ui32Base) |
void | I2CMasterIntDisableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
void | I2CSlaveIntDisable (uint32_t ui32Base) |
void | I2CSlaveIntDisableEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
bool | I2CMasterIntStatus (uint32_t ui32Base, bool bMasked) |
uint32_t | I2CMasterIntStatusEx (uint32_t ui32Base, bool bMasked) |
bool | I2CSlaveIntStatus (uint32_t ui32Base, bool bMasked) |
uint32_t | I2CSlaveIntStatusEx (uint32_t ui32Base, bool bMasked) |
void | I2CMasterIntClear (uint32_t ui32Base) |
void | I2CMasterIntClearEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
void | I2CSlaveIntClear (uint32_t ui32Base) |
void | I2CSlaveIntClearEx (uint32_t ui32Base, uint32_t ui32IntFlags) |
void | I2CMasterSlaveAddrSet (uint32_t ui32Base, uint8_t ui8SlaveAddr, bool bReceive) |
uint32_t | I2CMasterLineStateGet (uint32_t ui32Base) |
bool | I2CMasterBusy (uint32_t ui32Base) |
bool | I2CMasterBusBusy (uint32_t ui32Base) |
void | I2CMasterControl (uint32_t ui32Base, uint32_t ui32Cmd) |
uint32_t | I2CMasterErr (uint32_t ui32Base) |
void | I2CMasterDataPut (uint32_t ui32Base, uint8_t ui8Data) |
uint32_t | I2CMasterDataGet (uint32_t ui32Base) |
void | I2CMasterTimeoutSet (uint32_t ui32Base, uint32_t ui32Value) |
void | I2CSlaveACKOverride (uint32_t ui32Base, bool bEnable) |
void | I2CSlaveACKValueSet (uint32_t ui32Base, bool bACK) |
uint32_t | I2CSlaveStatus (uint32_t ui32Base) |
void | I2CSlaveDataPut (uint32_t ui32Base, uint8_t ui8Data) |
uint32_t | I2CSlaveDataGet (uint32_t ui32Base) |
void | I2CTxFIFOConfigSet (uint32_t ui32Base, uint32_t ui32Config) |
void | I2CTxFIFOFlush (uint32_t ui32Base) |
void | I2CRxFIFOConfigSet (uint32_t ui32Base, uint32_t ui32Config) |
void | I2CRxFIFOFlush (uint32_t ui32Base) |
uint32_t | I2CFIFOStatus (uint32_t ui32Base) |
void | I2CFIFODataPut (uint32_t ui32Base, uint8_t ui8Data) |
uint32_t | I2CFIFODataPutNonBlocking (uint32_t ui32Base, uint8_t ui8Data) |
uint32_t | I2CFIFODataGet (uint32_t ui32Base) |
uint32_t | I2CFIFODataGetNonBlocking (uint32_t ui32Base, uint8_t *pui8Data) |
void | I2CMasterBurstLengthSet (uint32_t ui32Base, uint8_t ui8Length) |
uint32_t | I2CMasterBurstCountGet (uint32_t ui32Base) |
void | I2CMasterGlitchFilterConfigSet (uint32_t ui32Base, uint32_t ui32Config) |
void | I2CSlaveFIFOEnable (uint32_t ui32Base, uint32_t ui32Config) |
void | I2CSlaveFIFODisable (uint32_t ui32Base) |
void | I2CLoopbackEnable (uint32_t ui32Base) |
The Inter-Integrated Circuit (I2C) API provides a set of functions for using the MSP432E4 I2C master and slave modules. Functions are provided to initialize the I2C modules, to send and receive data, obtain status, and to manage interrupts for the I2C modules.
The I2C master and slave modules provide the ability to communicate to other IC devices over an I2C bus. The I2C bus is specified to support devices that can both transmit and receive (write and read) data. Also, devices on the I2C bus can be designated as either a master or a slave. The MSP432E4 I2C modules support both sending and receiving data as either a master or a slave, and also support the simultaneous operation as both a master and a slave. Finally, the MSP432E4 I2C modules can operate at the following speeds: Standard (100 kbps), Fast (400 kbps), Fast plus (1 Mbps) and High Speed (3.33 Mbps).
Both the master and slave I2C modules can generate interrupts. The I2C master module generates interrupts when a transmit or receive operation is completed (or aborted due to an error); and on some devices when a clock low timeout has occurred. The I2C slave module generates interrupts when data has been sent or requested by a master; and on some devices, when a START or STOP condition is present.
When using this API to drive the I2C master module, the user must first initialize the I2C master module with a call to I2CMasterInitExpClk(). That function sets the bus speed and enables the master module.
The user may transmit or receive data after the successful initialization of the I2C master module. Data is transferred by first setting the slave address using I2CMasterSlaveAddrSet(). That function is also used to define whether the transfer is a send (a write to the slave from the master) or a receive (a read from the slave by the master). Then, if connected to an I2C bus that has multiple masters, the MSP432E4 I2C master must first call I2CMasterBusBusy() before attempting to initiate the desired transaction. After determining that the bus is not busy, if trying to send data, the user must call the I2CMasterDataPut() function. The transaction can then be initiated on the bus by calling the I2CMasterControl() function with any of the following commands:
Any of those commands results in the master arbitrating for the bus, driving the start sequence onto the bus, and sending the slave address and direction bit across the bus. The remainder of the transaction can then be driven using either a polling or interrupt-driven method.
For the single send and receive cases, the polling method involves looping on the return from I2CMasterBusy(). Once that function indicates that the I2C master is no longer busy, the bus transaction has been completed and can be checked for errors using I2CMasterErr(). If there are no errors, then the data has been sent or is ready to be read using I2CMasterDataGet(). For the burst send and receive cases, the polling method also involves calling the I2CMasterControl() function for each byte transmitted or received (using either the I2C_MASTER_CMD_BURST_SEND_CONT or I2C_MASTER_CMD_BURST_RECEIVE_CONT commands), and for the last byte sent or received (using either the I2C_MASTER_CMD_BURST_SEND_FINISH or I2C_MASTER_CMD_BURST_RECEIVE_FINISH commands). If any error is detected during the burst transfer, the I2CMasterControl() function should be called using the appropriate stop command (I2C_MASTER_CMD_BURST_SEND_ERROR_STOP or I2C_MASTER_CMD_BURST_RECEIVE_ERROR_STOP).
For the interrupt-driven transaction, the user must register an interrupt handler for the I2C devices and enable the I2C master interrupt; the interrupt occurs when the master is no longer busy.
When using this API to drive the I2C slave module, the user must first initialize the I2C slave module with a call to I2CSlaveInit(). This function enables the I2C slave module and initializes the slave's own address. After the initialization is complete, the user may poll the slave status using I2CSlaveStatus() to determine if a master requested a send or receive operation. Depending on the type of operation requested, the user can call I2CSlaveDataPut() or I2CSlaveDataGet() to complete the transaction. Alternatively, the I2C slave can handle transactions using an interrupt handler registered with I2CIntRegister(), and by enabling the I2C slave interrupt.
The I2C API is broken into three groups of functions: those that deal with interrupts, those that handle status and initialization, and those that deal with sending and receiving data.
The I2C master and slave interrupts are handled by the I2CIntRegister(), I2CIntUnregister(), I2CMasterIntEnable(), I2CMasterIntDisable(), I2CMasterIntClear(), I2CMasterIntStatus(), I2CSlaveIntEnable(), I2CSlaveIntDisable(), I2CSlaveIntClear(), I2CSlaveIntStatus(), I2CSlaveIntEnableEx(), I2CSlaveIntDisableEx(), I2CSlaveIntClearEx(), and I2CSlaveIntStatusEx() functions.
Status and initialization functions for the I2C modules are I2CMasterInitExpClk(), I2CMasterEnable(), I2CMasterDisable(), I2CMasterBusBusy(), I2CMasterBusy(), I2CMasterErr(), I2CSlaveInit(), I2CSlaveEnable(), I2CSlaveDisable(), and I2CSlaveStatus().
Sending and receiving data from the I2C modules are handled by the I2CMasterSlaveAddrSet(), I2CMasterControl(), I2CMasterDataGet(), I2CMasterDataPut(), I2CSlaveDataGet(), and I2CSlaveDataPut() functions.
The I2CMasterInit() API from previous versions of the peripheral driver library has been replaced by the I2CMasterInitExpClk() API. A macro has been provided in i2c.h
to map the old API to the new API, allowing existing applications to link and run with the new API. It is recommended that new applications utilize the new API in favor of the old one.
The following example shows how to use the I2C API to send data as a master for a TM4C123x device.
void I2CMasterInitExpClk | ( | uint32_t | ui32Base, |
uint32_t | ui32I2CClk, | ||
bool | bFast | ||
) |
Initializes the I2C Master block.
ui32Base | is the base address of the I2C module. |
ui32I2CClk | is the rate of the clock supplied to the I2C module. |
bFast | set up for fast data transfers. |
This function initializes operation of the I2C Master block by configuring the bus speed for the master and enabling the I2C Master block.
If the parameter bFast is true, then the master block is set up to transfer data at 400 Kbps; otherwise, it is set up to transfer data at 100 Kbps. If Fast Mode Plus (1 Mbps) is desired, software should manually write the I2CMTPR after calling this function. For High Speed (3.4 Mbps) mode, a specific command is used to switch to the faster clocks after the initial communication with the slave is done at either 100 Kbps or 400 Kbps.
The peripheral clock is the same as the processor clock. The frequency of the system clock is the value returned by SysCtlClockFreqSet(), or it can be explicitly hard coded if it is constant and known (to save the code/execution overhead of fetch of the variable call holding the return value of SysCtlClockFreqSet()).
References ASSERT, HWREG, I2C_MTPR_HS, I2C_O_MTPR, I2C_O_PP, I2C_PP_HS, and I2CMasterEnable().
void I2CSlaveInit | ( | uint32_t | ui32Base, |
uint8_t | ui8SlaveAddr | ||
) |
Initializes the I2C Slave block.
ui32Base | is the base address of the I2C module. |
ui8SlaveAddr | 7-bit slave address |
This function initializes operation of the I2C Slave block by configuring the slave address and enabling the I2C Slave block.
The parameter ui8SlaveAddr is the value that is compared against the slave address sent by an I2C master.
References ASSERT, HWREG, I2C_O_SOAR, and I2CSlaveEnable().
void I2CSlaveAddressSet | ( | uint32_t | ui32Base, |
uint8_t | ui8AddrNum, | ||
uint8_t | ui8SlaveAddr | ||
) |
Sets the I2C slave address.
ui32Base | is the base address of the I2C module. |
ui8AddrNum | determines which slave address is set. |
ui8SlaveAddr | is the 7-bit slave address |
This function writes the specified slave address. The ui32AddrNum field dictates which slave address is configured. For example, a value of 0 configures the primary address and a value of 1 configures the secondary.
References ASSERT, HWREG, I2C_O_SOAR, I2C_O_SOAR2, and I2C_SOAR2_OAR2EN.
void I2CMasterEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Master block.
ui32Base | is the base address of the I2C module. |
This function enables operation of the I2C Master block.
References ASSERT, HWREG, I2C_MCR_MFE, and I2C_O_MCR.
Referenced by I2CMasterInitExpClk().
void I2CSlaveEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Slave block.
ui32Base | is the base address of the I2C module. |
This fucntion enables operation of the I2C Slave block.
References ASSERT, HWREG, I2C_MCR_SFE, I2C_O_MCR, I2C_O_SCSR, and I2C_SCSR_DA.
Referenced by I2CSlaveInit().
void I2CMasterDisable | ( | uint32_t | ui32Base | ) |
Disables the I2C master block.
ui32Base | is the base address of the I2C module. |
This function disables operation of the I2C master block.
References ASSERT, HWREG, I2C_MCR_MFE, and I2C_O_MCR.
void I2CSlaveDisable | ( | uint32_t | ui32Base | ) |
Disables the I2C slave block.
ui32Base | is the base address of the I2C module. |
This function disables operation of the I2C slave block.
References ASSERT, HWREG, I2C_MCR_SFE, I2C_O_MCR, and I2C_O_SCSR.
void I2CIntRegister | ( | uint32_t | ui32Base, |
void(*)(void) | pfnHandler | ||
) |
Registers an interrupt handler for the I2C module.
ui32Base | is the base address of the I2C module. |
pfnHandler | is a pointer to the function to be called when the I2C interrupt occurs. |
This function sets the handler to be called when an I2C interrupt occurs. This function enables the global interrupt in the interrupt controller; specific I2C interrupts must be enabled via I2CMasterIntEnable() and I2CSlaveIntEnable(). If necessary, it is the interrupt handler's responsibility to clear the interrupt source via I2CMasterIntClear() and I2CSlaveIntClear().
References ASSERT.
void I2CIntUnregister | ( | uint32_t | ui32Base | ) |
Unregisters an interrupt handler for the I2C module.
ui32Base | is the base address of the I2C module. |
This function clears the handler to be called when an I2C interrupt occurs. This function also masks off the interrupt in the interrupt r controller so that the interrupt handler no longer is called.
References ASSERT.
void I2CMasterIntEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Master interrupt.
ui32Base | is the base address of the I2C module. |
This function enables the I2C Master interrupt source.
References ASSERT, HWREG, and I2C_O_MIMR.
void I2CMasterIntEnableEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Enables individual I2C Master interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is the bit mask of the interrupt sources to be enabled. |
This function enables the indicated I2C Master interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter is the logical OR of any of the following:
References ASSERT, HWREG, and I2C_O_MIMR.
void I2CSlaveIntEnable | ( | uint32_t | ui32Base | ) |
Enables the I2C Slave interrupt.
ui32Base | is the base address of the I2C module. |
This function enables the I2C Slave interrupt source.
References ASSERT, HWREG, I2C_O_SIMR, and I2C_SLAVE_INT_DATA.
void I2CSlaveIntEnableEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Enables individual I2C Slave interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is the bit mask of the interrupt sources to be enabled. |
This function enables the indicated I2C Slave interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter is the logical OR of any of the following:
References ASSERT, HWREG, and I2C_O_SIMR.
void I2CMasterIntDisable | ( | uint32_t | ui32Base | ) |
Disables the I2C Master interrupt.
ui32Base | is the base address of the I2C module. |
This function disables the I2C Master interrupt source.
References ASSERT, HWREG, and I2C_O_MIMR.
void I2CMasterIntDisableEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Disables individual I2C Master interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is the bit mask of the interrupt sources to be disabled. |
This function disables the indicated I2C Master interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter has the same definition as the ui32IntFlags parameter to I2CMasterIntEnableEx().
References ASSERT, HWREG, and I2C_O_MIMR.
void I2CSlaveIntDisable | ( | uint32_t | ui32Base | ) |
Disables the I2C Slave interrupt.
ui32Base | is the base address of the I2C module. |
This function disables the I2C Slave interrupt source.
References ASSERT, HWREG, I2C_O_SIMR, and I2C_SLAVE_INT_DATA.
void I2CSlaveIntDisableEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Disables individual I2C Slave interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is the bit mask of the interrupt sources to be disabled. |
This function disables the indicated I2C Slave interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter has the same definition as the ui32IntFlags parameter to I2CSlaveIntEnableEx().
References ASSERT, HWREG, and I2C_O_SIMR.
bool I2CMasterIntStatus | ( | uint32_t | ui32Base, |
bool | bMasked | ||
) |
Gets the current I2C Master interrupt status.
ui32Base | is the base address of the I2C module. |
bMasked | is false if the raw interrupt status is requested and true if the masked interrupt status is requested. |
This function returns the interrupt status for the I2C module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
References ASSERT, HWREG, I2C_O_MMIS, and I2C_O_MRIS.
uint32_t I2CMasterIntStatusEx | ( | uint32_t | ui32Base, |
bool | bMasked | ||
) |
Gets the current I2C Master interrupt status.
ui32Base | is the base address of the I2C module. |
bMasked | is false if the raw interrupt status is requested and true if the masked interrupt status is requested. |
This function returns the interrupt status for the I2C module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
References ASSERT, HWREG, I2C_O_MMIS, and I2C_O_MRIS.
bool I2CSlaveIntStatus | ( | uint32_t | ui32Base, |
bool | bMasked | ||
) |
Gets the current I2C Slave interrupt status.
ui32Base | is the base address of the I2C module. |
bMasked | is false if the raw interrupt status is requested and true if the masked interrupt status is requested. |
This function returns the interrupt status for the I2C Slave. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
References ASSERT, HWREG, I2C_O_SMIS, and I2C_O_SRIS.
uint32_t I2CSlaveIntStatusEx | ( | uint32_t | ui32Base, |
bool | bMasked | ||
) |
Gets the current I2C Slave interrupt status.
ui32Base | is the base address of the I2C module. |
bMasked | is false if the raw interrupt status is requested and true if the masked interrupt status is requested. |
This function returns the interrupt status for the I2C Slave. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
References ASSERT, HWREG, I2C_O_SMIS, and I2C_O_SRIS.
void I2CMasterIntClear | ( | uint32_t | ui32Base | ) |
Clears I2C Master interrupt sources.
ui32Base | is the base address of the I2C module. |
The I2C Master interrupt source is cleared, so that it no longer asserts. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.
References ASSERT, HWREG, I2C_MICR_IC, I2C_O_MICR, and I2C_O_MMIS.
void I2CMasterIntClearEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Clears I2C Master interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is a bit mask of the interrupt sources to be cleared. |
The specified I2C Master interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.
The ui32IntFlags parameter has the same definition as the ui32IntFlags parameter to I2CMasterIntEnableEx().
References ASSERT, HWREG, and I2C_O_MICR.
void I2CSlaveIntClear | ( | uint32_t | ui32Base | ) |
Clears I2C Slave interrupt sources.
ui32Base | is the base address of the I2C module. |
The I2C Slave interrupt source is cleared, so that it no longer asserts. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.
References ASSERT, HWREG, I2C_O_SICR, and I2C_SICR_DATAIC.
void I2CSlaveIntClearEx | ( | uint32_t | ui32Base, |
uint32_t | ui32IntFlags | ||
) |
Clears I2C Slave interrupt sources.
ui32Base | is the base address of the I2C module. |
ui32IntFlags | is a bit mask of the interrupt sources to be cleared. |
The specified I2C Slave interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.
The ui32IntFlags parameter has the same definition as the ui32IntFlags parameter to I2CSlaveIntEnableEx().
References ASSERT, HWREG, and I2C_O_SICR.
void I2CMasterSlaveAddrSet | ( | uint32_t | ui32Base, |
uint8_t | ui8SlaveAddr, | ||
bool | bReceive | ||
) |
Sets the address that the I2C Master places on the bus.
ui32Base | is the base address of the I2C module. |
ui8SlaveAddr | 7-bit slave address |
bReceive | flag indicating the type of communication with the slave |
This function configures the address that the I2C Master places on the bus when initiating a transaction. When the bReceive parameter is set to true, the address indicates that the I2C Master is initiating a read from the slave; otherwise the address indicates that the I2C Master is initiating a write to the slave.
uint32_t I2CMasterLineStateGet | ( | uint32_t | ui32Base | ) |
Reads the state of the SDA and SCL pins.
ui32Base | is the base address of the I2C module. |
This function returns the state of the I2C bus by providing the real time values of the SDA and SCL pins.
References ASSERT, HWREG, and I2C_O_MBMON.
bool I2CMasterBusy | ( | uint32_t | ui32Base | ) |
Indicates whether or not the I2C Master is busy.
ui32Base | is the base address of the I2C module. |
This function returns an indication of whether or not the I2C Master is busy transmitting or receiving data.
References ASSERT, HWREG, I2C_MCS_BUSY, and I2C_O_MCS.
bool I2CMasterBusBusy | ( | uint32_t | ui32Base | ) |
Indicates whether or not the I2C bus is busy.
ui32Base | is the base address of the I2C module. |
This function returns an indication of whether or not the I2C bus is busy. This function can be used in a multi-master environment to determine if another master is currently using the bus.
References ASSERT, HWREG, I2C_MCS_BUSBSY, and I2C_O_MCS.
void I2CMasterControl | ( | uint32_t | ui32Base, |
uint32_t | ui32Cmd | ||
) |
Controls the state of the I2C Master.
ui32Base | is the base address of the I2C module. |
ui32Cmd | command to be issued to the I2C Master. |
This function is used to control the state of the Master send and receive operations. The ui8Cmd parameter can be one of the following values:
References ASSERT, HWREG, I2C_MASTER_CMD_BURST_RECEIVE_CONT, I2C_MASTER_CMD_BURST_RECEIVE_ERROR_STOP, I2C_MASTER_CMD_BURST_RECEIVE_FINISH, I2C_MASTER_CMD_BURST_RECEIVE_START, I2C_MASTER_CMD_BURST_SEND_CONT, I2C_MASTER_CMD_BURST_SEND_ERROR_STOP, I2C_MASTER_CMD_BURST_SEND_FINISH, I2C_MASTER_CMD_BURST_SEND_START, I2C_MASTER_CMD_FIFO_BURST_RECEIVE_CONT, I2C_MASTER_CMD_FIFO_BURST_RECEIVE_ERROR_STOP, I2C_MASTER_CMD_FIFO_BURST_RECEIVE_FINISH, I2C_MASTER_CMD_FIFO_BURST_RECEIVE_START, I2C_MASTER_CMD_FIFO_BURST_SEND_CONT, I2C_MASTER_CMD_FIFO_BURST_SEND_ERROR_STOP, I2C_MASTER_CMD_FIFO_BURST_SEND_FINISH, I2C_MASTER_CMD_FIFO_BURST_SEND_START, I2C_MASTER_CMD_FIFO_SINGLE_RECEIVE, I2C_MASTER_CMD_FIFO_SINGLE_SEND, I2C_MASTER_CMD_HS_MASTER_CODE_SEND, I2C_MASTER_CMD_QUICK_COMMAND, I2C_MASTER_CMD_SINGLE_RECEIVE, I2C_MASTER_CMD_SINGLE_SEND, and I2C_O_MCS.
uint32_t I2CMasterErr | ( | uint32_t | ui32Base | ) |
Gets the error status of the I2C Master.
ui32Base | is the base address of the I2C module. |
This function is used to obtain the error status of the Master send and receive operations.
References ASSERT, HWREG, I2C_MASTER_ERR_NONE, I2C_MCS_ADRACK, I2C_MCS_ARBLST, I2C_MCS_BUSY, I2C_MCS_DATACK, I2C_MCS_ERROR, and I2C_O_MCS.
void I2CMasterDataPut | ( | uint32_t | ui32Base, |
uint8_t | ui8Data | ||
) |
uint32_t I2CMasterDataGet | ( | uint32_t | ui32Base | ) |
Receives a byte that has been sent to the I2C Master.
ui32Base | is the base address of the I2C module. |
This function reads a byte of data from the I2C Master Data Register.
void I2CMasterTimeoutSet | ( | uint32_t | ui32Base, |
uint32_t | ui32Value | ||
) |
Sets the Master clock timeout value.
ui32Base | is the base address of the I2C module. |
ui32Value | is the number of I2C clocks before the timeout is asserted. |
This function enables and configures the clock low timeout feature in the I2C peripheral. This feature is implemented as a 12-bit counter, with the upper 8-bits being programmable. For example, to program a timeout of 20ms with a 100-kHz SCL frequency, ui32Value is 0x7d.
References ASSERT, HWREG, and I2C_O_MCLKOCNT.
void I2CSlaveACKOverride | ( | uint32_t | ui32Base, |
bool | bEnable | ||
) |
Configures ACK override behavior of the I2C Slave.
ui32Base | is the base address of the I2C module. |
bEnable | enables or disables ACK override. |
This function enables or disables ACK override, allowing the user application to drive the value on SDA during the ACK cycle.
References ASSERT, HWREG, I2C_O_SACKCTL, and I2C_SACKCTL_ACKOEN.
void I2CSlaveACKValueSet | ( | uint32_t | ui32Base, |
bool | bACK | ||
) |
Writes the ACK value.
ui32Base | is the base address of the I2C module. |
bACK | chooses whether to ACK (true) or NACK (false) the transfer. |
This function puts the desired ACK value on SDA during the ACK cycle. The value written is only valid when ACK override is enabled using I2CSlaveACKOverride().
References ASSERT, HWREG, I2C_O_SACKCTL, and I2C_SACKCTL_ACKOVAL.
uint32_t I2CSlaveStatus | ( | uint32_t | ui32Base | ) |
Gets the I2C Slave status
ui32Base | is the base address of the I2C module. |
This function returns the action requested from a master, if any. Possible values are:
References ASSERT, HWREG, and I2C_O_SCSR.
void I2CSlaveDataPut | ( | uint32_t | ui32Base, |
uint8_t | ui8Data | ||
) |
uint32_t I2CSlaveDataGet | ( | uint32_t | ui32Base | ) |
void I2CTxFIFOConfigSet | ( | uint32_t | ui32Base, |
uint32_t | ui32Config | ||
) |
Configures the I2C transmit (TX) FIFO.
ui32Base | is the base address of the I2C module. |
ui32Config | is the configuration of the FIFO using specified macros. |
This configures the I2C peripheral's transmit FIFO. The transmit FIFO can be used by the master or slave, but not both. The following macros are used to configure the TX FIFO behavior for master or slave, with or without DMA:
I2C_FIFO_CFG_TX_MASTER, I2C_FIFO_CFG_TX_SLAVE, I2C_FIFO_CFG_TX_MASTER_DMA, I2C_FIFO_CFG_TX_SLAVE_DMA
To select the trigger level, one of the following macros should be used:
I2C_FIFO_CFG_TX_TRIG_1, I2C_FIFO_CFG_TX_TRIG_2, I2C_FIFO_CFG_TX_TRIG_3, I2C_FIFO_CFG_TX_TRIG_4, I2C_FIFO_CFG_TX_TRIG_5, I2C_FIFO_CFG_TX_TRIG_6, I2C_FIFO_CFG_TX_TRIG_7, I2C_FIFO_CFG_TX_TRIG_8
References ASSERT, HWREG, and I2C_O_FIFOCTL.
void I2CTxFIFOFlush | ( | uint32_t | ui32Base | ) |
Flushes the transmit (TX) FIFO.
ui32Base | is the base address of the I2C module. |
This function flushes the I2C transmit FIFO.
References ASSERT, HWREG, I2C_FIFOCTL_TXFLUSH, and I2C_O_FIFOCTL.
void I2CRxFIFOConfigSet | ( | uint32_t | ui32Base, |
uint32_t | ui32Config | ||
) |
Configures the I2C receive (RX) FIFO.
ui32Base | is the base address of the I2C module. |
ui32Config | is the configuration of the FIFO using specified macros. |
This configures the I2C peripheral's receive FIFO. The receive FIFO can be used by the master or slave, but not both. The following macros are used to configure the RX FIFO behavior for master or slave, with or without DMA:
I2C_FIFO_CFG_RX_MASTER, I2C_FIFO_CFG_RX_SLAVE, I2C_FIFO_CFG_RX_MASTER_DMA, I2C_FIFO_CFG_RX_SLAVE_DMA
To select the trigger level, one of the following macros should be used:
I2C_FIFO_CFG_RX_TRIG_1, I2C_FIFO_CFG_RX_TRIG_2, I2C_FIFO_CFG_RX_TRIG_3, I2C_FIFO_CFG_RX_TRIG_4, I2C_FIFO_CFG_RX_TRIG_5, I2C_FIFO_CFG_RX_TRIG_6, I2C_FIFO_CFG_RX_TRIG_7, I2C_FIFO_CFG_RX_TRIG_8
References ASSERT, HWREG, and I2C_O_FIFOCTL.
void I2CRxFIFOFlush | ( | uint32_t | ui32Base | ) |
Flushes the receive (RX) FIFO.
ui32Base | is the base address of the I2C module. |
This function flushes the I2C receive FIFO.
References ASSERT, HWREG, I2C_FIFOCTL_RXFLUSH, and I2C_O_FIFOCTL.
uint32_t I2CFIFOStatus | ( | uint32_t | ui32Base | ) |
Gets the current FIFO status.
ui32Base | is the base address of the I2C module. |
This function retrieves the status for both the transmit (TX) and receive (RX) FIFOs. The trigger level for the transmit FIFO is set using I2CTxFIFOConfigSet() and for the receive FIFO using I2CTxFIFOConfigSet().
References ASSERT, HWREG, and I2C_O_FIFOSTATUS.
void I2CFIFODataPut | ( | uint32_t | ui32Base, |
uint8_t | ui8Data | ||
) |
Writes a data byte to the I2C transmit FIFO.
ui32Base | is the base address of the I2C module. |
ui8Data | is the data to be placed into the transmit FIFO. |
This function adds a byte of data to the I2C transmit FIFO. If there is no space available in the FIFO, this function waits for space to become available before returning.
References ASSERT, HWREG, I2C_FIFOSTATUS_TXFF, I2C_O_FIFODATA, and I2C_O_FIFOSTATUS.
uint32_t I2CFIFODataPutNonBlocking | ( | uint32_t | ui32Base, |
uint8_t | ui8Data | ||
) |
Writes a data byte to the I2C transmit FIFO.
ui32Base | is the base address of the I2C module. |
ui8Data | is the data to be placed into the transmit FIFO. |
This function adds a byte of data to the I2C transmit FIFO. If there is no space available in the FIFO, this function returns a zero.
References ASSERT, HWREG, I2C_FIFOSTATUS_TXFF, I2C_O_FIFODATA, and I2C_O_FIFOSTATUS.
uint32_t I2CFIFODataGet | ( | uint32_t | ui32Base | ) |
Reads a byte from the I2C receive FIFO.
ui32Base | is the base address of the I2C module. |
This function reads a byte of data from I2C receive FIFO and places it in the location specified by the pui8Data parameter. If there is no data available, this function waits until data is received before returning.
References ASSERT, HWREG, I2C_FIFOSTATUS_RXFE, I2C_O_FIFODATA, and I2C_O_FIFOSTATUS.
uint32_t I2CFIFODataGetNonBlocking | ( | uint32_t | ui32Base, |
uint8_t * | pui8Data | ||
) |
Reads a byte from the I2C receive FIFO.
ui32Base | is the base address of the I2C module. |
pui8Data | is a pointer where the read data is stored. |
This function reads a byte of data from I2C receive FIFO and places it in the location specified by the pui8Data parameter. If there is no data available, this functions returns 0.
References ASSERT, HWREG, I2C_FIFOSTATUS_RXFE, I2C_O_FIFODATA, and I2C_O_FIFOSTATUS.
void I2CMasterBurstLengthSet | ( | uint32_t | ui32Base, |
uint8_t | ui8Length | ||
) |
Set the burst length for a I2C master FIFO operation.
ui32Base | is the base address of the I2C module. |
ui8Length | is the length of the burst transfer. |
This function configures the burst length for a I2C Master FIFO operation. The burst field is limited to 8 bits or 256 bytes. The burst length applies to a single I2CMCS BURST operation meaning that it specifies the burst length for only the current operation (can be TX or RX). Each burst operation must configure the burst length prior to writing the BURST bit in the I2CMCS using I2CMasterControl().
References ASSERT, HWREG, and I2C_O_MBLEN.
uint32_t I2CMasterBurstCountGet | ( | uint32_t | ui32Base | ) |
Returns the current value of the burst transfer counter.
ui32Base | is the base address of the I2C module. |
This function returns the current value of the burst transfer counter that is used by the FIFO mechanism. Software can use this value to determine how many bytes remain in a transfer, or where in the transfer the burst operation was if an error has occurred.
References ASSERT, HWREG, and I2C_O_MBCNT.
void I2CMasterGlitchFilterConfigSet | ( | uint32_t | ui32Base, |
uint32_t | ui32Config | ||
) |
Configures the I2C Master glitch filter.
ui32Base | is the base address of the I2C module. |
ui32Config | is the glitch filter configuration. |
This function configures the I2C Master glitch filter. The value passed in to ui32Config determines the sampling range of the glitch filter, which is configurable between 1 and 32 system clock cycles. The default configuration of the glitch filter is 0 system clock cycles, which means that it's disabled.
The ui32Config field should be any of the following values:
References ASSERT, HWREG, and I2C_O_MTPR.
void I2CSlaveFIFOEnable | ( | uint32_t | ui32Base, |
uint32_t | ui32Config | ||
) |
Enables FIFO usage for the I2C Slave.
ui32Base | is the base address of the I2C module. |
ui32Config | is the desired FIFO configuration of the I2C Slave. |
This function configures the I2C Slave to use the FIFO(s). This function should be used in combination with I2CTxFIFOConfigSet() and/or I2CRxFIFOConfigSet(), which configure the FIFO trigger level and tell the FIFO hardware whether to interact with the I2C Master or Slave. The application appropriate combination of I2C_SLAVE_TX_FIFO_ENABLE and I2C_SLAVE_RX_FIFO_ENABLE should be passed in to the ui32Config field.
The Slave I2CSCSR register is write-only, so any call to I2CSlaveEnable(), I2CSlaveDisable or I2CSlaveFIFOEnable() overwrites the slave configuration. Therefore, application software should call I2CSlaveEnable() followed by I2CSlaveFIFOEnable() with the desired FIFO configuration.
References ASSERT, HWREG, I2C_O_SCSR, and I2C_SCSR_DA.
void I2CSlaveFIFODisable | ( | uint32_t | ui32Base | ) |
Disable FIFO usage for the I2C Slave.
ui32Base | is the base address of the I2C module. |
This function disables the FIFOs for the I2C Slave. After calling this this function, the FIFOs are disabled, but the Slave remains active.
References ASSERT, HWREG, I2C_O_SCSR, and I2C_SCSR_DA.
void I2CLoopbackEnable | ( | uint32_t | ui32Base | ) |
Enables internal loopback mode for an I2C port.
ui32Base | is the base address of the I2C module. |
This function configures an I2C port in internal loopback mode to help with diagnostics and debug. In this mode, the SDA and SCL signals from master and slave modules are internally connected. This allows data to be transferred between the master and slave modules of the same I2C port, without having to go through I/O's. I2CMasterDataPut(), I2CSlaveDataPut(), I2CMasterDataGet(),I2CSlaveDataGet() can be used along with this function.
References ASSERT, HWREG, I2C_MCR_LPBK, and I2C_O_MCR.