SimpleLink Graphics Library  4.11.00.04
Functions
RadioButton_api

Functions

void Graphics_drawRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 
bool Graphics_isRadioButtonSelected (const Graphics_RadioButton *radioButton, uint16_t x, uint16_t y)
 
void Graphics_drawSelectedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 
void Graphics_drawReleasedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton)
 

Detailed Description

Function Documentation

§ Graphics_drawRadioButton()

void Graphics_drawRadioButton ( const Graphics_Context context,
const Graphics_RadioButton radioButton 
)

Draws a RadioButton.

Parameters
contextis a pointer to the drawing context to use.
radioButtonis a pointer to the structure containing the extents of the RadioButton.

This function draws a RadioButton . The RadioButton will contain the image passed in the RadioButton struct.

Returns
None.

References AUTO_STRING_LENGTH, Graphics_RadioButton::font, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_RadioButton::gap, Graphics_drawCircle(), Graphics_drawString(), Graphics_fillCircle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_RadioButton::selected, Graphics_RadioButton::selectedColor, Graphics_RadioButton::text, Graphics_RadioButton::textColor, TRANSPARENT_TEXT, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.

§ Graphics_isRadioButtonSelected()

bool Graphics_isRadioButtonSelected ( const Graphics_RadioButton radioButton,
uint16_t  x,
uint16_t  y 
)

Determines if x and y coordinates are contained in RadioButton.

Parameters
radioButtonis a pointer to the structure containing the extents of the RadioButton.
xx-coordinate to be determined if is inside RadioButton
yy-coordinate to be determined if is inside RadioButton

This function determines if x and y coordinates are contains inside RadioButton.

Returns
true if x and y coordinates are inside RadioButton, false if not

References Graphics_RadioButton::font, Graphics_RadioButton::gap, Graphics_RadioButton::numbOfChar, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.

§ Graphics_drawSelectedRadioButton()

void Graphics_drawSelectedRadioButton ( const Graphics_Context context,
const Graphics_RadioButton radioButton 
)

Draws a selected RadioButton.

Parameters
contextis a pointer to the drawing context to use.
radioButtonis a pointer to the structure containing the extents of the RadioButton.

This function draws a RadioButton using the selected parameters.

Returns
None.

References Graphics_RadioButton::font, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_fillCircle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_RadioButton::selectedColor, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.

§ Graphics_drawReleasedRadioButton()

void Graphics_drawReleasedRadioButton ( const Graphics_Context context,
const Graphics_RadioButton radioButton 
)

Draws a released RadioButton.

Parameters
contextis a pointer to the drawing context to use.
radioButtonis a pointer to the structure containing the extents of the RadioButton.

This function draws a RadioButton using the released parameters.

Returns
None.

References Graphics_RadioButton::font, Graphics_Context::foreground, g_sContext, Graphics_fillCircle(), Graphics_setForegroundColor(), Graphics_RadioButton::notSelectedColor, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.

Copyright 2018, Texas Instruments Incorporated