![]() |
![]() |
ADCBufMSP432E4 Channel setting These fields define channel-specific settings: GPIO, reference voltage, temperature mode, etc. These settings happen when ADCBuf_convert() is called. More...
#include <ADCBufMSP432E4.h>
Data Fields | |
uint32_t | refVoltage |
uint_fast16_t | adcPin |
ADCBufMSP432E4_Sequencer | adcSequence |
ADCBufMSP432E4_DifferentialMode | adcInputMode |
ADCBufMSP432E4_InternalSourceMode | adcInternalSource |
uint_fast16_t | adcDifferentialPin |
ADCBufMSP432E4 Channel setting These fields define channel-specific settings: GPIO, reference voltage, temperature mode, etc. These settings happen when ADCBuf_convert() is called.
uint32_t ADCBufMSP432E4_Channels::refVoltage |
ADC reference voltage in microVolts
uint_fast16_t ADCBufMSP432E4_Channels::adcPin |
ADC pin, port channel
ADCBufMSP432E4_Sequencer ADCBufMSP432E4_Channels::adcSequence |
ADC sequencer
ADCBufMSP432E4_DifferentialMode ADCBufMSP432E4_Channels::adcInputMode |
ADC differential mode option
ADCBufMSP432E4_InternalSourceMode ADCBufMSP432E4_Channels::adcInternalSource |
ADC internal source mode select
uint_fast16_t ADCBufMSP432E4_Channels::adcDifferentialPin |
ADC differential pin, if adcInputMode = 1, specify pin