51 #ifndef ti_drivers_adcbuf_ADCBufMSP432E4__include 52 #define ti_drivers_adcbuf_ADCBufMSP432E4__include 62 #include <ti/drivers/dpl/HwiP.h> 63 #include <ti/drivers/dpl/SemaphoreP.h> 65 #include <ti/devices/msp432e4/driverlib/adc.h> 87 #define ADCBufMSP432E4_PB_4_A10 ((10 << 16) | 0x5910) 88 #define ADCBufMSP432E4_PB_5_A11 ((11 << 16) | 0x5920) 91 #define ADCBufMSP432E4_PD_0_A15 ((15 << 16) | 0x5B01) 92 #define ADCBufMSP432E4_PD_1_A14 ((14 << 16) | 0x5B02) 93 #define ADCBufMSP432E4_PD_2_A13 ((13 << 16) | 0x5B04) 94 #define ADCBufMSP432E4_PD_3_A12 ((12 << 16) | 0x5B08) 95 #define ADCBufMSP432E4_PD_4_A7 ((7 << 16) | 0x5B10) 96 #define ADCBufMSP432E4_PD_5_A6 ((6 << 16) | 0x5B20) 97 #define ADCBufMSP432E4_PD_6_A5 ((5 << 16) | 0x5B40) 98 #define ADCBufMSP432E4_PD_7_A4 ((4 << 16) | 0x5B80) 101 #define ADCBufMSP432E4_PE_0_A3 ((3 << 16) | 0x5C01) 102 #define ADCBufMSP432E4_PE_1_A2 ((2 << 16) | 0x5C02) 103 #define ADCBufMSP432E4_PE_2_A1 ((1 << 16) | 0x5C04) 104 #define ADCBufMSP432E4_PE_3_A0 ((0 << 16) | 0x5C08) 105 #define ADCBufMSP432E4_PE_4_A9 ((9 << 16) | 0x5C10) 106 #define ADCBufMSP432E4_PE_5_A8 ((8 << 16) | 0x5C20) 107 #define ADCBufMSP432E4_PE_6_A20 ((20 << 16) | 0x5C40) 108 #define ADCBufMSP432E4_PE_7_A21 ((21 << 16) | 0x5C80) 111 #define ADCBufMSP432E4_PK_0_A16 ((16 << 16) | 0x6101) 112 #define ADCBufMSP432E4_PK_1_A17 ((17 << 16) | 0x6102) 113 #define ADCBufMSP432E4_PK_2_A18 ((18 << 16) | 0x6104) 114 #define ADCBufMSP432E4_PK_3_A19 ((19 << 16) | 0x6108) 117 #define ADCBufMSP432E4_PP_6_A22 ((22 << 16) | 0x6540) 118 #define ADCBufMSP432E4_PP_7_A23 ((23 << 16) | 0x6580) 125 #define ADCBufMSP432E4_PIN_NONE 0 128 #define MSP432E4_NUM_ADC_CHANNELS (24) 131 #define ADCBufMSP432E4_SEQUENCER_COUNT 4 323 HwiP_Handle sequencerHwiHandles[4];
325 uint_fast8_t pingpongFlag[4];
326 uint_fast8_t channelCount[4];
331 uint16_t *sampleBuffer[4];
332 uint_fast16_t sampleIndex[4];
333 uint_fast16_t sampleCount[4];
Definition: ADCBufMSP432E4.h:203
uint32_t timerInstances
Definition: ADCBufMSP432E4.h:347
Definition: ADCBufMSP432E4.h:202
Definition: ADCBufMSP432E4.h:145
struct ADCBufMSP432E4_Object ADCBufMSP432E4_Object
ADCBufMSP432E4 Object.
struct ADCBufMSP432E4_TimerSettings ADCBufMSP432E4_TimerSettings
MSP432E4 specfic extension to ADCBuf_Params.
Definition: ADCBufMSP432E4.h:251
Definition: ADCBufMSP432E4.h:157
enum ADCBuf_Recurrence_Mode_ ADCBuf_Recurrence_Mode
ADC trigger mode settings.
UDMAMSP432E4 Global configuration.
Definition: UDMAMSP432E4.h:151
ADCBufMSP432E4 Channel setting These fields define channel-specific settings: GPIO, reference voltage, temperature mode, etc. These settings happen when ADCBuf_convert() is called.
Definition: ADCBufMSP432E4.h:261
Definition: ADCBufMSP432E4.h:228
ADCBufMSP432E4_InternalSourceMode
ADCBufMSP432E4 Internal Source Mode These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify if a...
Definition: ADCBufMSP432E4.h:167
const ADCBuf_FxnTable ADCBufMSP432E4_fxnTable
struct ADCBufMSP432E4_ParamsExtension ADCBufMSP432E4_ParamsExtension
MSP432E4 specfic extension to ADCBuf_Params.
SemaphoreP_Handle convertComplete
Definition: ADCBufMSP432E4.h:322
An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perf...
Definition: ADCBuf.h:237
uint32_t adcBase
Definition: ADCBufMSP432E4.h:305
ADCBufMSP432E4_Sequencer
ADCBufMSP432E4 Sequencer These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify which ADC seque...
Definition: ADCBufMSP432E4.h:155
uDMA driver implementation for MSP432E4.
ADCBuf_Callback callBackFxn
Definition: ADCBufMSP432E4.h:329
UDMAMSP432E4_Handle dmaHandle
Definition: ADCBufMSP432E4.h:340
enum ADCBuf_Return_Mode_ ADCBuf_Return_Mode
ADC return mode settings.
Definition: ADCBufMSP432E4.h:178
Definition: ADCBufMSP432E4.h:169
Definition: ADCBufMSP432E4.h:226
Definition: ADCBufMSP432E4.h:204
Definition: ADCBufMSP432E4.h:209
uint8_t useDMA
Definition: ADCBufMSP432E4.h:312
Definition: ADCBufMSP432E4.h:207
Definition: ADCBufMSP432E4.h:146
uint32_t intPriority
Definition: ADCBufMSP432E4.h:304
Definition: ADCBufMSP432E4.h:159
uint_fast16_t adcDifferentialPin
Definition: ADCBufMSP432E4.h:267
Definition: ADCBufMSP432E4.h:206
Definition: ADCBufMSP432E4.h:198
uint32_t timerSource
Definition: ADCBufMSP432E4.h:346
SemaphoreP_Handle mutex
Definition: ADCBufMSP432E4.h:321
Definition: ADCBufMSP432E4.h:147
Definition: ADCBufMSP432E4.h:211
Definition: ADCBufMSP432E4.h:205
uint32_t refVoltage
Definition: ADCBufMSP432E4.h:262
ADCBufMSP432E4_Phase
ADCBufMSP432E4 phase delay These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify the phase del...
Definition: ADCBufMSP432E4.h:197
ADCBufMSP432E4_SequencePriorities
ADCBufMSP432E4 Sequencer Priorities These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify the ...
Definition: ADCBufMSP432E4.h:142
Definition: ADCBufMSP432E4.h:241
bool isOpen
Definition: ADCBufMSP432E4.h:341
Definition: ADCBufMSP432E4.h:213
The definition of an ADCBuf function table that contains the required set of functions to control a s...
Definition: ADCBuf.h:385
Definition: ADCBufMSP432E4.h:189
ADCBufMSP432E4_InternalSourceMode adcInternalSource
Definition: ADCBufMSP432E4.h:266
uint32_t adcTimerSource
Definition: ADCBufMSP432E4.h:306
ADCBuf_Recurrence_Mode recurrenceMode
Definition: ADCBufMSP432E4.h:338
Definition: ADCBufMSP432E4.h:212
ADCBufMSP432E4_SequencePriorities * sequencePriority
Definition: ADCBufMSP432E4.h:311
uint_fast16_t adcPin
Definition: ADCBufMSP432E4.h:263
ADCBufMSP432E4_DifferentialMode
ADCBufMSP432E4 Differential Mode These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify if ADC ...
Definition: ADCBufMSP432E4.h:177
Definition: ADCBufMSP432E4.h:227
uint32_t timerFrequency
Definition: ADCBufMSP432E4.h:348
ADCBufMSP432E4_Sequencer adcSequence
Definition: ADCBufMSP432E4.h:264
Definition: ADCBufMSP432E4.h:200
Definition: ADCBufMSP432E4.h:156
ADCBufMSP432E4_Phase modulePhase
Definition: ADCBufMSP432E4.h:309
ADCBufMSP432E4_ReferenceSource
ADCBufMSP432E4 reference source These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify the refe...
Definition: ADCBufMSP432E4.h:239
Definition: ADCBufMSP432E4.h:143
Definition: ADCBufMSP432E4.h:345
Definition: ADCBufMSP432E4.h:208
Definition: ADCBufMSP432E4.h:168
ADCBufMSP432E4_SamplingDuration samplingDuration
Definition: ADCBufMSP432E4.h:252
ADCBufMSP432E4_ReferenceSource refSource
Definition: ADCBufMSP432E4.h:310
struct ADCBufMSP432E4_HWAttrsV1 ADCBufMSP432E4_HWAttrsV1
ADCBufMSP432E4 Hardware attributes These fields are populated by PinMux tool but user is allowed to c...
bool isInitialized
Definition: ADCBufMSP432E4.h:349
Definition: ADCBufMSP432E4.h:229
ADCBufMSP432E4_SamplingDuration samplingDuration
Definition: ADCBufMSP432E4.h:335
ADCBufMSP432E4_SamplingDuration
ADCMSP432E4 sampling duration These fields define the MSP432E4 ADC sampling duration (sample and hold...
Definition: ADCBufMSP432E4.h:223
ADCBufMSP432E4_DifferentialMode adcInputMode
Definition: ADCBufMSP432E4.h:265
Definition: ADCBufMSP432E4.h:224
uint32_t semaphoreTimeout
Definition: ADCBufMSP432E4.h:336
ADCBufMSP432E4_TriggerSource
ADCBufMSP432E4 trigger source These fields are used by ADCBufMSP432E4_HWAttrsV1 to specify the trigge...
Definition: ADCBufMSP432E4.h:187
Definition: ADCBufMSP432E4.h:158
Definition: ADCBufMSP432E4.h:240
struct ADCBufMSP432E4_Channels ADCBufMSP432E4_Channels
ADCBufMSP432E4 Channel setting These fields define channel-specific settings: GPIO, reference voltage, temperature mode, etc. These settings happen when ADCBuf_convert() is called.
Definition: ADCBufMSP432E4.h:199
void(* ADCBuf_Callback)(ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel)
The definition of a callback function used by the ADC driver when used in ADCBuf_RETURN_MODE_CALLBACK...
Definition: ADCBuf.h:251
Definition: ADCBufMSP432E4.h:210
uint32_t samplingFrequency
Definition: ADCBufMSP432E4.h:337
Definition: ADCBufMSP432E4.h:225
Definition: ADCBufMSP432E4.h:179
Definition: ADCBufMSP432E4.h:201
ADCBufMSP432E4 Hardware attributes These fields are populated by PinMux tool but user is allowed to c...
Definition: ADCBufMSP432E4.h:303
ADCBufMSP432E4_Channels * channelSetting
Definition: ADCBufMSP432E4.h:307
Definition: ADCBufMSP432E4.h:188
Definition: ADCBufMSP432E4.h:144
ADCBufMSP432E4 Object.
Definition: ADCBufMSP432E4.h:320
ADCBufMSP432E4_TriggerSource * adcTriggerSource
Definition: ADCBufMSP432E4.h:308
Definition: ADCBufMSP432E4.h:230
ADCBuf_Return_Mode returnMode
Definition: ADCBufMSP432E4.h:339