![]() |
![]() |
This structure defines the implementation of a display driver. More...
#include <grlib.h>
Data Fields | |
| void(*const | pfnPixelDraw )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY, uint16_t ulValue) |
| A pointer to the function to draw a pixel on this display. More... | |
| void(*const | pfnPixelDrawMultiple )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY, int16_t lX0, int16_t lCount, int16_t lBPP, const uint8_t *pucData, const uint32_t *pucPalette) |
| A pointer to the function to draw multiple pixels on this display. More... | |
| void(*const | pfnLineDrawH )(const Graphics_Display *pDisplay, int16_t lX1, int16_t lX2, int16_t lY, uint16_t ulValue) |
| A pointer to the function to draw a horizontal line on this display. More... | |
| void(*const | pfnLineDrawV )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY1, int16_t lY2, uint16_t ulValue) |
| A pointer to the function to draw a vertical line on this display. More... | |
| void(*const | pfnRectFill )(const Graphics_Display *pDisplay, const Graphics_Rectangle *pRect, uint16_t ulValue) |
| A pointer to the function to draw a filled rectangle on this display. More... | |
| uint32_t(*const | pfnColorTranslate )(const Graphics_Display *pDisplay, uint32_t ulValue) |
| void(*const | pfnFlush )(const Graphics_Display *pDisplay) |
| void(*const | pfnClearDisplay )(const Graphics_Display *pDisplay, uint16_t ulValue) |
This structure defines the implementation of a display driver.
| void(*const Graphics_Display_Functions::pfnPixelDraw) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY, uint16_t ulValue) |
A pointer to the function to draw a pixel on this display.
Referenced by Graphics_drawPixelOnDisplay().
| void(*const Graphics_Display_Functions::pfnPixelDrawMultiple) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY, int16_t lX0, int16_t lCount, int16_t lBPP, const uint8_t *pucData, const uint32_t *pucPalette) |
A pointer to the function to draw multiple pixels on this display.
Referenced by Graphics_drawMultiplePixelsOnDisplay().
| void(*const Graphics_Display_Functions::pfnLineDrawH) (const Graphics_Display *pDisplay, int16_t lX1, int16_t lX2, int16_t lY, uint16_t ulValue) |
A pointer to the function to draw a horizontal line on this display.
Referenced by Graphics_drawHorizontalLineOnDisplay().
| void(*const Graphics_Display_Functions::pfnLineDrawV) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY1, int16_t lY2, uint16_t ulValue) |
A pointer to the function to draw a vertical line on this display.
Referenced by Graphics_drawVerticalLineOnDisplay().
| void(*const Graphics_Display_Functions::pfnRectFill) (const Graphics_Display *pDisplay, const Graphics_Rectangle *pRect, uint16_t ulValue) |
A pointer to the function to draw a filled rectangle on this display.
Referenced by Graphics_fillRectangleOnDisplay().
| uint32_t(*const Graphics_Display_Functions::pfnColorTranslate) (const Graphics_Display *pDisplay, uint32_t ulValue) |
A pointer to the function to translate 24-bit RGB colors to display-specific colors.
Referenced by Graphics_translateColorOnDisplay().
| void(*const Graphics_Display_Functions::pfnFlush) (const Graphics_Display *pDisplay) |
A pointer to the function to flush any cached drawing operations on this display.
Referenced by Graphics_flushOnDisplay().
| void(*const Graphics_Display_Functions::pfnClearDisplay) (const Graphics_Display *pDisplay, uint16_t ulValue) |
A pointer to the function to clears Display. Contents of display buffer unmodified
Referenced by Graphics_clearDisplayOnDisplay().