![]() |
![]() |
Data Structures | |
| struct | Graphics_Image |
| This structure defines the characteristics of a Bitmap Image. More... | |
| struct | Graphics_Rectangle |
| struct | Graphics_Display_Functions |
| This structure defines the implementation of a display driver. More... | |
| struct | Graphics_Display |
| This structure defines the characteristics of a display driver. More... | |
| struct | Graphics_Font |
| This structure describes a font used for drawing text onto the screen. More... | |
| struct | Graphics_FontEx |
| struct | Graphics_Context |
Typedefs | |
| typedef struct Graphics_Image | Graphics_Image |
| This structure defines the characteristics of a Bitmap Image. More... | |
| typedef struct Graphics_Rectangle | Graphics_Rectangle |
| typedef struct Graphics_Display | Graphics_Display |
| typedef struct Graphics_Display_Functions | Graphics_Display_Functions |
| This structure defines the implementation of a display driver. More... | |
| typedef struct Graphics_Font | Graphics_Font |
| This structure describes a font used for drawing text onto the screen. More... | |
| typedef struct Graphics_FontEx | Graphics_FontEx |
| typedef struct Graphics_Context | Graphics_Context |
Functions | |
| void | Graphics_drawCircle (const Graphics_Context *context, int32_t x, int32_t y, int32_t lRadius) |
| void | Graphics_fillCircle (const Graphics_Context *context, int32_t x, int32_t y, int32_t lRadius) |
| void | Graphics_setClipRegion (Graphics_Context *context, Graphics_Rectangle *rect) |
| void | Graphics_initContext (Graphics_Context *context, Graphics_Display *display, const Graphics_Display_Functions *pFxns) |
| void | Graphics_drawImage (const Graphics_Context *context, const Graphics_Image *pBitmap, int16_t x, int16_t y) |
| void | Graphics_drawLine (const Graphics_Context *context, int32_t x1, int32_t y1, int32_t x2, int32_t y2) |
| void | Graphics_drawLineH (const Graphics_Context *context, int32_t x1, int32_t x2, int32_t y) |
| void | Graphics_drawLineV (const Graphics_Context *context, int32_t x, int32_t y1, int32_t y2) |
| void | Graphics_drawRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect) |
| void | Graphics_fillRectangle (const Graphics_Context *context, const Graphics_Rectangle *rect) |
| void | Graphics_drawString (const Graphics_Context *context, int8_t *string, int32_t lLength, int32_t x, int32_t y, bool opaque) |
| int32_t | Graphics_getStringWidth (const Graphics_Context *context, const int8_t *string, int32_t lLength) |
| int32_t | Graphics_isOverlappingRectangle (Graphics_Rectangle *psRect1, Graphics_Rectangle *psRect2) |
| int32_t | Graphics_getRectangleIntersection (Graphics_Rectangle *psRect1, Graphics_Rectangle *psRect2, Graphics_Rectangle *psIntersect) |
| void | Graphics_setBackgroundColor (Graphics_Context *context, int32_t value) |
| uint16_t | Graphics_getDisplayWidth (Graphics_Context *context) |
| uint16_t | Graphics_getDisplayHeight (Graphics_Context *context) |
| void | Graphics_setFont (Graphics_Context *context, const Graphics_Font *font) |
| uint8_t | Graphics_getFontBaseline (const Graphics_Font *font) |
| void | Graphics_setForegroundColor (Graphics_Context *context, int32_t value) |
| void | Graphics_setForegroundColorTranslated (Graphics_Context *context, int32_t value) |
| uint8_t | Graphics_getFontHeight (const Graphics_Font *font) |
| uint8_t | Graphics_getFontMaxWidth (const Graphics_Font *font) |
| uint16_t | Graphics_getImageColors (const Graphics_Image *image) |
| uint16_t | Graphics_getImageHeight (const Graphics_Image *image) |
| uint16_t | Graphics_getImageWidth (const Graphics_Image *image) |
| uint32_t | Graphics_getOffscreen1BppImageSize (uint16_t width, uint16_t height) |
| uint32_t | Graphics_getOffscreen4BppImageSize (uint16_t width, uint16_t height) |
| uint32_t | Graphics_getOffScreen8BPPSize (uint16_t width, uint16_t height) |
| void | Graphics_drawStringCentered (const Graphics_Context *context, int8_t *string, int32_t length, int32_t x, int32_t y, bool opaque) |
| uint8_t | Graphics_getStringHeight (const Graphics_Context *context) |
| uint8_t | Graphics_getStringMaxWidth (const Graphics_Context *context) |
| uint8_t | Graphics_getStringBaseline (const Graphics_Context *context) |
| uint32_t | Graphics_translateColorOnDisplay (const Graphics_Display *display, uint32_t value) |
| void | Graphics_drawHorizontalLineOnDisplay (const Graphics_Display *display, uint16_t x1, uint16_t x2, uint16_t y, uint32_t value) |
| void | Graphics_drawVerticalLineOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y1, uint16_t y2, uint16_t value) |
| void | Graphics_fillRectangleOnDisplay (const Graphics_Display *display, const Graphics_Rectangle *rect, uint16_t value) |
| void | Graphics_flushOnDisplay (const Graphics_Display *display) |
| void | Graphics_drawPixel (const Graphics_Context *context, uint16_t x, uint16_t y) |
| void | Graphics_clearDisplay (const Graphics_Context *context) |
| uint16_t | Graphics_getHeightOfDisplay (const Graphics_Display *display) |
| void | Graphics_flushBuffer (const Graphics_Context *context) |
| uint16_t | Graphics_getWidthOfDisplay (const Graphics_Display *display) |
| bool | Graphics_isPointWithinRectangle (const Graphics_Rectangle *rect, uint16_t x, uint16_t y) |
| void | Graphics_drawPixelOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y, uint16_t value) |
| void | Graphics_clearDisplayOnDisplay (const Graphics_Display *display, uint16_t value) |
| void | Graphics_drawMultiplePixelsOnDisplay (const Graphics_Display *display, uint16_t x, uint16_t y, uint16_t x0, uint16_t count, uint16_t bPP, const uint8_t *data, const uint32_t *pucPalette) |
| void | Graphics_initOffscreen1BppImage (Graphics_Display *display, uint8_t *image, int32_t width, int32_t height) |
| void | Graphics_initOffscreen4BppImage (Graphics_Display *display, uint8_t *image, int32_t width, int32_t height) |
| void | Graphics_setOffscreen4BppPalette (Graphics_Display *display, uint32_t *ppalette, uint32_t offset, uint32_t count) |
| void | Graphics_initOffscreen8BppImage (Graphics_Display *display, uint8_t *image, int32_t width, int32_t height) |
| void | Graphics_setOffscreen8BppPalette (Graphics_Display *display, uint32_t *ppalette, uint32_t offset, uint32_t count) |
| #define min | ( | a, | |
| b | |||
| ) | (((a) < (b)) ? (a) : (b)) |
Referenced by Graphics_getRectangleIntersection().
| #define max | ( | a, | |
| b | |||
| ) | (((a) < (b)) ? (b) : (a)) |
Referenced by Graphics_getRectangleIntersection().
| #define ClrAliceBlue GRAPHICS_COLOR_ALICE_BLUE |
| #define ClrAntiqueWhite GRAPHICS_COLOR_ANTIQUE_WHITE |
| #define ClrAqua GRAPHICS_COLOR_AQUA |
| #define ClrAquamarine GRAPHICS_COLOR_AQUAMARINE |
| #define ClrAzure GRAPHICS_COLOR_AZURE |
| #define ClrBeige GRAPHICS_COLOR_BEIGE |
| #define ClrBisque GRAPHICS_COLOR_BISQUE |
| #define ClrBlack GRAPHICS_COLOR_BLACK |
| #define ClrBlack GRAPHICS_COLOR_BLACK |
| #define ClrBlanchedAlmond GRAPHICS_COLOR_BLANCHED_ALMOND |
| #define ClrBlue GRAPHICS_COLOR_BLUE |
| #define ClrBlueViolet GRAPHICS_COLOR_BLUE_VIOLET |
| #define ClrBrown GRAPHICS_COLOR_BROWN |
| #define ClrBurlyWood GRAPHICS_COLOR_BURLY_WOOD |
| #define ClrCadetBlue GRAPHICS_COLOR_CADET_BLUE |
| #define ClrChartreuse GRAPHICS_COLOR_CHARTREUSE |
| #define ClrChocolate GRAPHICS_COLOR_CHOCOLATE |
| #define ClrCoral GRAPHICS_COLOR_CORAL |
| #define ClrCornflowerBlue GRAPHICS_COLOR_CORNFLOWER_BLUE |
| #define ClrCornsilk GRAPHICS_COLOR_CORNSILK |
| #define ClrCrimson GRAPHICS_COLOR_CRIMSON |
| #define ClrCyan GRAPHICS_COLOR_CYAN |
| #define ClrDarkBlue GRAPHICS_COLOR_DARK_BLUE |
| #define ClrDarkCyan GRAPHICS_COLOR_DARK_CYAN |
| #define ClrDarkGoldenrod GRAPHICS_COLOR_DARK_GOLDENROD |
| #define ClrDarkGray GRAPHICS_COLOR_DARK_GRAY |
| #define ClrDarkGreen GRAPHICS_COLOR_DARK_GREEN |
| #define ClrDarkKhaki GRAPHICS_COLOR_DARK_KHAKI |
| #define ClrDarkMagenta GRAPHICS_COLOR_DARK_MAGENTA |
| #define ClrDarkOliveGreen GRAPHICS_COLOR_DARK_OLIVE_GREEN |
| #define ClrDarkOrange GRAPHICS_COLOR_DARK_ORANGE |
| #define ClrDarkOrchid GRAPHICS_COLOR_DARK_ORCHID |
| #define ClrDarkRed GRAPHICS_COLOR_DARK_RED |
| #define ClrDarkSalmon GRAPHICS_COLOR_DARK_SALMON |
| #define ClrDarkSeaGreen GRAPHICS_COLOR_DARK_SEA_GREEN |
| #define ClrDarkSlateBlue GRAPHICS_COLOR_DARK_SLATE_BLUE |
| #define ClrDarkSlateGray GRAPHICS_COLOR_DARK_SLATE_GRAY |
| #define ClrDarkTurquoise GRAPHICS_COLOR_DARK_TURQUOISE |
| #define ClrDarkViolet GRAPHICS_COLOR_DARK_VIOLET |
| #define ClrDeepPink GRAPHICS_COLOR_DEEP_PINK |
| #define ClrDeepSkyBlue GRAPHICS_COLOR_DEEP_SKY_BLUE |
| #define ClrDimGray GRAPHICS_COLOR_DIM_GRAY |
| #define ClrDodgerBlue GRAPHICS_COLOR_DODGER_BLUE |
| #define ClrFireBrick GRAPHICS_COLOR_FIRE_BRICK |
| #define ClrFloralWhite GRAPHICS_COLOR_FLORAL_WHITE |
| #define ClrForestGreen GRAPHICS_COLOR_FOREST_GREEN |
| #define ClrFuchsia GRAPHICS_COLOR_FUCHSIA |
| #define ClrGainsboro GRAPHICS_COLOR_GAINSBORO |
| #define ClrGhostWhite GRAPHICS_COLOR_GHOST_WHITE |
| #define ClrGold GRAPHICS_COLOR_GOLD |
| #define ClrGoldenrod GRAPHICS_COLOR_GOLDENRON |
| #define ClrGray GRAPHICS_COLOR_GRAY |
| #define ClrGreen GRAPHICS_COLOR_GREEN |
| #define ClrGreenYellow GRAPHICS_COLOR_GREEN_YELLOW |
| #define ClrHoneydew GRAPHICS_COLOR_HONEYDEW |
| #define ClrHotPink GRAPHICS_COLOR_HOT_PINK |
| #define ClrIndianRed GRAPHICS_COLOR_INDIAN_RED |
| #define ClrIndigo GRAPHICS_COLOR_INDIGO |
| #define ClrIvory GRAPHICS_COLOR_IVORY |
| #define ClrKhaki GRAPHICS_COLOR_KHAKI |
| #define ClrLavender GRAPHICS_COLOR_LAVENDER |
| #define ClrLavenderBlush GRAPHICS_COLOR_LAVENDER_BLUSH |
| #define ClrLawnGreen GRAPHICS_COLOR_LAWN_GREEN |
| #define ClrLemonChiffon GRAPHICS_COLOR_LEMON_CHIFFON |
| #define ClrLightBlue GRAPHICS_COLOR_LIGHT_BLUE |
| #define ClrLightCoral GRAPHICS_COLOR_LIGHT_CORAL |
| #define ClrLightCyan GRAPHICS_COLOR_LIGHT_CYAN |
| #define ClrLightGoldenrodYellow GRAPHICS_COLOR_LIGHT_GOLDENRON_YELLOW |
| #define ClrLightGreen GRAPHICS_COLOR_LIGHT_GREEN |
| #define ClrLightGrey GRAPHICS_COLOR_LIGHT_GRAY |
| #define ClrLightPink GRAPHICS_COLOR_LIGHT_PINK |
| #define ClrLightSalmon GRAPHICS_COLOR_LIGHT_SALMON |
| #define ClrLightSeaGreen GRAPHICS_COLOR_LIGHT_SEA_GREEN |
| #define ClrLightSkyBlue GRAPHICS_COLOR_LIGHT_SKY_BLUE |
| #define ClrLightSlateGray GRAPHICS_COLOR_LIGHT_SLATE_GRAY |
| #define ClrLightSteelBlue GRAPHICS_COLOR_LIGHT_STEEL_BLUE |
| #define ClrLightYellow GRAPHICS_COLOR_LIGHT_YELLOW |
| #define ClrLime GRAPHICS_COLOR_LIME |
| #define ClrLimeGreen GRAPHICS_COLOR_LIME_GREEN |
| #define ClrLinen GRAPHICS_COLOR_LINEN |
| #define ClrMagenta GRAPHICS_COLOR_MAGENTA |
| #define ClrMaroon GRAPHICS_COLOR_MAROON |
| #define ClrMediumAquamarine GRAPHICS_COLOR_MEDIUM_AQUAMARINE |
| #define ClrMediumBlue GRAPHICS_COLOR_MEDIUM_BLUE |
| #define ClrMediumOrchid GRAPHICS_COLOR_MEDIUM_ORCHID |
| #define ClrMediumPurple GRAPHICS_COLOR_MEDIUM_PURPLE |
| #define ClrMediumSeaGreen GRAPHICS_COLOR_MEDIUM_SEA_GREEN |
| #define ClrMediumSlateBlue GRAPHICS_COLOR_MEDIUM_SLATE_BLUE |
| #define ClrMediumSpringGreen GRAPHICS_COLOR_MEDIUM_SPRING_GREEN |
| #define ClrMediumTurquoise GRAPHICS_COLOR_MEDIUM_TURQUOISE |
| #define ClrMediumVioletRed GRAPHICS_COLOR_MEDIUM_VIOLET_RED |
| #define ClrMidnightBlue GRAPHICS_COLOR_MIGNIGHT_BLUE |
| #define ClrMintCream GRAPHICS_COLOR_MINT_CREAM |
| #define ClrMistyRose GRAPHICS_COLOR_MISTY_ROSE |
| #define ClrMoccasin GRAPHICS_COLOR_MOCCASIN |
| #define ClrNavajoWhite GRAPHICS_COLOR_NAVAJO_WHITE |
| #define ClrNavy GRAPHICS_COLOR_NAVY |
| #define ClrOldLace GRAPHICS_COLOR_OLD_LACE |
| #define ClrOlive GRAPHICS_COLOR_OLIVE |
| #define ClrOliveDrab GRAPHICS_COLOR_OLIVE_DRAB |
| #define ClrOrange GRAPHICS_COLOR_ORANGE |
| #define ClrOrangeRed GRAPHICS_COLOR_ORANGE_RED |
| #define ClrOrchid GRAPHICS_COLOR_ORCHID |
| #define ClrPaleGoldenrod GRAPHICS_COLOR_PALE_GOLDENRON |
| #define ClrPaleGreen GRAPHICS_COLOR_PALE_GREEN |
| #define ClrPaleTurquoise GRAPHICS_COLOR_PALE_TURQUOISE |
| #define ClrPaleVioletRed GRAPHICS_COLOR_PALE_VIOLET_RED |
| #define ClrPapayaWhip GRAPHICS_COLOR_PAPAYA_WHIP |
| #define ClrPeachPuff GRAPHICS_COLOR_PEACH_PUFF |
| #define ClrPeru GRAPHICS_COLOR_PERU |
| #define ClrPink GRAPHICS_COLOR_PINK |
| #define ClrPlum GRAPHICS_COLOR_PLUM |
| #define ClrPowderBlue GRAPHICS_COLOR_POWDER_BLUE |
| #define ClrPurple GRAPHICS_COLOR_PURPLE |
| #define ClrRed GRAPHICS_COLOR_RED |
| #define ClrRosyBrown GRAPHICS_COLOR_ROSY_BROWN |
| #define ClrRoyalBlue GRAPHICS_COLOR_ROYAL_BLUE |
| #define ClrSaddleBrown GRAPHICS_COLOR_SADDLE_BROWN |
| #define ClrSalmon GRAPHICS_COLOR_SALMON |
| #define ClrSandyBrown GRAPHICS_COLOR_SANDY_BROWN |
| #define ClrSeaGreen GRAPHICS_COLOR_SEA_GREEN |
| #define ClrSeashell GRAPHICS_COLOR_SEASHELL |
| #define ClrSienna GRAPHICS_COLOR_SIENNA |
| #define ClrSilver GRAPHICS_COLOR_SILVER |
| #define ClrSkyBlue GRAPHICS_COLOR_SKY_BLUE |
| #define ClrSlateBlue GRAPHICS_COLOR_SLATE_BLUE |
| #define ClrSlateGray GRAPHICS_COLOR_SLATE_GRAY |
| #define ClrSnow GRAPHICS_COLOR_SNOW |
| #define ClrSpringGreen GRAPHICS_COLOR_SPRING_GREEN |
| #define ClrSteelBlue GRAPHICS_COLOR_STEEL_BLUE |
| #define ClrTan GRAPHICS_COLOR_TAN |
| #define ClrTeal GRAPHICS_COLOR_TEAL |
| #define ClrThistle GRAPHICS_COLOR_THISTLE |
| #define ClrTomato GRAPHICS_COLOR_TOMATO |
| #define ClrTurquoise GRAPHICS_COLOR_TURQUOISE |
| #define ClrViolet GRAPHICS_COLOR_VIOLET |
| #define ClrWheat GRAPHICS_COLOR_WHEAT |
| #define ClrWhite GRAPHICS_COLOR_WHITE |
| #define ClrWhiteSmoke GRAPHICS_COLOR_WHITE_SMOKE |
| #define ClrYellow GRAPHICS_COLOR_YELLOW |
| #define ClrYellowGreen GRAPHICS_COLOR_YELLOW_GREEN |
| #define FONT_FMT_UNCOMPRESSED GRAPHICS_FONT_FMT_UNCOMPRESSED |
| #define FONT_FMT_PIXEL_RLE GRAPHICS_FONT_FMT_PIXEL_RLE |
| #define FONT_EX_MARKER GRAPHICS_FONT_EX_MARKER |
| #define FONT_FMT_EX_UNCOMPRESSED GRAPHICS_FONT_FMT_EX_UNCOMPRESSED |
| #define FONT_FMT_EX_PIXEL_RLE GRAPHICS_FONT_FMT_EX_PIXEL_RLE |
| #define AUTO_STRING_LENGTH GRAPHICS_AUTO_STRING_LENGTH |
Referenced by Graphics_drawCheckBox(), and Graphics_drawRadioButton().
| #define OPAQUE_TEXT GRAPHICS_OPAQUE_TEXT |
| #define TRANSPARENT_TEXT GRAPHICS_TRANSPARENT_TEXT |
Referenced by Graphics_drawCheckBox(), and Graphics_drawRadioButton().
| #define IMAGE_FMT_1BPP_UNCOMP GRAPHICS_IMAGE_FMT_1BPP_UNCOMP |
| #define IMAGE_FMT_2BPP_UNCOMP GRAPHICS_IMAGE_FMT_2BPP_UNCOMP |
| #define IMAGE_FMT_2BPP_UNCOMP GRAPHICS_IMAGE_FMT_2BPP_UNCOMP |
| #define IMAGE_FMT_4BPP_UNCOMP GRAPHICS_IMAGE_FMT_4BPP_UNCOMP |
| #define IMAGE_FMT_8BPP_UNCOMP GRAPHICS_IMAGE_FMT_8BPP_UNCOMP |
| #define IMAGE_FMT_1BPP_COMP_RLE4 GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE4 |
| #define IMAGE_FMT_4BPP_COMP_RLE4 GRAPHICS_IMAGE_FMT_4BPP_COMP_RLE4 |
| #define IMAGE_FMT_1BPP_COMP_RLE7 GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE7 |
| #define IMAGE_FMT_1BPP_COMP_RLE8 GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE8 |
| #define IMAGE_FMT_2BPP_COMP_RLE8 GRAPHICS_IMAGE_FMT_2BPP_COMP_RLE8 |
| #define IMAGE_FMT_4BPP_COMP_RLE8 GRAPHICS_IMAGE_FMT_4BPP_COMP_RLE8 |
| #define IMAGE_FMT_8BPP_COMP_RLE8 GRAPHICS_IMAGE_FMT_8BPP_COMP_RLE8 |
| #define IMAGE_FMT_8BPP_COMP_RLEBLEND GRAPHICS_IMAGE_FMT_8BPP_COMP_RLEBLEND |
| #define tFontEx Graphics_FontEx |
| #define tFont Graphics_Font |
| #define tDisplay Graphics_Display |
| #define tRectangle Graphics_Rectangle |
| #define tImage Graphics_Image |
| #define tContext Graphics_Context |
| #define sXMax xMax |
| #define sXMin xMin |
| #define sYMax yMax |
| #define sYMin yMin |
| #define GrCircleDraw Graphics_drawCircle |
| #define GrCircleFill Graphics_fillCircle |
| #define GrContextClipRegionSet Graphics_setClipRegion |
| #define GrContextInit Graphics_initContext |
| #define GrImageDraw Graphics_drawImage |
| #define GrLineDraw Graphics_drawLine |
| #define GrLineDrawH Graphics_drawLineH |
| #define GrLineDrawV Graphics_drawLineV |
| #define GrRectDraw Graphics_drawRectangle |
| #define GrRectFill Graphics_fillRectangle |
| #define GrStringDraw Graphics_drawString |
| #define GrStringWidthGet Graphics_getStringWidth |
| #define GrRectOverlapCheck Graphics_isOverlappingRectangle |
| #define GrRectIntersectGet Graphics_getRectangleIntersection |
| #define GrContextBackgroundSet Graphics_setBackgroundColor |
| #define GrContextBackgroundSetTranslated Graphics_setBackgroundColorTranslated |
| #define GrContextDpyWidthGet Graphics_getDisplayWidth |
| #define GrContextDpyHeightGet Graphics_getDisplayHeight |
| #define GrContextFontSet Graphics_setFont |
| #define GrContextForegroundSet Graphics_setForegroundColor |
| #define GrContextForegroundSetTranslated Graphics_setForegroundColorTranslated |
| #define GrFlush Graphics_flushBuffer |
| #define GrClearDisplay Graphics_clearDisplay |
| #define GrFontBaselineGet Graphics_getFontBaseline |
| #define GrFontHeightGet Graphics_getFontHeight |
| #define GrFontMaxWidthGet Graphics_getFontMaxWidth |
| #define GrImageColorsGet Graphics_getImageColors |
| #define GrImageHeightGet Graphics_getImageHeight |
| #define GrImageWidthGet Graphics_getImageWidth |
| #define GrOffScreen1BPPSize Graphics_getOffscreen1BppImageSize |
| #define GrOffScreen4BPPSize Graphics_getOffscreen4BppImageSize |
| #define GrOffScreen8BPPSize Graphics_getOffscreen8BppImageSize |
| #define GrPixelDraw Graphics_drawPixel |
| #define GrStringBaselineGet Graphics_getStringBaseline |
| #define GrStringDrawCentered Graphics_drawStringCentered |
| #define GrStringHeightGet Graphics_getStringHeight |
| #define GrStringMaxWidthGet Graphics_getStringMaxWidth |
| #define DpyColorTranslate Graphics_translateColorOnDisplay |
| #define DpyFlush Graphics_flushOnDisplay |
| #define DpyClearDisplay Graphics_clearDisplayOnDisplay |
| #define DpyHeightGet Graphics_getHeightOfDisplay |
| #define DpyLineDrawH Graphics_drawHorizontalLineOnDisplay |
| #define DpyLineDrawV Graphics_drawVerticalLineOnDisplay |
| #define DpyPixelDraw Graphics_drawPixelOnDisplay |
| #define DpyPixelDrawMultiple Graphics_drawMultiplePixelsOnDisplay |
| #define DpyRectFill Graphics_fillRectangleOnDisplay |
| #define DpyWidthGet Graphics_getWidthOfDisplay |
| #define GrRectContainsPoint Graphics_isPointWithinRectangle |
| #define GRAPHICS_FONT_FMT_UNCOMPRESSED 0x00 |
Indicates that the font data is stored in an uncompressed format.
Referenced by Graphics_drawString().
| #define GRAPHICS_FONT_FMT_PIXEL_RLE 0x01 |
Indicates that the font data is stored using a pixel-based RLE format.
| #define GRAPHICS_FONT_EX_MARKER 0x80 |
A marker used in the format field of a font to indicates that the font data is stored using the new tFontEx structure.
Referenced by Graphics_drawString(), and Graphics_getStringWidth().
| #define GRAPHICS_FONT_FMT_EX_UNCOMPRESSED |
Indicates that the font data is stored in an uncompressed format and uses the tFontEx structure format.
| #define GRAPHICS_FONT_FMT_EX_PIXEL_RLE |
Indicates that the font data is stored using a pixel-based RLE format and uses the tFontEx structure format.
| #define GRAPHICS_AUTO_STRING_LENGTH -1 |
Value to automatically draw the entire length of the string (subject to clipping)
| #define GRAPHICS_OPAQUE_TEXT 1 |
Value to draw text opaque The text foreground and background are drawn together
| #define GRAPHICS_TRANSPARENT_TEXT 0 |
Value to draw text transparently The text only (no background) is drawn
| #define GRAPHICS_IMAGE_FMT_1BPP_UNCOMP 0x01 |
Indicates that the image data is not compressed and represents each pixel with a single bit.
| #define GRAPHICS_IMAGE_FMT_2BPP_UNCOMP 0x02 |
Indicates that the image data is not compressed and represents each pixel with two bits.
| #define GRAPHICS_IMAGE_FMT_4BPP_UNCOMP 0x04 |
Indicates that the image data is not compressed and represents each pixel with four bits.
| #define GRAPHICS_IMAGE_FMT_8BPP_UNCOMP 0x08 |
Indicates that the image data is not compressed and represents each pixel with eight bits.
| #define GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE4 0x41 |
Indicates that the image data is compressed with 4 bit Run Length Encoding and represents each pixel with a single bit.
| #define GRAPHICS_IMAGE_FMT_2BPP_COMP_RLE4 0x42 |
Indicates that the image data is compressed with 4 bit Run Length Encoding and represents each pixel with two bits.
| #define GRAPHICS_IMAGE_FMT_4BPP_COMP_RLE4 0x44 |
Indicates that the image data is compressed with 4 bit Run Length Encoding and represents each pixel with four bits.
| #define GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE7 0x71 |
Indicates that the image data is compressed with 7 bit Run Length Encoding and represents each pixel with a single bit.
| #define GRAPHICS_IMAGE_FMT_1BPP_COMP_RLE8 0x81 |
Indicates that the image data is compressed with 8 bit Run Length Encoding and represents each pixel with a single bit.
| #define GRAPHICS_IMAGE_FMT_2BPP_COMP_RLE8 0x82 |
Indicates that the image data is compressed with 8 bit Run Length Encoding and represents each pixel with two bits.
| #define GRAPHICS_IMAGE_FMT_4BPP_COMP_RLE8 0x84 |
Indicates that the image data is compressed with 8 bit Run Length Encoding and represents each pixel with four bits.
| #define GRAPHICS_IMAGE_FMT_8BPP_COMP_RLE8 0x88 |
Indicates that the image data is compressed with 8 bit Run Length Encoding and represents each pixel with eight bits.
| #define GRAPHICS_IMAGE_FMT_8BPP_COMP_RLEBLEND 0x28 |
Indicates that the image data is compressed and represents each pixel with info bits.
| #define GRAPHICS_COLOR_ALICE_BLUE 0x00F0F8FF |
| #define GRAPHICS_COLOR_ANTIQUE_WHITE 0x00FAEBD7 |
| #define GRAPHICS_COLOR_AQUA 0x0000FFFF |
| #define GRAPHICS_COLOR_AQUAMARINE 0x007FFFD4 |
| #define GRAPHICS_COLOR_AZURE 0x00F0FFFF |
| #define GRAPHICS_COLOR_BEIGE 0x00F5F5DC |
| #define GRAPHICS_COLOR_BISQUE 0x00FFE4C4 |
| #define GRAPHICS_COLOR_BLACK 0x00000000 |
| #define GRAPHICS_COLOR_BLACK 0x00000000 |
| #define GRAPHICS_COLOR_BLANCHED_ALMOND 0x00FFEBCD |
| #define GRAPHICS_COLOR_BLUE 0x000000FF |
| #define GRAPHICS_COLOR_BLUE_VIOLET 0x008A2BE2 |
| #define GRAPHICS_COLOR_BROWN 0x00A52A2A |
| #define GRAPHICS_COLOR_BURLY_WOOD 0x00DEB887 |
| #define GRAPHICS_COLOR_CADET_BLUE 0x005F9EA0 |
| #define GRAPHICS_COLOR_CHARTREUSE 0x007FFF00 |
| #define GRAPHICS_COLOR_CHOCOLATE 0x00D2691E |
| #define GRAPHICS_COLOR_CORAL 0x00FF7F50 |
| #define GRAPHICS_COLOR_CORNFLOWER_BLUE 0x006495ED |
| #define GRAPHICS_COLOR_CORNSILK 0x00FFF8DC |
| #define GRAPHICS_COLOR_CRIMSON 0x00DC143C |
| #define GRAPHICS_COLOR_CYAN 0x0000FFFF |
| #define GRAPHICS_COLOR_DARK_BLUE 0x0000008B |
| #define GRAPHICS_COLOR_DARK_CYAN 0x00008B8B |
| #define GRAPHICS_COLOR_DARK_GOLDENROD 0x00B8860B |
| #define GRAPHICS_COLOR_DARK_GRAY 0x00A9A9A9 |
| #define GRAPHICS_COLOR_DARK_GREEN 0x00006400 |
| #define GRAPHICS_COLOR_DARK_KHAKI 0x00BDB76B |
| #define GRAPHICS_COLOR_DARK_MAGENTA 0x008B008B |
| #define GRAPHICS_COLOR_DARK_OLIVE_GREEN 0x00556B2F |
| #define GRAPHICS_COLOR_DARK_ORANGE 0x00FF8C00 |
| #define GRAPHICS_COLOR_DARK_ORCHID 0x009932CC |
| #define GRAPHICS_COLOR_DARK_RED 0x008B0000 |
| #define GRAPHICS_COLOR_DARK_SALMON 0x00E9967A |
| #define GRAPHICS_COLOR_DARK_SEA_GREEN 0x008FBC8F |
| #define GRAPHICS_COLOR_DARK_SLATE_BLUE 0x00483D8B |
| #define GRAPHICS_COLOR_DARK_SLATE_GRAY 0x002F4F4F |
| #define GRAPHICS_COLOR_DARK_TURQUOISE 0x0000CED1 |
| #define GRAPHICS_COLOR_DARK_VIOLET 0x009400D3 |
| #define GRAPHICS_COLOR_DEEP_PINK 0x00FF1493 |
| #define GRAPHICS_COLOR_DEEP_SKY_BLUE 0x0000BFFF |
| #define GRAPHICS_COLOR_DIM_GRAY 0x00696969 |
| #define GRAPHICS_COLOR_DODGER_BLUE 0x001E90FF |
| #define GRAPHICS_COLOR_FIRE_BRICK 0x00B22222 |
| #define GRAPHICS_COLOR_FLORAL_WHITE 0x00FFFAF0 |
| #define GRAPHICS_COLOR_FOREST_GREEN 0x00228B22 |
| #define GRAPHICS_COLOR_FUCHSIA 0x00FF00FF |
| #define GRAPHICS_COLOR_GAINSBORO 0x00DCDCDC |
| #define GRAPHICS_COLOR_GHOST_WHITE 0x00F8F8FF |
| #define GRAPHICS_COLOR_GOLD 0x00FFD700 |
| #define GRAPHICS_COLOR_GOLDENRON 0x00DAA520 |
| #define GRAPHICS_COLOR_GRAY 0x00808080 |
| #define GRAPHICS_COLOR_GREEN 0x00008000 |
| #define GRAPHICS_COLOR_GREEN_YELLOW 0x00ADFF2F |
| #define GRAPHICS_COLOR_HONEYDEW 0x00F0FFF0 |
| #define GRAPHICS_COLOR_HOT_PINK 0x00FF69B4 |
| #define GRAPHICS_COLOR_INDIAN_RED 0x00CD5C5C |
| #define GRAPHICS_COLOR_INDIGO 0x004B0082 |
| #define GRAPHICS_COLOR_IVORY 0x00FFFFF0 |
| #define GRAPHICS_COLOR_KHAKI 0x00F0E68C |
| #define GRAPHICS_COLOR_LAVENDER 0x00E6E6FA |
| #define GRAPHICS_COLOR_LAVENDER_BLUSH 0x00FFF0F5 |
| #define GRAPHICS_COLOR_LAWN_GREEN 0x007CFC00 |
| #define GRAPHICS_COLOR_LEMON_CHIFFON 0x00FFFACD |
| #define GRAPHICS_COLOR_LIGHT_BLUE 0x00ADD8E6 |
| #define GRAPHICS_COLOR_LIGHT_CORAL 0x00F08080 |
| #define GRAPHICS_COLOR_LIGHT_CYAN 0x00E0FFFF |
| #define GRAPHICS_COLOR_LIGHT_GOLDENRON_YELLOW 0x00FAFAD2 |
| #define GRAPHICS_COLOR_LIGHT_GREEN 0x0090EE90 |
| #define GRAPHICS_COLOR_LIGHT_GRAY 0x00D3D3D3 |
| #define GRAPHICS_COLOR_LIGHT_PINK 0x00FFB6C1 |
| #define GRAPHICS_COLOR_LIGHT_SALMON 0x00FFA07A |
| #define GRAPHICS_COLOR_LIGHT_SEA_GREEN 0x0020B2AA |
| #define GRAPHICS_COLOR_LIGHT_SKY_BLUE 0x0087CEFA |
| #define GRAPHICS_COLOR_LIGHT_SLATE_GRAY 0x00778899 |
| #define GRAPHICS_COLOR_LIGHT_STEEL_BLUE 0x00B0C4DE |
| #define GRAPHICS_COLOR_LIGHT_YELLOW 0x00FFFFE0 |
| #define GRAPHICS_COLOR_LIME 0x0000FF00 |
| #define GRAPHICS_COLOR_LIME_GREEN 0x0032CD32 |
| #define GRAPHICS_COLOR_LINEN 0x00FAF0E6 |
| #define GRAPHICS_COLOR_MAGENTA 0x00FF00FF |
| #define GRAPHICS_COLOR_MAROON 0x00800000 |
| #define GRAPHICS_COLOR_MEDIUM_AQUAMARINE 0x0066CDAA |
| #define GRAPHICS_COLOR_MEDIUM_BLUE 0x000000CD |
| #define GRAPHICS_COLOR_MEDIUM_ORCHID 0x00BA55D3 |
| #define GRAPHICS_COLOR_MEDIUM_PURPLE 0x009370DB |
| #define GRAPHICS_COLOR_MEDIUM_SEA_GREEN 0x003CB371 |
| #define GRAPHICS_COLOR_MEDIUM_SLATE_BLUE 0x007B68EE |
| #define GRAPHICS_COLOR_MEDIUM_SPRING_GREEN 0x0000FA9A |
| #define GRAPHICS_COLOR_MEDIUM_TURQUOISE 0x0048D1CC |
| #define GRAPHICS_COLOR_MEDIUM_VIOLET_RED 0x00C71585 |
| #define GRAPHICS_COLOR_MIGNIGHT_BLUE 0x00191970 |
| #define GRAPHICS_COLOR_MINT_CREAM 0x00F5FFFA |
| #define GRAPHICS_COLOR_MISTY_ROSE 0x00FFE4E1 |
| #define GRAPHICS_COLOR_MOCCASIN 0x00FFE4B5 |
| #define GRAPHICS_COLOR_NAVAJO_WHITE 0x00FFDEAD |
| #define GRAPHICS_COLOR_NAVY 0x00000080 |
| #define GRAPHICS_COLOR_OLD_LACE 0x00FDF5E6 |
| #define GRAPHICS_COLOR_OLIVE 0x00808000 |
| #define GRAPHICS_COLOR_OLIVE_DRAB 0x006B8E23 |
| #define GRAPHICS_COLOR_ORANGE 0x00FFA500 |
| #define GRAPHICS_COLOR_ORANGE_RED 0x00FF4500 |
| #define GRAPHICS_COLOR_ORCHID 0x00DA70D6 |
| #define GRAPHICS_COLOR_PALE_GOLDENRON 0x00EEE8AA |
| #define GRAPHICS_COLOR_PALE_GREEN 0x0098FB98 |
| #define GRAPHICS_COLOR_PALE_TURQUOISE 0x00AFEEEE |
| #define GRAPHICS_COLOR_PALE_VIOLET_RED 0x00DB7093 |
| #define GRAPHICS_COLOR_PAPAYA_WHIP 0x00FFEFD5 |
| #define GRAPHICS_COLOR_PEACH_PUFF 0x00FFDAB9 |
| #define GRAPHICS_COLOR_PERU 0x00CD853F |
| #define GRAPHICS_COLOR_PINK 0x00FFC0CB |
| #define GRAPHICS_COLOR_PLUM 0x00DDA0DD |
| #define GRAPHICS_COLOR_POWDER_BLUE 0x00B0E0E6 |
| #define GRAPHICS_COLOR_PURPLE 0x00800080 |
| #define GRAPHICS_COLOR_RED 0x00FF0000 |
| #define GRAPHICS_COLOR_ROSY_BROWN 0x00BC8F8F |
| #define GRAPHICS_COLOR_ROYAL_BLUE 0x004169E1 |
| #define GRAPHICS_COLOR_SADDLE_BROWN 0x008B4513 |
| #define GRAPHICS_COLOR_SALMON 0x00FA8072 |
| #define GRAPHICS_COLOR_SANDY_BROWN 0x00F4A460 |
| #define GRAPHICS_COLOR_SEA_GREEN 0x002E8B57 |
| #define GRAPHICS_COLOR_SEASHELL 0x00FFF5EE |
| #define GRAPHICS_COLOR_SIENNA 0x00A0522D |
| #define GRAPHICS_COLOR_SILVER 0x00C0C0C0 |
| #define GRAPHICS_COLOR_SKY_BLUE 0x0087CEEB |
| #define GRAPHICS_COLOR_SLATE_BLUE 0x006A5ACD |
| #define GRAPHICS_COLOR_SLATE_GRAY 0x00708090 |
| #define GRAPHICS_COLOR_SNOW 0x00FFFAFA |
| #define GRAPHICS_COLOR_SPRING_GREEN 0x0000FF7F |
| #define GRAPHICS_COLOR_STEEL_BLUE 0x004682B4 |
| #define GRAPHICS_COLOR_TAN 0x00D2B48C |
| #define GRAPHICS_COLOR_TEAL 0x00008080 |
| #define GRAPHICS_COLOR_THISTLE 0x00D8BFD8 |
| #define GRAPHICS_COLOR_TOMATO 0x00FF6347 |
| #define GRAPHICS_COLOR_TURQUOISE 0x0040E0D0 |
| #define GRAPHICS_COLOR_VIOLET 0x00EE82EE |
| #define GRAPHICS_COLOR_WHEAT 0x00F5DEB3 |
| #define GRAPHICS_COLOR_WHITE 0x00FFFFFF |
| #define GRAPHICS_COLOR_WHITE_SMOKE 0x00F5F5F5 |
| #define GRAPHICS_COLOR_YELLOW 0x00FFFF00 |
| #define GRAPHICS_COLOR_YELLOW_GREEN 0x009ACD32 |
| #define ClrRedMask 0x00FF0000 |
| #define ClrRedShift 16 |
| #define ClrGreenMask 0x0000FF00 |
| #define ClrGreenShift 8 |
| #define ClrBlueMask 0x000000FF |
| #define ClrBlueShift 0 |
| #define GrLangZhPRC 0x0804 |
| #define GrLangZhTW 0x0404 |
| #define GrLangEnUS 0x0409 |
| #define GrLangEnUK 0x0809 |
| #define GrLangEnAUS 0x0C09 |
| #define GrLangEnCA 0x1009 |
| #define GrLangEnNZ 0x1409 |
| #define GrLangFr 0x040C |
| #define GrLangDe 0x0407 |
| #define GrLangHi 0x0439 |
| #define GrLangIt 0x0410 |
| #define GrLangJp 0x0411 |
| #define GrLangKo 0x0412 |
| #define GrLangEsMX 0x080A |
| #define GrLangEsSP 0x0C0A |
| #define GrLangSwKE 0x0441 |
| #define GrLangUrIN 0x0820 |
| #define GrLangUrPK 0x0420 |
| typedef struct Graphics_Image Graphics_Image |
This structure defines the characteristics of a Bitmap Image.
| typedef struct Graphics_Rectangle Graphics_Rectangle |
This structure defines the extents of a rectangle. All points greater than or equal to the minimum and less than or equal to the maximum are part of the rectangle.
| typedef struct Graphics_Display Graphics_Display |
| typedef struct Graphics_Display_Functions Graphics_Display_Functions |
This structure defines the implementation of a display driver.
| typedef struct Graphics_Font Graphics_Font |
This structure describes a font used for drawing text onto the screen.
| typedef struct Graphics_FontEx Graphics_FontEx |
This is a newer version of the structure which describes a font used for drawing text onto the screen. This variant allows a font to contain an arbitrary, contiguous block of codepoints from the 256 basic characters in an ISO8859-n font and allows support for accented characters in Western European languages and any left-to-right typeface supported by an ISO8859 variant. Fonts encoded in this format may be used interchangeably with the original fonts merely by casting the structure pointer when calling any function or macro which expects a font pointer as a parameter.
| typedef struct Graphics_Context Graphics_Context |
This structure defines a drawing context to be used to draw onto the screen. Multiple drawing contexts may exist at any time.
| void Graphics_drawCircle | ( | const Graphics_Context * | context, |
| int32_t | x, | ||
| int32_t | y, | ||
| int32_t | radius | ||
| ) |
Draws a circle.
| context | is a pointer to the drawing context to use. |
| x | is the X coordinate of the center of the circle. |
| y | is the Y coordinate of the center of the circle. |
| radius | is the radius of the circle. |
This function draws a circle, utilizing the Bresenham circle drawing algorithm. The extent of the circle is from x - radius to x + radius and y - radius to y + radius, inclusive.
References Graphics_Context::clipRegion, Graphics_drawPixel(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawRadioButton().
| void Graphics_fillCircle | ( | const Graphics_Context * | context, |
| int32_t | x, | ||
| int32_t | y, | ||
| int32_t | radius | ||
| ) |
Draws a filled circle.
| context | is a pointer to the drawing context to use. |
| x | is the X coordinate of the center of the circle. |
| y | is the Y coordinate of the center of the circle. |
| radius | is the radius of the circle. |
This function draws a filled circle, utilizing the Bresenham circle drawing algorithm. The extent of the circle is from x - radius to x + radius and y - radius to y + radius, inclusive.
References Graphics_Context::clipRegion, Graphics_drawLineH(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawRadioButton(), Graphics_drawReleasedRadioButton(), and Graphics_drawSelectedRadioButton().
| void Graphics_setClipRegion | ( | Graphics_Context * | context, |
| Graphics_Rectangle * | rect | ||
| ) |
Sets the extents of the clipping region.
| context | is a pointer to the drawing context to use. |
| rect | is a pointer to the structure containing the extents of the clipping region. |
This function sets the extents of the clipping region. The clipping region is not allowed to exceed the extents of the screen, but may be a portion of the screen.
The supplied coordinate are inclusive; xMin of 1 and xMax of 1 will define a clipping region that will display only the pixels in the X = 1 column. A consequence of this is that the clipping region must contain at least one row and one column.
References Graphics_Context::clipRegion, Graphics_Context::display, Graphics_getHeightOfDisplay(), Graphics_getWidthOfDisplay(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
| void Graphics_initContext | ( | Graphics_Context * | context, |
| Graphics_Display * | display, | ||
| const Graphics_Display_Functions * | pFxns | ||
| ) |
Initializes a drawing context.
| context | is a pointer to the drawing context to initialize. |
| display | is a pointer to the Graphics_Display Info structure that describes the display driver to use. |
| pFxns | isa pointer to driver functions. |
This function initializes a drawing context, preparing it for use. The provided display driver will be used for all subsequent graphics operations, and the default clipping region will be set to the extent of the screen.
References Graphics_Context::background, Graphics_Context::clipRegion, Graphics_Context::display, Graphics_Context::font, Graphics_Context::foreground, Graphics_Display::heigth, Graphics_Display::pFxns, Graphics_Context::size, Graphics_Display::width, Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
| void Graphics_drawImage | ( | const Graphics_Context * | context, |
| const Graphics_Image * | bitmap, | ||
| int16_t | x, | ||
| int16_t | y | ||
| ) |
Draws a bitmap image.
| context | is a pointer to the drawing context to use. |
| bitmap | is a pointer to the image to draw. |
| x | is the X coordinate of the upper left corner of the image. |
| y | is the Y coordinate of the upper left corner of the image. |
This function draws a bitmap image. The image may be 1 bit per pixel, 4 bits per pixel or 8 bits per pixel (using a palette supplied in the image data). It can be uncompressed data, or it can be compressed using several different compression types. Compression options are 4-bit run length encoding, 8-bit run length encoding, and a custom run length encoding variation written for complex 8-bit per pixel images.
References Graphics_Image::bPP, Graphics_Context::clipRegion, Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Image::xSize, Graphics_Rectangle::yMax, Graphics_Rectangle::yMin, and Graphics_Image::ySize.
Referenced by Graphics_drawImageButton(), Graphics_drawReleasedImageButton(), and Graphics_drawSelectedImageButton().
| void Graphics_drawLine | ( | const Graphics_Context * | context, |
| int32_t | x1, | ||
| int32_t | y1, | ||
| int32_t | x2, | ||
| int32_t | y2 | ||
| ) |
Draws a line.
| context | is a pointer to the drawing context to use. |
| x1 | is the X coordinate of the start of the line. |
| y1 | is the Y coordinate of the start of the line. |
| x2 | is the X coordinate of the end of the line. |
| y2 | is the Y coordinate of the end of the line. |
This function draws a line, utilizing Graphics_drawLineH() and Graphics_drawLineV() to draw the line as efficiently as possible. The line is clipped to the clippping rectangle using the Cohen-Sutherland clipping algorithm, and then scan converted using Bresenham's line drawing algorithm.
References Graphics_drawLineH(), and Graphics_drawLineV().
Referenced by Graphics_drawCheckBox(), and Graphics_drawSelectedCheckBox().
| void Graphics_drawLineH | ( | const Graphics_Context * | context, |
| int32_t | x1, | ||
| int32_t | x2, | ||
| int32_t | y | ||
| ) |
Draws a horizontal line.
| context | is a pointer to the drawing context to use. |
| x1 | is the X coordinate of one end of the line. |
| x2 | is the X coordinate of the other end of the line. |
| y | is the Y coordinate of the line. |
This function draws a horizontal line, taking advantage of the fact that the line is horizontal to draw it more efficiently. The clipping of the horizontal line to the clipping rectangle is performed within this routine; the display driver's horizontal line routine is used to perform the actual line drawing.
References Graphics_Context::clipRegion, Graphics_Context::display, Graphics_Context::foreground, Graphics_drawHorizontalLineOnDisplay(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, and Graphics_Rectangle::yMax.
Referenced by Graphics_drawLine(), Graphics_drawRectangle(), and Graphics_fillCircle().
| void Graphics_drawLineV | ( | const Graphics_Context * | context, |
| int32_t | x, | ||
| int32_t | y1, | ||
| int32_t | y2 | ||
| ) |
Draws a vertical line.
| context | is a pointer to the drawing context to use. |
| x | is the X coordinate of the line. |
| y1 | is the Y coordinate of one end of the line. |
| y2 | is the Y coordinate of the other end of the line. |
This function draws a vertical line, taking advantage of the fact that the line is vertical to draw it more efficiently. The clipping of the vertical line to the clipping rectangle is performed within this routine; the display driver's vertical line routine is used to perform the actual line drawing.
References Graphics_Context::clipRegion, Graphics_Context::display, Graphics_Context::foreground, Graphics_drawVerticalLineOnDisplay(), Graphics_Rectangle::xMax, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawLine(), and Graphics_drawRectangle().
| void Graphics_drawRectangle | ( | const Graphics_Context * | context, |
| const Graphics_Rectangle * | rect | ||
| ) |
Draws a rectangle.
| context | is a pointer to the drawing context to use. |
| rect | is a pointer to the structure containing the extents of the rectangle. |
This function draws a rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive.
References Graphics_drawLineH(), Graphics_drawLineV(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawCheckBox(), and Graphics_drawReleasedCheckBox().
| void Graphics_fillRectangle | ( | const Graphics_Context * | context, |
| const Graphics_Rectangle * | rect | ||
| ) |
Draws a filled rectangle.
| context | is a pointer to the drawing context to use. |
| rect | is a pointer to the structure containing the extents of the rectangle. |
This function draws a filled rectangle. The rectangle will extend from xMin to xMax and yMin to yMax, inclusive. The clipping of the rectangle to the clipping rectangle is performed within this routine; the display driver's rectangle fill routine is used to perform the actual rectangle fill.
References Graphics_Context::clipRegion, Graphics_Context::display, Graphics_Context::foreground, Graphics_fillRectangleOnDisplay(), Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawCheckBox(), Graphics_drawImageButton(), Graphics_drawReleasedCheckBox(), Graphics_drawReleasedImageButton(), and Graphics_drawSelectedImageButton().
| void Graphics_drawString | ( | const Graphics_Context * | context, |
| int8_t * | string, | ||
| int32_t | length, | ||
| int32_t | x, | ||
| int32_t | y, | ||
| bool | opaque | ||
| ) |
Draws a string.
| context | is a pointer to the drawing context to use. |
| string | is a pointer to the string to be drawn. |
| length | is the number of characters from the string that should be drawn on the screen. |
| x | is the X coordinate of the upper left corner of the string position on the screen. |
| y | is the Y coordinate of the upper left corner of the string position on the screen. |
| opaque | is true if the background of each character should be drawn and false if it should not (leaving the background as is). |
This function draws a string of test on the screen. The length parameter allows a portion of the string to be examined without having to insert a NULL character at the stopping point (which would not be possible if the string was located in flash); specifying a length of -1 will cause the entire string to be rendered (subject to clipping).
References Graphics_Context::clipRegion, Graphics_Font::data, Graphics_FontEx::data, Graphics_FontEx::first, Graphics_Context::font, Graphics_Font::format, GRAPHICS_ABSENT_CHAR_REPLACEMENT, GRAPHICS_FONT_EX_MARKER, GRAPHICS_FONT_FMT_UNCOMPRESSED, Graphics_FontEx::last, Graphics_Font::offset, Graphics_FontEx::offset, Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, and Graphics_Rectangle::yMax.
Referenced by Graphics_drawCheckBox(), Graphics_drawRadioButton(), and Graphics_drawStringCentered().
| int32_t Graphics_getStringWidth | ( | const Graphics_Context * | context, |
| const int8_t * | string, | ||
| int32_t | length | ||
| ) |
Determines the width of a string.
| context | is a pointer to the drawing context to use. |
| string | is the string in question. |
| length | is the length of the string. |
This function determines the width of a string (or portion of the string) when drawn with a particular font. The length parameter allows a portion of the string to be examined without having to insert a NULL character at the stopping point (would not be possible if the string was located in flash); specifying a length of -1 will cause the width of the entire string to be computed.
References Graphics_Font::data, Graphics_FontEx::data, Graphics_FontEx::first, Graphics_Context::font, Graphics_Font::format, GRAPHICS_ABSENT_CHAR_REPLACEMENT, GRAPHICS_FONT_EX_MARKER, Graphics_FontEx::last, Graphics_Font::offset, and Graphics_FontEx::offset.
Referenced by Graphics_drawStringCentered().
| int32_t Graphics_isOverlappingRectangle | ( | Graphics_Rectangle * | psRect1, |
| Graphics_Rectangle * | psRect2 | ||
| ) |
| int32_t Graphics_getRectangleIntersection | ( | Graphics_Rectangle * | rect1, |
| Graphics_Rectangle * | rect2, | ||
| Graphics_Rectangle * | intersect | ||
| ) |
Determines the intersection of two rectangles.
| rect1 | is a pointer to the first rectangle. |
| rect2 | is a pointer to the second rectangle. |
| intersect | is a pointer to a rectangle which will be written with the intersection of rect1 and rect2. |
This function determines if two rectangles overlap and, if they do, calculates the rectangle representing their intersection. If the rectangles do not overlap, 0 is returned and intersect is not written.
References Graphics_isRectangleOverlap(), max, min, Graphics_Rectangle::xMax, Graphics_Rectangle::xMin, Graphics_Rectangle::yMax, and Graphics_Rectangle::yMin.
| void Graphics_setBackgroundColor | ( | Graphics_Context * | context, |
| int32_t | value | ||
| ) |
Sets the background color to be used.
| context | is a pointer to the drawing context to modify. |
| value | is the 24-bit RGB color to be used. |
This function sets the background color to be used for drawing operations in the specified drawing context.
References Graphics_Context::background, Graphics_Context::display, and Graphics_translateColorOnDisplay().
| uint16_t Graphics_getDisplayWidth | ( | Graphics_Context * | context | ) |
Gets the width of the display being used by this drawing context.
| context | is a pointer to the drawing context to query. |
This function returns the width of the display that is being used by this drawing context.
References Graphics_Context::display, and Graphics_Display::width.
| uint16_t Graphics_getDisplayHeight | ( | Graphics_Context * | context | ) |
Gets the height of the display being used by this drawing context.
| context | is a pointer to the drawing context to query. |
This function returns the height of the display that is being used by this drawing context.
References Graphics_Context::display, and Graphics_Display::heigth.
| void Graphics_setFont | ( | Graphics_Context * | context, |
| const Graphics_Font * | font | ||
| ) |
Sets the font to be used.
| context | is a pointer to the drawing context to modify. |
| font | is a pointer to the font to be used. |
This function sets the font to be used for string drawing operations in the specified drawing context. If a tFontEx type font is to be used, cast its pointer to a font pointer before passing it as the font parameter.
References Graphics_Context::font.
Referenced by Graphics_drawCheckBox(), Graphics_drawImageButton(), Graphics_drawRadioButton(), Graphics_drawReleasedImageButton(), Graphics_drawSelectedImageButton(), and Graphics_drawSelectedRadioButton().
| uint8_t Graphics_getFontBaseline | ( | const Graphics_Font * | font | ) |
Gets the baseline of a font.
| font | is a pointer to the font to query. |
This function determines the baseline position of a font. The baseline is the offset between the top of the font and the bottom of the capital letters. The only font data that exists below the baseline are the descenders on some lower-case letters (such as ``y'').
References Graphics_Font::baseline.
| void Graphics_setForegroundColor | ( | Graphics_Context * | context, |
| int32_t | value | ||
| ) |
Sets the foreground color to be used.
| context | is a pointer to the drawing context to modify. |
| value | is the 24-bit RGB color to be used. |
This function sets the color to be used for drawing operations in the specified drawing context.
References Graphics_Context::display, Graphics_Context::foreground, and Graphics_translateColorOnDisplay().
Referenced by Graphics_drawCheckBox(), Graphics_drawImageButton(), Graphics_drawRadioButton(), Graphics_drawReleasedCheckBox(), Graphics_drawReleasedImageButton(), Graphics_drawReleasedRadioButton(), Graphics_drawSelectedCheckBox(), Graphics_drawSelectedImageButton(), and Graphics_drawSelectedRadioButton().
| void Graphics_setForegroundColorTranslated | ( | Graphics_Context * | context, |
| int32_t | value | ||
| ) |
Sets the foreground color to be used.
| context | is a pointer to the drawing context to modify. |
| value | is the display driver-specific color to be used. |
This function sets the foreground color to be used for drawing operations in the specified drawing context, using a color that has been previously translated to a driver-specific color (for example, via Graphics_translateColorDisplay()).
References Graphics_Context::foreground.
| uint8_t Graphics_getFontHeight | ( | const Graphics_Font * | font | ) |
Gets the height of a font.
| font | is a pointer to the font to query. |
This function determines the height of a font. The height is the offset between the top of the font and the bottom of the font, including any ascenders and descenders.
References Graphics_Font::height.
| uint8_t Graphics_getFontMaxWidth | ( | const Graphics_Font * | font | ) |
Gets the maximum width of a font.
| font | is a pointer to the font to query. |
This function determines the maximum width of a font. The maximum width is the width of the widest individual character in the font.
References Graphics_Font::maxWidth.
| uint16_t Graphics_getImageColors | ( | const Graphics_Image * | image | ) |
Gets the number of colors in an image.
| image | is a tImage struct |
This function determines the number of colors in the palette of an image. This is only valid for 4bpp and 8bpp images; 1bpp images do not contain a palette.
References Graphics_Image::numColors.
| uint16_t Graphics_getImageHeight | ( | const Graphics_Image * | image | ) |
Gets the height of an image.
| image | is a tImage struct |
This function determines the height of an image in pixels.
References Graphics_Image::ySize.
| uint16_t Graphics_getImageWidth | ( | const Graphics_Image * | image | ) |
Gets the width of an image.
| image | is a tImage struct |
This function determines the width of an image in pixels.
References Graphics_Image::xSize.
| uint32_t Graphics_getOffscreen1BppImageSize | ( | uint16_t | width, |
| uint16_t | height | ||
| ) |
Determines the size of the buffer for a 1 BPP off-screen image.
| width | is the width of the image in pixels. |
| height | is the height of the image in pixels. |
This function determines the size of the memory buffer required to hold a 1 BPP off-screen image of the specified geometry.
| uint32_t Graphics_getOffscreen4BppImageSize | ( | uint16_t | width, |
| uint16_t | height | ||
| ) |
Determines the size of the buffer for a 4 BPP off-screen image.
| width | is the width of the image in pixels. |
| height | is the height of the image in pixels. |
This function determines the size of the memory buffer required to hold a 4 BPP off-screen image of the specified geometry.
| uint32_t Graphics_getOffScreen8BPPSize | ( | uint16_t | width, |
| uint16_t | height | ||
| ) |
Determines the size of the buffer for an 8 BPP off-screen image.
| width | is the width of the image in pixels. |
| height | is the height of the image in pixels. |
This function determines the size of the memory buffer required to hold an 8 BPP off-screen image of the specified geometry.
| void Graphics_drawStringCentered | ( | const Graphics_Context * | context, |
| int8_t * | string, | ||
| int32_t | length, | ||
| int32_t | x, | ||
| int32_t | y, | ||
| bool | opaque | ||
| ) |
Draws a centered string.
| context | is a pointer to the drawing context to use. |
| string | is a pointer to the string to be drawn. |
| length | is the number of characters from the string that should be drawn on the screen. |
| x | is the X coordinate of the center of the string position on the screen. |
| y | is the Y coordinate of the center of the string position on the screen. |
| opaque | is true if the background of each character should be drawn and false if it should not (leaving the background as is). |
This function draws a string of test on the screen centered upon the provided position. The lLength parameter allows a portion of the string to be examined without having to insert a NULL character at the stopping point (which would not be possible if the string was located in flash); specifying a length of -1 will cause the entire string to be rendered (subject to clipping).
References Graphics_Font::baseline, Graphics_Context::font, Graphics_drawString(), and Graphics_getStringWidth().
| uint8_t Graphics_getStringHeight | ( | const Graphics_Context * | context | ) |
Gets the height of a string.
| context | is a pointer to the drawing context to query. |
This function determines the height of a string. The height is the offset between the top of the string and the bottom of the string, including any ascenders and descenders. Note that this will not account for the case where the string in question does not have any characters that use descenders but the font in the drawing context does contain characters with descenders.
References Graphics_Context::font, and Graphics_Font::height.
| uint8_t Graphics_getStringMaxWidth | ( | const Graphics_Context * | context | ) |
Gets the maximum width of a character in a string.
| context | is a pointer to the drawing context to query. |
This function determines the maximum width of a character in a string. The maximum width is the width of the widest individual character in the font used to render the string, which may be wider than the widest character that is used to render a particular string.
References Graphics_Context::font, and Graphics_Font::maxWidth.
| uint8_t Graphics_getStringBaseline | ( | const Graphics_Context * | context | ) |
Gets the baseline of a string.
| context | is a pointer to the drawing context to query. |
This function determines the baseline position of a string. The baseline is the offset between the top of the string and the bottom of the capital letters. The only string data that exists below the baseline are the descenders on some lower-case letters (such as ``y'').
References Graphics_Font::baseline, and Graphics_Context::font.
| uint32_t Graphics_translateColorOnDisplay | ( | const Graphics_Display * | display, |
| uint32_t | value | ||
| ) |
Translates a 24-bit RGB color to a display driver-specific color.
| display | is the pointer to the display driver structure for the display to operate upon. |
| value | is the 24-bit RGB color. The least-significant byte is the blue channel, the next byte is the green channel, and the third byte is the red channel. |
This function translates a 24-bit RGB color into a value that can be written into the display's frame buffer in order to reproduce that color, or the closest possible approximation of that color.
References Graphics_Display_Functions::pfnColorTranslate, and Graphics_Display::pFxns.
Referenced by Graphics_setBackgroundColor(), and Graphics_setForegroundColor().
| void Graphics_drawHorizontalLineOnDisplay | ( | const Graphics_Display * | display, |
| uint16_t | x1, | ||
| uint16_t | x2, | ||
| uint16_t | y, | ||
| uint32_t | value | ||
| ) |
Draws a horizontal line on a display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| x1 | is the starting X coordinate of the line. |
| x2 | is the ending X coordinate of the line. |
| y | is the Y coordinate of the line. |
| value | is the color to draw the line. |
This function draws a horizontal line on a display. This assumes that clipping has already been performed, and that both end points of the line are within the extents of the display.
References Graphics_Display_Functions::pfnLineDrawH, and Graphics_Display::pFxns.
Referenced by Graphics_drawLineH().
| void Graphics_drawVerticalLineOnDisplay | ( | const Graphics_Display * | display, |
| uint16_t | x, | ||
| uint16_t | y1, | ||
| uint16_t | y2, | ||
| uint16_t | value | ||
| ) |
Draws a vertical line on a display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| x | is the X coordinate of the line. |
| y1 | is the starting Y coordinate of the line. |
| y2 | is the ending Y coordinate of the line. |
| value | is the color to draw the line. |
This function draws a vertical line on a display. This assumes that clipping has already been performed, and that both end points of the line are within the extents of the display.
References Graphics_Display_Functions::pfnLineDrawV, and Graphics_Display::pFxns.
Referenced by Graphics_drawLineV().
| void Graphics_fillRectangleOnDisplay | ( | const Graphics_Display * | display, |
| const Graphics_Rectangle * | rect, | ||
| uint16_t | value | ||
| ) |
Fills a rectangle on a display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| rect | is a pointer to the structure describing the rectangle to fill. |
| value | is the color to fill the rectangle. |
This function fills a rectangle on the display. This assumes that clipping has already been performed, and that all sides of the rectangle are within the extents of the display.
References Graphics_Display_Functions::pfnRectFill, and Graphics_Display::pFxns.
Referenced by Graphics_fillRectangle().
| void Graphics_flushOnDisplay | ( | const Graphics_Display * | display | ) |
Flushes cached drawing operations.
| display | is the pointer to the display driver structure for the display to operate upon. |
This function flushes any cached drawing operations on a display.
References Graphics_Display_Functions::pfnFlush, and Graphics_Display::pFxns.
Referenced by Graphics_flushBuffer().
| void Graphics_drawPixel | ( | const Graphics_Context * | context, |
| uint16_t | x, | ||
| uint16_t | y | ||
| ) |
Draws a pixel.
| context | is a pointer to the drawing context to use. |
| x | is the X coordinate of the pixel. |
| y | is the Y coordinate of the pixel. |
This function draws a pixel if it resides within the clipping region.
References Graphics_Context::clipRegion, Graphics_Context::display, Graphics_Context::foreground, Graphics_drawPixelOnDisplay(), Graphics_Rectangle::xMin, and Graphics_Rectangle::yMin.
Referenced by Graphics_drawCircle().
| void Graphics_clearDisplay | ( | const Graphics_Context * | context | ) |
Forces a clear screen. Contents of Display buffer unmodified
| context | is a pointer to the drawing context to use. |
This function forces a clear screen.
References Graphics_Context::background, Graphics_Context::display, and Graphics_clearDisplayOnDisplay().
| uint16_t Graphics_getHeightOfDisplay | ( | const Graphics_Display * | display | ) |
Gets the height of the display.
| display | is a pointer to the display driver structure for the display to query. |
This function determines the height of the display.
References Graphics_Display::heigth.
Referenced by Graphics_setClipRegion().
| void Graphics_flushBuffer | ( | const Graphics_Context * | context | ) |
Flushes any cached drawing operations.
| context | is a pointer to the drawing context to use. |
This function flushes any cached drawing operations. For display drivers that draw into a local frame buffer before writing to the actual display, calling this function will cause the display to be updated to match the contents of the local frame buffer.
References Graphics_Context::display, and Graphics_flushOnDisplay().
| uint16_t Graphics_getWidthOfDisplay | ( | const Graphics_Display * | display | ) |
Gets the width of the display.
| display | is a pointer to the display driver structure for the display to query. |
This function determines the width of the display.
References Graphics_Display::width.
Referenced by Graphics_setClipRegion().
| bool Graphics_isPointWithinRectangle | ( | const Graphics_Rectangle * | rect, |
| uint16_t | x, | ||
| uint16_t | y | ||
| ) |
Determines if a point lies within a given rectangle.
| rect | is a pointer to the rectangle which the point is to be checked against. |
| x | is the X coordinate of the point to be checked. |
| y | is the Y coordinate of the point to be checked. |
This function determines whether point (x, y) lies within the rectangle described by rect.
| void Graphics_drawPixelOnDisplay | ( | const Graphics_Display * | display, |
| uint16_t | x, | ||
| uint16_t | y, | ||
| uint16_t | value | ||
| ) |
Draws a pixel on a display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| x | is the X coordinate of the pixel. |
| y | is the Y coordinate of the pixel. |
| value | is the color to draw the pixel. |
This function draws a pixel on a display. This assumes that clipping has already been performed.
References Graphics_Display_Functions::pfnPixelDraw, and Graphics_Display::pFxns.
Referenced by Graphics_drawPixel().
| void Graphics_clearDisplayOnDisplay | ( | const Graphics_Display * | display, |
| uint16_t | value | ||
| ) |
Forces a clear Display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| value | is the current background color to fill the screen with. |
This function clears the Display
References Graphics_Display_Functions::pfnClearDisplay, and Graphics_Display::pFxns.
Referenced by Graphics_clearDisplay().
| void Graphics_drawMultiplePixelsOnDisplay | ( | const Graphics_Display * | display, |
| uint16_t | x, | ||
| uint16_t | y, | ||
| uint16_t | x0, | ||
| uint16_t | count, | ||
| uint16_t | bPP, | ||
| const uint8_t * | data, | ||
| const uint32_t * | palette | ||
| ) |
Draws a horizontal sequence of pixels on a display.
| display | is the pointer to the display driver structure for the display to operate upon. |
| x | is the X coordinate of the first pixel. |
| y | is the Y coordinate of the first pixel. |
| x0 | is sub-pixel offset within the pixel data, which is valid for 1 or 4 bit per pixel formats. |
| count | is the number of pixels to draw. |
| bPP | is the number of bits per pixel; must be 1, 4, or 8. |
| data | is a pointer to the pixel data. For 1 and 4 bit per pixel formats, the most significant bit(s) represent the left-most pixel. |
| palette | is a pointer to the palette used to draw the pixels. |
This function draws a horizontal sequence of pixels on a display, using the supplied palette. For 1 bit per pixel format, the palette contains pre-translated colors; for 4 and 8 bit per pixel formats, the palette contains 24-bit RGB values that must be translated before being written to the display.
References Graphics_Display_Functions::pfnPixelDrawMultiple, and Graphics_Display::pFxns.
| void Graphics_initOffscreen1BppImage | ( | Graphics_Display * | display, |
| uint8_t * | image, | ||
| int32_t | width, | ||
| int32_t | height | ||
| ) |
| void Graphics_initOffscreen4BppImage | ( | Graphics_Display * | display, |
| uint8_t * | image, | ||
| int32_t | width, | ||
| int32_t | height | ||
| ) |
| void Graphics_setOffscreen4BppPalette | ( | Graphics_Display * | display, |
| uint32_t * | ppalette, | ||
| uint32_t | offset, | ||
| uint32_t | count | ||
| ) |
| void Graphics_initOffscreen8BppImage | ( | Graphics_Display * | display, |
| uint8_t * | image, | ||
| int32_t | width, | ||
| int32_t | height | ||
| ) |
| void Graphics_setOffscreen8BppPalette | ( | Graphics_Display * | display, |
| uint32_t * | ppalette, | ||
| uint32_t | offset, | ||
| uint32_t | count | ||
| ) |
| const Graphics_Font g_sFontCm12 |
| const Graphics_Font g_sFontCm12b |
| const Graphics_Font g_sFontCm12i |
| const Graphics_Font g_sFontCm14 |
| const Graphics_Font g_sFontCm14b |
| const Graphics_Font g_sFontCm14i |
| const Graphics_Font g_sFontCm16 |
| const Graphics_Font g_sFontCm16b |
| const Graphics_Font g_sFontCm16i |
| const Graphics_Font g_sFontCm18 |
| const Graphics_Font g_sFontCm18b |
| const Graphics_Font g_sFontCm18i |
| const Graphics_Font g_sFontCm20 |
| const Graphics_Font g_sFontCm20b |
| const Graphics_Font g_sFontCm20i |
| const Graphics_Font g_sFontCm22 |
| const Graphics_Font g_sFontCm22b |
| const Graphics_Font g_sFontCm22i |
| const Graphics_Font g_sFontCm24 |
| const Graphics_Font g_sFontCm24b |
| const Graphics_Font g_sFontCm24i |
| const Graphics_Font g_sFontCm26 |
| const Graphics_Font g_sFontCm26b |
| const Graphics_Font g_sFontCm26i |
| const Graphics_Font g_sFontCm28 |
| const Graphics_Font g_sFontCm28b |
| const Graphics_Font g_sFontCm28i |
| const Graphics_Font g_sFontCm30 |
| const Graphics_Font g_sFontCm30b |
| const Graphics_Font g_sFontCm30i |
| const Graphics_Font g_sFontCm32 |
| const Graphics_Font g_sFontCm32b |
| const Graphics_Font g_sFontCm32i |
| const Graphics_Font g_sFontCm34 |
| const Graphics_Font g_sFontCm34b |
| const Graphics_Font g_sFontCm34i |
| const Graphics_Font g_sFontCm36 |
| const Graphics_Font g_sFontCm36b |
| const Graphics_Font g_sFontCm36i |
| const Graphics_Font g_sFontCm38 |
| const Graphics_Font g_sFontCm38b |
| const Graphics_Font g_sFontCm38i |
| const Graphics_Font g_sFontCm40 |
| const Graphics_Font g_sFontCm40b |
| const Graphics_Font g_sFontCm40i |
| const Graphics_Font g_sFontCm42 |
| const Graphics_Font g_sFontCm42b |
| const Graphics_Font g_sFontCm42i |
| const Graphics_Font g_sFontCm44 |
| const Graphics_Font g_sFontCm44b |
| const Graphics_Font g_sFontCm44i |
| const Graphics_Font g_sFontCm46 |
| const Graphics_Font g_sFontCm46b |
| const Graphics_Font g_sFontCm46i |
| const Graphics_Font g_sFontCm48 |
| const Graphics_Font g_sFontCm48b |
| const Graphics_Font g_sFontCm48i |
| const Graphics_Font g_sFontCmsc12 |
| const Graphics_Font g_sFontCmsc14 |
| const Graphics_Font g_sFontCmsc16 |
| const Graphics_Font g_sFontCmsc18 |
| const Graphics_Font g_sFontCmsc20 |
| const Graphics_Font g_sFontCmsc22 |
| const Graphics_Font g_sFontCmsc24 |
| const Graphics_Font g_sFontCmsc26 |
| const Graphics_Font g_sFontCmsc28 |
| const Graphics_Font g_sFontCmsc30 |
| const Graphics_Font g_sFontCmsc32 |
| const Graphics_Font g_sFontCmsc34 |
| const Graphics_Font g_sFontCmsc36 |
| const Graphics_Font g_sFontCmsc38 |
| const Graphics_Font g_sFontCmsc40 |
| const Graphics_Font g_sFontCmsc42 |
| const Graphics_Font g_sFontCmsc44 |
| const Graphics_Font g_sFontCmsc46 |
| const Graphics_Font g_sFontCmsc48 |
| const Graphics_Font g_sFontCmss12 |
| const Graphics_Font g_sFontCmss12b |
| const Graphics_Font g_sFontCmss12i |
| const Graphics_Font g_sFontCmss14 |
| const Graphics_Font g_sFontCmss14b |
| const Graphics_Font g_sFontCmss14i |
| const Graphics_Font g_sFontCmss16 |
| const Graphics_Font g_sFontCmss16b |
| const Graphics_Font g_sFontCmss16i |
| const Graphics_Font g_sFontCmss18 |
| const Graphics_Font g_sFontCmss18b |
| const Graphics_Font g_sFontCmss18i |
| const Graphics_Font g_sFontCmss20 |
| const Graphics_Font g_sFontCmss20b |
| const Graphics_Font g_sFontCmss20i |
| const Graphics_Font g_sFontCmss22 |
| const Graphics_Font g_sFontCmss22b |
| const Graphics_Font g_sFontCmss22i |
| const Graphics_Font g_sFontCmss24 |
| const Graphics_Font g_sFontCmss24b |
| const Graphics_Font g_sFontCmss24i |
| const Graphics_Font g_sFontCmss26 |
| const Graphics_Font g_sFontCmss26b |
| const Graphics_Font g_sFontCmss26i |
| const Graphics_Font g_sFontCmss28 |
| const Graphics_Font g_sFontCmss28b |
| const Graphics_Font g_sFontCmss28i |
| const Graphics_Font g_sFontCmss30 |
| const Graphics_Font g_sFontCmss30b |
| const Graphics_Font g_sFontCmss30i |
| const Graphics_Font g_sFontCmss32 |
| const Graphics_Font g_sFontCmss32b |
| const Graphics_Font g_sFontCmss32i |
| const Graphics_Font g_sFontCmss34 |
| const Graphics_Font g_sFontCmss34b |
| const Graphics_Font g_sFontCmss34i |
| const Graphics_Font g_sFontCmss36 |
| const Graphics_Font g_sFontCmss36b |
| const Graphics_Font g_sFontCmss36i |
| const Graphics_Font g_sFontCmss38 |
| const Graphics_Font g_sFontCmss38b |
| const Graphics_Font g_sFontCmss38i |
| const Graphics_Font g_sFontCmss40 |
| const Graphics_Font g_sFontCmss40b |
| const Graphics_Font g_sFontCmss40i |
| const Graphics_Font g_sFontCmss42 |
| const Graphics_Font g_sFontCmss42b |
| const Graphics_Font g_sFontCmss42i |
| const Graphics_Font g_sFontCmss44 |
| const Graphics_Font g_sFontCmss44b |
| const Graphics_Font g_sFontCmss44i |
| const Graphics_Font g_sFontCmss46 |
| const Graphics_Font g_sFontCmss46b |
| const Graphics_Font g_sFontCmss46i |
| const Graphics_Font g_sFontCmss48 |
| const Graphics_Font g_sFontCmss48b |
| const Graphics_Font g_sFontCmss48i |
| const Graphics_Font g_sFontCmtt12 |
| const Graphics_Font g_sFontCmtt14 |
| const Graphics_Font g_sFontCmtt16 |
| const Graphics_Font g_sFontCmtt18 |
| const Graphics_Font g_sFontCmtt20 |
| const Graphics_Font g_sFontCmtt22 |
| const Graphics_Font g_sFontCmtt24 |
| const Graphics_Font g_sFontCmtt26 |
| const Graphics_Font g_sFontCmtt28 |
| const Graphics_Font g_sFontCmtt30 |
| const Graphics_Font g_sFontCmtt32 |
| const Graphics_Font g_sFontCmtt34 |
| const Graphics_Font g_sFontCmtt36 |
| const Graphics_Font g_sFontCmtt38 |
| const Graphics_Font g_sFontCmtt40 |
| const Graphics_Font g_sFontCmtt42 |
| const Graphics_Font g_sFontCmtt44 |
| const Graphics_Font g_sFontCmtt46 |
| const Graphics_Font g_sFontCmtt48 |
| const Graphics_Font g_sFontFixed6x8 |