![]() |
![]() |
#include <usbdcomp.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in mA. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnCallback |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
const uint32_t | ui32NumDevices |
The number of devices in the psDevices array. More... | |
tCompositeEntry *const | psDevices |
tCompositeInstance | sPrivateData |
The structure used by the application to define operating parameters for the composite device class.
const uint16_t tUSBDCompositeDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
const uint16_t tUSBDCompositeDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
const uint16_t tUSBDCompositeDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in mA.
const uint8_t tUSBDCompositeDevice::ui8PwrAttributes |
Indicates whether the device is self or bus-powered and whether or not it supports remote wake up. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
const tUSBCallback tUSBDCompositeDevice::pfnCallback |
A pointer to the callback function which will be called to notify the application of events relating to the operation of the composite device.
const uint8_t* const* tUSBDCompositeDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1), Composite device interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDCompositeInit().
const uint32_t tUSBDCompositeDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be 1 + ((5 + (number of strings)) * (number of languages)).
const uint32_t tUSBDCompositeDevice::ui32NumDevices |
The number of devices in the psDevices array.
tCompositeEntry* const tUSBDCompositeDevice::psDevices |
This application supplied array holds the the top level device class information as well as the Instance data for that class.
Referenced by BuildCompositeDescriptor().
tCompositeInstance tUSBDCompositeDevice::sPrivateData |
The private data for this device instance. This memory must remain accessible for as long as the composite device is in use and must not be modified by any code outside the composite class driver.
Referenced by BuildCompositeDescriptor(), and USBDCompositeInit().