EMACMSP432E4 Hardware attributes. More...
#include <EMACMSP432E4.h>
Data Fields | |
uint32_t | baseAddr |
uint32_t | intNum |
uint32_t | intPriority |
uint32_t | led0Pin |
uint32_t | led1Pin |
uint8_t * | macAddress |
EMACMSP432E4 Hardware attributes.
intPriority is the EMAC peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
uint32_t EMACMSP432E4_HWAttrs::baseAddr |
EMAC port
uint32_t EMACMSP432E4_HWAttrs::intNum |
Interrupt Vector Id
uint32_t EMACMSP432E4_HWAttrs::intPriority |
Interrupt priority
uint32_t EMACMSP432E4_HWAttrs::led0Pin |
LED0 Pin
uint32_t EMACMSP432E4_HWAttrs::led1Pin |
LED1 Pin
uint8_t* EMACMSP432E4_HWAttrs::macAddress |
Pointer to MAC address