47 #ifndef ti_drivers_emac_EMACMSP432E4__include 48 #define ti_drivers_emac_EMACMSP432E4__include 56 #include <ti/devices/msp432e4/inc/msp432.h> 58 #include <ti/devices/msp432e4/driverlib/pin_map.h> 62 #include <ti/ndk/inc/stkmain.h> 67 #define EMACMSP432E4_PF0_EN0LED0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 0, GPIO_PF0_EN0LED0) 72 #define EMACMSP432E4_PK4_EN0LED0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 4, GPIO_PK4_EN0LED0) 77 #define EMACMSP432E4_PF4_EN0LED1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 4, GPIO_PF4_EN0LED1) 82 #define EMACMSP432E4_PK6_EN0LED1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 6, GPIO_PK6_EN0LED1) 87 #define EMACMSP432E4_PF1_EN0LED2 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 1, GPIO_PF1_EN0LED2) 92 #define EMACMSP432E4_PK5_EN0LED2 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 5, GPIO_PK5_EN0LED2) uint32_t intPriority
Definition: EMACMSP432E4.h:110
EMACMSP432E4 Hardware attributes.
Definition: EMACMSP432E4.h:107
uint32_t led1Pin
Definition: EMACMSP432E4.h:112
int EMACMSP432E4_NIMUInit(STKEVENT_Handle hEvent)
This function is included in the NIMUDeviceTable that is used by the NDK to initialize and register t...
struct EMACMSP432E4_HWAttrs EMACMSP432E4_HWAttrs
EMACMSP432E4 Hardware attributes.
uint8_t * macAddress
Definition: EMACMSP432E4.h:113
uint32_t baseAddr
Definition: EMACMSP432E4.h:108
bool EMACMSP432E4_isLinkUp()
This function returns the link state of the EMACMSP432E4 driver.
uint32_t led0Pin
Definition: EMACMSP432E4.h:111
uint32_t intNum
Definition: EMACMSP432E4.h:109