All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
Macros | Functions
Onewire_api

Macros

#define ONEWIRE_TXN_MASK
 
#define ONEWIRE_TXN_SIZE_LSHIFT   3
 
#define ONEWIRE_TXN_BSIZE_LSHIFT   16
 
#define ONEWIRE_INIT_SPD_STD   0x00000000
 
#define ONEWIRE_INIT_SPD_OD   0x00000020
 
#define ONEWIRE_INIT_READ_STD   0x00000000
 
#define ONEWIRE_INIT_READ_LATE   0x00000040
 
#define ONEWIRE_INIT_ATR   0x00000000
 
#define ONEWIRE_INIT_NO_ATR   0x00000080
 
#define ONEWIRE_INIT_STD_POL   0x00000000
 
#define ONEWIRE_INIT_ALT_POL   0x40000000
 
#define ONEWIRE_INIT_1_WIRE_CFG   0x00000000
 
#define ONEWIRE_INIT_2_WIRE_CFG   0x80000000
 
#define ONEWIRE_BUS_STATUS_BUSY   0x00000100
 
#define ONEWIRE_BUS_STATUS_NO_SLAVE   0x00000200
 
#define ONEWIRE_BUS_STATUS_STUCK   0x00000400
 
#define ONEWIRE_OP_RESET   0x00000001
 
#define ONEWIRE_OP_READ   0x00000002
 
#define ONEWIRE_OP_WRITE   0x00000004
 
#define ONEWIRE_DMA_BUS_RESET   0x00000001
 
#define ONEWIRE_DMA_OP_READ   0x00000002
 
#define ONEWIRE_DMA_OP_MULTI_WRITE   0x00000004
 
#define ONEWIRE_DMA_OP_MULTI_READ   0x00000006
 
#define ONEWIRE_DMA_MODE_SG   0x00000008
 
#define ONEWIRE_DMA_OP_SZ_8   0x00000000
 
#define ONEWIRE_DMA_OP_SZ_16   0x00000800
 
#define ONEWIRE_DMA_OP_SZ_32   0x00001800
 
#define ONEWIRE_INT_RESET_DONE   0x00000001
 
#define ONEWIRE_INT_OP_DONE   0x00000002
 
#define ONEWIRE_INT_NO_SLAVE   0x00000004
 
#define ONEWIRE_INT_STUCK   0x00000008
 
#define ONEWIRE_INT_DMA_DONE   0x00000010
 

Functions

void OneWireInit (uint32_t ui32Base, uint32_t ui32InitFlags)
 
void OneWireBusReset (uint32_t ui32Base)
 
uint32_t OneWireBusStatus (uint32_t ui32Base)
 
void OneWireDataGet (uint32_t ui32Base, uint32_t *pui32Data)
 
bool OneWireDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data)
 
void OneWireIntClear (uint32_t ui32Base, uint32_t ui32IntFlags)
 
void OneWireIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags)
 
void OneWireIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags)
 
uint32_t OneWireIntStatus (uint32_t ui32Base, bool bMasked)
 
void OneWireIntRegister (uint32_t ui32Base, void(*pfnHandler)(void))
 
void OneWireIntUnregister (uint32_t ui32Base)
 
void OneWireDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 
void OneWireDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 
void OneWireTransaction (uint32_t ui32Base, uint32_t ui32OpMode, uint32_t ui32Data, uint32_t ui32BitCnt)
 

Detailed Description

Macro Definition Documentation

§ ONEWIRE_TXN_MASK

#define ONEWIRE_TXN_MASK
Value:
ONEWIRE_CS_BSIZE_M)
#define ONEWIRE_CS_SZ_M
Definition: hw_onewire.h:79
#define ONEWIRE_CS_OP_M
Definition: hw_onewire.h:80

Referenced by OneWireDMADisable(), OneWireDMAEnable(), and OneWireTransaction().

§ ONEWIRE_TXN_SIZE_LSHIFT

#define ONEWIRE_TXN_SIZE_LSHIFT   3

Referenced by OneWireTransaction().

§ ONEWIRE_TXN_BSIZE_LSHIFT

#define ONEWIRE_TXN_BSIZE_LSHIFT   16

Referenced by OneWireTransaction().

§ ONEWIRE_INIT_SPD_STD

#define ONEWIRE_INIT_SPD_STD   0x00000000

§ ONEWIRE_INIT_SPD_OD

#define ONEWIRE_INIT_SPD_OD   0x00000020

§ ONEWIRE_INIT_READ_STD

#define ONEWIRE_INIT_READ_STD   0x00000000

§ ONEWIRE_INIT_READ_LATE

#define ONEWIRE_INIT_READ_LATE   0x00000040

§ ONEWIRE_INIT_ATR

#define ONEWIRE_INIT_ATR   0x00000000

§ ONEWIRE_INIT_NO_ATR

#define ONEWIRE_INIT_NO_ATR   0x00000080

§ ONEWIRE_INIT_STD_POL

#define ONEWIRE_INIT_STD_POL   0x00000000

§ ONEWIRE_INIT_ALT_POL

#define ONEWIRE_INIT_ALT_POL   0x40000000

§ ONEWIRE_INIT_1_WIRE_CFG

#define ONEWIRE_INIT_1_WIRE_CFG   0x00000000

§ ONEWIRE_INIT_2_WIRE_CFG

#define ONEWIRE_INIT_2_WIRE_CFG   0x80000000

§ ONEWIRE_BUS_STATUS_BUSY

#define ONEWIRE_BUS_STATUS_BUSY   0x00000100

§ ONEWIRE_BUS_STATUS_NO_SLAVE

#define ONEWIRE_BUS_STATUS_NO_SLAVE   0x00000200

§ ONEWIRE_BUS_STATUS_STUCK

#define ONEWIRE_BUS_STATUS_STUCK   0x00000400

§ ONEWIRE_OP_RESET

#define ONEWIRE_OP_RESET   0x00000001

Referenced by OneWireTransaction().

§ ONEWIRE_OP_READ

#define ONEWIRE_OP_READ   0x00000002

Referenced by OneWireTransaction().

§ ONEWIRE_OP_WRITE

#define ONEWIRE_OP_WRITE   0x00000004

Referenced by OneWireTransaction().

§ ONEWIRE_DMA_BUS_RESET

#define ONEWIRE_DMA_BUS_RESET   0x00000001

§ ONEWIRE_DMA_OP_READ

#define ONEWIRE_DMA_OP_READ   0x00000002

§ ONEWIRE_DMA_OP_MULTI_WRITE

#define ONEWIRE_DMA_OP_MULTI_WRITE   0x00000004

§ ONEWIRE_DMA_OP_MULTI_READ

#define ONEWIRE_DMA_OP_MULTI_READ   0x00000006

§ ONEWIRE_DMA_MODE_SG

#define ONEWIRE_DMA_MODE_SG   0x00000008

§ ONEWIRE_DMA_OP_SZ_8

#define ONEWIRE_DMA_OP_SZ_8   0x00000000

§ ONEWIRE_DMA_OP_SZ_16

#define ONEWIRE_DMA_OP_SZ_16   0x00000800

§ ONEWIRE_DMA_OP_SZ_32

#define ONEWIRE_DMA_OP_SZ_32   0x00001800

§ ONEWIRE_INT_RESET_DONE

#define ONEWIRE_INT_RESET_DONE   0x00000001

§ ONEWIRE_INT_OP_DONE

#define ONEWIRE_INT_OP_DONE   0x00000002

§ ONEWIRE_INT_NO_SLAVE

#define ONEWIRE_INT_NO_SLAVE   0x00000004

§ ONEWIRE_INT_STUCK

#define ONEWIRE_INT_STUCK   0x00000008

§ ONEWIRE_INT_DMA_DONE

#define ONEWIRE_INT_DMA_DONE   0x00000010

Function Documentation

§ OneWireInit()

void OneWireInit ( uint32_t  ui32Base,
uint32_t  ui32InitFlags 
)

Initializes the 1-Wire module.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
ui32InitFlagsprovides the initialization flags.

This function configures and initializes the 1-Wire interface for use.

The ui32InitFlags parameter is a combination of the following:

  • ONEWIRE_INIT_SPD_STD - standard speed bus timings
  • ONEWIRE_INIT_SPD_OD - overdrive speed bus timings
  • ONEWIRE_INIT_READ_STD - standard read sampling timing
  • ONEWIRE_INIT_READ_LATE - late read sampling timing
  • ONEWIRE_INIT_ATR - standard answer-to-reset presence detect
  • ONEWIRE_INIT_NO_ATR - no answer-to-reset presence detect
  • ONEWIRE_INIT_STD_POL - normal signal polarity
  • ONEWIRE_INIT_ALT_POL - alternate (reverse) signal polarity
  • ONEWIRE_INIT_1_WIRE_CFG - standard 1-Wire (1 data pin) setup
  • ONEWIRE_INIT_2_WIRE_CFG - alternate 2-Wire (2 data pin) setup
Returns
None.

References ASSERT, HWREG, and ONEWIRE_O_CS.

§ OneWireBusReset()

void OneWireBusReset ( uint32_t  ui32Base)

Issues a reset on the 1-Wire bus.

Parameters
ui32Basespecifies the base address of the 1-Wire module.

This function causes the 1-Wire module to generate a reset signal on the 1-Wire bus.

Returns
None.

References ASSERT, HWREG, ONEWIRE_CS_RST, and ONEWIRE_O_CS.

§ OneWireBusStatus()

uint32_t OneWireBusStatus ( uint32_t  ui32Base)

Retrieves the 1-Wire bus condition status.

Parameters
ui32Basespecifies the base address of the 1-Wire module.

This function returns the 1-Wire bus conditions reported by the 1-Wire module. These conditions could be a logical OR of any of the following:

  • ONEWIRE_BUS_STATUS_BUSY - A read, write, or reset is active.
  • ONEWIRE_BUS_STATUS_NO_SLAVE - No slave presence pulses detected.
  • ONEWIRE_BUS_STATUS_STUCK - The bus is being held low by non-master.
Returns
Returns the 1-Wire bus conditions if detected else zero.

References ASSERT, HWREG, ONEWIRE_CS_BUSY, ONEWIRE_CS_NOATR, ONEWIRE_CS_STUCK, and ONEWIRE_O_CS.

§ OneWireDataGet()

void OneWireDataGet ( uint32_t  ui32Base,
uint32_t *  pui32Data 
)

Retrieves data from the 1-Wire interface.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
pui32Datais a pointer to storage to hold the read data.

This function reads data from the 1-Wire module once all active bus operations are completed. By protocol definition, bit data defaults to a 1. Thus if a slave did not signal any 0-bit data, this read returns 0xffffffff.

Returns
None.

References ASSERT, HWREG, ONEWIRE_CS_BUSY, ONEWIRE_O_CS, and ONEWIRE_O_DATR.

§ OneWireDataGetNonBlocking()

bool OneWireDataGetNonBlocking ( uint32_t  ui32Base,
uint32_t *  pui32Data 
)

Retrieves data from the 1-Wire interface.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
pui32Datais a pointer to storage to hold the read data.

This function reads data from the 1-Wire module if there are no active operations on the bus. Otherwise it returns without reading the data from the module.

By protocol definition, bit data defaults to a 1. Thus if a slave did not signal any 0-bit data, this read returns 0xffffffff.

Returns
Returns true if a data read was performed, or false if the bus was not idle and no data was read.

References ASSERT, HWREG, ONEWIRE_CS_BUSY, ONEWIRE_O_CS, and ONEWIRE_O_DATR.

§ OneWireIntClear()

void OneWireIntClear ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)

Clears the 1-Wire module interrupt sources.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
ui32IntFlagsis a bit mask of the interrupt sources to be cleared.

This function clears the specified 1-Wire interrupt sources so that they no longer assert. This function must be called in the interrupt handler to keep the interrupts from being triggered again immediately upon exit. The ui32IntFlags parameter can be a logical OR of any of the following:

  • ONEWIRE_INT_RESET_DONE - Bus reset has just completed.
  • ONEWIRE_INT_OP_DONE - Read or write operation completed. If a combined write and read operation was set up, the interrupt signals the read is done.
  • ONEWIRE_INT_NO_SLAVE - No presence detect was signaled by a slave.
  • ONEWIRE_INT_STUCK - Bus is being held low by non-master.
  • ONEWIRE_INT_DMA_DONE - DMA operation has completed.
Note
Because there is a write buffer in the Cortex-M processor, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted).
Returns
None.

References ASSERT, HWREG, ONEWIRE_IM_DMA, ONEWIRE_IM_NOATR, ONEWIRE_IM_OPC, ONEWIRE_IM_RST, ONEWIRE_IM_STUCK, and ONEWIRE_O_ICR.

§ OneWireIntDisable()

void OneWireIntDisable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)

Disables individual 1-Wire module interrupt sources.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
ui32IntFlagsis a bit mask of the interrupt sources to be disabled.

This function disables the indicated 1-Wire interrupt sources. The ui32IntFlags parameter can be a logical OR of any of the following:

  • ONEWIRE_INT_RESET_DONE - Bus reset has just completed.
  • ONEWIRE_INT_OP_DONE - Read or write operation completed. If a combined write and read operation was set up, the interrupt signals the read is done.
  • ONEWIRE_INT_NO_SLAVE - No presence detect was signaled by a slave.
  • ONEWIRE_INT_STUCK - Bus is being held low by non-master.
  • ONEWIRE_INT_DMA_DONE - DMA operation has completed
Returns
None.

References ASSERT, HWREG, ONEWIRE_IM_DMA, ONEWIRE_IM_NOATR, ONEWIRE_IM_OPC, ONEWIRE_IM_RST, ONEWIRE_IM_STUCK, and ONEWIRE_O_IM.

§ OneWireIntEnable()

void OneWireIntEnable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)

Enables individual 1-Wire module interrupt sources.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
ui32IntFlagsis a bit mask of the interrupt sources to be enabled.

This function enables the indicated 1-Wire interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor. The ui32IntFlags parameter can be a logical OR of any of the following:

  • ONEWIRE_INT_RESET_DONE - Bus reset has just completed.
  • ONEWIRE_INT_OP_DONE - Read or write operation completed. If a combined write and read operation was set up, the interrupt signals the read is done.
  • ONEWIRE_INT_NO_SLAVE - No presence detect was signaled by a slave.
  • ONEWIRE_INT_STUCK - Bus is being held low by non-master.
  • ONEWIRE_INT_DMA_DONE - DMA operation has completed
Returns
None.

References ASSERT, HWREG, ONEWIRE_IM_DMA, ONEWIRE_IM_NOATR, ONEWIRE_IM_OPC, ONEWIRE_IM_RST, ONEWIRE_IM_STUCK, and ONEWIRE_O_IM.

§ OneWireIntStatus()

uint32_t OneWireIntStatus ( uint32_t  ui32Base,
bool  bMasked 
)

Gets the current 1-Wire interrupt status.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
bMaskedis false if the raw interrupt status is required or true if the masked interrupt status is required.

This function returns the interrupt status for the 1-Wire module. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.

Returns
Returns the masked or raw 1-Wire interrupt status, as a bit field of any of the following values:
  • ONEWIRE_INT_RESET_DONE - Bus reset has just completed.
  • ONEWIRE_INT_OP_DONE - Read or write operation completed.
  • ONEWIRE_INT_NO_SLAVE - No presence detect was signaled by a slave.
  • ONEWIRE_INT_STUCK - Bus is being held low by non-master.
  • ONEWIRE_INT_DMA_DONE - DMA operation has completed

References ASSERT, HWREG, ONEWIRE_O_MIS, and ONEWIRE_O_RIS.

§ OneWireIntRegister()

void OneWireIntRegister ( uint32_t  ui32Base,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for the 1-Wire module.

Parameters
ui32Baseis the base address of the 1-Wire module.
pfnHandleris a pointer to the function to be called when the 1-Wire interrupt occurs.

This function sets the handler to be called when a 1-Wire interrupt occurs. This function enables the global interrupt in the interrupt controller; specific 1-Wire interrupts must be enabled via OneWireIntEnable(). If necessary, it is the interrupt handler's responsibility to clear the interrupt source via OneWireIntClear().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ OneWireIntUnregister()

void OneWireIntUnregister ( uint32_t  ui32Base)

Unregisters an interrupt handler for the 1-Wire module.

Parameters
ui32Baseis the base address of the 1-Wire module.

This function clears the handler to be called when an 1-Wire interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ OneWireDMADisable()

void OneWireDMADisable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)

Disables 1-Wire DMA operations.

Parameters
ui32Baseis the base address of the 1-Wire module.
ui32DMAFlagsis a bit mask of the DMA features to disable.

This function is used to disable 1-Wire DMA features that were enabled by OneWireDMAEnable(). The specified 1-Wire DMA features are disabled. The ui32DMAFlags parameter is a combination of the following:

  • ONEWIRE_DMA_BUS_RESET - Issue a 1-Wire bus reset before starting
  • ONEWIRE_DMA_OP_READ - Read after each module transaction
  • ONEWIRE_DMA_OP_MULTI_WRITE - Write after each previous write
  • ONEWIRE_DMA_OP_MULTI_READ - Read after each previous read
  • ONEWIRE_DMA_MODE_SG - Start DMA on enable then repeat on each completion
  • ONEWIRE_DMA_OP_SZ_8 - Bus read/write of 8 bits
  • ONEWIRE_DMA_OP_SZ_16 - Bus read/write of 16 bits
  • ONEWIRE_DMA_OP_SZ_32 - Bus read/write of 32 bits
Returns
None.

References ASSERT, HWREG, ONEWIRE_O_CS, ONEWIRE_O_DMA, and ONEWIRE_TXN_MASK.

§ OneWireDMAEnable()

void OneWireDMAEnable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)

Enables 1-Wire DMA operations.

Parameters
ui32Baseis the base address of the 1-Wire module.
ui32DMAFlagsis a bit mask of the DMA features to enable.

This function enables the specified 1-Wire DMA features. The 1-Wire module can be configured for write operations, read operations, small write and read operations, and scatter-gather support of mixed operations.

The ui32DMAFlags parameter is a combination of the following:

  • ONEWIRE_DMA_BUS_RESET - Issue a 1-Wire bus reset before starting
  • ONEWIRE_DMA_OP_READ - Read after each module transaction
  • ONEWIRE_DMA_OP_MULTI_WRITE - Write after each previous write
  • ONEWIRE_DMA_OP_MULTI_READ - Read after each previous read
  • ONEWIRE_DMA_MODE_SG - Start DMA on enable then repeat on each completion
  • ONEWIRE_DMA_OP_SZ_8 - Bus read/write of 8 bits
  • ONEWIRE_DMA_OP_SZ_16 - Bus read/write of 16 bits
  • ONEWIRE_DMA_OP_SZ_32 - Bus read/write of 32 bits
Note
The uDMA controller must be properly configured before DMA can be used with the 1-Wire module.
Returns
None.

References ASSERT, HWREG, ONEWIRE_DMA_DMAOP_RDMUL, ONEWIRE_DMA_DMAOP_RDSNG, ONEWIRE_DMA_SG, ONEWIRE_O_CS, ONEWIRE_O_DATW, ONEWIRE_O_DMA, ONEWIRE_TXN_MASK, and SysCtlDelay().

§ OneWireTransaction()

void OneWireTransaction ( uint32_t  ui32Base,
uint32_t  ui32OpMode,
uint32_t  ui32Data,
uint32_t  ui32BitCnt 
)

Performs a 1-Wire protocol transaction on the bus.

Parameters
ui32Basespecifies the base address of the 1-Wire module.
ui32OpModesets the transaction type.
ui32Datais the data for a write operation.
ui32BitCntspecifies the number of valid bits (1-32) for the operation.

This function performs a 1-Wire protocol transaction, read and/or write, on the bus. The application should confirm the bus is idle before starting a read or write transaction.

The ui32OpMode defines the activity for the bus operations and is a logical OR of the following:

  • ONEWIRE_OP_RESET - Indicates the operation should be started with a bus reset.
  • ONEWIRE_OP_WRITE - A write operation
  • ONEWIRE_OP_READ - A read operation
Note
If both a read and write operation are requested, the write will be performed prior to the read.
Returns
None.

References ASSERT, HWREG, ONEWIRE_CS_OP_RD, ONEWIRE_CS_OP_WR, ONEWIRE_O_CS, ONEWIRE_O_DATW, ONEWIRE_OP_READ, ONEWIRE_OP_RESET, ONEWIRE_OP_WRITE, ONEWIRE_TXN_BSIZE_LSHIFT, ONEWIRE_TXN_MASK, and ONEWIRE_TXN_SIZE_LSHIFT.

Copyright 2017, Texas Instruments Incorporated