Data Fields
_Timer_A_PWMConfig Struct Reference

Type definition for _Timer_A_PWMConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t clockSource
 
uint_fast16_t clockSourceDivider
 
uint_fast16_t timerPeriod
 
uint_fast16_t compareRegister
 
uint_fast16_t compareOutputMode
 
uint_fast16_t dutyCycle
 

Detailed Description

Type definition for _Timer_A_PWMConfig structure.

ypedef Timer_A_PWMConfig

Configuration structure for PWM mode in the Timer_A module. See Timer_A_generatePWM for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_PWMConfig::clockSource

Referenced by Timer_A_generatePWM().

uint_fast16_t _Timer_A_PWMConfig::clockSourceDivider

Referenced by Timer_A_generatePWM().

uint_fast16_t _Timer_A_PWMConfig::timerPeriod

Referenced by Timer_A_generatePWM().

uint_fast16_t _Timer_A_PWMConfig::compareRegister

Referenced by Timer_A_generatePWM().

uint_fast16_t _Timer_A_PWMConfig::compareOutputMode

Referenced by Timer_A_generatePWM().

uint_fast16_t _Timer_A_PWMConfig::dutyCycle

Referenced by Timer_A_generatePWM().


The documentation for this struct was generated from the following file:

Copyright 2019, Texas Instruments Incorporated