Data Fields
_Timer_A_ContinuousModeConfig Struct Reference

Type definition for _Timer_A_ContinuousModeConfig structure. More...

#include <timer_a.h>

Data Fields

uint_fast16_t clockSource
 
uint_fast16_t clockSourceDivider
 
uint_fast16_t timerInterruptEnable_TAIE
 
uint_fast16_t timerClear
 

Detailed Description

Type definition for _Timer_A_ContinuousModeConfig structure.

ypedef Timer_A_ContinuousModeConfig

Configuration structure for continuous mode in the Timer_A module. See Timer_A_configureContinuousMode for parameter documentation.

Field Documentation

uint_fast16_t _Timer_A_ContinuousModeConfig::clockSource
uint_fast16_t _Timer_A_ContinuousModeConfig::clockSourceDivider
uint_fast16_t _Timer_A_ContinuousModeConfig::timerInterruptEnable_TAIE
uint_fast16_t _Timer_A_ContinuousModeConfig::timerClear

The documentation for this struct was generated from the following file:

Copyright 2019, Texas Instruments Incorporated