Real Time Clock with alarm support and tamper protection.  
More...
|  | 
| #define | RTC_C_CALIBRATIONFREQ_OFF   (RTC_C_CTL13_CALF_0) | 
|  | 
| #define | RTC_C_CALIBRATIONFREQ_512HZ   (RTC_C_CTL13_CALF_1) | 
|  | 
| #define | RTC_C_CALIBRATIONFREQ_256HZ   (RTC_C_CTL13_CALF_2) | 
|  | 
| #define | RTC_C_CALIBRATIONFREQ_1HZ   (RTC_C_CTL13_CALF_3) | 
|  | 
| #define | RTC_C_CALIBRATION_DOWN1PPM   ( !(RTC_C_OCAL_OCALS) ) | 
|  | 
| #define | RTC_C_CALIBRATION_UP1PPM   (RTC_C_OCAL_OCALS) | 
|  | 
| #define | RTC_C_COMPENSATION_DOWN1PPM   ( !(RTC_C_TCMP_TCMPS) ) | 
|  | 
| #define | RTC_C_COMPENSATION_UP1PPM   (RTC_C_TCMP_TCMPS) | 
|  | 
| #define | RTC_C_FORMAT_BINARY   ( !(RTC_C_CTL13_BCD) ) | 
|  | 
| #define | RTC_C_FORMAT_BCD   (RTC_C_CTL13_BCD) | 
|  | 
| #define | RTC_C_ALARMCONDITION_OFF   (0x80) | 
|  | 
| #define | RTC_C_CALENDAREVENT_MINUTECHANGE   (RTC_C_CTL13_TEV_0) | 
|  | 
| #define | RTC_C_CALENDAREVENT_HOURCHANGE   (RTC_C_CTL13_TEV_1) | 
|  | 
| #define | RTC_C_CALENDAREVENT_NOON   (RTC_C_CTL13_TEV_2) | 
|  | 
| #define | RTC_C_CALENDAREVENT_MIDNIGHT   (RTC_C_CTL13_TEV_3) | 
|  | 
| #define | RTC_C_PRESCALE_0   (0x0) | 
|  | 
| #define | RTC_C_PRESCALE_1   (0x1) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_2   (RTC_C_PS0CTL_RT0IP_0) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_4   (RTC_C_PS0CTL_RT0IP_1) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_8   (RTC_C_PS0CTL_RT0IP_2) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_16   (RTC_C_PS0CTL_RT0IP_3) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_32   (RTC_C_PS0CTL_RT0IP_4) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_64   (RTC_C_PS0CTL_RT0IP_5) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_128   (RTC_C_PS0CTL_RT0IP_6) | 
|  | 
| #define | RTC_C_PSEVENTDIVIDER_256   (RTC_C_PS0CTL_RT0IP_7) | 
|  | 
| #define | RTC_C_OSCILLATOR_FAULT_INTERRUPT   RTC_C_CTL0_OFIE | 
|  | 
| #define | RTC_C_TIME_EVENT_INTERRUPT   RTC_C_CTL0_TEVIE | 
|  | 
| #define | RTC_C_CLOCK_ALARM_INTERRUPT   RTC_C_CTL0_AIE | 
|  | 
| #define | RTC_C_CLOCK_READ_READY_INTERRUPT   RTC_C_CTL0_RDYIE | 
|  | 
| #define | RTC_C_PRESCALE_TIMER0_INTERRUPT   0x02 | 
|  | 
| #define | RTC_C_PRESCALE_TIMER1_INTERRUPT   0x01 | 
|  | 
| #define | RTC_C_startClockMultipleInstance(a)   RTC_C_startClock() | 
|  | 
| #define | RTC_C_holdClockMultipleInstance(a)   RTC_C_holdClock() | 
|  | 
| #define | RTC_C_setCalibrationFrequencyMultipleInstance(a, b)   RTC_C_setCalibrationFrequency(b) | 
|  | 
| #define | RTC_C_setCalibrationDataMultipleInstance(a, b, c)   RTC_C_setCalibrationData(b,c) | 
|  | 
| #define | RTC_C_setTemperatureCompensationMultipleInstance(a, b, c)   RTC_C_setTemperatureCompensation(b,c) | 
|  | 
| #define | RTC_C_initCalendarMultipleInstance(a, b, c)   RTC_C_initCalendar(b,c) | 
|  | 
| #define | RTC_C_getCalendarTimeMultipleInstance(a)   RTC_C_getCalendarTime() | 
|  | 
| #define | RTC_C_setCalendarAlarmMultipleInstance(a, b, c, d, e)   RTC_C_setCalendarAlarm(b,c,d,e) | 
|  | 
| #define | RTC_C_setCalendarEventMultipleInstance(a, b)   RTC_C_setCalendarEvent(b) | 
|  | 
| #define | RTC_C_definePrescaleEventMultipleInstance(a, b, c)   RTC_C_definePrescaleEvent(b,c) | 
|  | 
| #define | RTC_C_getPrescaleValueMultipleInstance(a, b)   RTC_C_getPrescaleValue(b) | 
|  | 
| #define | RTC_C_setPrescaleValueMultipleInstance(a, b, c)   RTC_C_setPrescaleValue(b,c) | 
|  | 
| #define | RTC_C_convertBCDToBinaryMultipleInstance(a, b)   RTC_C_convertBCDToBinary(b) | 
|  | 
| #define | RTC_C_convertBinaryToBCDMultipleInstance(a, b)   RTC_C_convertBinaryToBCD(b) | 
|  | 
| #define | RTC_C_enableInterruptMultipleInstance(a, b)   RTC_C_enableInterrupt(b) | 
|  | 
| #define | RTC_C_disableInterruptMultipleInstance(a, b)   RTC_C_disableInterrupt(b) | 
|  | 
| #define | RTC_C_getInterruptStatusMultipleInstance(a)   RTC_C_getInterruptStatus() | 
|  | 
| #define | RTC_C_getEnabledInterruptStatusMultipleInstance(a)   RTC_C_getEnabledInterruptStatus() | 
|  | 
| #define | RTC_C_clearInterruptFlagMultipleInstance(a, b)   RTC_C_clearInterruptFlag(b) | 
|  | 
| #define | RTC_C_registerInterruptMultipleInstance(a, b)   RTC_C_registerInterrupt(b) | 
|  | 
| #define | RTC_C_unregisterInterruptMultipleInstance(a)   RTC_C_unregisterInterrupt() | 
|  | 
Real Time Clock with alarm support and tamper protection. 
 
 Module Operation 
 The Real Time Clock (RTC_C) API provides a set of functions for using the SDK L RTC_C modules. Functions are provided to calibrate the clock, initialize the RTC_C modules in Calendar mode, and setup conditions for, and enable, interrupts for the RTC_C modules.
The RTC_C module provides the ability to keep track of the current time and date in calendar mode.
The RTC_C module generates multiple interrupts. There are 2 interrupts that can be defined in calendar mode, and 1 interrupt in counter mode for counter overflow, as well as an interrupt for each prescaler.   
 Programming Example 
 The DriverLib package contains a variety of different code examples that demonstrate the usage of the RTC_C module. These code examples are accessible under the examples/ folder of the SDK release as well as through TI Resource Explorer if using Code Composer Studio. These code examples provide a comprehensive list of use cases as well as practical applications involving each module.
Below is a very brief code example showing how to configure the RTC_C module and create a calendar event.
The following is the configuration structure that sets the date: 
 Next are the actual calls to DriverLib that configure the module: 
      
        
          | #define RTC_C_CALIBRATIONFREQ_OFF   (RTC_C_CTL13_CALF_0) | 
      
 
 
      
        
          | #define RTC_C_CALIBRATIONFREQ_512HZ   (RTC_C_CTL13_CALF_1) | 
      
 
 
      
        
          | #define RTC_C_CALIBRATIONFREQ_256HZ   (RTC_C_CTL13_CALF_2) | 
      
 
 
      
        
          | #define RTC_C_CALIBRATIONFREQ_1HZ   (RTC_C_CTL13_CALF_3) | 
      
 
 
      
        
          | #define RTC_C_CALIBRATION_DOWN1PPM   ( !(RTC_C_OCAL_OCALS) ) | 
      
 
 
      
        
          | #define RTC_C_CALIBRATION_UP1PPM   (RTC_C_OCAL_OCALS) | 
      
 
 
      
        
          | #define RTC_C_COMPENSATION_DOWN1PPM   ( !(RTC_C_TCMP_TCMPS) ) | 
      
 
 
      
        
          | #define RTC_C_COMPENSATION_UP1PPM   (RTC_C_TCMP_TCMPS) | 
      
 
 
      
        
          | #define RTC_C_FORMAT_BINARY   ( !(RTC_C_CTL13_BCD) ) | 
      
 
 
      
        
          | #define RTC_C_FORMAT_BCD   (RTC_C_CTL13_BCD) | 
      
 
 
      
        
          | #define RTC_C_ALARMCONDITION_OFF   (0x80) | 
      
 
 
      
        
          | #define RTC_C_CALENDAREVENT_MINUTECHANGE   (RTC_C_CTL13_TEV_0) | 
      
 
 
      
        
          | #define RTC_C_CALENDAREVENT_HOURCHANGE   (RTC_C_CTL13_TEV_1) | 
      
 
 
      
        
          | #define RTC_C_CALENDAREVENT_NOON   (RTC_C_CTL13_TEV_2) | 
      
 
 
      
        
          | #define RTC_C_CALENDAREVENT_MIDNIGHT   (RTC_C_CTL13_TEV_3) | 
      
 
 
      
        
          | #define RTC_C_PRESCALE_0   (0x0) | 
      
 
 
      
        
          | #define RTC_C_PRESCALE_1   (0x1) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_2   (RTC_C_PS0CTL_RT0IP_0) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_4   (RTC_C_PS0CTL_RT0IP_1) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_8   (RTC_C_PS0CTL_RT0IP_2) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_16   (RTC_C_PS0CTL_RT0IP_3) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_32   (RTC_C_PS0CTL_RT0IP_4) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_64   (RTC_C_PS0CTL_RT0IP_5) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_128   (RTC_C_PS0CTL_RT0IP_6) | 
      
 
 
      
        
          | #define RTC_C_PSEVENTDIVIDER_256   (RTC_C_PS0CTL_RT0IP_7) | 
      
 
 
      
        
          | #define RTC_C_OSCILLATOR_FAULT_INTERRUPT   RTC_C_CTL0_OFIE | 
      
 
 
      
        
          | #define RTC_C_TIME_EVENT_INTERRUPT   RTC_C_CTL0_TEVIE | 
      
 
 
      
        
          | #define RTC_C_CLOCK_ALARM_INTERRUPT   RTC_C_CTL0_AIE | 
      
 
 
      
        
          | #define RTC_C_CLOCK_READ_READY_INTERRUPT   RTC_C_CTL0_RDYIE | 
      
 
 
      
        
          | #define RTC_C_PRESCALE_TIMER0_INTERRUPT   0x02 | 
      
 
 
      
        
          | #define RTC_C_PRESCALE_TIMER1_INTERRUPT   0x01 | 
      
 
 
      
        
          | void RTC_C_startClock | ( | void |  | ) |  | 
      
 
Starts the RTC.
This function clears the RTC main hold bit to allow the RTC to function.
- Returns
- None 
 
 
      
        
          | void RTC_C_holdClock | ( | void |  | ) |  | 
      
 
Holds the RTC.
This function sets the RTC main hold bit to disable RTC functionality.
- Returns
- None 
Referenced by PCM_gotoLPM4().
 
 
      
        
          | void RTC_C_setCalibrationFrequency | ( | uint_fast16_t | frequencySelect | ) |  | 
      
 
Allows and Sets the frequency output to RTCLK pin for calibration measurement.
- Parameters
- 
  
    | frequencySelect | is the frequency output to RTCLK. Valid values are 
RTC_C_CALIBRATIONFREQ_OFF - turn off calibration output [Default]RTC_C_CALIBRATIONFREQ_512HZ - output signal at 512Hz for calibrationRTC_C_CALIBRATIONFREQ_256HZ - output signal at 256Hz for calibrationRTC_C_CALIBRATIONFREQ_1HZ - output signal at 1Hz for calibration |  
 
This function sets a frequency to measure at the RTCLK output pin. After testing the set frequency, the calibration could be set accordingly.
- Returns
- None 
 
 
      
        
          | void RTC_C_setCalibrationData | ( | uint_fast8_t | offsetDirection, | 
        
          |  |  | uint_fast8_t | offsetValue | 
        
          |  | ) |  |  | 
      
 
Sets the specified calibration for the RTC.
- Parameters
- 
  
    | offsetDirection | is the direction that the calibration offset will go. Valid values are 
RTC_C_CALIBRATION_DOWN1PPM - calibrate at steps of -1RTC_C_CALIBRATION_UP1PPM - calibrat at steps of +1  |  | offsetValue | is the value that the offset will be a factor of; a valid value is any integer from 1-240. |  
 
This function sets the calibration offset to make the RTC as accurate as possible. The offsetDirection can be either +1-ppm or -1-ppm, and the offsetValue should be from 1-240 and is multiplied by the direction setting (i.e. +1-ppm * 8 (offsetValue) = +8-ppm).
- Returns
- None 
 
 
      
        
          | bool RTC_C_setTemperatureCompensation | ( | uint_fast16_t | offsetDirection, | 
        
          |  |  | uint_fast8_t | offsetValue | 
        
          |  | ) |  |  | 
      
 
Sets the specified temperature compensation for the RTC.
- Parameters
- 
  
    | offsetDirection | is the direction that the calibration offset will go. Valid values are 
RTC_C_COMPENSATION_DOWN1PPM - calibrate at steps of -1RTC_C_COMPENSATION_UP1PPM - calibrate at steps of +1  |  | offsetValue | is the value that the offset will be a factor of; a value is any integer from 1-240. |  
 
This function sets the calibration offset to make the RTC as accurate as possible. The offsetDirection can be either +1-ppm or -1-ppm, and the offsetValue should be from 1-240 and is multiplied by the direction setting (i.e. +1-ppm * 8 (offsetValue) = +8-ppm).
- Returns
- true if calibration was set, false if it could not be set 
 
 
      
        
          | void RTC_C_initCalendar | ( | const RTC_C_Calendar * | calendarTime, | 
        
          |  |  | uint_fast16_t | formatSelect | 
        
          |  | ) |  |  | 
      
 
Initializes the settings to operate the RTC in Calendar mode.
- Parameters
- 
  
    | calendarTime | is the structure containing the values for the Calendar to be initialized to. Valid values should be of type Calendar and should contain the following members and corresponding values: 
seconds between 0-59minutes between 0-59hours between 0-23dayOfWeek between 0-6dayOfmonth between 1-31month between 1-12year between 0-4095  |  
 
- Note
- Values beyond the ones specified may result in erratic behavior. 
- Parameters
- 
  
    | formatSelect | is the format for the Calendar registers to use. Valid values are 
RTC_C_FORMAT_BINARY [Default]RTC_C_FORMAT_BCD  |  
 
This function initializes the Calendar mode of the RTC module.
- Returns
- None 
References _RTC_C_Calendar::dayOfmonth, _RTC_C_Calendar::dayOfWeek, _RTC_C_Calendar::hours, _RTC_C_Calendar::minutes, _RTC_C_Calendar::month, _RTC_C_Calendar::seconds, and _RTC_C_Calendar::year.
 
 
      
        
          | void RTC_C_setCalendarAlarm | ( | uint_fast8_t | minutesAlarm, | 
        
          |  |  | uint_fast8_t | hoursAlarm, | 
        
          |  |  | uint_fast8_t | dayOfWeekAlarm, | 
        
          |  |  | uint_fast8_t | dayOfmonthAlarm | 
        
          |  | ) |  |  | 
      
 
Sets and Enables the desired Calendar Alarm settings.
- Parameters
- 
  
    | minutesAlarm | is the alarm condition for the minutes. Valid values are 
An integer between 0-59, ORRTC_C_ALARMCONDITION_OFF [Default]  |  | hoursAlarm | is the alarm condition for the hours. Valid values are 
An integer between 0-24, ORRTC_C_ALARMCONDITION_OFF [Default]  |  | dayOfWeekAlarm | is the alarm condition for the day of week. Valid values are 
An integer between 0-6, ORRTC_C_ALARMCONDITION_OFF [Default]  |  | dayOfmonthAlarm | is the alarm condition for the day of the month. Valid values are 
An integer between 0-31, ORRTC_C_ALARMCONDITION_OFF [Default] |  
 
This function sets a Calendar interrupt condition to assert the RTCAIFG interrupt flag. The condition is a logical and of all of the parameters. For example if the minutes and hours alarm is set, then the interrupt will only assert when the minutes AND the hours change to the specified setting. Use the RTC_ALARM_OFF for any alarm settings that should not be apart of the alarm condition.
- Returns
- None 
 
 
      
        
          | void RTC_C_setCalendarEvent | ( | uint_fast16_t | eventSelect | ) |  | 
      
 
Sets a single specified Calendar interrupt condition.
- Parameters
- 
  
    | eventSelect | is the condition selected. Valid values are 
RTC_C_CALENDAREVENT_MINUTECHANGE - assert interrupt on every minuteRTC_C_CALENDAREVENT_HOURCHANGE - assert interrupt on every hourRTC_C_CALENDAREVENT_NOON - assert interrupt when hour is 12RTC_C_CALENDAREVENT_MIDNIGHT - assert interrupt when hour is 0 |  
 
This function sets a specified event to assert the RTCTEVIFG interrupt. This interrupt is independent from the Calendar alarm interrupt.
- Returns
- None 
 
 
      
        
          | void RTC_C_definePrescaleEvent | ( | uint_fast8_t | prescaleSelect, | 
        
          |  |  | uint_fast8_t | prescaleEventDivider | 
        
          |  | ) |  |  | 
      
 
Sets up an interrupt condition for the selected Prescaler.
- Parameters
- 
  
    | prescaleSelect | is the prescaler to define an interrupt for. Valid values are 
RTC_C_PRESCALE_0 RTC_C_PRESCALE_1  |  | prescaleEventDivider | is a divider to specify when an interrupt can occur based on the clock source of the selected prescaler. (Does not affect timer of the selected prescaler). Valid values are 
RTC_C_PSEVENTDIVIDER_2 [Default]RTC_C_PSEVENTDIVIDER_4 RTC_C_PSEVENTDIVIDER_8 RTC_C_PSEVENTDIVIDER_16 RTC_C_PSEVENTDIVIDER_32 RTC_C_PSEVENTDIVIDER_64 RTC_C_PSEVENTDIVIDER_128 RTC_C_PSEVENTDIVIDER_256  |  
 
This function sets the condition for an interrupt to assert based on the individual prescalers.
- Returns
- None 
References HWREG8, RTC_C_PRESCALE_0, and RTC_C_PRESCALE_1.
 
 
      
        
          | uint_fast8_t RTC_C_getPrescaleValue | ( | uint_fast8_t | prescaleSelect | ) |  | 
      
 
Returns the selected Prescaler value.
- Parameters
- 
  
    | prescaleSelect | is the prescaler to obtain the value of. Valid values are 
RTC_C_PRESCALE_0 RTC_C_PRESCALE_1  |  
 
This function returns the value of the selected prescale counter register. The counter should be held before reading. If in counter mode, the individual prescaler can be held, while in Calendar mode the whole RTC must be held.
- Returns
- The value of the specified Prescaler count register 
References RTC_C_PRESCALE_0, and RTC_C_PRESCALE_1.
 
 
      
        
          | void RTC_C_setPrescaleValue | ( | uint_fast8_t | prescaleSelect, | 
        
          |  |  | uint_fast8_t | prescaleCounterValue | 
        
          |  | ) |  |  | 
      
 
Sets the selected Prescaler value.
- Parameters
- 
  
    | prescaleSelect | is the prescaler to set the value for. Valid values are 
RTC_C_PRESCALE_0 RTC_C_PRESCALE_1  |  | prescaleCounterValue | is the specified value to set the prescaler to; a valid value is any integer from 0-255. |  
 
This function sets the prescale counter value. Before setting the prescale counter, it should be held.
- Returns
- None 
References RTC_C_PRESCALE_0, and RTC_C_PRESCALE_1.
 
 
      
        
          | uint16_t RTC_C_convertBCDToBinary | ( | uint16_t | valueToConvert | ) |  | 
      
 
Returns the given BCD value in Binary Format
- Parameters
- 
  
    | valueToConvert | is the raw value in BCD format to convert to Binary. |  
 
This function converts BCD values to Binary format.
- Returns
- The Binary version of the valueToConvert parameter. 
 
 
      
        
          | uint16_t RTC_C_convertBinaryToBCD | ( | uint16_t | valueToConvert | ) |  | 
      
 
Returns the given Binary value in BCD Format
- Parameters
- 
  
    | valueToConvert | is the raw value in Binary format to convert to BCD. |  
 
This function converts Binary values to BCD format.
- Returns
- The BCD version of the valueToConvert parameter. 
 
 
      
        
          | void RTC_C_enableInterrupt | ( | uint8_t | interruptMask | ) |  | 
      
 
Enables selected RTC interrupt sources.
- Parameters
- 
  
    | interruptMask | is a bit mask of the interrupts to enable. Mask Value is the logical OR of any of the following 
RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by setCalendarEvent() is met.RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.RTC_C_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running. |  
 
This function enables the selected RTC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Returns
- None 
References RTC_C_PRESCALE_TIMER0_INTERRUPT, and RTC_C_PRESCALE_TIMER1_INTERRUPT.
 
 
      
        
          | void RTC_C_disableInterrupt | ( | uint8_t | interruptMask | ) |  | 
      
 
Disables selected RTC interrupt sources.
- Parameters
- 
  
    | interruptMask | is a bit mask of the interrupts to disable. Mask Value is the logical OR of any of the following 
RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by setCalendarEvent() is met.RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.RTC_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running. |  
 
This function disables the selected RTC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
- Returns
- None 
References RTC_C_PRESCALE_TIMER0_INTERRUPT, and RTC_C_PRESCALE_TIMER1_INTERRUPT.
 
 
      
        
          | uint_fast8_t RTC_C_getInterruptStatus | ( | void |  | ) |  | 
      
 
 
      
        
          | uint_fast8_t RTC_C_getEnabledInterruptStatus | ( | void |  | ) |  | 
      
 
Returns the status of the interrupts flags masked with the enabled interrupts. This function is useful to call in ISRs to get a list of pending interrupts that are actually enabled and could have caused the ISR.
- Returns
- A bit mask of the selected interrupt flag's status. Mask Value is the logical OR of any of the following
- RTC_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by setCalendarEvent() is met.
- RTC_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.
- RTC_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.
- RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.
- RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.
- RTC_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running. 
 
References RTC_C_CLOCK_ALARM_INTERRUPT, RTC_C_CLOCK_READ_READY_INTERRUPT, RTC_C_getInterruptStatus(), RTC_C_OSCILLATOR_FAULT_INTERRUPT, RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, and RTC_C_TIME_EVENT_INTERRUPT.
 
 
      
        
          | void RTC_C_clearInterruptFlag | ( | uint_fast8_t | interruptFlagMask | ) |  | 
      
 
Clears selected RTC interrupt flags.
- Parameters
- 
  
    | interruptFlagMask | is a bit mask of the interrupt flags to be cleared. Mask Value is the logical OR of any of the following 
RTC_C_TIME_EVENT_INTERRUPT - asserts when counter overflows in counter mode or when Calendar event condition defined by setCalendarEvent() is met.RTC_C_CLOCK_ALARM_INTERRUPT - asserts when alarm condition in Calendar mode is met.RTC_C_CLOCK_READ_READY_INTERRUPT - asserts when Calendar registers are settled.RTC_C_PRESCALE_TIMER0_INTERRUPT - asserts when Prescaler 0 event condition is met.RTC_C_PRESCALE_TIMER1_INTERRUPT - asserts when Prescaler 1 event condition is met.RTC_C_OSCILLATOR_FAULT_INTERRUPT - asserts if there is a problem with the 32kHz oscillator, while the RTC is running. |  
 
This function clears the RTC interrupt flag is cleared, so that it no longer asserts.
- Returns
- None 
References RTC_C_CLOCK_ALARM_INTERRUPT, RTC_C_CLOCK_READ_READY_INTERRUPT, RTC_C_OSCILLATOR_FAULT_INTERRUPT, RTC_C_PRESCALE_TIMER0_INTERRUPT, RTC_C_PRESCALE_TIMER1_INTERRUPT, and RTC_C_TIME_EVENT_INTERRUPT.
 
 
      
        
          | void RTC_C_registerInterrupt | ( | void(*)(void) | intHandler | ) |  | 
      
 
Registers an interrupt handler for the RTC interrupt.
- Parameters
- 
  
    | intHandler | is a pointer to the function to be called when the RTC interrupt occurs. |  
 
This function registers the handler to be called when a RTC interrupt occurs. This function enables the global interrupt in the interrupt controller; specific AES interrupts must be enabled via RTC_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source via RTC_clearInterruptFlag().
- Returns
- None. 
References INT_RTC_C, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().
 
 
      
        
          | void RTC_C_unregisterInterrupt | ( | void |  | ) |  |