Data Fields
PowerMSP432_Freqs Struct Reference

Structure holding device frequencies (in Hz) More...

#include <PowerMSP432.h>

Data Fields

unsigned int MCLK
 
unsigned int HSMCLK
 
unsigned int SMCLK
 
unsigned int BCLK
 
unsigned int ACLK
 

Detailed Description

Structure holding device frequencies (in Hz)

Field Documentation

§ MCLK

unsigned int PowerMSP432_Freqs::MCLK

MCLK frequency (in Hz)

§ HSMCLK

unsigned int PowerMSP432_Freqs::HSMCLK

HSMCLK frequency (in Hz)

§ SMCLK

unsigned int PowerMSP432_Freqs::SMCLK

SMCLK frequency (in Hz)

§ BCLK

unsigned int PowerMSP432_Freqs::BCLK

BCLK frequency (in Hz)

§ ACLK

unsigned int PowerMSP432_Freqs::ACLK

ACLK frequency (in Hz)


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale