55 #include <ti/devices/msp432p4xx/inc/msp.h>
56 #include <ti/devices/msp432p4xx/driverlib/eusci.h>
59 #define EUSCI_SPI_CLOCKSOURCE_ACLK EUSCI_B_CTLW0_SSEL__ACLK
60 #define EUSCI_SPI_CLOCKSOURCE_SMCLK EUSCI_B_CTLW0_SSEL__SMCLK
62 #define EUSCI_SPI_MSB_FIRST EUSCI_B_CTLW0_MSB
63 #define EUSCI_SPI_LSB_FIRST 0x00
65 #define EUSCI_SPI_BUSY EUSCI_A_STATW_BUSY
66 #define EUSCI_SPI_NOT_BUSY 0x00
68 #define EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT 0x00
69 #define EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT EUSCI_B_CTLW0_CKPH
71 #define EUSCI_SPI_3PIN EUSCI_B_CTLW0_MODE_0
72 #define EUSCI_SPI_4PIN_UCxSTE_ACTIVE_HIGH EUSCI_B_CTLW0_MODE_1
73 #define EUSCI_SPI_4PIN_UCxSTE_ACTIVE_LOW EUSCI_B_CTLW0_MODE_2
75 #define EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH EUSCI_B_CTLW0_CKPL
76 #define EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_LOW 0x00
78 #define EUSCI_SPI_TRANSMIT_INTERRUPT EUSCI_B_IE_TXIE
79 #define EUSCI_SPI_RECEIVE_INTERRUPT EUSCI_B_IE_RXIE
81 #define EUSCI_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE EUSCI_B_CTLW0_STEM
82 #define EUSCI_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS 0x00
206 uint_fast8_t select4PinFunctionality);
234 uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
319 uint_fast16_t clockPhase, uint_fast16_t clockPolarity);
347 uint_fast8_t transmitData);
493 extern uint_fast8_t
SPI_isBusy(uint32_t moduleInstance);
675 void (*intHandler)(
void));
705 #define EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT 0x00
706 #define EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT EUSCI_B_CTLW0_CKPH
708 #define EUSCI_B_SPI_MSB_FIRST EUSCI_B_CTLW0_MSB
709 #define EUSCI_B_SPI_LSB_FIRST 0x00
711 #define EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH EUSCI_B_CTLW0_CKPL
712 #define EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW 0x00
714 #define EUSCI_B_SPI_CLOCKSOURCE_ACLK EUSCI_B_CTLW0_SSEL__ACLK
715 #define EUSCI_B_SPI_CLOCKSOURCE_SMCLK EUSCI_B_CTLW0_SSEL__SMCLK
717 #define EUSCI_B_SPI_3PIN EUSCI_B_CTLW0_MODE_0
718 #define EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH EUSCI_B_CTLW0_MODE_1
719 #define EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_LOW EUSCI_B_CTLW0_MODE_2
721 #define EUSCI_B_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS 0x00
722 #define EUSCI_B_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE EUSCI_B_CTLW0_STEM
724 #define EUSCI_B_SPI_TRANSMIT_INTERRUPT EUSCI_B_IE_TXIE0
725 #define EUSCI_B_SPI_RECEIVE_INTERRUPT EUSCI_B_IE_RXIE0
727 #define EUSCI_B_SPI_BUSY EUSCI_B_STATW_BBUSY
728 #define EUSCI_B_SPI_NOT_BUSY 0x00
730 #define EUSCI_A_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT 0x00
731 #define EUSCI_A_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT EUSCI_A_CTLW0_CKPH
733 #define EUSCI_A_SPI_MSB_FIRST EUSCI_A_CTLW0_MSB
734 #define EUSCI_A_SPI_LSB_FIRST 0x00
736 #define EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_HIGH EUSCI_A_CTLW0_CKPL
737 #define EUSCI_A_SPI_CLOCKPOLARITY_INACTIVITY_LOW 0x00
739 #define EUSCI_A_SPI_CLOCKSOURCE_ACLK EUSCI_A_CTLW0_SSEL__ACLK
740 #define EUSCI_A_SPI_CLOCKSOURCE_SMCLK EUSCI_A_CTLW0_SSEL__SMCLK
742 #define EUSCI_A_SPI_3PIN EUSCI_A_CTLW0_MODE_0
743 #define EUSCI_A_SPI_4PIN_UCxSTE_ACTIVE_HIGH EUSCI_A_CTLW0_MODE_1
744 #define EUSCI_A_SPI_4PIN_UCxSTE_ACTIVE_LOW EUSCI_A_CTLW0_MODE_2
746 #define EUSCI_A_SPI_PREVENT_CONFLICTS_WITH_OTHER_MASTERS 0x00
747 #define EUSCI_A_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE EUSCI_A_CTLW0_STEM
749 #define EUSCI_A_SPI_TRANSMIT_INTERRUPT EUSCI_A_IE_TXIE
750 #define EUSCI_A_SPI_RECEIVE_INTERRUPT EUSCI_A_IE_RXIE
752 #define EUSCI_A_SPI_BUSY EUSCI_B_STATW_BBUSY
753 #define EUSCI_A_SPI_NOT_BUSY 0x00
756 uint8_t select4PinFunctionality);
758 uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
760 uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode);
762 uint16_t clockPhase, uint16_t clockPolarity);
764 uint8_t transmitData);
775 uint32_t baseAddress);
778 uint8_t select4PinFunctionality);
780 uint32_t clockSourceFrequency, uint32_t desiredSpiClock);
782 uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode);
784 uint16_t clockPhase, uint16_t clockPolarity);
786 uint8_t transmitData);
797 uint32_t baseAddress);
bool SPI_initMaster(uint32_t moduleInstance, const eUSCI_SPI_MasterConfig *config)
Definition: spi.c:52
uint_fast16_t clockPhase
Definition: spi.h:118
uint_fast8_t selectClockSource
Definition: spi.h:96
Type definition for _eUSCI_SPI_SlaveConfig structure.
Definition: spi.h:115
uint8_t EUSCI_A_SPI_receiveData(uint32_t baseAddress)
Receives a byte that has been sent to the SPI Module.
Definition: spi.c:1155
bool SPI_initSlave(uint32_t moduleInstance, const eUSCI_SPI_SlaveConfig *config)
Definition: spi.c:197
void SPI_registerInterrupt(uint32_t moduleInstance, void(*intHandler)(void))
Definition: spi.c:439
uint32_t SPI_getReceiveBufferAddressForDMA(uint32_t moduleInstance)
Definition: spi.c:338
void EUSCI_A_SPI_enable(uint32_t baseAddress)
Enables the SPI block.
Definition: spi.c:1285
bool EUSCI_B_SPI_isBusy(uint32_t baseAddress)
Indicates whether or not the SPI bus is busy.
Definition: spi.c:945
void SPI_changeMasterClock(uint32_t moduleInstance, uint32_t clockSourceFrequency, uint32_t desiredSpiClock)
Definition: spi.c:182
void EUSCI_B_SPI_transmitData(uint32_t baseAddress, uint8_t transmitData)
Transmits a byte from the SPI Module.
Definition: spi.c:727
void EUSCI_B_SPI_disable(uint32_t baseAddress)
Disables the SPI block.
Definition: spi.c:893
void SPI_disableModule(uint32_t moduleInstance)
Definition: spi.c:326
void SPI_enableInterrupt(uint32_t moduleInstance, uint_fast16_t mask)
Definition: spi.c:374
void EUSCI_B_SPI_disableInterrupt(uint32_t baseAddress, uint16_t mask)
Disables individual SPI interrupt sources.
Definition: spi.c:797
void EUSCI_A_SPI_select4PinFunctionality(uint32_t baseAddress, uint8_t select4PinFunctionality)
Selects 4Pin Functionality.
Definition: spi.c:969
uint_fast8_t SPI_getInterruptStatus(uint32_t moduleInstance, uint16_t mask)
Definition: spi.c:398
struct _eUSCI_SPI_SlaveConfig eUSCI_SPI_SlaveConfig
void EUSCI_B_SPI_masterChangeClock(uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock)
Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled...
Definition: spi.c:585
uint_fast16_t clockPhase
Definition: spi.h:100
void EUSCI_B_SPI_changeClockPhasePolarity(uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity)
Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabl...
Definition: spi.c:689
void EUSCI_B_SPI_enable(uint32_t baseAddress)
Enables the SPI block.
Definition: spi.c:874
void SPI_enableModule(uint32_t moduleInstance)
Definition: spi.c:314
void SPI_unregisterInterrupt(uint32_t moduleInstance)
Definition: spi.c:488
void EUSCI_A_SPI_changeClockPhasePolarity(uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity)
Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabl...
Definition: spi.c:1100
void SPI_clearInterruptFlag(uint32_t moduleInstance, uint_fast16_t mask)
Definition: spi.c:427
void EUSCI_A_SPI_disable(uint32_t baseAddress)
Disables the SPI block.
Definition: spi.c:1304
void SPI_changeClockPhasePolarity(uint32_t moduleInstance, uint_fast16_t clockPhase, uint_fast16_t clockPolarity)
Definition: spi.c:275
void EUSCI_A_SPI_disableInterrupt(uint32_t baseAddress, uint16_t mask)
Disables individual SPI interrupt sources.
Definition: spi.c:1208
void SPI_transmitData(uint32_t moduleInstance, uint_fast8_t transmitData)
Definition: spi.c:290
uint32_t desiredSpiClock
Definition: spi.h:98
void EUSCI_B_SPI_enableInterrupt(uint32_t baseAddress, uint16_t mask)
Enables individual SPI interrupt sources.
Definition: spi.c:768
void SPI_disableInterrupt(uint32_t moduleInstance, uint_fast16_t mask)
Definition: spi.c:386
uint_fast16_t spiMode
Definition: spi.h:102
uint32_t EUSCI_B_SPI_getTransmitBufferAddressForDMA(uint32_t baseAddress)
Returns the address of the TX Buffer of the SPI for the DMA module.
Definition: spi.c:928
uint_fast16_t clockPolarity
Definition: spi.h:101
uint_fast16_t msbFirst
Definition: spi.h:117
Type definition for _eUSCI_SPI_MasterConfig structure.
Definition: spi.h:94
uint_fast16_t spiMode
Definition: spi.h:120
uint_fast16_t msbFirst
Definition: spi.h:99
bool EUSCI_B_SPI_slaveInit(uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode)
Initializes the SPI Slave block.
Definition: spi.c:633
void SPI_selectFourPinFunctionality(uint32_t moduleInstance, uint_fast8_t select4PinFunctionality)
Definition: spi.c:167
struct _eUSCI_SPI_MasterConfig eUSCI_SPI_MasterConfig
void EUSCI_B_SPI_select4PinFunctionality(uint32_t baseAddress, uint8_t select4PinFunctionality)
Selects 4Pin Functionality.
Definition: spi.c:558
void EUSCI_B_SPI_clearInterruptFlag(uint32_t baseAddress, uint16_t mask)
Clears the selected SPI interrupt status flag.
Definition: spi.c:851
uint8_t SPI_receiveData(uint32_t moduleInstance)
Definition: spi.c:302
uint_fast8_t SPI_getEnabledInterruptStatus(uint32_t moduleInstance)
Definition: spi.c:410
bool EUSCI_A_SPI_slaveInit(uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode)
Initializes the SPI Slave block.
Definition: spi.c:1044
uint32_t SPI_getTransmitBufferAddressForDMA(uint32_t moduleInstance)
Definition: spi.c:350
uint_fast16_t clockPolarity
Definition: spi.h:119
uint8_t EUSCI_B_SPI_receiveData(uint32_t baseAddress)
Receives a byte that has been sent to the SPI Module.
Definition: spi.c:744
uint32_t EUSCI_A_SPI_getTransmitBufferAddressForDMA(uint32_t baseAddress)
Returns the address of the TX Buffer of the SPI for the DMA module.
Definition: spi.c:1339
uint32_t EUSCI_B_SPI_getReceiveBufferAddressForDMA(uint32_t baseAddress)
Returns the address of the RX Buffer of the SPI for the DMA module.
Definition: spi.c:911
uint8_t EUSCI_B_SPI_getInterruptStatus(uint32_t baseAddress, uint8_t mask)
Gets the current SPI interrupt status.
Definition: spi.c:826
uint_fast8_t SPI_isBusy(uint32_t moduleInstance)
Definition: spi.c:362
uint8_t EUSCI_A_SPI_getInterruptStatus(uint32_t baseAddress, uint8_t mask)
Gets the current SPI interrupt status.
Definition: spi.c:1237
void EUSCI_A_SPI_enableInterrupt(uint32_t baseAddress, uint16_t mask)
Enables individual SPI interrupt sources.
Definition: spi.c:1179
void EUSCI_A_SPI_clearInterruptFlag(uint32_t baseAddress, uint16_t mask)
Clears the selected SPI interrupt status flag.
Definition: spi.c:1262
void EUSCI_A_SPI_masterChangeClock(uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock)
Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled...
Definition: spi.c:996
uint32_t clockSourceFrequency
Definition: spi.h:97
uint32_t EUSCI_A_SPI_getReceiveBufferAddressForDMA(uint32_t baseAddress)
Returns the address of the RX Buffer of the SPI for the DMA module.
Definition: spi.c:1322
bool EUSCI_A_SPI_isBusy(uint32_t baseAddress)
Indicates whether or not the SPI bus is busy.
Definition: spi.c:1355
void EUSCI_A_SPI_transmitData(uint32_t baseAddress, uint8_t transmitData)
Transmits a byte from the SPI Module.
Definition: spi.c:1138