System Control A module used for miscellaneous system configurations on MSP432P4111.
More...
System Control A module used for miscellaneous system configurations on MSP432P4111.
Module Operation
Note that this module is for use exclusively on the MSP432P4111. If using the MSP432P401, please refer to the non-a variant.
The SysCtl_A module is a conglomeration of miscellaneous system control modules that do not fit into any specific hardware peripheral.
Some of the functionalities of the SysCtl_A module include:
- Configure and enable/disable NMI sources
- Retrieve the SRAM/Flash size through software calls
- Disable/enable SRAM banks completely as well as disable retention during sleep
- Enable/disable GPIO glitch filters
- Change the type of reset that occurs on a WDT violation
Programming Example
| #define SYSCTL_A_HARD_RESET 1 |
| #define SYSCTL_A_SOFT_RESET 0 |
| #define SYSCTL_A_PERIPH_LCD SYSCTL_A_PERIHALT_CTL_HALT_LCD |
| #define SYSCTL_A_PERIPH_DMA SYSCTL_A_PERIHALT_CTL_HALT_DMA |
| #define SYSCTL_A_PERIPH_WDT SYSCTL_A_PERIHALT_CTL_HALT_WDT |
| #define SYSCTL_A_PERIPH_ADC SYSCTL_A_PERIHALT_CTL_HALT_ADC |
| #define SYSCTL_A_PERIPH_EUSCIB3 SYSCTL_A_PERIHALT_CTL_HALT_EUB3 |
| #define SYSCTL_A_PERIPH_EUSCIB2 SYSCTL_A_PERIHALT_CTL_HALT_EUB2 |
| #define SYSCTL_A_PERIPH_EUSCIB1 SYSCTL_A_PERIHALT_CTL_HALT_EUB1 |
| #define SYSCTL_A_PERIPH_EUSCIB0 SYSCTL_A_PERIHALT_CTL_HALT_EUB0 |
| #define SYSCTL_A_PERIPH_EUSCIA3 SYSCTL_A_PERIHALT_CTL_HALT_EUA3 |
| #define SYSCTL_A_PERIPH_EUSCIA2 SYSCTL_A_PERIHALT_CTL_HALT_EUA2 |
| #define SYSCTL_A_PERIPH_EUSCIA1 SYSCTL_A_PERIHALT_CTL_HALT_EUA1 |
| #define SYSCTL_A_PERIPH_EUSCIA0 SYSCTL_A_PERIHALT_CTL_HALT_EUA0 |
| #define SYSCTL_A_PERIPH_TIMER32_0_MODULE SYSCTL_A_PERIHALT_CTL_HALT_T32_0 |
| #define SYSCTL_A_PERIPH_TIMER16_3 SYSCTL_A_PERIHALT_CTL_HALT_T16_3 |
| #define SYSCTL_A_PERIPH_TIMER16_2 SYSCTL_A_PERIHALT_CTL_HALT_T16_2 |
| #define SYSCTL_A_PERIPH_TIMER16_1 SYSCTL_A_PERIHALT_CTL_HALT_T16_1 |
| #define SYSCTL_A_PERIPH_TIMER16_0 SYSCTL_A_PERIHALT_CTL_HALT_T16_0 |
| #define SYSCTL_A_NMIPIN_SRC SYSCTL_A_NMI_CTLSTAT_PIN_SRC |
| #define SYSCTL_A_PCM_SRC SYSCTL_A_NMI_CTLSTAT_PCM_SRC |
| #define SYSCTL_A_PSS_SRC SYSCTL_A_NMI_CTLSTAT_PSS_SRC |
| #define SYSCTL_A_CS_SRC SYSCTL_A_NMI_CTLSTAT_CS_SRC |
| #define SYSCTL_A_REBOOT_KEY 0x6900 |
| #define SYSCTL_A_1_2V_REF (uint32_t)&TLV->ADC14_REF1P2V_TS30C - (uint32_t)TLV_BASE |
| #define SYSCTL_A_1_45V_REF (uint32_t)&TLV->ADC14_REF1P45V_TS30C - (uint32_t)TLV_BASE |
| #define SYSCTL_A_2_5V_REF (uint32_t)&TLV->ADC14_REF2P5V_TS30C - (uint32_t)TLV_BASE |
| #define SYSCTL_A_85_DEGREES_C 4 |
| #define SYSCTL_A_30_DEGREES_C 0 |
| #define SYSCTL_A_BANKMASK 0x80000000 |
| #define SRAMCTL_CTL0_BANK 0x10000000 |
| #define SRAMCTL_CTL1_BANK 0x20000000 |
| #define SRAMCTL_CTL2_BANK 0x30000000 |
| #define SRAMCTL_CTL3_BANK 0x40000000 |
| #define TLV_START 0x00201004 |
| #define TLV_TAG_RESERVED1 1 |
| #define TLV_TAG_RESERVED2 2 |
| #define TLV_TAG_FLASHCTL 4 |
| #define TLV_TAG_RESERVED6 6 |
| #define TLV_TAG_RESERVED7 7 |
| #define TLV_TAG_RESERVED9 9 |
| #define TLV_TAG_RESERVED10 10 |
| #define TLV_TAG_DEVINFO 11 |
| #define TLV_TAG_DIEREC 12 |
| #define TLV_TAG_RANDNUM 13 |
| #define TLV_TAG_RESERVED14 14 |
| #define TLV_TAGEND 0x0BD0E11D |
| uint_least32_t SysCtl_A_getSRAMSize |
( |
void |
| ) |
|
| uint_least32_t SysCtl_A_getFlashSize |
( |
void |
| ) |
|
Gets the size of the flash.
- Returns
- The total number of bytes of main flash memory.
- Note
- This returns the total amount of main memory flash. To find how much INFO memory is available, use the SysCtl_A_getInfoFlashSize function.
Referenced by __FlashCtl_A_remaskBurstDataPost(), __FlashCtl_A_remaskBurstDataPre(), __FlashCtl_A_remaskData32Post(), __FlashCtl_A_remaskData32Pre(), __FlashCtl_A_remaskData8Post(), __FlashCtl_A_remaskData8Pre(), FlashCtl_A_eraseSector(), FlashCtl_A_getMemoryInfo(), FlashCtl_A_initiateSectorErase(), FlashCtl_A_isMemoryProtected(), FlashCtl_A_performMassErase(), FlashCtl_A_protectMemory(), FlashCtl_A_unprotectMemory(), and FlashCtl_A_verifyMemory().
| uint_least32_t SysCtl_A_getInfoFlashSize |
( |
void |
| ) |
|
| void SysCtl_A_rebootDevice |
( |
void |
| ) |
|
Reboots the device and causes the device to re-initialize itself.
- Returns
- This function does not return.
References SYSCTL_A_REBOOT_KEY.
| void SysCtl_A_getTLVInfo |
( |
uint_fast8_t |
tag, |
|
|
uint_fast8_t |
instance, |
|
|
uint_fast8_t * |
length, |
|
|
uint32_t ** |
data_address |
|
) |
| |
The TLV structure uses a tag or base address to identify segments of the table where information is stored. Some examples of TLV tags are Peripheral Descriptor, Interrupts, Info Block and Die Record. This function retrieves the value of a tag and the length of the tag.
- Parameters
-
| tag | represents the tag for which the information needs to be retrieved. Valid values are:
- TLV_TAG_RESERVED1
- TLV_TAG_RESERVED2
- TLV_TAG_CS
- TLV_TAG_FLASHCTL
- TLV_TAG_ADC14
- TLV_TAG_RESERVED6
- TLV_TAG_RESERVED7
- TLV_TAG_REF
- TLV_TAG_RESERVED9
- TLV_TAG_RESERVED10
- TLV_TAG_DEVINFO
- TLV_TAG_DIEREC
- TLV_TAG_RANDNUM
- TLV_TAG_RESERVED14
|
| instance | In some cases a specific tag may have more than one instance. For example there may be multiple instances of timer calibration data present under a single Timer Cal tag. This variable specifies the instance for which information is to be retrieved (0, 1, etc.). When only one instance exists; 0 is passed. |
| length | Acts as a return through indirect reference. The function retrieves the value of the TLV tag length. This value is pointed to by *length and can be used by the application level once the function is called. If the specified tag is not found then the pointer is null 0. |
| data_address | acts as a return through indirect reference. Once the function is called data_address points to the pointer that holds the value retrieved from the specified TLV tag. If the specified tag is not found then the pointer is null 0. |
- Returns
- None
References TLV_START, and TLV_TAGEND.
Referenced by CS_getDCOFrequency(), CS_setDCOFrequency(), FlashCtl_A_eraseSector(), FlashCtl_A_performMassErase(), and FlashCtl_A_programMemory().
| bool SysCtl_A_enableSRAM |
( |
uint32_t |
addr | ) |
|
Enables areas of SRAM memory. This can be used to optimize power consumption when every SRAM bank isn't needed. This function takes in a 32-bit address to the area in SRAM to to enable. It will convert this address into the corresponding register settings and set them in the register accordingly. Note that passing an address to an area other than SRAM will result in unreliable behavior. Addresses should be given with reference to the SRAM_DATA area of SRAM (usually starting at 0x20000000).
- Parameters
-
| addr | Break address of SRAM to enable. All SRAM below this address will also be enabled. If an unaligned address is given the appropriate aligned address will be calculated. |
- Note
- The first bank of SRAM is reserved and always enabled.
- Returns
- true if banks were set, false otherwise. If the BNKEN_RDY bit is not set in the STAT register, this function will return false.
References SysCtl_A_getSRAMSize().
| bool SysCtl_A_disableSRAM |
( |
uint32_t |
addr | ) |
|
Disables areas of SRAM memory. This can be used to optimize power consumption when every SRAM bank isn't needed. It is important to note that when a higher bank is disabled, all of the SRAM banks above that bank are also disabled. For example, if the address of 0x2001FA0 is given, all SRAM banks from 0x2001FA0 to the top of SRAM will be disabled. This function takes in a 32-bit address to the area in SRAM to to disable. It will convert this address into the corresponding register settings and set them in the register accordingly. Note that passing an address to an area other than SRAM will result in unreliable behavior. Addresses should be given with reference to the SRAM_DATA area of SRAM (usually starting at 0x20000000).
- Parameters
-
| addr | Break address of SRAM to disable. All SRAM above this address will also be disabled. If an unaligned address is given the appropriate aligned address will be calculated. |
- Note
- The first bank of SRAM is reserved and always enabled.
- Returns
- true if banks were set, false otherwise. If the BNKEN_RDY bit is not set in the STAT register, this function will return false.
References SysCtl_A_getSRAMSize().
| bool SysCtl_A_enableSRAMRetention |
( |
uint32_t |
startAddr, |
|
|
uint32_t |
endAddr |
|
) |
| |
Enables retention of the specified SRAM block address range when the device goes into LPM3 mode. When the system is placed in LPM3 mode, the SRAM banks specified with this function will be placed into retention mode. Retention of individual blocks can be set without the restrictions of the enable/disable functions. Note that any memory range given outside of SRAM will result in unreliable behavior. Also note that any unaligned addresses will be truncated to the closest aligned address before the address given. Addresses should be given with reference to the SRAM_DATA area of SRAM (usually starting at 0x20000000).
- Parameters
-
| startAddr | Start address to enable retention |
| endtAddr | End address to enable retention |
- Note
- Block 0 is reserved and retention is always enabled.
- Returns
- true if banks were set, false otherwise. If the BLKEN_RDY bit is not set in the STAT register, this function will return false.
References SysCtl_A_getSRAMSize().
| bool SysCtl_A_disableSRAMRetention |
( |
uint32_t |
startAddr, |
|
|
uint32_t |
endAddr |
|
) |
| |
Disables retention of the specified SRAM block address range when the device goes into LPM3 mode. When the system is placed in LPM3 mode, the SRAM banks specified with this function will be placed into retention mode. Retention of individual blocks can be set without the restrictions of the enable/disable functions. Note that any memory range given outside of SRAM will result in unreliable behavior. Also note that any unaligned addresses will be truncated to the closest aligned address before the address given. Addresses should be given with reference to the SRAM_DATA area of SRAM (usually starting at 0x20000000).
- Parameters
-
| startAddr | Start address to disable retention |
| endtAddr | End address to disable retention |
- Note
- Block 0 is reserved and retention is always enabled.
- Returns
- true if banks were set, false otherwise. If the BLKEN_RDY bit is not set in the STAT register, this function will return false.
References SysCtl_A_getSRAMSize().
| void SysCtl_A_enablePeripheralAtCPUHalt |
( |
uint_fast16_t |
devices | ) |
|
Makes it so that the provided peripherals will either halt execution after a CPU HALT. Parameters in this function can be combined to account for multiple peripherals. By default, all peripherals keep running after a CPU HALT.
- Parameters
-
| devices | The peripherals to continue running after a CPU HALT This can be a bitwise OR of the following values:
- SYSCTL_A_PERIPH_LCD,
- SYSCTL_A_PERIPH_DMA,
- SYSCTL_A_PERIPH_WDT,
- SYSCTL_A_PERIPH_ADC,
- SYSCTL_A_PERIPH_EUSCIB3,
- SYSCTL_A_PERIPH_EUSCIB2,
- SYSCTL_A_PERIPH_EUSCIB1
- SYSCTL_A_PERIPH_EUSCIB0,
- SYSCTL_A_PERIPH_EUSCIA3,
- SYSCTL_A_PERIPH_EUSCIA2
- SYSCTL_A_PERIPH_EUSCIA1,
- SYSCTL_A_PERIPH_EUSCIA0,
- SYSCTL_A_PERIPH_TIMER32_0_MODULE,
- SYSCTL_A_PERIPH_TIMER16_3,
- SYSCTL_A_PERIPH_TIMER16_2,
- SYSCTL_A_PERIPH_TIMER16_1,
- SYSCTL_A_PERIPH_TIMER16_0
|
- Returns
- None.
| void SysCtl_A_disablePeripheralAtCPUHalt |
( |
uint_fast16_t |
devices | ) |
|
Makes it so that the provided peripherals will either halt execution after a CPU HALT. Parameters in this function can be combined to account for multiple peripherals. By default, all peripherals keep running after a CPU HALT.
- Parameters
-
| devices | The peripherals to disable after a CPU HALT |
The devices parameter can be a bitwise OR of the following values: This can be a bitwise OR of the following values:
- SYSCTL_A_PERIPH_LCD,
- SYSCTL_A_PERIPH_DMA,
- SYSCTL_A_PERIPH_WDT,
- SYSCTL_A_PERIPH_ADC,
- SYSCTL_A_PERIPH_EUSCIB3,
- SYSCTL_A_PERIPH_EUSCIB2,
- SYSCTL_A_PERIPH_EUSCIB1
- SYSCTL_A_PERIPH_EUSCIB0,
- SYSCTL_A_PERIPH_EUSCIA3,
- SYSCTL_A_PERIPH_EUSCIA2
- SYSCTL_A_PERIPH_EUSCIA1,
- SYSCTL_A_PERIPH_EUSCIA0,
- SYSCTL_A_PERIPH_TIMER32_0_MODULE,
- SYSCTL_A_PERIPH_TIMER16_3,
- SYSCTL_A_PERIPH_TIMER16_2,
- SYSCTL_A_PERIPH_TIMER16_1,
- SYSCTL_A_PERIPH_TIMER16_0
- Returns
- None.
| void SysCtl_A_setWDTTimeoutResetType |
( |
uint_fast8_t |
resetType | ) |
|
Sets the type of RESET that happens when a watchdog timeout occurs.
- Parameters
-
| resetType | The type of reset to set |
The resetType parameter must be only one of the following values:
- SYSCTL_A_HARD_RESET,
- SYSCTL_A_SOFT_RESET
- Returns
- None.
Referenced by WDT_A_setTimeoutReset().
| void SysCtl_A_setWDTPasswordViolationResetType |
( |
uint_fast8_t |
resetType | ) |
|
Sets the type of RESET that happens when a watchdog password violation occurs.
- Parameters
-
| resetType | The type of reset to set |
The resetType parameter must be only one of the following values:
- SYSCTL_A_HARD_RESET,
- SYSCTL_A_SOFT_RESET
- Returns
- None.
Referenced by WDT_A_setPasswordViolationReset().
| void SysCtl_A_disableNMISource |
( |
uint_fast8_t |
flags | ) |
|
Disables NMIs for the provided modules. When disabled, a NMI flag will not occur when a fault condition comes from the corresponding modules.
- Parameters
-
| flags | The NMI sources to disable Can be a bitwise OR of the following parameters:
- SYSCTL_A_NMIPIN_SRC,
- SYSCTL_A_PCM_SRC,
- SYSCTL_A_PSS_SRC,
- SYSCTL_A_CS_SRC
|
Referenced by CS_startHFXTWithTimeout(), and CS_startLFXTWithTimeout().
| void SysCtl_A_enableNMISource |
( |
uint_fast8_t |
flags | ) |
|
Enables NMIs for the provided modules. When enabled, a NMI flag will occur when a fault condition comes from the corresponding modules.
- Parameters
-
| flags | The NMI sources to enable Can be a bitwise OR of the following parameters:
- SYSCTL_A_NMIPIN_SRC,
- SYSCTL_A_PCM_SRC,
- SYSCTL_A_PSS_SRC,
- SYSCTL_A_CS_SRC
|
Referenced by CS_startHFXTWithTimeout(), and CS_startLFXTWithTimeout().
| uint_fast8_t SysCtl_A_getNMISourceStatus |
( |
void |
| ) |
|
| void SysCtl_A_enableGlitchFilter |
( |
void |
| ) |
|
Enables glitch suppression on the reset pin of the device. Refer to the device data sheet for specific information about glitch suppression
- Returns
- None.
| void SysCtl_A_disableGlitchFilter |
( |
void |
| ) |
|
Disables glitch suppression on the reset pin of the device. Refer to the device data sheet for specific information about glitch suppression
- Returns
- None.
| uint_fast16_t SysCtl_A_getTempCalibrationConstant |
( |
uint32_t |
refVoltage, |
|
|
uint32_t |
temperature |
|
) |
| |
Retrieves the calibration constant of the temperature sensor to be used in temperature calculation.
- Parameters
-
| refVoltage | Reference voltage being used. |
The refVoltage parameter must be only one of the following values:
- SYSCTL_A_1_2V_REF
- SYSCTL_A_1_45V_REF
- SYSCTL_A_2_5V_REF
- Parameters
-
| temperature | is the calibration temperature that the user wants to be returned. |
The temperature parameter must be only one of the following values:
- SYSCTL_A_30_DEGREES_C
- SYSCTL_A_85_DEGREES_C
- Returns
- None.
References HWREG16.